1 /********************************************************************************************************
2 * FILE PURPOSE: IBL configuration and control definitions
3 ********************************************************************************************************
4 * FILE NAME: ibl.h
5 *
6 * DESCRIPTION: Defines the data structure used to handle initial configuration and control
7 * of the ibl. This data structure resides at a fixed location in the device memory
8 * map. It is initially populated either during the rom boot. The table can be
9 * over-written during the ibl process to redirect the boot. For example the ibl
10 * can initially load from an i2c which repopulates this table with parameters
11 * for an ethernet boot.
12 *
13 * @file ibl.h
14 *
15 * @brief
16 * This file defines the configuration and control of the IBL
17 *
18 *
19 ********************************************************************************************************/
20 #ifndef IBL_H
21 #define IBL_H
23 #include "types.h"
25 /* Information used to make generate a bootp request */
26 /**
27 * @brief
28 * Defines parameters used for making a bootp request
29 *
30 * @details
31 * The bootp request parameters are created from these fields
32 */
33 typedef struct iblBootp_s
34 {
35 uint8 hwAddress[6]; /**< The hardware (mac) address of this device. If set to 0
36 the ibl will values from e-fuse */
38 uint8 ipDest[4]; /**< The IP address of this device. This is typically set
39 to IP broadcast */
41 } iblBootp_t;
44 /**
45 * @brief
46 * This structure contains information used for tftp boot.
47 *
48 * @details These fields are typically filled in by the bootp packet, but
49 * can be provided if bootp will not be used.
50 */
51 typedef struct iblEthBootInfo_s
52 {
53 uint8 ipAddr[4]; /**< The IP address of this device */
54 uint8 serverIp[4]; /**< The IP address of the tftp server */
55 uint8 gatewayIp[4]; /**< The IP address of the gateway */
56 uint8 netmask[4]; /**< The IP netmask */
57 uint8 hwAddress[6]; /**< The hardware (mac) address of this device */
58 char8 fileName[128]; /**< The file name to load */
60 } iblEthBootInfo_t;
63 /**
64 * @def ibl_ETH_PORT_FROM_RBL
65 */
66 #define ibl_ETH_PORT_FROM_RBL -1 /**< The ethernet port used is the same one used
67 during the ROM boot load process. */
70 /**
71 * @defgroup iblBootFormats
72 *
73 * @ingroup iblBootFormats
74 * @{
75 */
76 #define ibl_BOOT_FORMAT_AUTO 0 /**< Auto determine the boot format from the data */
77 #define ibl_BOOT_FORMAT_NAME 1 /**< Determines the boot format based on file name (bootp/tftp only) */
78 #define ibl_BOOT_FORMAT_BIS 2 /**< Boot TI AIS format */
79 #define ibl_BOOT_FORMAT_COFF 3 /**< Boot a COFF file */
80 #define ibl_BOOT_FORMAT_ELF 4 /**< Boot an ELF file */
81 #define ibl_BOOT_FORMAT_BBLOB 5 /**< Boot a binary blob */
82 #define ibl_BOOT_FORMAT_BTBL 6 /**< Boot a TI boot table file */
84 /* @} */
86 /**
87 * @defgroup iblPeriphPriority Defines the boot sequence
88 *
89 * @ingroup iblPeriphPriority
90 * @{
91 * @def ibl_LOWEST_PRIORITY
92 */
93 #define ibl_LOWEST_PRIORITY 10 /**< The lowest priority assignable to a peripheral for boot */
95 /**
96 * @def ibl_HIGHEST_PRIORITY
97 */
98 #define ibl_HIGHEST_PRIORITY 1 /**< The highest priority assignable to a peripheral for boot */
100 /**
101 * @def ibl_DEVICE_NOBOOT
102 */
103 #define ibl_DEVICE_NOBOOT 20 /**< Indicates that the device is not to be used for boot */
105 /* @} */
108 /**
109 * @brief
110 * Emif controller 3.1 configuration
111 *
112 * @details
113 * The paramters are directly placed into the emif controller
114 */
115 typedef struct iblEmif3p1_s
116 {
117 uint32 sdcfg; /**< SD configuration register */
118 uint32 sdrfc; /**< Refresh timing register */
119 uint32 sdtim1; /**< DDR timing register 1 */
120 uint32 sdtim2; /**< DDR timing register 2 */
121 uint32 dmcctl; /**< CAS match timing */
123 } iblEmif3p1_t;
126 /**
127 * @brief
128 * Emif controller 4.0 configuration
129 *
130 * @details
131 * The parameters are placed directly into the emif controller
132 */
133 typedef struct iblEmif4p0_s
134 {
135 uint32 dummy; /**< placeholder */
137 } iblEmif4p0_t;
139 /**
140 * @brief
141 * This structure is used to configure the DDR interface
142 *
143 * @details
144 * The DDR configuration parameters are setup
145 *
146 */
147 typedef struct idblDdr_s
148 {
149 bool configDdr; /**< Set to non-zero to enable EMIF configuration */
151 union {
153 iblEmif3p1_t emif3p1; /**< Configuration of devices with emif controller version 3.1 */
154 iblEmif4p0_t emif4p0; /**< Configuration of devices with emif controller version 4.0 */
155 } uEmif;
157 } iblDdr_t;
159 /**
160 * @brief
161 * This structure is used to identify binary blob load parameters.
162 *
163 * @details
164 * Since binary blob is formatless the start address, size and branch to address
165 * can be specified. In the case of network boot, boot will terminate when no
166 * more data is received (or timed out), even if the size is not reached.
167 */
168 typedef struct iblBinBlob_s
169 {
170 uint32 startAddress; /**< Where the loaded data is placed */
171 uint32 sizeBytes; /**< How much data to load */
172 uint32 branchAddress; /**< Where to branch to when the load is complete */
174 } iblBinBlob_t;
176 /**
177 * @brief
178 * This structure is used to control the operation of the ibl ethernet boot.
179 *
180 * @details
181 * The ethernet port and bootp request are controlled through this structure.
182 */
183 typedef struct iblEth_s
184 {
185 uint32 ethPriority; /**< The ethernet boot priority. @ref iblPeriphPriority */
186 int32 port; /**< The ethernet port to use, or @ref ibl_ETH_PORT_FROM_RBL */
187 bool doBootp; /**< If true a bootp request is generated. If false the @ref iblEthBootInfo_t
188 table must be populated before the ibl begins execution */
189 bool useBootpServerIp; /**< If TRUE then the server IP received from the bootp server
190 is used, if FALSE the one in the ethInfo field is used */
191 bool useBootpFileName; /**< If TRUE then the file name received from the bootp server
192 is used, if FALSE the one in the ethInfo field is used */
193 int32 bootFormat; /**< The format of the boot data file. @ref iblBootFormats */
195 iblBinBlob_t blob; /**< Used only if the format is ibl_BOOT_FORMAT_BBLOB */
197 iblEthBootInfo_t ethInfo; /**< Low level ethernet information */
199 } iblEth_t;
202 /**
203 * @brief
204 * This structure is used to control the operation of the ibl sgmii ports
205 *
206 * @details
207 * The physical register configuration is provided
208 */
209 typedef struct iblSgmii_s
210 {
211 uint32 adviseAbility; /**< The advise ability register */
212 uint32 control; /**< The control register */
213 uint32 txConfig; /**< Serdes Tx config */
214 uint32 rxConfig; /**< Serdes Rx config */
215 uint32 auxConfig; /**< Serdes Aux config */
217 } iblSgmii_t;
220 /**
221 * @def ibl_N_ETH_PORTS
222 */
223 #define ibl_N_ETH_PORTS 2 /**< The number of ethernet port configurations available */
225 /**
226 * @def ibl_N_MDIO_CFGS
227 */
228 #define ibl_N_MDIO_CFGS 16 /**< The maximum number of mdio configurations */
231 /**
232 * @brief
233 * This structure is used to configure phys through the mdio interface
234 *
235 * @details
236 * Defines optional configuration through MDIO.
237 *
238 * The mdio transaction values are mapped as follows:
239 *
240 * /-------------------------------------------------------------\
241 * | 31 | 30 | 29 26 | 25 21 | 20 16 | 15 0|
242 * | rsvd | write | rsvd | register | phy addr | data |
243 * \-------------------------------------------------------------/
244 */
245 typedef struct iblMdio_s
246 {
247 int16 nMdioOps; /**< The number of mdio writes to perform */
248 uint16 mdioClkDiv; /**< The divide down of the mac clock which drives the mdio */
250 uint32 interDelay; /**< The number of cpu cycles to wait between mdio writes */
252 uint32 mdio[ibl_N_MDIO_CFGS]; /* The MDIO transactions */
254 } iblMdio_t;
257 /**
258 * @brief
259 * This structure defines the physical parameters of the NAND device
260 */
261 typedef struct nandDevInfo_s
262 {
263 uint32 busWidthBits; /**< 8 or 16 bit bus width */
264 uint32 pageSizeBytes; /**< The size of each page */
265 uint32 pageEccBytes; /**< Number of ecc bytes in each page */
266 uint32 pagesPerBlock; /**< The number of pages in each block */
267 uint32 totalBlocks; /**< The total number of blocks in a device */
269 uint32 addressBytes; /**< Number of bytes in the address */
270 bool lsbFirst; /**< Set to true if the LSB is output first, otherwise msb is first */
271 uint32 blockOffset; /**< Address bits which specify the block number */
272 uint32 pageOffset; /**< Address bits which specify the page number */
273 uint32 columnOffset; /**< Address bits which specify the column number */
275 uint8 resetCommand; /**< The command to reset the flash */
276 uint8 readCommandPre; /**< The read command sent before the address */
277 uint8 readCommandPost; /**< The read command sent after the address */
278 bool postCommand; /**< If TRUE the post command is sent */
280 } nandDevInfo_t;
283 /**
284 * @brief
285 * This structure is used to control the operation of the NAND boot
286 *
287 */
288 typedef struct iblNand_s
289 {
291 uint32 nandPriority; /**< The nand boot priority. @ref iblPeriphPriority */
292 int32 bootFormat; /**< The format of the boot data file. @ref iblBootFormats */
293 iblBinBlob_t blob; /**< Used only if the format is ibl_BOOT_FORMAT_BBLOB */
296 nandDevInfo_t nandInfo; /** Low level device info */
298 } iblNand_t;
301 /**
302 * @brief
303 * This structure is used to control the programming of the device PLL
304 *
305 * @details
306 * The system PLLs are optionally configured
307 */
308 typedef struct iblPll_s {
310 bool doEnable; /**< If true the PLL is configured */
312 Uint32 prediv; /**< The pll pre-divisor */
313 Uint32 mult; /**< The pll multiplier */
314 Uint32 postdiv; /**< The pll post divider */
316 Uint32 pllOutFreqMhz; /**< The resulting output frequency, required for timer setup */
318 } iblPll_t;
321 /**
322 * @defgroup iblPllNum
323 *
324 * @ingroup iblPllNum
325 * @{
326 *
327 * @def ibl_MAIN_PLL
328 */
329 #define ibl_MAIN_PLL 0 /**< The main cpu pll */
331 /**
332 * @def ibl_DDR_PLL
333 */
334 #define ibl_DDR_PLL 1 /**< The ddr pll */
336 /**
337 * @def ibl_NET_PLL
338 */
339 #define ibl_NET_PLL 2 /**< The network pll */
341 /**
342 * @def the number of PLL configuration entries in the table
343 */
344 #define ibl_N_PLL_CFGS (ibl_NET_PLL + 1)
346 /* @} */
351 /**
352 * @def ibl_MAGIC_VALUE
353 */
354 #define ibl_MAGIC_VALUE 0xCEC11EBB /**< Indicates that the configuration table is valid */
356 /**
357 * @brief
358 * The main configuration/control structure for the ibl
359 *
360 * @details
361 * The operation of the ibl is configured/controlled based on the values in this structure.
362 * This structure resides at a fixed location in the memory map. It can be changed during
363 * the boot operation itself by loading new values into it, but these changes must occur
364 * as part of the boot process itself (not through an asynchronous write through a master
365 * peripheral).
366 *
367 * Each boot mode is assigned a priority, with lower values indicating a higher
368 * priority. The lowest valid priority is @ref ibl_LOWEST_BOOT_PRIORITY, and the value
369 * @ref ibl_DEVICE_NOBOOT indicates no boot will be attempted on that peripheral.
370 */
371 typedef struct ibl_s
372 {
373 uint32 iblMagic; /**< @ref ibl_MAGIC_VALUE */
375 iblPll_t pllConfig[ibl_N_PLL_CFGS]; /**< PLL Configuration. @ref iblPll_t */
377 iblDdr_t ddrConfig; /**< DDR configuration @ref iblDdr_t */
379 iblEth_t ethConfig[ibl_N_ETH_PORTS]; /**< Ethernet boot configuration. @ref iblEth_t */
381 iblSgmii_t sgmiiConfig[ibl_N_ETH_PORTS]; /**< SGMII boot configuration. @ref iblSgmii_t */
383 iblMdio_t mdioConfig; /**< MDIO configuration. @ref iblMdio_t */
385 iblNand_t nandConfig; /**< NAND configuration @ref iblNand_t */
387 uint16 chkSum; /**< Ones complement checksum over the whole config structure */
390 /* iblI2c_t i2cConfig; */
391 /* iblSpi_t spiConfig; */
394 } ibl_t;
397 extern ibl_t ibl;
401 /**
402 * @defgroup iblActivePeriph
403 *
404 * @ingroup iblActivePeriph
405 * @{
406 * @def ibl_ACTIVE_PERIPH_ETH
407 */
408 #define ibl_ACTIVE_PERIPH_ETH 100 /**< An ethernet boot in progress */
410 /**
411 * @def ibl_ACTIVE_PERIPH_NAND
412 */
413 #define ibl_ACTIVE_PERIPH_NAND 101 /**< A nand boot in progress */
415 /**
416 * @def ibl_ACTIVE_PERIPH_I2C
417 */
418 #define ibl_ACTIVE_PERIPH_I2C 102 /**< An i2c boot in progress */
420 /**
421 * @def ibl_ACTIVE_PERIPH_SPI
422 */
423 #define ibl_ACTIVE_PERIPH_SPI 103 /**< An SPI boot in progress */
425 /* @} */
428 /**
429 * @defgroup iblFailCode
430 *
431 * @ingroup iblFailCode
432 * @{
433 * @def ibl_FAIL_CODE_INVALID_I2C_ADDRESS
434 */
435 #define ibl_FAIL_CODE_INVALID_I2C_ADDRESS 700 /**< Invalid i2c eeprom address encountered */
437 /**
438 * @def ibl_FAIL_CODE_BTBL_FAIL
439 */
440 #define ibl_FAIL_CODE_BTBL_FAIL 701 /**< Boot table processing function error */
443 /* @} */
446 /**
447 * @brief
448 * Provide status on the boot operation
449 *
450 * @details
451 * Run time status of the IBL is provided to aid in debugging
452 *
453 */
454 typedef struct iblStatus_s
455 {
456 uint32 iblMagic; /**< The @ref ibl_MAGIC_VALUE is placed here to indicate the boot has begun */
458 uint32 iblFail; /**< If non-zero the IBL has encountered a fatal error */
460 uint32 i2cRetries; /**< Count of I2C read retries */
461 uint32 magicRetries; /**< Count of I2C re-reads because the magic number was incorrect */
462 uint32 mapSizeFail; /**< Number of times an invalid map table size was read from the i2c */
463 uint32 mapRetries; /**< Number of times the checksum failed on the read of the i2c map */
464 uint32 i2cDataRetries; /**< Number of retries while reading block data from the i2c */
466 int32 tableLoadFail; /**< If non-zero then the load of the parameter table from i2c failed */
468 int32 heartBeat; /**< An increasing value as long as the boot code is running */
469 int32 noMagic; /**< A non-zero value here indicates that @ref ibl_MAGIC_VALUE was not found
470 in the @ref ibl_t magic field, and default values were loaded. */
471 int32 activePeriph; /**< Describes the active boot peripheral @ref iblActivePeriph */
472 int32 activeFormat; /**< Describes the format being decoded */
474 int32 autoDetectFailCnt; /**< Counts the number of times an auto detect of the data format failed */
475 int32 nameDetectFailCnt; /**< Counts the number of times an name detect of the data format failed */
477 int32 invalidDataFormatSpec; /**< Counts the number of times the main boot found an invalid boot format request */
479 uint32 exitAddress; /**< If non-zero the IBL exited and branched to this address */
481 iblEthBootInfo_t ethParams; /**< Last ethernet boot attemp parameters */
483 } iblStatus_t;
485 extern iblStatus_t iblStatus;
488 /**
489 * @brief
490 * The i2c map structure
491 *
492 * @details
493 * The i2c eeprom contains a structure which identifies the location of the big and little
494 * endian ibl images on the eeprom.
495 */
496 typedef struct iblI2cMap_s
497 {
498 uint16 length; /**< Size of the structure in bytes */
499 uint16 chkSum; /**< Value which makes the ones complement checksum over the block equal to 0 or -0 */
500 uint32 addrLe; /**< Base address of the boot tables for the little endian image */
501 uint32 addrBe; /**< Base address of the boot tables for the big endian image */
503 } iblI2cMap_t;
512 #endif /* IBL_H */