1 /****************************************************************************
2 * FILE PURPOSE: Local inter-module definitions for the IBL
3 ****************************************************************************
4 * FILE NAME: iblloc.h
5 *
6 * DESCRIPTION: Defines global structures used throughout the IBL
7 *
8 * @file iblloc.h
9 *
10 * @brief
11 * Provides global inter-module definitions
12 *
13 *****************************************************************************/
14 #ifndef IBLLOC_H
15 #define IBLLOC_H
17 #include "types.h"
19 typedef struct BOOT_MODULE_FXN_TABLE
20 {
21 /**
22 * @brief The API is called by the kernel to open the specific
23 * boot module. This is used by boot module to initialize themselves
24 * and the peripheral drivers.
25 */
26 Int32 (*open)(void* ptr_driver, void (*asyncComplete)(void *));
28 /**
29 * @brief The API is called by the kernel to close the boot module
30 * Boot Modules use this API and to close themselves and the peripheral
31 * drivers.
32 */
33 Int32 (*close)(void);
35 /**
36 * @brief The API is called by the kernel to read a specific number
37 * of bytes from the boot module and to populate the data buffer.
38 */
39 Int32 (*read)(Uint8* ptr_buf, Uint32 num_bytes);
41 /**
42 * @brief The API is called by the kernel to write a specific number
43 * of bytes to the boot module from the data buffer. This is *optional*
44 */
45 Int32 (*write)(Uint8* ptr_buf, Uint32 num_bytes);
47 /**
48 * @brief This API is called by the kernal to peek at some bytes
49 * without removing them from the buffer
50 */
51 Int32 (*peek)(Uint8 *ptr_buf, Uint32 num_bytes);
53 /**
54 * @brief This API is called by the kernel to move the read/write
55 * pointers in the buffer. The values of parameter from
56 * match those of fseek - 0 = from start of file,
57 * 1 = from current position, 2 = from end of file.
58 * Returns 0 if the seek is successful, -1 if it failed.
59 */
60 Int32 (*seek)(Int32 loc, Int32 from);
62 /**
63 * @brief This API is called by the kernel to determine how much data
64 * is currently available for immediate read. Returns -1 if
65 * the stream has been closed.
66 */
67 Int32 (*query)(void);
70 }BOOT_MODULE_FXN_TABLE;
73 /* Prototypes */
74 Uint32 iblBoot (BOOT_MODULE_FXN_TABLE *bootFxn, int32 dataFormat, void *formatParams);
77 /* squash printfs */
78 void mprintf(char *x, ...);
80 #endif /* _IBLLOC_H */