UART: Start adding UART code
[keystone-rtos/ibl.git] / src / iblloc.h
1 /*
2  *
3  * Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/ 
4  * 
5  * 
6  *  Redistribution and use in source and binary forms, with or without 
7  *  modification, are permitted provided that the following conditions 
8  *  are met:
9  *
10  *    Redistributions of source code must retain the above copyright 
11  *    notice, this list of conditions and the following disclaimer.
12  *
13  *    Redistributions in binary form must reproduce the above copyright
14  *    notice, this list of conditions and the following disclaimer in the 
15  *    documentation and/or other materials provided with the   
16  *    distribution.
17  *
18  *    Neither the name of Texas Instruments Incorporated nor the names of
19  *    its contributors may be used to endorse or promote products derived
20  *    from this software without specific prior written permission.
21  *
22  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
23  *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
24  *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
25  *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
26  *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
27  *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
28  *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
29  *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
30  *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
31  *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
32  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
33  *
34 */
38 /****************************************************************************
39  * FILE PURPOSE: Local inter-module definitions for the IBL
40  ****************************************************************************
41  * FILE NAME: iblloc.h
42  *
43  * DESCRIPTION: Defines global structures used throughout the IBL
44  *
45  * @file iblloc.h
46  *
47  * @brief
48  *    Provides global inter-module definitions
49  *
50  *****************************************************************************/
51 #ifndef IBLLOC_H
52 #define IBLLOC_H
54 #include "types.h"
56 typedef struct BOOT_MODULE_FXN_TABLE
57 {
58     /**
59      * @brief   The API is called by the kernel to open the specific
60      * boot module. This is used by boot module to initialize themselves
61      * and the peripheral drivers.
62      */
63     Int32 (*open)(void* ptr_driver, void (*asyncComplete)(void *));
65     /**
66      * @brief   The API is called by the kernel to close the boot module
67      * Boot Modules use this API and to close themselves and the peripheral 
68      * drivers.
69      */
70     Int32 (*close)(void);
72     /**
73      * @brief   The API is called by the kernel to read a specific number
74      * of bytes from the boot module and to populate the data buffer.
75      */
76     Int32 (*read)(Uint8* ptr_buf, Uint32 num_bytes);
78     /**
79      * @brief   The API is called by the kernel to write a specific number
80      * of bytes to the boot module from the data buffer. This is *optional*
81      */
82     Int32 (*write)(Uint8* ptr_buf, Uint32 num_bytes);
84     /**
85      * @brief   This API is called by the kernal to peek at some bytes
86      * without removing them from the buffer
87      */
88     Int32 (*peek)(Uint8 *ptr_buf, Uint32 num_bytes);
89     
90     /**
91      * @brief   This API is called by the kernel to move the read/write
92      *          pointers in the buffer. The values of parameter from
93      *          match those of fseek - 0 = from start of file,
94      *          1 = from current position, 2 = from end of file.
95      *          Returns 0 if the seek is successful, -1 if it failed.
96      */
97     Int32 (*seek)(Int32 loc, Int32 from);
98     
99    /**
100     * @brief    This API is called by the kernel to determine how much data
101     *           is currently available for immediate read. Returns -1 if
102     *           the stream has been closed.
103     */
104    Int32 (*query)(void);
105     
106     
107 }BOOT_MODULE_FXN_TABLE;
110 /* Prototypes */
111 Uint32 iblBoot (BOOT_MODULE_FXN_TABLE *bootFxn, int32 dataFormat, void *formatParams);
113 /* Stdlibs referenced through functions to use a single copy in the two stage boot */
114 void *iblMalloc (Uint32 size);
115 void  iblFree   (void *mem);
116 void *iblMemset (void *mem, Int32 ch, Uint32 n);
117 void *iblMemcpy (void *s1, const void *s2, Uint32 n);
119 /* squash printfs */
120 void mprintf(char *x, ...);
123 /* Initial Boot Devices */
124 #define BOOT_DEVICE_INVALID    -1
125 #define BOOT_DEVICE_I2C         0
126 #define BOOT_DEVICE_SPI_NOR     1
127 #define BOOT_DEVICE_SPI_NAND    2
129 BOOT_MODULE_FXN_TABLE *iblInitI2c     (void);
130 BOOT_MODULE_FXN_TABLE *iblInitSpiNor  (void);
131 BOOT_MODULE_FXN_TABLE *iblInitSpiNand (void);
133 #endif /* _IBLLOC_H */