]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - keystone-rtos/ibl.git/blob - src/interp/blob/blob.c
Version 0.4 from Mike Line
[keystone-rtos/ibl.git] / src / interp / blob / blob.c
1 /************************************************************************************
2  * FILE PURPOSE: Boot a binary blob
3  ************************************************************************************
4  * FILE NAME: blob.c
5  *
6  * DESCRIPTION: A binary blob is booted.
7  *
8  * @file blob.c
9  *
10  * @brief
11  *   This file reads data from the boot device as a binary blob
12  *
13  ************************************************************************************/
14 #include "types.h"
15 #include "ibl.h"
16 #include "iblloc.h"
17 #include "iblblob.h"
21 /**
22  * @b Description
23  * @n
24  *
25  * A simple read from the boot device is done until one of the following
26  * conditions occurs:
27  *    - The complete data block is read
28  *    - The read request fails
29  */
31 void iblBootBlob (BOOT_MODULE_FXN_TABLE *bootFxn, Uint32 *entry, void *formatParams)
32 {
33     Int32   dataSize;
34     Uint32  remainSize;
35     Uint32  dummyVal;
36     Uint32  bytesRead    = 0;
37     Int32   erVal        = 0;
38     Uint8  *datap;
40     iblBinBlob_t *blobParams = (iblBinBlob_t *)formatParams;
42     datap  = (Uint8 *)blobParams->startAddress;
43     *entry = 0;
45     for (remainSize = blobParams->sizeBytes; (remainSize > 0) && (erVal == 0);   )  {
47         /* If there is any data waiting go ahead and process it */
48         dataSize = (*bootFxn->query)();
50         /* The query function will return a negative value when the stream has
51          * closed */
52         if (dataSize < 0)
53             break;
55         if (dataSize > 0)  {
57             (*bootFxn->read)(datap, dataSize);
58             datap      = datap      + dataSize;
59             remainSize = remainSize - dataSize;
60             bytesRead  = bytesRead  + dataSize;
62         }  else  {
64             /* If there is no data waiting peek for more. On error assume
65              * that the device has completed the transfer. This is valid
66              * since the read includes a timeout. */
67             erVal = (*bootFxn->peek)((Uint8 *)&dummyVal, 1);
69         }
71     }
73    /* Assume that if any data was read the boot was successful. 
74     * A check could be added to see if the entry address was
75     * actually written, but this assumes there was no data already
76     * at the entry point */
77    if (bytesRead > 0)
78       *entry = blobParams->branchAddress;
80 }
83      
84