Merge branch 'newI2cMap' into tmp-mike2
[keystone-rtos/ibl.git] / src / interp / btbl / btbl.h
1 #ifndef __BTBL_H__
2 #define __BTBL_H__
3 /*******************************************************************************
4  * FILE PURPOSE: Defines API and public data definitions for the Boot table (BTBL) 
5  *******************************************************************************
6  * FILE NAME: BTBL.h  
7  *
8  * DESCRIPTION: Defines API and public data definitions for boot table 
9  *              processing (BTBL) module
10  *
11  * (C) Copyright 2004, TELOGY Networks, Inc.
12  ******************************************************************************/
14 /* System level header files */
15 #include "types.h"
17 #if 0
18 #include "device.h"
19 #endif
21 /* BTBL error codes */
22 enum {
23   BTBL_NOERR                    = 0,
24   BTBL_ERR_GEN                  = 1,
25   BTBL_ERR_INVALID_STATE        = 2,
26   BTBL_ERR_INVALID_SECTION_ADDR = 3,
27   BTBL_ERR_INVALID_START_VECTOR = 4
28 };
30 /* 
31  * We need to reserve some space in the front of the buffer used to store 
32  * the partial content of the boot table since the data may be shifted to 
33  * achieve the 32-bit data alignment for PDMA transfer during the boot table
34  * processing
35  */    
36 #define BOOT_TBL_RESERVED_HEADER_SIZE  CHIP_BTBL_RSVD_SIZE_UINT16     /* in terms of 16-bit word */ 
39 /*******************************************************************************
40  *  Data Definition :  BOOT_TBL_T
41  *******************************************************************************
42  *  DESCRIPTION :  
43  *    This is an instance of a boot table  procssing control block.  
44  *    It defines all the variables used during the boot table processing
45  ******************************************************************************/
46 typedef struct boot_tbl_cb_s
47 {
48     UINT16              state;             /* Boot table prossing state      */
49     BOOL                f_wait_lsw;        /* TRUE: waiting for the least significant
50                                                     16-bit word of the control 
51                                                     word such as I/O register
52                                                     configuration, code section
53                                                     byte count and etc. */ 
54     UINT32              code_start_addr;   /* record the entry point byte addr */
55     UINT32              num_io_regs;       /* number of the remaining IO registers 
56                                               needed to be initialized */
57     UINT16              io_addr;           /* Record the address of the IO register
58                                               to be processed */                                           
59     UINT16              core_start_vector; /* Record the core start vector */
60     /* 
61      * Record the size and address of the remaining portion of the code section
62      * to be programmed
63      */                                          
64     UINT32              section_size_bytes; /* In bytes */     
65     UINT32              section_addr;       /* 32-bit byte address */
66     UINT16              last_word;          /* Record the last UINT16 word in the
67                                                previous code section */
68                                               
69                                              
70     UINT16*             p_data;            /* Point to the UINT16 data to be 
71                                               processed  */
72     UINT32              data_size_uint16;  /* the size of the remaing 16-bit
73                                               data needs to be processed */
74 } BOOT_TBL_CB_T;
77 /*******************************************************************************
78  * Public function prototypes
79  ******************************************************************************/
80 /*******************************************************************************
81  * FUNCTION PURPOSE: Initialize the boot table control instance
82  *******************************************************************************
83  * DESCRIPTION: Allocate and initializea boot table control instance 
84  *
85  * void boot_init_boot_tbl_inst (
86  *   void         **p_inst)  - A pointer to Boot Table Control instance
87  *
88  *****************************************************************************/
89 void boot_init_boot_tbl_inst(BOOT_TBL_CB_T *inst);
91 /*******************************************************************************
92  * FUNCTION PURPOSE: Process the boot table
93  *******************************************************************************
94  * DESCRIPTION: Process the whole or partial boot table received by going 
95  *              through the boot table processing state machine until all
96  *              the UINT16 words are processed or the end of table condition
97  *              (section size == 0) is satisfied. 
98  *
99  * void boot_proc_boot_tbl (
100  *   UINT16       *p_data,  - 16-bit boot table content to be processed
101  *   UINT32       size)     - number of 16-bit words  
102  *
103  *
104  * Note: It is up to the caller to reserve 4 16-bit word space in front of the
105  *       input buffer since the data may be moved to achieve 32-bit alignment
106  *       requirement for PDMA transfer
107  *****************************************************************************/
108 void boot_proc_boot_tbl(BOOT_TBL_CB_T *inst, UINT16* p_data, UINT32 size);
110 /* Generic block boot table information for non-secure boot over a master periheral.
111  * The data section of the block contains boot table data */
112 typedef struct bootTableBlock_s
114     UINT32 blockLenBytes;
115     UINT32 data;
116     
117 } bootTableBlock_t;
120 #endif  /*  __BTBL_H__ */
122 /* Nothing past this point */