]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - keystone-rtos/ibl.git/blob - src/interp/btbl/btblpr.c
Port makefiles to Linux (while still supporting Windows)
[keystone-rtos/ibl.git] / src / interp / btbl / btblpr.c
1 /******************************************************************************
2  * FILE PURPOSE: Boot TaBLe (btbl) processing file
3  ******************************************************************************
4  * FILE NAME:   btblpr.c  
5  *
6  * DESCRIPTION: This file contains the main boot table processing state machine.
7  *
8  * For reference here is the Boot table format:
9  *
10  * (32-bit) Entry point byte address : Code Execution start address
11  * (32-bit) Number of I/O Registers, delay and etc.
12  * (32-bit) 1st Word for I/O Register configuration(optional)
13  *  ... 
14  * (32-bit) Nth Word for I/O Register configuration(optional) 
15  * (32-bit) Words for added delay in CPU cycles (optional)
16  * (32-bit) Words for Core Start Vector (optional)
17  * (32-bit) 1st code section byte count
18  * (32-bit) 1st code section starting address in bytes
19  * 1st section code byte
20  * ...
21  * (32-bit) Nth code section byte count
22  * (32-bit) Nth code section starting address in bytes
23  * Nth section code byte
24  * ...
25  * Last word of Nth section code type
26  * (32-bit) Zero byte count
27  *
28  * Note1: Core start vector and added delay are special format of I/O Registers
29  *        0xFFFF: NOP execution
30  *        0xFFFE: core start vector   
31  * 
32  * Note2: There will be a padded byte added if the code section contains odd 
33  *        number of bytes   
34  *              
35  * FUNCTION                     DESCRIPTION
36  * --------                     -----------
37  *
38  * btblpr.c:
39  * boot_init_boot_tbl_inst()    Initialize the boot table control instance
40  * boot_proc_boot_tbl()         Boot Table main processing routine
41  * boot_proc_boot_tbl_xxx()     Boot Table procssing routine in xxx state
42  *
43  * (C) Copyright 2004, TELOGY Networks, Inc.
44  *****************************************************************************/
45 /* types.h must be included before stdlib.h for splint to work */
46 #include "types.h"
48 /* Ansi header files */
49 #include <stdlib.h>
50 #include <string.h>   /* For memset() */
52 #include "btblwrap.h"
54 #if 0
56 /* System utility files */
57 #include "tiboot.h"
59 /* Main level */
60 #include "rmain.h"
62 /* Device utilities */
63 #include "device.h"
65 #endif
67 /* Module specific file */
68 #include "btbl.h"
69 #include "btblloc.h"
71 /* Build specific Configuration */
72 #include "iblcfg.h"
74 /*******************************************************************************
75  * Private prototypes
76  ******************************************************************************/
77 /*  boot table processing state machine functions */
78 void boot_proc_boot_tbl_init(BOOT_TBL_CB_T* p_inst);
79 void boot_proc_boot_tbl_io_cnt(BOOT_TBL_CB_T* p_inst);
80 void boot_proc_boot_tbl_io_regs(BOOT_TBL_CB_T* p_inst);
81 void boot_proc_boot_tbl_size(BOOT_TBL_CB_T* p_inst);
82 void boot_proc_boot_tbl_addr(BOOT_TBL_CB_T* p_inst);
83 void boot_proc_boot_tbl_data(BOOT_TBL_CB_T* p_inst);
84 void boot_proc_boot_tbl_flush(BOOT_TBL_CB_T* p_inst);
86 /*******************************************************************************
87  * Local variables 
88  ******************************************************************************/
89 BOOT_TBL_CB_T   btbl_inst;  /* Boot table Control Instance */
91 /*******************************************************************************
92  * DATA DEFINITION: Boot Table Processing State Machine
93  ******************************************************************************/
94 BootTblProcFcn_t btbl_st_proc_fcn[BOOT_TBL_NUM_STATES];
96 /*******************************************************************************
97  * FUNCTION PURPOSE: Process the boot table in Init State
98  *******************************************************************************
99  * DESCRIPTION: Process the boot table in Init State
100  *              Record the entry point 
101  *
102  * void boot_proc_boot_tbl_init (
103  *   BOOT_TBL_CB_T        *p_inst)  - A pointer to Boot Table Control instance
104  *
105  *****************************************************************************/
106 void boot_proc_boot_tbl_init(BOOT_TBL_CB_T* p_inst)
108     if(p_inst->f_wait_lsw)
109     {
110         /* Process the entry point LSW */
111         p_inst->code_start_addr += (*p_inst->p_data & 0xFFFF);
114         /* C55x boot tables contain an I/O space config. C6x boot tables
115          * do not */
116 #ifdef BOOTCONFIG_NO_BTBL_IO
117         p_inst->state = BOOT_TBL_STATE_SIZE; 
118 #else
119         p_inst->state = BOOT_TBL_STATE_IO_CNT;
120 #endif
123         p_inst->f_wait_lsw = FALSE;
124     }
125     else
126     {
127         /* Process the entry point MSW */
128         p_inst->code_start_addr = ((UINT32)(*p_inst->p_data & 0xFFFF)) << 16;   
129         p_inst->f_wait_lsw = (bool)TRUE; 
130     }
131     
132     /* Update data buffer and counter */
133     p_inst->p_data++;
134     p_inst->data_size_uint16--;
137 /*******************************************************************************
138  * FUNCTION PURPOSE: Process the boot table in IO_CNT State
139  *******************************************************************************
140  * DESCRIPTION: Process the boot table in IO_CNT State
141  *              Record the number of IO Registers 
142  *
143  * void boot_proc_boot_tbl_io_cnt (
144  *   BOOT_TBL_CB_T        *p_inst)  - A pointer to Boot Table Control instance
145  *
146  *****************************************************************************/
147 #ifndef BOOTCONFIG_NO_BTBL_IO
148 void boot_proc_boot_tbl_io_cnt(BOOT_TBL_CB_T* p_inst)
150     if(p_inst->f_wait_lsw)
151     {
152         /* LSW processing */
153         p_inst->num_io_regs += (*p_inst->p_data & 0xFFFF);
154         p_inst->f_wait_lsw = FALSE;
155         if(p_inst->num_io_regs)
156         {
157             p_inst->state = BOOT_TBL_STATE_IO_REGS;    
158         }
159         else
160         {
161             p_inst->state = BOOT_TBL_STATE_SIZE; 
162         }
163         
164       }
165     else
166     {
167         /* MSW processing */
168         p_inst->num_io_regs = ((UINT32)(*p_inst->p_data & 0xFFFF)) << 16;   
169         p_inst->f_wait_lsw = TRUE; 
170     }
171     
172     /* Update data buffer and counter */
173     p_inst->p_data++;
174     p_inst->data_size_uint16--;
176 #endif
178 /*******************************************************************************
179  * FUNCTION PURPOSE: Process the boot table in IO_REGS State
180  *******************************************************************************
181  * DESCRIPTION: Process the boot table in IO_REG State
182  *              Process IO Register configuration 
183  *
184  * void boot_proc_boot_tbl_io_regs (
185  *   BOOT_TBL_CB_T        *p_inst)  - A pointer to Boot Table Control instance
186  *
187  *****************************************************************************/
188 #ifndef BOOTCONFIG_NO_BTBL_IO
189 void boot_proc_boot_tbl_io_regs(BOOT_TBL_CB_T* p_inst)
191     UINT16 data;
192     
193     if(p_inst->f_wait_lsw)
194     {
195         /* LSW processing */
196         data = *p_inst->p_data;
197         
198         /* proess the IO register configuration based on its address (opcode) */
199         switch(p_inst->io_addr)
200         {
201             case BOOT_TBL_IO_CFG_DELAY:
202                 /* perform the delay loop requested */
203                 chipDelay(data);
204                 break;    
205                 
206             case BOOT_TBL_IO_CFG_START_CORE:
207                 /* Verify whether the start_vector is valid */
208                 if(data >= (BOOT_BIT_TO_MASK(chipReadNumCores())))
209                 {
210                     BOOT_EXCEPTION(BOOT_ERROR_CODE(BOOT_MODULE_ID_BTBL, 
211                                                    BTBL_ERR_INVALID_START_VECTOR));
212                 }
213                 /* record the core start vector */
214                 p_inst->core_start_vector = data;
215                 break;    
216                 
217             default:
218                 /* IO Configuration */
219                 chipIoWrite(p_inst->io_addr, data);
220                 break;                
221                 
222         }
223         p_inst->f_wait_lsw = FALSE;
224         
225         /* Is it the last IO Register to be configured */
226         if((--p_inst->num_io_regs) == 0)
227         {
228             p_inst->state = BOOT_TBL_STATE_SIZE;
229         }
230     }
231     else
232     {
233         /* MSW processing */
234         p_inst->io_addr = *p_inst->p_data;   
235         p_inst->f_wait_lsw = TRUE; 
236     }
237     
238     /* Update data buffer and counter */
239     p_inst->p_data++;
240     p_inst->data_size_uint16--;
242 #endif
244 /*******************************************************************************
245  * FUNCTION PURPOSE: Process the boot table in SIZE State
246  *******************************************************************************
247  * DESCRIPTION: Process the boot table in SIZE State
248  *              Record the size of the new code section 
249  *              perform end of table processing if size = 0
250  *
251  * void boot_proc_boot_tbl_size (
252  *   BOOT_TBL_CB_T        *p_inst)  - A pointer to Boot Table Control instance
253  *
254  *****************************************************************************/
255 void boot_proc_boot_tbl_size(BOOT_TBL_CB_T* p_inst)
257     if(p_inst->f_wait_lsw)
258     {
259         /* LSW processing */
260         p_inst->section_size_bytes += (*p_inst->p_data & 0xFFFF);
261         
262         /* Is it the end of the boot table */
263         if(p_inst->section_size_bytes == 0)
264         {
265             chipStartCore(p_inst->code_start_addr,
266                                  (UINT32)p_boot_entry_addr,
267                                   p_inst->core_start_vector);
268                     
269             /* End of Boot table:Clear the instance */
270             p_inst->state = BOOT_TBL_STATE_FLUSH;
271             p_inst->f_wait_lsw = FALSE;
272             return;    
273         }
274         
275         p_inst->state = BOOT_TBL_STATE_ADDR;
276         p_inst->f_wait_lsw = FALSE;
277         
278         /* Update statistics */
279         bootStats.btbl.num_sections++;
280     }
281     else
282     {
283         /* MSW processing */
284         p_inst->section_size_bytes = ((UINT32)(*p_inst->p_data & 0xFFFF)) << 16;   
285         p_inst->f_wait_lsw = (bool)TRUE; 
286     }
287     
288     /* Update data buffer and counter */
289     p_inst->p_data++;
290     p_inst->data_size_uint16--;
293 /*******************************************************************************
294  * FUNCTION PURPOSE: Process the boot table in ADDR State
295  *******************************************************************************
296  * DESCRIPTION: Process the boot table in ADDR State
297  *              Record the start address of the new code section 
298  *
299  * void boot_proc_boot_tbl_addr (
300  *   BOOT_TBL_CB_T        *p_inst)  - A pointer to Boot Table Control instance
301  *
302  *****************************************************************************/
303 void boot_proc_boot_tbl_addr(BOOT_TBL_CB_T* p_inst)
305     if(p_inst->f_wait_lsw)
306     {
307         /* LSW processing */
308         p_inst->section_addr += (*p_inst->p_data & 0xFFFF);
309         p_inst->state = BOOT_TBL_STATE_DATA;
310         p_inst->f_wait_lsw = FALSE;
311     }
312     else
313     {
314         /* MSW processing */
315         p_inst->section_addr = ((UINT32)(*p_inst->p_data & 0xFFFF)) << 16;   
316         p_inst->f_wait_lsw = (bool)TRUE; 
317     }
318     
319     /* Update data buffer and counter */
320     p_inst->p_data++;
321     p_inst->data_size_uint16--;
324 /*******************************************************************************
325  * FUNCTION PURPOSE: Process the boot table in DATA State
326  *******************************************************************************
327  * DESCRIPTION: Process the boot table in DATA State
328  *              Copy the received section data to the destination memory 
329  *              locations 
330  *
331  * void boot_proc_boot_tbl_data (
332  *   BOOT_TBL_CB_T        *p_inst)  - A pointer to Boot Table Control instance
333  *
334  *****************************************************************************/
335 #define MIN(a,b)  (a)<(b) ? (a) : (b)
336 void boot_proc_boot_tbl_data(BOOT_TBL_CB_T* p_inst)
338     UINT32  num_bytes;         /* number of bytes to be copy         */
339     UINT32  num_uint16_words;  /* number of 16 bit words to copy     */
340     UINT16  error;
341     
342     num_bytes = MIN (p_inst->section_size_bytes, CHIP_UINT16_TO_BYTES(p_inst->data_size_uint16));
343     num_uint16_words = CHIP_BYTES_TO_UINT16(num_bytes);
345     /* Some processors add padding to the memwidth used in the rom (created by tools) */
346     num_uint16_words = chipAddBtblUint16Pad (num_uint16_words);
347     
348     /* 
349      * Record the last UINT16 word and copy the data to the destination
350      * locations
351      */
352     
353     if((error = coreCopyData(p_inst->section_addr, p_inst->p_data, num_bytes, 
354                              p_inst->core_start_vector))
355        != CORE_NOERR)
356     {
357         /* Error Processing */ 
358         BOOT_EXCEPTION(BOOT_ERROR_CODE(BOOT_MODULE_ID_CHIP, 
359                                        error));
360     } 
361     
362     /* Update instance variables for the next code section */
363     p_inst->data_size_uint16 -= num_uint16_words;
364     p_inst->p_data           += num_uint16_words;
365     
366     p_inst->section_addr       += num_bytes;
367     p_inst->section_size_bytes -= num_bytes;
368     
369     if(p_inst->section_size_bytes == 0)
370     {
371         p_inst->state = BOOT_TBL_STATE_SIZE;    
373         /* Chip specific post block handling. Can be defined to an empty statement */
374         chipBtblBlockDone();
375     }
376     
377     /* update statistics */
378     bootStats.btbl.num_pdma_copies++;
381 /*******************************************************************************
382  * FUNCTION PURPOSE: Process the boot table in Flush State
383  *******************************************************************************
384  * DESCRIPTION: Process the boot table in Flush State
385  *              We will enter this state when the end of table or error
386  *              condition occurs
387  *              set data_size to 0, i.e. ignore the reamining data
388  *
389  * void boot_proc_boot_tbl_error (
390  *   BOOT_TBL_CB_T        *p_inst)  - A pointer to Boot Table Control instance
391  *
392  *****************************************************************************/
393 void boot_proc_boot_tbl_flush(BOOT_TBL_CB_T* p_inst)
395     p_inst->data_size_uint16 = 0;
398 /* ------------------- PUBLIC FUNCTIONS START HERE ----------------------- */
399 /*******************************************************************************
400  * FUNCTION PURPOSE: Initialize the boot table control instance
401  *******************************************************************************
402  * DESCRIPTION: Initialize and allocate the boot table control instance  
403  *              Initialize all the variables to zero
404  *              Set the state to Init
405  *
406  * void boot_init_boot_tbl_inst ( void )
407  *
408  * Note: only one instance is used at this moment
409  *       a free instance function will be needed when multiple instances are
410  *       supported
411  *
412  *****************************************************************************/
413 void boot_init_boot_tbl_inst(BOOT_TBL_CB_T *p_btbl_inst)
415     memset(p_btbl_inst, 0, sizeof(BOOT_TBL_CB_T));
416     p_btbl_inst->state = BOOT_TBL_STATE_INIT;
417     
418     /*
419      * Set the core start vector to start core A only as its default value
420      * in case the boot table does not contain the setting of the core
421      * start vector.
422      */
423     p_btbl_inst->core_start_vector = 1; 
424     
425     
426     /* Initialize the toot table processing function table */
427     btbl_st_proc_fcn[BOOT_TBL_STATE_INIT]    = boot_proc_boot_tbl_init;
429 #ifndef BOOTCONFIG_NO_BTBL_IO
430     btbl_st_proc_fcn[BOOT_TBL_STATE_IO_CNT]  = boot_proc_boot_tbl_io_cnt;
431     btbl_st_proc_fcn[BOOT_TBL_STATE_IO_REGS] = boot_proc_boot_tbl_io_regs;
432 #endif
434     btbl_st_proc_fcn[BOOT_TBL_STATE_SIZE]    = boot_proc_boot_tbl_size;
435     btbl_st_proc_fcn[BOOT_TBL_STATE_ADDR]    = boot_proc_boot_tbl_addr;
436     btbl_st_proc_fcn[BOOT_TBL_STATE_DATA]    = boot_proc_boot_tbl_data;
437     btbl_st_proc_fcn[BOOT_TBL_STATE_FLUSH]   = boot_proc_boot_tbl_flush;
438     
439 } /* end of boot_init_boot_tbl_inst() */
441 /*******************************************************************************
442  * FUNCTION PURPOSE: Process the boot table
443  *******************************************************************************
444  * DESCRIPTION: Process the whole or partial boot table received by going 
445  *              through the boot table processing state machine until all
446  *              the UINT16 words are processed or the end of table condition
447  *              (section size == 0) is satisfied. 
448  *
449  * void boot_proc_boot_tbl (
450  *   UINT16       *p_data,  - 16-bit boot table content to be processed
451  *   UINT16       size)     - number of 16-bit words  
452  *
453  *
454  * Note: It is up to the caller to reserve 4 16-bit word space in front of the
455  *       input buffer since the data may be moved to achieve 32-bit alignment
456  *       requirement for PDMA transfer
457  *****************************************************************************/
458 void boot_proc_boot_tbl(BOOT_TBL_CB_T *p_btbl_inst, UINT16* p_data, UINT32 size)
460     
461     /* Record the input data buffer and size */
462     p_btbl_inst->p_data           = p_data;
463     p_btbl_inst->data_size_uint16 = size;
464     
465     /* Optional: verify the inst state is valid */
466     if(p_btbl_inst->state > BOOT_TBL_LAST_STATE)
467     {
468         /* Error Processing */
469         BOOT_EXCEPTION(BOOT_ERROR_CODE(BOOT_MODULE_ID_BTBL, 
470                                        BTBL_ERR_INVALID_STATE));
471          
472     }
473     
474     /*
475      * Invoke the Boot table processing state machine until all the input
476      * data are processed or the end of table condition is satified
477      */
478     while (p_btbl_inst->data_size_uint16 != 0)
479     {
480         btbl_st_proc_fcn[p_btbl_inst->state](p_btbl_inst);
481     }
482     
483 } /* end of boot_proc_boot_tbl() */