Added an optional second ibl config area to the i2c eeprom
[keystone-rtos/ibl.git] / src / interp / btbl / btblwrap.c
1 /************************************************************************************
2  * FILE PURPOSE: Wrapper for the TI boot table processor
3  ************************************************************************************
4  * FILE NAME: btblwrap.c
5  *
6  * DESCRIPTION: The IBL wrapper for the boot table processor.
7  *
8  ************************************************************************************/
9 #include "types.h"
10 #include "ibl.h"
11 #include "iblloc.h"
12 #include "btblwrap.h"
13 #include "btbl.h"
14 #include "btblloc.h"
15 #include "iblbtbl.h"
16 #include <stdlib.h>
17 #include <string.h>
20 /* Globals used by the TI boot table processor */
22 BOOT_TBL_CB_T tiBootTable;
23 bootStats_t   bootStats;
24 Uint32        btblEcode;
25 Int32         btblWrapEcode;
28 #define MIN(a,b)  ((a) < (b)) ? (a) : (b)
31 /************************************************************************************
32  * FUNCTION PURPOSE: The main boot wrapper for the TI boot table processor
33  ************************************************************************************
34  * DESCRIPTION: Interfaces the IBL to the TI boot table driver. 
35  *              The TI boot table driver operates in a push data mode, the
36  *              IBL operates in a pull data mode. This function pulls data
37  *              from the interface and pushes is to the TI driver. To do this
38  *              the internal state of the TI boot table driver is used
39  *              to determine how much data to pull.
40  ************************************************************************************/
41 void iblBootBtbl (BOOT_MODULE_FXN_TABLE *bootFxn, Uint32 *entry_point)
42 {
43     Uint32  readSize;
44     Uint32  blockSize;
45     Uint32  blockSize16;
46     Uint8  *data;
47     Uint16 *data16;
48     Uint16  t16;
50     Int32 i, j;
52     *entry_point  = 0;
53     btblEcode     = 0;
54     btblWrapEcode = 0;
56     /* Initialize stats and btbl state */
57     iblMemset (&bootStats, 0, sizeof(bootStats_t));
58     
59     boot_init_boot_tbl_inst (&tiBootTable);    
61     data = iblMalloc (TI_BTBL_BLOCK_SIZE);
62     if (data == NULL)  {
63         btblWrapEcode = BTBL_WRAP_ECODE_MALLOC_FAIL;
64         return;
65     }
67     data16 = (Uint16 *)data;
69     while ((tiBootTable.state != BOOT_TBL_STATE_FLUSH) && (btblEcode == 0)) {
71         switch (tiBootTable.state)  {
73             case BOOT_TBL_STATE_PAD:   readSize = 2;
74                                        break;
76             case BOOT_TBL_STATE_INIT:  
77             case BOOT_TBL_STATE_SIZE:  
78             case BOOT_TBL_STATE_ADDR:  readSize = 4;
79                                        break;
81             case BOOT_TBL_STATE_DATA:  readSize = tiBootTable.section_size_bytes;
82                                        break;
83         }
86         while (readSize > 0)  {
88             blockSize   = MIN(readSize, TI_BTBL_BLOCK_SIZE);
89             blockSize16 = (blockSize + 1) >> 1;
91             /* No recovery on block read failure */
92             if ((*bootFxn->read)(data, blockSize) < 0)  {
93                 btblWrapEcode = BTBL_WRAP_ECODE_READ_FAIL;
94                 iblFree (data);
95                 return;
96             }
98             /* The data has been read as a byte stream. This data must
99              * be re-formatted as a 16 bit word stream */
100             for (j = i = 0; j < blockSize16; j++, i += 2)  {
102                 t16 = (data[i+0] << 8) | data[i+1];
103                 data16[j] = t16;
105             }
108             /* Process the block */
109             boot_proc_boot_tbl (&tiBootTable, data16, blockSize16);
111             readSize = readSize - blockSize;
113         }
115     }
117     if (btblEcode == 0)
118         *entry_point = tiBootTable.code_start_addr;
120     iblFree (data);
124 /***********************************************************************************
125  * FUNCTION PURPOSE: Handle a fatal error from the boot table processor
126  ***********************************************************************************
127  * DESCRIPTION: The error code is stored. Processing is terminated
128  *              through the global ecode value.
129  ***********************************************************************************/
130 void btblBootException (UINT32 ecode)
132     btblEcode     = ecode;
133     btblWrapEcode = BTBL_WRAP_ECODE_BTBL_FAIL;
137