]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - keystone-rtos/ibl.git/blob - src/interp/btbl/btblwrap.h
Update copyright information
[keystone-rtos/ibl.git] / src / interp / btbl / btblwrap.h
1 /*
2  *
3  * Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/ 
4  * 
5  * 
6  *  Redistribution and use in source and binary forms, with or without 
7  *  modification, are permitted provided that the following conditions 
8  *  are met:
9  *
10  *    Redistributions of source code must retain the above copyright 
11  *    notice, this list of conditions and the following disclaimer.
12  *
13  *    Redistributions in binary form must reproduce the above copyright
14  *    notice, this list of conditions and the following disclaimer in the 
15  *    documentation and/or other materials provided with the   
16  *    distribution.
17  *
18  *    Neither the name of Texas Instruments Incorporated nor the names of
19  *    its contributors may be used to endorse or promote products derived
20  *    from this software without specific prior written permission.
21  *
22  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
23  *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
24  *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
25  *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
26  *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
27  *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
28  *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
29  *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
30  *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
31  *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
32  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
33  *
34 */
38 #ifndef BTBLWRAP_H
39 #define BTBLWRAP_H
40 /********************************************************************************
41  * FILE PURPOSE: Define the IBL wrapper for the TI boot table processor
42  ********************************************************************************
43  * FILE NAM:E btblwrap.h
44  *
45  * DESCRIPTION: Definitions required for the IBL wrapper of the TI boot table
46  *                              processor
47  *
48  ********************************************************************************/
50 /* chipStartCore does nothing, since multiple core start is not supported */
51 #define chipStartCore(x,y,z)
53 /* A minimal boot stats structure */
54 typedef struct bootTblStats_s  {
56     UINT32 num_sections;
57     UINT32 num_pdma_copies;
58     
59 } bootTblStats_t;
62 typedef struct bootStats_s  {
63     
64     bootTblStats_t btbl;
65     
66 } bootStats_t;
68 extern bootStats_t      bootStats;
70 /****************************************************************************
71  * Definition: The c64x boot table tools will always pad boot table
72  *             entries to 32 bit elements. The boot table works in 16 bit
73  *             element sizes. If the size is not an even number of 16 bit
74  *             elements, add one word of padding.
75  ****************************************************************************/
76 #define chipAddBtblUint16Pad(x)     (((x)+1) & 0xfffffffe)
78 /* Return values */
79 #define CORE_NOERR      0
81 /* Module number */
82 #define BOOT_MODULE_ID_CHIP     0
83 #define BOOT_MODULE_ID_BTBL     1
85 /* Error code creation */
86 #define BOOT_ERROR_CODE(modnum,errnum)      (((modnum) << 16) | (errnum))
88 /* Fatal error handling */
89 #define BOOT_EXCEPTION      btblBootException
91 /* Macros */
92 #define CHIP_UINT16_TO_BYTES(x)     ((x) << 1)
93 #define CHIP_BYTES_TO_UINT16(x)     (((x) + 1) >> 1)
96 /* No interblock processing required */
97 #define chipBtblBlockDone()
99 /* No tracing dummy function */
100 #define chipDummy(x)
102         
103 /* gem.c prototypes */
104 UINT16 coreCopyData (UINT32 dest_addr, UINT16 *p_data, UINT32 sizeBytes, UINT16 start_vector);
106 /* btblwrap.c prototypes */
107 void btblBootException (UINT32 ecode);
109 /* The block size allocated through malloc. Chosen to match the value defined
110  * for the coff loader. malloc is used so the same heap section can be used. */
111 #define  TI_BTBL_BLOCK_SIZE   0x4000
112  
113 /* Read/Write 32bit values */
114 #define chipStoreWord(x,y)      *(x) = (y)
115 #define chipReadWord(x)         *(x)
117 /* Boot table wrapper error codes */
118 #define BTBL_WRAP_ECODE_MALLOC_FAIL     100
119 #define BTBL_WRAP_ECODE_READ_FAIL       101
120 #define BTBL_WRAP_ECODE_BTBL_FAIL       102
123 #endif /* BTBLWRAP_H */