Version 0.4 from Mike Line
[keystone-rtos/ibl.git] / src / interp / coff / osal.c
1 /*****************************************************************************
2  * FILE PURPOSE: IBL wrapper for the coff loader
3  *****************************************************************************
4  * FILE NAME: osal.c
5  *
6  * DESCRIPTION: Provides a boot wrapper to attach the coff loader 
7  *              to the IBL. 
8  *
9  *****************************************************************************/
10 #include "types.h"
11 #include "ibl.h"
12 #include "iblloc.h"
13 #include "header.h"
16 /*****************************************************************************
17  * FUNCTION PURPOSE: The main wrapper
18  *****************************************************************************
19  * DESCRIPTION: Attaches the coff loader to the IBL. The input parameters
20  *              are associated with globals defined in cload.c. 
21  *****************************************************************************/
22 void iblBootCoff (BOOT_MODULE_FXN_TABLE *bootFxn, Uint32 *ientry_point)
23 {
24     
25     /* Fin is declared as a FILE * in cload.c In osal.h FILE is
26      * defined to be BOOT_MODULE_FXN_TABLE, and reads/seeks
27      * are defined (in osal.h) to call through the BOOT_MODULE_FXN_TABLE
28      * calls. */
29     fin = bootFxn;
31    /* cload is the main coff loader function. It returns 0 on success.
32     * The entry point will be in the global entry_point declared in
33     * cload.c */
34    if (cload () == 0) 
35       *ientry_point = entry_point;
36    else
37       *ientry_point = 0;
39 }
42 /******************************************************************************
43  * FUNCTION PURPOSE: Determine if a file could be a coff file
44  ******************************************************************************
45  * DESCRIPTION: Examines the magic number and returns TRUE if it is one of 
46  *              the coff numbers (different numbers for different versions
47  ******************************************************************************/
48 bool iblIsCoff (Uint16 cv)
49 {
50     if (ISCOFF(cv))
51         return (TRUE);
53     /* Try an endian swap an recheck */
54     cv = ((cv >> 8) & 0x00ff) | ((cv << 8) & 0xff00);
55     if (ISCOFF(cv))
56         return (TRUE);
58     return (FALSE);
60 }
62 /******************************************************************************
63  * This is copied directly from cload_main.c from the original source
64  ******************************************************************************/
65 unsigned int reloc = 0;                 /* RELOCATION AMOUNT               */
66 int set_reloc_amount()
67 {
68   int i;
70   for (i = 0; i<  n_sections; ++i) reloc_amount[i] = reloc;
71   return 1;
72 }