Merge branch 'tmp-mike2'
[keystone-rtos/ibl.git] / src / main / iblinit.c
1 /**
2  *  @file iblinit.c
3  *
4  *  @brief
5  *              This file contains code which runs prior to loading the full IBL
6  *
7  *  @details
8  *              The IBL loads itself in a two stage process. The ROM boot loader
9  *              loads this first stage IBL first. This entire program must be
10  *              endian independent in execution.
11  *
12  *      This first loader reads the IBL parameters, and will endian
13  *      switch them if required. The PLL is configured if indicated
14  *      by the parameters.
15  *
16  *      The I2C block which contains the I2C EEPROM address for both
17  *      the big and little endian images is then read. Based on the
18  *      endianness of the device the rest of the IBL is read from
19  *      the I2C EEPROM, and execution is transferred to the full
20  *      IBL.
21  *
22  *      The subsequent reads are allowed to cross 16 bit i2c EEPROM
23  *      addresses. When the boundary is crossed the i2c address
24  *      field is incremented.
25  *
26  */
28 #include "ibl.h"
29 #include "iblloc.h"
30 #include "iblcfg.h"
31 #include "device.h"
32 #include "iblbtbl.h"
33 #include "i2c.h"
34 #include <string.h>
37 /**
38  *  @brief
39  *      Data structures shared between the 1st and 2nd stage IBL load
40  *      are declared in a single header file, included in both stages
41  */
42 #include "iblStage.h"
44 /**
45  *  @brief
46  *      byte swapping of i2c data must be done when in little endian mode
47  */
48 bool littleEndian;
50 /**
51  *  @brief
52  *      The boot table processing status is declared in the boot table wrapper,
53  *      and used here in the main status fields.
54  */
55 extern Int32 btblWrapEcode;
57 /**
58  *  @brief
59  *      The malloc function used for both boot stages of the ibl
60  */
61 void *iblMalloc (Uint32 size)
62 {
63     return (malloc (size));
64 }
66 /**
67  *  @brief
68  *      The free function used for both stages of the ibl
69  */
70 void iblFree (void *mem)
71 {
72     free (mem);
73 }
75 /**
76  *  @brief
77  *      The memset function used for both stages of the ibl
78  */
79 void *iblMemset (void *mem, Int32 ch, Uint32 n)
80 {
81     return (memset (mem, ch, n));
82 }
84 /**
85  *  @brief
86  *      The memcpy function used for both stages of the ibl
87  */
88 void *iblMemcpy (void *s1, const void *s2, Uint32 n)
89 {
90     return (memcpy (s1, s2, n));
92 }
94 /**
95  *  @brief
96  *      Ones complement addition
97  */
98 inline uint16 onesComplementAdd (uint16 value1, uint16 value2)
99 {
100   uint32 result;
102   result = (uint32)value1 + (uint32)value2;
104   result = (result >> 16) + (result & 0xFFFF); /* add in carry   */
105   result += (result >> 16);                    /* maybe one more */
106   return ((uint16)result);
110 /**
111  *  @brief
112  *      Ones complement checksum computation 
113  */
114 uint16 onesComplementChksum (uint16 * restrict p_data, uint16 len)
116   uint16 chksum = 0;
118   while (len > 0)
119   {
120     chksum = onesComplementAdd(chksum, *p_data);
121     p_data++;
122     len--;
123   }
124   return (chksum);
125
129 /**
130  *  @brief
131  *      Do a 4 byte endian swap
132  */
133 uint32 swap32val (uint32 v)
135     v =  (((v >> 24) & 0xff) <<  0)  |
136          (((v >> 16) & 0xff) <<  8)  |
137          (((v >>  8) & 0xff) << 16)  |
138          (((v >>  0) & 0xff) << 24);
140     return (v);
144 /**
145  *  @brief
146  *      Do a 2 byte endian swap
147  */
148 uint16 swap16val (uint16 v)
150     v = (((v >> 8) & 0xff) << 0)  |
151         (((v >> 0) & 0xff) << 8);
153     return (v);
157 /**
158  *  @brief
159  *  Do an endian swap on the ibl structure
160  */
161 void iblSwap (void)
163     int i;
165     ibl.iblMagic = swap32val (ibl.iblMagic);
167     for (i = 0; i < ibl_N_PLL_CFGS; i++)  {
168         ibl.pllConfig[i].doEnable      = swap16val (ibl.pllConfig[i].doEnable);
169         ibl.pllConfig[i].prediv        = swap32val (ibl.pllConfig[i].prediv);
170         ibl.pllConfig[i].mult          = swap32val (ibl.pllConfig[i].mult);
171         ibl.pllConfig[i].postdiv       = swap32val (ibl.pllConfig[i].postdiv);
172         ibl.pllConfig[i].pllOutFreqMhz = swap32val (ibl.pllConfig[i].pllOutFreqMhz);
173     }
175     ibl.ddrConfig.configDdr = swap16val (ibl.ddrConfig.configDdr);
177     ibl.ddrConfig.uEmif.emif3p1.sdcfg  = swap32val(ibl.ddrConfig.uEmif.emif3p1.sdcfg);
178     ibl.ddrConfig.uEmif.emif3p1.sdrfc  = swap32val(ibl.ddrConfig.uEmif.emif3p1.sdrfc);
179     ibl.ddrConfig.uEmif.emif3p1.sdtim1 = swap32val(ibl.ddrConfig.uEmif.emif3p1.sdtim1);
180     ibl.ddrConfig.uEmif.emif3p1.sdtim2 = swap32val(ibl.ddrConfig.uEmif.emif3p1.sdtim2);
181     ibl.ddrConfig.uEmif.emif3p1.dmcctl = swap32val(ibl.ddrConfig.uEmif.emif3p1.dmcctl);
183     for (i = 0; i < ibl_N_ETH_PORTS; i++)  {
184         ibl.ethConfig[i].ethPriority        = swap32val (ibl.ethConfig[i].ethPriority);
185         ibl.ethConfig[i].port               = swap32val (ibl.ethConfig[i].port);
186         ibl.ethConfig[i].doBootp            = swap16val (ibl.ethConfig[i].doBootp);
187         ibl.ethConfig[i].useBootpServerIp   = swap16val (ibl.ethConfig[i].useBootpServerIp);
188         ibl.ethConfig[i].useBootpFileName   = swap16val (ibl.ethConfig[i].useBootpFileName);
189         ibl.ethConfig[i].bootFormat         = swap32val (ibl.ethConfig[i].bootFormat);
190         ibl.ethConfig[i].blob.startAddress  = swap32val (ibl.ethConfig[i].blob.startAddress);
191         ibl.ethConfig[i].blob.sizeBytes     = swap32val (ibl.ethConfig[i].blob.sizeBytes);
192         ibl.ethConfig[i].blob.branchAddress = swap32val (ibl.ethConfig[i].blob.branchAddress);
194         ibl.sgmiiConfig[i].adviseAbility = swap32val (ibl.sgmiiConfig[i].adviseAbility);
195         ibl.sgmiiConfig[i].control       = swap32val (ibl.sgmiiConfig[i].control);
196         ibl.sgmiiConfig[i].txConfig      = swap32val (ibl.sgmiiConfig[i].txConfig);
197         ibl.sgmiiConfig[i].rxConfig      = swap32val (ibl.sgmiiConfig[i].rxConfig);
198         ibl.sgmiiConfig[i].auxConfig     = swap32val (ibl.sgmiiConfig[i].auxConfig);
199     }
201     ibl.mdioConfig.nMdioOps   = swap16val (ibl.mdioConfig.nMdioOps);
202     ibl.mdioConfig.mdioClkDiv = swap16val (ibl.mdioConfig.mdioClkDiv);
203     ibl.mdioConfig.interDelay = swap32val (ibl.mdioConfig.interDelay);
205     for (i = 0; i < ibl_N_MDIO_CFGS; i++)
206         ibl.mdioConfig.mdio[i] = swap32val (ibl.mdioConfig.mdio[i]);
208     ibl.nandConfig.nandPriority       = swap32val (ibl.nandConfig.nandPriority);
209     ibl.nandConfig.bootFormat         = swap32val (ibl.nandConfig.bootFormat);
210     ibl.nandConfig.blob.startAddress  = swap32val (ibl.nandConfig.blob.startAddress);
211     ibl.nandConfig.blob.sizeBytes     = swap32val (ibl.nandConfig.blob.sizeBytes);
212     ibl.nandConfig.blob.branchAddress = swap32val (ibl.nandConfig.blob.branchAddress);
214     ibl.nandConfig.nandInfo.busWidthBits  = swap32val (ibl.nandConfig.nandInfo.busWidthBits);
215     ibl.nandConfig.nandInfo.pageSizeBytes = swap32val (ibl.nandConfig.nandInfo.pageSizeBytes);
216     ibl.nandConfig.nandInfo.pageEccBytes  = swap32val (ibl.nandConfig.nandInfo.pageEccBytes);
217     ibl.nandConfig.nandInfo.pagesPerBlock = swap32val (ibl.nandConfig.nandInfo.pagesPerBlock);
218     ibl.nandConfig.nandInfo.totalBlocks   = swap32val (ibl.nandConfig.nandInfo.totalBlocks);
219     ibl.nandConfig.nandInfo.addressBytes  = swap32val (ibl.nandConfig.nandInfo.addressBytes);
220     ibl.nandConfig.nandInfo.lsbFirst      = swap16val (ibl.nandConfig.nandInfo.lsbFirst);
221     ibl.nandConfig.nandInfo.blockOffset   = swap32val (ibl.nandConfig.nandInfo.blockOffset);
222     ibl.nandConfig.nandInfo.pageOffset    = swap32val (ibl.nandConfig.nandInfo.pageOffset);
223     ibl.nandConfig.nandInfo.columnOffset  = swap32val (ibl.nandConfig.nandInfo.columnOffset);
224     ibl.nandConfig.nandInfo.postCommand   = swap16val (ibl.nandConfig.nandInfo.postCommand);
226     ibl.chkSum = swap16val (ibl.chkSum);
229         
231 /**
232  *  @brief
233  *      The i2c load context consists of the address of the next block 
234  *      to read, and a simple fifo holding any existing data.
235  */
236 #define I2C_MAX_BLOCK_SIZE      0x80
237 uint32 i2cReadAddress;
239 uint32 i2cFifoIn  = 0;
240 uint32 i2cFifoOut = 0;
241 uint8  i2cData[I2C_MAX_BLOCK_SIZE];
242 uint16 i2cSum[I2C_MAX_BLOCK_SIZE >> 1];
245 /**
246  *  @brief
247  *      Return the number of elements in the fifo
248  */
249 Uint32 i2cFifoCount (void)
251     Int32 count;
253     if (i2cFifoIn >= i2cFifoOut)
254         count = i2cFifoIn - i2cFifoOut;
255     else
256         count = i2cFifoIn + I2C_MAX_BLOCK_SIZE - i2cFifoOut;
258     return (count);
262     
263 /**
264  *  @brief
265  *      Read a byte from the fifo
266  */
267 Uint8 i2cFifoRead(void)
269     Uint8 v;
271     v = i2cData[i2cFifoOut];
273     i2cFifoOut += 1;
275     if (i2cFifoOut == i2cFifoIn)
276         i2cFifoOut = i2cFifoIn = 0;
278     if (i2cFifoOut >= I2C_MAX_BLOCK_SIZE)
279         i2cFifoOut = 0;
281     return (v);
285 /**
286  *  @brief
287  *      Read a block of data from the I2C eeprom and put it in the fifo
288  */
289 void i2cReadBlock (void)
291     uint16 len;
292     int32  i, j;
293     uint32 v;
295     for (;;) {
296         while (hwI2cMasterRead (i2cReadAddress & 0xffff,    /* The address on the eeprom of the table */
297                                 4,                          /* The number of bytes to read */
298                                 i2cData,                    /* Where to store the bytes */
299                                 i2cReadAddress >> 16,       /* The bus address of the eeprom */
300                                 IBL_I2C_CFG_ADDR_DELAY)     /* The delay between sending the address and reading data */
301     
302              != I2C_RET_OK)  {
304             iblStatus.i2cDataRetries += 1;
305         }
307         /* Form the length. The received bytes are always in big endian format */
308         len    = (i2cData[0] << 8) | i2cData[1];
311         if (len > I2C_MAX_BLOCK_SIZE)
312             continue;
315         while (hwI2cMasterRead (i2cReadAddress & 0xffff,    /* The address on the eeprom of the table */
316                                 len,                        /* The number of bytes to read */
317                                 i2cData,                    /* Where to store the bytes */
318                                 i2cReadAddress >> 16,       /* The bus address of the eeprom */
319                                 IBL_I2C_CFG_ADDR_DELAY)     /* The delay between sending the address and reading data */
320     
321              != I2C_RET_OK)  {
323             iblStatus.i2cDataRetries += 1;
324         }
327         /* Must do endian conversion to verify the checksum */
328         for (i = j = 0; i < len; i += 2, j += 1) 
329             i2cSum[j] = (i2cData[i+0] << 8) | i2cData[i+1];
331         v = onesComplementChksum (i2cSum, j);
332         if ((v == 0) || (v == 0xffff))
333             break;
335         
336         iblStatus.i2cDataRetries += 1;
338     }
341     i2cReadAddress += len;
342     
343     i2cFifoIn  = len;
344     i2cFifoOut = 4;    /* The i2c header is effectively removed */
348              
351 /**
352  *  @brief
353  *      Read data from the I2C to pass to the interpreter
354  */
355 Int32 iblI2cRead (Uint8 *buf, Uint32 num_bytes)
357     int i;
359     for (i = 0; i < num_bytes; i++)  {
361         if (i2cFifoCount() == 0)
362             i2cReadBlock ();
364         buf[i] = i2cFifoRead();
365     }
367     return (0);
371 #define iblBITMASK(x,y)      (   (   (  ((UINT32)1 << (((UINT32)x)-((UINT32)y)+(UINT32)1) ) - (UINT32)1 )   )   <<  ((UINT32)y)   )
372 #define iblREAD_BITFIELD(z,x,y)   (((UINT32)z) & iblBITMASK(x,y)) >> (y)
373 /**
374  *  @brief
375  *      Return the lower 16 bits of a 32 bit value. A function is used (with cross-function optomization off)
376  *      which results in an endian independent version
377  */
378 uint16 readLower16 (uint32 v)
380     return (iblREAD_BITFIELD(v,15,0));
384 /**
385  * @brief
386  *      Return the upper 16 bits of a 32 bit value. A function is used to force an endian independent version
387  */
388 uint16 readUpper16 (uint32 v)
390   return (iblREAD_BITFIELD(v,31,16));
394 /**
395  *  @brief
396  *      The module function table used for boot from i2c
397  */
398 BOOT_MODULE_FXN_TABLE i2cinit_boot_module = 
400     NULL,           /* Open  API */
401     NULL,           /* Close API */
402     iblI2cRead,     /* Read  API */
403     NULL,           /* Write API */
404     NULL,           /* Peek  API */
405     NULL,           /* Seek  API */
406     NULL            /* Query API */
407 };
411 /**
412  *  @brief
413  *      The main function
414  *
415  *  @details
416  *      The ibl configuration parameters are read from the i2c, 
417  *      followed by the i2c mapping information. The second stage
418  *      of the IBL is then loaded, and execution transferred 
419  *      to the second stage.
420  */
421 void main (void)
424     uint16       v;
425     uint16       configAddrLsw;
426     uint16       configAddrMsw;
427     uint32       entry;
428     void         (*exit)();
429     iblI2cMap_t  map;
431     memset (&iblStatus, 0, sizeof(iblStatus_t));
432     iblStatus.iblMagic     = ibl_MAGIC_VALUE;
433     iblStatus.activePeriph = ibl_ACTIVE_PERIPH_I2C;
435     /* Read the endianness setting of the device */
436     littleEndian = deviceIsLittleEndian();
437     
438     /* Load the default configuration table from the i2c. The actual speed of the device
439      * isn't really known here, since it is part of the table, so a compile time
440      * value is used (the pll may have been configured during the initial load) */
441     hwI2Cinit (IBL_I2C_DEV_FREQ_MHZ,        /* The CPU frequency during I2C data load */
442                DEVICE_I2C_MODULE_DIVISOR,   /* The divide down of CPU that drives the i2c */
443                IBL_I2C_CLK_FREQ_KHZ,        /* The I2C data rate used during table load */
444                IBL_I2C_OWN_ADDR);           /* The address used by this device on the i2c bus */
447     /* Read the I2C mapping information from the eeprom */
448     for (;;)  {
449         if (hwI2cMasterRead (IBL_I2C_MAP_TABLE_DATA_ADDR,     /* The address on the eeprom of the data mapping */
450                              sizeof(iblI2cMap_t),             /* The number of bytes to read */
451                              (UINT8 *)&map,                   /* Where to store the bytes */
452                              IBL_I2C_MAP_TABLE_DATA_BUS_ADDR, /* The bus address of the eeprom */
453                              IBL_I2C_CFG_ADDR_DELAY)          /* The delay between sending the address and reading data */
455              == I2C_RET_OK)  {
457                 /* On the I2C EEPROM the table is always formatted with the most significant
458                  * byte first. So if the device is running little endain the endian must be
459                  * swapped */
460                 if (littleEndian == TRUE)  {
461                     map.length   = swap16val (map.length);
462                     map.chkSum   = swap16val (map.chkSum);
463                     map.addrLe   = swap32val (map.addrLe);
464                     map.configLe = swap32val (map.configLe);
465                     map.addrBe   = swap32val (map.addrBe);
466                     map.configBe = swap32val (map.configBe);
468                     configAddrLsw = readLower16 (map.configLe);
469                     configAddrMsw = readUpper16 (map.configLe);
471                 }  else  {
472                     configAddrLsw = readLower16 (map.configBe);
473                     configAddrMsw = readUpper16 (map.configLe);
475                 }
478                 if (map.length != sizeof(iblI2cMap_t))  {
479                     iblStatus.mapSizeFail += 1;
480                     continue;
481                 }
483                 if (map.chkSum != 0)  {
484                     
485                     v = onesComplementChksum ((UINT16 *)&map, sizeof(iblI2cMap_t));
486                     if ((v != 0) && (v != 0xffff))  {
487                         iblStatus.mapRetries += 1;
488                         continue;
489                     }
490                 }
492                 break;
493         }
495         iblStatus.mapRetries += 1;
497     }
500     /* Read the i2c configuration tables until the checksum passes and the magic number
501      * matches. The checksum must be verified before the endian re-ordering is done */
502     for (;;)  {
504         if (hwI2cMasterRead (configAddrLsw,                  /* The address on the eeprom of the table */
505                              sizeof(ibl_t),                  /* The number of bytes to read */
506                              (UINT8 *)&ibl,                  /* Where to store the bytes */
507                              configAddrMsw,                  /* The bus address of the eeprom */
508                              IBL_I2C_CFG_ADDR_DELAY)         /* The delay between sending the address and reading data */
510              == I2C_RET_OK)  {
512                  if (ibl.chkSum != 0)  {
514                     v = onesComplementChksum ((UINT16 *)&ibl, sizeof(ibl_t) / sizeof(UINT16));
515                     if ((v != 0) && (v != 0xffff))  {
516                         iblStatus.i2cRetries += 1;
517                         continue;
518                     }
520                  }  
523                 if (ibl.iblMagic == ibl_MAGIC_VALUE)
524                     break;
526                 if (swap32val (ibl.iblMagic) == ibl_MAGIC_VALUE)  {
527                     iblSwap ();
528                     break;
529                 }
531                 iblStatus.magicRetries += 1;
533             }
535             iblStatus.i2cRetries += 1;
536     }
538     /* Pll configuration is device specific */
539     devicePllConfig ();
542     /* The rest of the IBL is in boot table format. Read and process the data */
543     if (littleEndian == TRUE) 
544         i2cReadAddress = map.addrLe;
545     else
546         i2cReadAddress = map.addrBe;
548     if (i2cReadAddress == 0xffffffff)  {
549         iblStatus.iblFail = ibl_FAIL_CODE_INVALID_I2C_ADDRESS;
550         for (;;);
551     }
554     /* Pass control to the boot table processor */
555     iblBootBtbl (&i2cinit_boot_module, &entry);
557     if (btblWrapEcode != 0)  {
558         iblStatus.iblFail = ibl_FAIL_CODE_BTBL_FAIL;
559         for (;;);
560     }
562     /* jump to the exit point, which will be the entry point for the full IBL */
563     exit = (void (*)())entry;
564     (*exit)();