5dd5ff1d438e370f628514e18b70d4f87caa40ae
1 @REM ******************************************************************************
2 @REM * FILE PURPOSE: Environment Setup for building Bootloader
3 @REM ******************************************************************************
4 @REM * FILE NAME: setupenv.bat
5 @REM *
6 @REM * DESCRIPTION:
7 @REM * Configures and sets up the Build Environment for Bootloader in DOS environment.
8 @REM *
9 @REM * Customers are expected to modify this file as per their build environment.
10 @REM *
11 @REM * USAGE:
12 @REM * setupenv.bat
13 @REM *
14 @REM * Copyright (C) 2010, Texas Instruments, Inc.
15 @REM *****************************************************************************
17 @echo off
19 REM Setup the ibl build environment if using cygwin for build
21 REM Modify following lines based on target environment for the toolset installed
22 REM Dependency is related to path for Cygwin and CGEN installed
24 REM Specify the path to cygwin binaries and the code gen tools
25 REM If the path has directory names with spaces use the below format to specify
26 REM for e.g PATH=G:\cygwin\bin;C:\PROGRA~1\TEXASI~1\C6000C~1.12\bin
27 set PATH=G:\cygwin\bin;t:\c6xx\cgen6_1_12\c6000\cgtools\bin
29 REM Specify the base directory of the c6000 compiler with UNIX style path separator
30 set TOOLSC6X=t:/c6xx/cgen6_1_12/c6000/cgtools
32 REM Specify the base directory of the c6000 compiler with DOS style path separator
33 set TOOLSC6XDOS=t:\c6xx\cgen6_1_12\c6000\cgtools
35 REM # Don't modify the below variables. They are derived from the above definitions
36 set PATH=%PATH%;%SystemRoot%\system32;%SystemRoot%;
37 set BISONSKEL=yacc.c