Make updates for big endian
[keystone-rtos/ibl.git] / src / util / btoccs / bfaddsect.c
1 /* Append a boot table section to the end of a boot table 
2  * usage: bfaddsect infile addr byte1 [bytes2 [byte3 [...]]]
3  * The output is to stdout
4  * 
5  * All values are taken to be btye values */
8 #include <stdio.h>
9 #include <malloc.h>
13 int asciiByte (unsigned char c)
14 {
15   if ((c >= '0') && (c <= '9'))
16     return (1);
18   if ((c >= 'A') && (c <= 'F'))
19     return (1);
21   return (0);
22 }
24 int toNum (unsigned char c)
25 {
26   if ((c >= '0') && (c <= '9'))
27     return (c - '0');
29   return (c - 'A' + 10);
31 }
34 /* Copy a line from s to stdout */
35 void  lineCpy (FILE *s)
36 {
37   char iline[132];
39   fgets (iline, 131, s);
40   fputs (iline, stdout);
42 }
44 /* Read a .b file. */
45 int readBFile (FILE *s, unsigned char *data, unsigned maxSize)
46 {
47   unsigned char x, y;
48   int byteCount = 0;
50   for (;;) {
52     /* read the 1st ascii char */
53     do  {
54       x = fgetc (s);
55       if (x == (unsigned char)EOF)
56         return (byteCount);
58     } while (!asciiByte(x));
60     /* Read the next ascii char */
61     y = fgetc (s);
62     if (y == (unsigned char)EOF)
63       return (byteCount);
64     if (asciiByte(y))
65       data[byteCount++] = (toNum(x) << 4) | toNum (y);
67     if (byteCount >= maxSize)  {
68       fprintf (stderr, "Max input array size exceeded\n");
69       return (-1);
70     }
72   }
74 }
76 unsigned dwordConvert (unsigned char *data)
77 {
78   unsigned value;
79   unsigned char c[4];
80   int i;
82   c[0] = c[1] = c[2] = c[3] = 0;
83   
84   for (i = 0; i < 4; i++)  {
85     c[i] = data[i];
86   }
88   value = c[3] | (c[2] << 8) | (c[1] << 16) | (c[0] << 24);
90   return (value);
92 }
94 #define SIZE    0x100000  /* max number of bytes in the array */
95 #define MAX_BYTES   64    /* max size of the boot table       */
97 int main (int argc, char *argv[])
98 {
99   FILE *strin;
100   unsigned char *dataSet;
101   unsigned int addr;
102   unsigned int secsize;
103   unsigned char newchars[MAX_BYTES];
104   int i;
105   int nbytes;
106   int asize;
107   int p;
110   /* get the args */
111   if (argc < 4)  {
112     fprintf (stderr, "usage: %s infile hex_addr byte1 [byte2 [byte3 [ ...byte64]]]\n", argv[0]);
113     return (-1);
114   }
116   /* input file */
117   strin = fopen (argv[1], "r");
118   if (strin == NULL)  {
119     fprintf (stderr, "%s: Could not open file %s\n", argv[0], argv[1]);
120     return (-1);
121   }
123   /* Address */
124   sscanf (argv[2], "%x", &addr);
126   /* Number of bytes */
127   nbytes = argc - 3;
128   for (i = 0; i < nbytes; i++)
129     sscanf (argv[i+3], "%x", &newchars[i]);
132   /* Allocate memory for the data set */
133   dataSet = malloc (SIZE * sizeof (unsigned char));
134   if (dataSet == NULL)  {
135     fprintf (stderr, "%s: malloc failure\n", argv[0]);
136     return (-1);
137   }
139   /* Copy the first two lines of the input file to stdout */
140   lineCpy (strin);
141   lineCpy (strin);
143   /* Read the data into the byte stream */
144   asize = readBFile (strin, dataSet, SIZE);
145   fclose (strin);
146   
147   /* Parse the input file. Prepend the new section at the end */
149   /* Just skip the entry address */
150   p = 4;
152   do  {
153     secsize = dwordConvert (&dataSet[p]);
154     secsize = (secsize + 3) & 0xfffffffc;  /* segment pad */
155     p = p + secsize + 8;  /* 4 bytes length, 4 bytes address */
156   } while (secsize);
158   /* back up to the zero section size */
159   p = p - 8; 
161   /* p now points to the 0 length entry. Put the new data here */
162   /* The section size */
163   dataSet[p++] = (nbytes >> 24) & 0xff;
164   dataSet[p++] = (nbytes >> 16) & 0xff;
165   dataSet[p++] = (nbytes >>  8) & 0xff;
166   dataSet[p++] = (nbytes >>  0) & 0xff;
168   /* Put the section address */
169   dataSet[p++] = (addr >> 24) & 0xff;
170   dataSet[p++] = (addr >> 16) & 0xff;
171   dataSet[p++] = (addr >>  8) & 0xff;
172   dataSet[p++] = (addr >>  0) & 0xff;
174   /* Put the data */
175   for (i = 0; i < nbytes; i++)
176     dataSet[p++] = newchars[i];
178   while (p % 4)
179     dataSet[p++] = 0;
181   /* Add the 0 length section */
182   for (i = 0; i < 4; i++)
183     dataSet[p++] = 0;
186   /* Write out the data */
187   for (i = 0; i < p; i++)  {
188     fprintf (stdout, "%02X", dataSet[i]);
190     if ( ((i+1) % 24) )
191       fprintf (stdout, " ");
192     else
193       fprintf (stdout, "\n");
195   }
197   /* Write the trailing character */
198   fprintf (stdout, "\n%c",3);
200   free (dataSet);
202   return (0);
206