Make updates for big endian
[keystone-rtos/ibl.git] / src / util / btoccs / bfmerge.c
1 /* Combine two boot tables. 
2  * usage bfmerge file1 file2 [file3 [file4 [...]]]
3  * The output is to stdout
4  *
5  * */
7 #include <stdio.h>
8 #include <malloc.h>
10 int asciiByte (unsigned char c)
11 {
12   if ((c >= '0') && (c <= '9'))
13     return (1);
15   if ((c >= 'A') && (c <= 'F'))
16     return (1);
18   return (0);
19 }
21 int toNum (unsigned char c)
22 {
23   if ((c >= '0') && (c <= '9'))
24     return (c - '0');
26   return (c - 'A' + 10);
28 }
31 /* Copy a line from s to stdout */
32 void  lineCpy (FILE *s)
33 {
34   char iline[132];
36   fgets (iline, 131, s);
37   fputs (iline, stdout);
39 }
41 /* Toss a line */
42 void lineToss (FILE *s)
43 {
44   char iline[132];
46   fgets (iline, 131, s);
48 }
50 /* Read a .b file. */
51 int readBFile (FILE *s, unsigned char *data, unsigned maxSize)
52 {
53   unsigned char x, y;
54   int byteCount = 0;
56   for (;;) {
58     /* read the 1st ascii char */
59     do  {
60       x = fgetc (s);
61       if (x == (unsigned char)EOF)
62         return (byteCount);
64     } while (!asciiByte(x));
66     /* Read the next ascii char */
67     y = fgetc (s);
68     if (y == (unsigned char)EOF)
69       return (byteCount);
70     if (asciiByte(y))
71       data[byteCount++] = (toNum(x) << 4) | toNum (y);
73     if (byteCount >= maxSize)  {
74       fprintf (stderr, "Max input array size exceeded\n");
75       return (-1);
76     }
78   }
80 }
82 unsigned dwordConvert (unsigned char *data)
83 {
84   unsigned value;
85   unsigned char c[4];
86   int i;
88   c[0] = c[1] = c[2] = c[3] = 0;
89   
90   for (i = 0; i < 4; i++)  {
91     c[i] = data[i];
92   }
94   value = c[3] | (c[2] << 8) | (c[1] << 16) | (c[0] << 24);
96   return (value);
98 }
101 int bparse (unsigned char *dataSet, int l)
103   unsigned int secsize;
105   do  {
107     secsize = dwordConvert (&dataSet[l]);
108     secsize = (secsize + 3) & 0xfffffffc; /* segment pad */
109     l = l + secsize + 8;  /* 4 bytes length, 4 bytes address */
110   
111   } while (secsize);
113   /* Back up to the zero section size */
114   l = l - 8;
116   return (l);
121 #define SIZE    1000000
122 #define APPEND   100000
124 int main (int argc, char *argv[])
126   FILE *strin;
127   unsigned char *dataSet;
128   unsigned char *appSet;
129   unsigned int addr;
130   unsigned int secsize;
131   int asize;
132   int i, j;
133   int nbytes;
134   int p;
136   /* Must have at least two input files */ 
137   if (argc < 3)  { 
138     fprintf (stderr, "usage: %s file1 file2 [file3 [file4 [...]]]\n", argv[0]); 
139     return (-1); 
140   } 
141   
142   /* Allocate memory for the data set */ 
143   dataSet = malloc (SIZE * sizeof (unsigned char));
144   if (dataSet == NULL)  {
145     fprintf (stderr, "%s: malloc failure\n", argv[0]);
146     return (-1);
147   }
149   appSet = malloc (APPEND * sizeof (unsigned char ));
150   if (appSet == NULL)  {
151     fprintf (stderr, "%s malloc failure\n", argv[0]);
152     return (-1);
153   }
156   /* The first data file is handled seperately */
157   strin = fopen (argv[1], "r");
158   if (strin == NULL)  {
159     fprintf (stderr, "%s: Could not open file %s\n", argv[0], argv[1]);
160     free (dataSet);
161     return (-1);
162   }
164   /* Copy the first two lines of the input file to stdout */
165   lineCpy (strin);
166   lineCpy (strin);
168   /* Read in the first data set */
169   asize = readBFile (strin, dataSet, SIZE);
170   fclose (strin);
172   /* Parse the file, skipping the entry symbol */
173   p = 4;
174   p = bparse (dataSet, p);
177   /* Add the remaining data sets */
179   for (i = 2; i < argc; i++)  {
181     strin = fopen (argv[i], "r");
182     if (strin == NULL)  {
183       fprintf (stderr, "%s: Could not open file %s\n", argv[0], argv[i]);
184       free (dataSet);
185       return (-1);
186     }
188     /* Toss the first two lines */
189     lineToss (strin);
190     lineToss (strin);
192     asize = readBFile (strin, appSet, APPEND);
193     fclose (strin);
195     /* Append the new data set, skip the 4 bytes of entry symbol */
196     for (j = 0; j < asize-4; j++)
197       dataSet[p+j] = appSet[j+4];
199     /* reparse from the current point */
200     p = bparse (dataSet, p);
202   }
204   /* Add the 0 section size */
205   for (i = 0; i < 4; i++)
206     dataSet[p++] = 0;
209   /* Write out the data */
210   for (i = 0; i < p; i++)  {
211     fprintf (stdout, "%02X", dataSet[i]);
213     if ( ((i+1) % 24) )
214       fprintf (stdout, " ");
215     else
216       fprintf (stdout, "\n");
218   }
220   /* Write the trailing character */
221   fprintf (stdout, "\n%c",3);
223   free (dataSet);
225   return (0);