Updated romparse utility to specify device address
[keystone-rtos/ibl.git] / src / util / i2cConfig / i2cConfig.gel
1 #define TRUE  1
2 #define FALSE 0
4 #define ibl_MAGIC_VALUE                  0xCEC11EBB
6 #define ibl_HIGHEST_PRIORITY     1  
7 #define ibl_LOWEST_PRIORITY     10
8 #define ibl_DEVICE_NOBOOT       20
10 #define SETIP(array,i0,i1,i2,i3)      array[0]=(i0);  \
11                                       array[1]=(i1);  \
12                                       array[2]=(i2);  \
13                                       array[3]=(i3)
15 #define ibl_BOOT_FORMAT_AUTO    0
16 #define ibl_BOOT_FORMAT_NAME    1
17 #define ibl_BOOT_FORMAT_BIS     2
18 #define ibl_BOOT_FORMAT_COFF    3
19 #define ibl_BOOT_FORMAT_ELF     4
20 #define ibl_BOOT_FORMAT_BBLOB   5
21 #define ibl_BOOT_FORMAT_BTBL    6
23 #define ibl_MAIN_PLL    0
24 #define ibl_DDR_PLL     1
25 #define ibl_NET_PLL     2
28 menuitem "EVM c6472 IBL";
30 hotmenu setConfig_c6472()
31 {
32     ibl.iblMagic = ibl_MAGIC_VALUE;
34     ibl.pllConfig[ibl_MAIN_PLL].doEnable      = TRUE;
35     ibl.pllConfig[ibl_MAIN_PLL].prediv        = 1;
36     ibl.pllConfig[ibl_MAIN_PLL].mult          = 28;
37     ibl.pllConfig[ibl_MAIN_PLL].postdiv       = 1;
38     ibl.pllConfig[ibl_MAIN_PLL].pllOutFreqMhz = 700;
40     /* The DDR PLL. The multipliers/dividers are fixed, so are really dont cares */
41     ibl.pllConfig[ibl_DDR_PLL].doEnable = TRUE;
43     /* The network PLL. The multipliers/dividers are fixed */
44     ibl.pllConfig[ibl_NET_PLL].doEnable = TRUE;
46     /* EMIF configuration. The values are for DDR at 533 MHz  */
47     ibl.ddrConfig.configDdr = TRUE;
49     ibl.ddrConfig.uEmif.emif3p1.sdcfg  = 0x00538832; /* timing, 32bit wide */
50     ibl.ddrConfig.uEmif.emif3p1.sdrfc  = 0x0000073B; /* Refresh 533Mhz */ 
51     ibl.ddrConfig.uEmif.emif3p1.sdtim1 = 0x47245BD2; /* Timing 1 */
52     ibl.ddrConfig.uEmif.emif3p1.sdtim2 = 0x0125DC44; /* Timing 2 */
53     ibl.ddrConfig.uEmif.emif3p1.dmcctl = 0x50001906; /* PHY read latency for CAS 5 is 5 + 2 - 1 */
55     /* Ethernet configuration for port 0 */
56     ibl.ethConfig[0].ethPriority      = ibl_HIGHEST_PRIORITY;
57     ibl.ethConfig[0].port             = 0;
59     /* Bootp is disabled. The server and file name are provided here */
60     ibl.ethConfig[0].doBootp          = FALSE;
61     ibl.ethConfig[0].useBootpServerIp = FALSE;
62     ibl.ethConfig[0].useBootpFileName = FALSE;
63     ibl.ethConfig[0].bootFormat       = ibl_BOOT_FORMAT_BBLOB;
66     SETIP(ibl.ethConfig[0].ethInfo.ipAddr,    10,218,109,35);
67     SETIP(ibl.ethConfig[0].ethInfo.serverIp,  10,218,109,196);
68     SETIP(ibl.ethConfig[0].ethInfo.gatewayIp, 10,218,109,1);
69     SETIP(ibl.ethConfig[0].ethInfo.netmask,   255,255,255,0);
71     /* Leave the hardware address as 0 so the e-fuse value will be used */
73     strcpy (ibl.ethConfig[0].ethInfo.fileName, "test.blob");
75     /* Even though the entire range of DDR2 is chosen, the load will
76      * stop when the ftp reaches the end of the file */
77     ibl.ethConfig[0].blob.startAddress  = 0xe0000000;       /* Base address of DDR2 */
78     ibl.ethConfig[0].blob.sizeBytes     = 0x20000000;       /* All of DDR2 */
79     ibl.ethConfig[0].blob.branchAddress = 0xe0000000;       /* Base of DDR2 */
81     /* For port 1 use bootp */
82     /* Ethernet configuration for port 0 */
83     ibl.ethConfig[1].ethPriority      = ibl_HIGHEST_PRIORITY + 1;
84     ibl.ethConfig[1].port             = 1;
86     /* Bootp is disabled. The server and file name are provided here */
87     ibl.ethConfig[1].doBootp          = TRUE;
88     ibl.ethConfig[1].useBootpServerIp = TRUE;
89     ibl.ethConfig[1].useBootpFileName = TRUE;
90     ibl.ethConfig[1].bootFormat       = ibl_BOOT_FORMAT_BBLOB;
93     /* SGMII not present */
94         ibl.sgmiiConfig[0].adviseAbility = 0;
95         ibl.sgmiiConfig[0].control       = 0;
96         ibl.sgmiiConfig[0].txConfig      = 0;
97         ibl.sgmiiConfig[0].rxConfig      = 0;
98         ibl.sgmiiConfig[0].auxConfig     = 0;
100         ibl.sgmiiConfig[1].adviseAbility = 0;
101         ibl.sgmiiConfig[1].control       = 0;
102         ibl.sgmiiConfig[1].txConfig      = 0;
103         ibl.sgmiiConfig[1].rxConfig      = 0;
104         ibl.sgmiiConfig[1].auxConfig     = 0;
107     /* Leave the hardware address as 0 so the e-fuse value will be used */
108     /* Leave all remaining fields as 0 since bootp will fill them in */
111     /* Even though the entire range of DDR2 is chosen, the load will
112      * stop when the ftp reaches the end of the file */
113     ibl.ethConfig[1].blob.startAddress  = 0xe0000000;       /* Base address of DDR2 */
114     ibl.ethConfig[1].blob.sizeBytes     = 0x20000000;       /* All of DDR2 */
115     ibl.ethConfig[1].blob.branchAddress = 0xe0000000;       /* Base of DDR2 */
116     
119     /* MDIO configuration */
120     ibl.mdioConfig.nMdioOps = 8;
121     ibl.mdioConfig.mdioClkDiv = 0x20;
122     ibl.mdioConfig.interDelay = 1400;   /* ~2ms at 700 MHz */
124     ibl.mdioConfig.mdio[0] =  (1 << 30) | (27 << 21) | (24 << 16) | 0x848b;
125     ibl.mdioConfig.mdio[1] =  (1 << 30) | (20 << 21) | (24 << 16) | 0x0ce0;
126     ibl.mdioConfig.mdio[2] =  (1 << 30) | (24 << 21) | (24 << 16) | 0x4101;
127     ibl.mdioConfig.mdio[3] =  (1 << 30) | ( 0 << 21) | (24 << 16) | 0x9140;
129     ibl.mdioConfig.mdio[4] =  (1 << 30) | (27 << 21) | (25 << 16) | 0x848b;
130     ibl.mdioConfig.mdio[5] =  (1 << 30) | (20 << 21) | (25 << 16) | 0x0ce0;
131     ibl.mdioConfig.mdio[6] =  (1 << 30) | (24 << 21) | (25 << 16) | 0x4101;
132     ibl.mdioConfig.mdio[7] =  (1 << 30) | ( 0 << 21) | (25 << 16) | 0x9140;
135     /* Nand boot is disabled */
136     ibl.nandConfig.nandPriority = ibl_DEVICE_NOBOOT;
141 menuitem "EVM c6474 Mez IBL";
143 hotmenu setConfig_c6474()
145     ibl.iblMagic = ibl_MAGIC_VALUE;
147     ibl.pllConfig[ibl_MAIN_PLL].doEnable      = TRUE;
148     ibl.pllConfig[ibl_MAIN_PLL].prediv        = 1;
149     ibl.pllConfig[ibl_MAIN_PLL].mult          = 20;
150     ibl.pllConfig[ibl_MAIN_PLL].postdiv       = 1;
151     ibl.pllConfig[ibl_MAIN_PLL].pllOutFreqMhz = 1000;
153     /* The DDR PLL. The multipliers/dividers are fixed, so are really dont cares */
154     ibl.pllConfig[ibl_DDR_PLL].doEnable = TRUE;
156     /* The network PLL. The multipliers/dividers are fixed */
157     ibl.pllConfig[ibl_NET_PLL].doEnable = TRUE;
159     /* EMIF configuration. The values are for DDR at 533 MHz  */
160     ibl.ddrConfig.configDdr = TRUE;
162     ibl.ddrConfig.uEmif.emif3p1.sdcfg  = 0x00d38a32; /* cas5, 8 banks, 10 bit column */
163     ibl.ddrConfig.uEmif.emif3p1.sdrfc  = 0x00000a29; /* Refresh 333Mhz */ 
164     ibl.ddrConfig.uEmif.emif3p1.sdtim1 = 0x4d246c9a; /* Timing 1 */
165     ibl.ddrConfig.uEmif.emif3p1.sdtim2 = 0x00993c42; /* Timing 2 */
166     ibl.ddrConfig.uEmif.emif3p1.dmcctl = 0x50001906; /* PHY read latency for CAS 5 is 5 + 2 - 1 */
169     /* Ethernet configuration for port 0 */
170     ibl.ethConfig[0].ethPriority      = ibl_HIGHEST_PRIORITY;
171     ibl.ethConfig[0].port             = 0;
173     /* Bootp is disabled. The server and file name are provided here */
174     ibl.ethConfig[0].doBootp          = FALSE;
175     ibl.ethConfig[0].useBootpServerIp = FALSE;
176     ibl.ethConfig[0].useBootpFileName = FALSE;
177     ibl.ethConfig[0].bootFormat       = ibl_BOOT_FORMAT_BLOB;
179     SETIP(ibl.ethConfig[0].ethInfo.ipAddr,    10,218,109,35);
180     SETIP(ibl.ethConfig[0].ethInfo.serverIp,  10,218,109,196);
181     SETIP(ibl.ethConfig[0].ethInfo.gatewayIp, 10,218,109,1);
182     SETIP(ibl.ethConfig[0].ethInfo.netmask,   255,255,255,0);
184     /* Set the hardware address as 0 so the e-fuse value will be used */
185     ibl.ethConfig[0].hwAddress[0] = 0;
186     ibl.ethConfig[0].hwAddress[1] = 0;
187     ibl.ethConfig[0].hwAddress[2] = 0;
188     ibl.ethConfig[0].hwAddress[3] = 0;
189     ibl.ethConfig[0].hwAddress[4] = 0;
190     ibl.ethConfig[0].hwAddress[5] = 0;
193     ibl.ethConfig[0].ethInfo.fileName[0]  = 't';
194     ibl.ethConfig[0].ethInfo.fileName[1]  = 'e';
195     ibl.ethConfig[0].ethInfo.fileName[2]  = 's';
196     ibl.ethConfig[0].ethInfo.fileName[3]  = 't';
197     ibl.ethConfig[0].ethInfo.fileName[4]  = '.';
198     ibl.ethConfig[0].ethInfo.fileName[5]  = 'b';
199     ibl.ethConfig[0].ethInfo.fileName[6]  = 'l';
200     ibl.ethConfig[0].ethInfo.fileName[7]  = 'o';
201     ibl.ethConfig[0].ethInfo.fileName[8]  = 'b';
202     ibl.ethConfig[0].ethInfo.fileName[9]  = '\0';
203     ibl.ethConfig[0].ethInfo.fileName[10] = '\0';
204     ibl.ethConfig[0].ethInfo.fileName[11] = '\0';
205     ibl.ethConfig[0].ethInfo.fileName[12] = '\0';
206     ibl.ethConfig[0].ethInfo.fileName[13] = '\0';
207     ibl.ethConfig[0].ethInfo.fileName[14] = '\0';
210     /* Even though the entire range of DDR2 is chosen, the load will
211      * stop when the ftp reaches the end of the file */
212     ibl.ethConfig[0].blob.startAddress  = 0xe0000000;       /* Base address of DDR2 */
213     ibl.ethConfig[0].blob.sizeBytes     = 0x20000000;       /* All of DDR2 */
214     ibl.ethConfig[0].blob.branchAddress = 0xe0000000;       /* Base of DDR2 */
216     /* There is no port 1 on the 6474 */
217     ibl.ethConfig[1].ethPriority      = ibl_DEVICE_NOBOOT;
220     /* MDIO configuration */
221     ibl.mdioConfig.nMdioOps = 8;
222     ibl.mdioConfig.mdioClkDiv = 0x26;
223     ibl.mdioConfig.interDelay = 2000;   /* ~2ms at 1000 MHz */
225     ibl.mdioConfig.mdio[0] =  (1 << 30) | ( 4 << 21) | (27 << 16) | 0x0081;
226     ibl.mdioConfig.mdio[1] =  (1 << 30) | (26 << 21) | (15 << 16) | 0x0047;
227     ibl.mdioConfig.mdio[2] =  (1 << 30) | (26 << 21) | (14 << 16) | 0x0047;
228     ibl.mdioConfig.mdio[3] =  (1 << 30) | ( 0 << 21) | (15 << 16) | 0x8140;
230     ibl.mdioConfig.mdio[4] =  (1 << 30) | ( 0 << 21) | (14 << 16) | 0x8140;
231     ibl.mdioConfig.mdio[5] =  (1 << 30) | ( 1 << 21) | (22 << 16) | 0x043e;
232     ibl.mdioConfig.mdio[6] =  (1 << 30) | ( 1 << 21) | (22 << 16) | 0x043e;
233     ibl.mdioConfig.mdio[7] =  (1 << 30) | ( 0 << 21) | ( 1 << 16) | 0xa100;
236     /* Nand boot is disabled */
237     ibl.nandConfig.nandPriority = ibl_DEVICE_NOBOOT;
242 menuitem "EVM c6455 IBL";
244 hotmenu setConfig_c6455()
246     ibl.iblMagic = ibl_MAGIC_VALUE;
248     ibl.pllConfig[ibl_MAIN_PLL].doEnable      = TRUE;
249     ibl.pllConfig[ibl_MAIN_PLL].prediv        = 1;
250     ibl.pllConfig[ibl_MAIN_PLL].mult          = 20;
251     ibl.pllConfig[ibl_MAIN_PLL].postdiv       = 1;
252     ibl.pllConfig[ibl_MAIN_PLL].pllOutFreqMhz = 1000;
254     /* The DDR PLL. The multipliers/dividers are fixed, so are really dont cares */
255     ibl.pllConfig[ibl_DDR_PLL].doEnable = TRUE;
257     /* The network PLL. The multipliers/dividers are fixed */
258     ibl.pllConfig[ibl_NET_PLL].doEnable = TRUE;
260     /* EMIF configuration. The values are for DDR at 500 MHz  */
261     ibl.ddrConfig.configDdr = TRUE;
263     ibl.ddrConfig.uEmif.emif3p1.sdcfg  = 0x00538822; /* timing, 32bit wide */
264     ibl.ddrConfig.uEmif.emif3p1.sdrfc  = 0x000007a2; /* Refresh 500Mhz */ 
265     ibl.ddrConfig.uEmif.emif3p1.sdtim1 = 0x3edb4b91; /* Timing 1 */
266     ibl.ddrConfig.uEmif.emif3p1.sdtim2 = 0x00a2c722; /* Timing 2 */
267     ibl.ddrConfig.uEmif.emif3p1.dmcctl = 0x00000005; /* PHY read latency for CAS 4 is 4 + 2 - 1 */
269     /* Ethernet configuration for port 0 */
270     ibl.ethConfig[0].ethPriority      = ibl_HIGHEST_PRIORITY;
271     ibl.ethConfig[0].port             = 0;
273     /* Bootp is disabled. The server and file name are provided here */
274     ibl.ethConfig[0].doBootp          = FALSE;
275     ibl.ethConfig[0].useBootpServerIp = FALSE;
276     ibl.ethConfig[0].useBootpFileName = FALSE;
277     ibl.ethConfig[0].bootFormat       = ibl_BOOT_FORMAT_BBLOB;
280     SETIP(ibl.ethConfig[0].ethInfo.ipAddr,    10,218,109,35);
281     SETIP(ibl.ethConfig[0].ethInfo.serverIp,  10,218,109,196);
282     SETIP(ibl.ethConfig[0].ethInfo.gatewayIp, 10,218,109,1);
283     SETIP(ibl.ethConfig[0].ethInfo.netmask,   255,255,255,0);
285     /* There is no e-fuse mac address. A value must be assigned
286     ibl.ethConfig[0].hwAddress[0] = 0x00;
287     ibl.ethConfig[0].hwAddress[1] = 0xe0;
288     ibl.ethConfig[0].hwAddress[2] = 0xa6;
289     ibl.ethConfig[0].hwAddress[3] = 0x66;
290     ibl.ethConfig[0].hwAddress[4] = 0x57;
291     ibl.ethConfig[0].hwAddress[5] = 0x19;
294     ibl.ethConfig[0].ethInfo.fileName[0]  = 't';
295     ibl.ethConfig[0].ethInfo.fileName[1]  = 'e';
296     ibl.ethConfig[0].ethInfo.fileName[2]  = 's';
297     ibl.ethConfig[0].ethInfo.fileName[3]  = 't';
298     ibl.ethConfig[0].ethInfo.fileName[4]  = '.';
299     ibl.ethConfig[0].ethInfo.fileName[5]  = 'b';
300     ibl.ethConfig[0].ethInfo.fileName[6]  = 'l';
301     ibl.ethConfig[0].ethInfo.fileName[7]  = 'o';
302     ibl.ethConfig[0].ethInfo.fileName[8]  = 'b';
303     ibl.ethConfig[0].ethInfo.fileName[9]  = '\0';
304     ibl.ethConfig[0].ethInfo.fileName[10] = '\0';
305     ibl.ethConfig[0].ethInfo.fileName[11] = '\0';
306     ibl.ethConfig[0].ethInfo.fileName[12] = '\0';
307     ibl.ethConfig[0].ethInfo.fileName[13] = '\0';
308     ibl.ethConfig[0].ethInfo.fileName[14] = '\0';
311     /* Even though the entire range of DDR2 is chosen, the load will
312      * stop when the ftp reaches the end of the file */
313     ibl.ethConfig[0].blob.startAddress  = 0xe0000000;       /* Base address of DDR2 */
314     ibl.ethConfig[0].blob.sizeBytes     = 0x20000000;       /* All of DDR2 */
315     ibl.ethConfig[0].blob.branchAddress = 0xe0000000;       /* Base of DDR2 */
317     /* There is no ethernet port 1 */
318     ibl.ethConfig[1].ethPriority      = ibl_DEVICE_NOBOOT;
321     /* SGMII not present */
322         ibl.sgmiiConfig[0].adviseAbility = 0;
323         ibl.sgmiiConfig[0].control       = 0;
324         ibl.sgmiiConfig[0].txConfig      = 0;
325         ibl.sgmiiConfig[0].rxConfig      = 0;
326         ibl.sgmiiConfig[0].auxConfig     = 0;
328         ibl.sgmiiConfig[1].adviseAbility = 0;
329         ibl.sgmiiConfig[1].control       = 0;
330         ibl.sgmiiConfig[1].txConfig      = 0;
331         ibl.sgmiiConfig[1].rxConfig      = 0;
332         ibl.sgmiiConfig[1].auxConfig     = 0;
336     /* MDIO configuration */
337     ibl.mdioConfig.nMdioOps = 0;
338     ibl.mdioConfig.mdioClkDiv = 0x20;
339     ibl.mdioConfig.interDelay = 2000;   /* ~2ms at 1000 MHz */
341     ibl.mdioConfig.mdio[0] =  (1 << 30) | (14 << 21) | (0 << 16) | 0xd5d0;
344     /* Nand boot is disabled */
345     ibl.nandConfig.nandPriority = ibl_DEVICE_NOBOOT;