1 /*
2 *
3 * Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/
4 *
5 *
6 * Redistribution and use in source and binary forms, with or without
7 * modification, are permitted provided that the following conditions
8 * are met:
9 *
10 * Redistributions of source code must retain the above copyright
11 * notice, this list of conditions and the following disclaimer.
12 *
13 * Redistributions in binary form must reproduce the above copyright
14 * notice, this list of conditions and the following disclaimer in the
15 * documentation and/or other materials provided with the
16 * distribution.
17 *
18 * Neither the name of Texas Instruments Incorporated nor the names of
19 * its contributors may be used to endorse or promote products derived
20 * from this software without specific prior written permission.
21 *
22 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
23 * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
24 * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
25 * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
26 * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
27 * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
28 * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
29 * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
30 * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
31 * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
32 * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
33 *
34 */
38 #ifndef _ROMPARSE_H
39 #define _ROMPARSE_H
40 /*************************************************************************************
41 * FILE PURPOSE: Define boot data structures
42 *************************************************************************************
43 * FILE NAME: romparse.h
44 *
45 * DESCRIPTION: Defines the structures used to create the boot parameter
46 * table
47 *
48 *************************************************************************************/
50 /* tiboot.h defines the boot parameters structure that will be created */
51 #if defined(c6472)
52 #include "tiboot_c6472.h"
53 #elif defined(c6474) || defined(c6474l)
54 #include "tiboot_c6474.h"
55 #elif defined(c6455)
56 #include "tiboot_c6455.h"
57 #elif defined(c6457)
58 #include "tiboot_c6457.h"
59 #elif defined(c66x)
60 #include "tiboot_c66x.h"
61 #else
62 #error invalid or missing device specification
63 #endif
65 /* Define the number of boot parameter tables that will be put on the rom */
66 #define NUM_BOOT_PARAM_TABLES 8
68 /* Define the size reserved for the PCI configuration table */
69 #define PCI_EEAI_PARAM_SIZE 0x20
71 /* Define a structure mapping the boot parameter table number to a program file
72 * to an eeprom byte address */
73 #define MAX_FNAME_LEN 132
74 #define MAX_DATA_LEN_32bit 32768
75 typedef struct {
76 char fname[MAX_FNAME_LEN];
77 int sizeBytes;
78 unsigned int addressBytes;
79 unsigned int data[MAX_DATA_LEN_32bit];
80 int tag[NUM_BOOT_PARAM_TABLES]; /* identifies boot parameter tables which use this file */
81 int align; /* alignment requirements for the file */
82 } progFile_t;
84 /* Define the PCI parameter structure */
85 #define PCI_DATA_LEN_32bit 8
86 typedef struct {
87 char fname[MAX_FNAME_LEN];
88 int sizeBytes;
89 int addressBytes;
90 unsigned int data[PCI_DATA_LEN_32bit];
91 } pciFile_t;
94 /* Distinguish between a layout and pad */
95 #define PLT_PAD 10
96 #define PLT_FILE 11
97 typedef struct {
98 int type;
99 int index;
100 } plt_t;
102 /* Define a layout table. A layout table is a block of data which contains the addresses
103 * of data files. Each address is 32 bits, with the upper 16 bits specifying the i2c
104 * id, the lower address the byte address of the 1st block in the table */
105 #define MAX_LAYOUTS 2
106 #define MAX_LAYOUT_FILES 8
107 typedef struct {
108 int nPlt; /* Number of elements in the plt array */
109 plt_t plt[MAX_LAYOUT_FILES]; /* Index of each file/pad in order */
111 unsigned int address; /* I2c data address of the table */
112 unsigned int dev_addr; /* I2c device address of the table */
113 int align;
114 } layout_t;
117 /* Pad section. The pad section creates a gap in the i2c memory map */
118 #define MAX_PADS 8
119 typedef struct {
120 int id;
121 unsigned int address; /* I2C data address */
122 unsigned int dev_addr; /* I2C device address */
123 unsigned int len;
124 } pad_t;
127 /* Layout/pad interleave. The rom specification must be in order, so this structure tracks
128 * the arrangement of layouts and pads */
129 typedef struct
130 {
131 int type; /* Either PAD or LAYOUT */
132 int index; /* The array index for the pad/layout */
134 } padLayoutOrder_t;
139 #endif /* ROMPARSE_H */