1 /*
2 *
3 * Copyright (C) 2010-2017 Texas Instruments Incorporated - http://www.ti.com/
4 *
5 *
6 * Redistribution and use in source and binary forms, with or without
7 * modification, are permitted provided that the following conditions
8 * are met:
9 *
10 * Redistributions of source code must retain the above copyright
11 * notice, this list of conditions and the following disclaimer.
12 *
13 * Redistributions in binary form must reproduce the above copyright
14 * notice, this list of conditions and the following disclaimer in the
15 * documentation and/or other materials provided with the
16 * distribution.
17 *
18 * Neither the name of Texas Instruments Incorporated nor the names of
19 * its contributors may be used to endorse or promote products derived
20 * from this software without specific prior written permission.
21 *
22 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
23 * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
24 * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
25 * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
26 * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
27 * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
28 * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
29 * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
30 * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
31 * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
32 * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
33 *
34 */
38 #ifndef _ROMPARSE_H
39 #define _ROMPARSE_H
40 /*************************************************************************************
41 * FILE PURPOSE: Define boot data structures
42 *************************************************************************************
43 * FILE NAME: romparse.h
44 *
45 * DESCRIPTION: Defines the structures used to create the boot parameter
46 * table
47 *
48 *************************************************************************************/
50 /* tiboot.h defines the boot parameters structure that will be created */
51 #if defined(c6472)
52 #include "tiboot_c6472.h"
53 #elif defined(c6474) || defined(c6474l)
54 #include "tiboot_c6474.h"
55 #elif defined(c6455)
56 #include "tiboot_c6455.h"
57 #elif defined(c6457)
58 #include "tiboot_c6457.h"
59 #elif defined(c66x)
60 #include "tiboot_c66x.h"
61 #elif defined(c665x)
62 #include "tiboot_c665x.h"
63 #elif defined(c66xk2x)
64 #include "tiboot_c66xk2x.h"
65 #else
66 #error invalid or missing device specification
67 #endif
69 /* Define the number of boot parameter tables that will be put on the rom */
70 #define NUM_BOOT_PARAM_TABLES 8
72 /* Define the size reserved for the PCI configuration table */
73 #define PCI_EEAI_PARAM_SIZE 0x20
75 /* Define a structure mapping the boot parameter table number to a program file
76 * to an eeprom byte address */
77 #define MAX_FNAME_LEN 132
78 #define MAX_DATA_LEN_32bit 0x200000
79 typedef struct {
80 char fname[MAX_FNAME_LEN];
81 int sizeBytes;
82 unsigned int addressBytes;
83 unsigned int data[MAX_DATA_LEN_32bit];
84 int tag[NUM_BOOT_PARAM_TABLES]; /* identifies boot parameter tables which use this file */
85 int align; /* alignment requirements for the file */
86 } progFile_t;
88 /* Define the PCI parameter structure */
89 #define PCI_DATA_LEN_32bit 8
90 typedef struct {
91 char fname[MAX_FNAME_LEN];
92 int sizeBytes;
93 int addressBytes;
94 unsigned int data[PCI_DATA_LEN_32bit];
95 } pciFile_t;
98 /* Distinguish between a layout and pad */
99 #define PLT_PAD 10
100 #define PLT_FILE 11
101 typedef struct {
102 int type;
103 int index;
104 } plt_t;
106 /* Define a layout table. A layout table is a block of data which contains the addresses
107 * of data files. Each address is 32 bits, with the upper 16 bits specifying the i2c
108 * id, the lower address the byte address of the 1st block in the table */
109 #define MAX_LAYOUTS 2
110 #define MAX_LAYOUT_FILES 8
111 typedef struct {
112 int nPlt; /* Number of elements in the plt array */
113 plt_t plt[MAX_LAYOUT_FILES]; /* Index of each file/pad in order */
115 unsigned int address; /* I2c data address of the table */
116 unsigned int dev_addr; /* I2c device address of the table */
117 int align;
118 } layout_t;
121 /* Pad section. The pad section creates a gap in the i2c memory map */
122 #define MAX_PADS 8
123 typedef struct {
124 int id;
125 unsigned int address; /* I2C data address */
126 unsigned int dev_addr; /* I2C device address */
127 unsigned int len;
128 } pad_t;
131 /* Layout/pad interleave. The rom specification must be in order, so this structure tracks
132 * the arrangement of layouts and pads */
133 typedef struct
134 {
135 int type; /* Either PAD or LAYOUT */
136 int index; /* The array index for the pad/layout */
138 } padLayoutOrder_t;
143 #endif /* ROMPARSE_H */