IBL Configuration
Data Fields
iblBootMap_s Struct Reference

The ibl boot map structure. More...

#include <ibl.h>

Data Fields

uint16 length
uint16 chkSum
uint32 addrLe
uint32 configLe
uint32 addrBe
uint32 configBe

Detailed Description

The ibl boot map structure.

The ibl boot device contains a structure which identifies the location of the big and little endian ibl images on the external device.


Field Documentation

uint32 addrBe

Base address of the boot tables for the big endian image

uint32 addrLe

Base address of the boot tables for the little endian image

uint16 chkSum

Value which makes the ones complement checksum over the block equal to 0 or -0

uint32 configBe

Base address of the ibl structure for use with the big endian image

uint32 configLe

Base address of the ibl structure for use with the little endian image

uint16 length

Size of the structure in bytes


The documentation for this struct was generated from the following file:
 All Data Structures Variables