IBL Configuration
|
This structure contains information used for tftp boot. More...
#include <ibl.h>
Data Fields | |
uint8 | ipAddr [4] |
uint8 | serverIp [4] |
uint8 | gatewayIp [4] |
uint8 | netmask [4] |
uint8 | hwAddress [6] |
char8 | fileName [64] |
This structure contains information used for tftp boot.
These fields are typically filled in by the bootp packet, but can be provided if bootp will not be used.
char8 fileName[64] |
The file name to load
uint8 gatewayIp[4] |
The IP address of the gateway
uint8 hwAddress[6] |
The hardware (mac) address of this device
uint8 ipAddr[4] |
The IP address of this device
uint8 netmask[4] |
The IP netmask
uint8 serverIp[4] |
The IP address of the tftp server