IBL Configuration
|
This structure is used to control the programming of the device PLL. More...
#include <ibl.h>
Data Fields | |
bool | doEnable |
Uint32 | prediv |
Uint32 | mult |
Uint32 | postdiv |
Uint32 | pllOutFreqMhz |
This structure is used to control the programming of the device PLL.
The system PLLs are optionally configured
bool doEnable |
If true the PLL is configured
Uint32 mult |
The pll multiplier
Uint32 pllOutFreqMhz |
The resulting output frequency, required for timer setup
Uint32 postdiv |
The pll post divider
Uint32 prediv |
The pll pre-divisor