IBL Configuration
Data Fields
iblSgmii_s Struct Reference

This structure is used to control the operation of the ibl sgmii ports. More...

#include <ibl.h>

Data Fields

bool configure
uint32 adviseAbility
uint32 control
uint32 txConfig
uint32 rxConfig
uint32 auxConfig

Detailed Description

This structure is used to control the operation of the ibl sgmii ports.

The physical register configuration is provided


Field Documentation

uint32 adviseAbility

The advise ability register

uint32 auxConfig

Serdes Aux config

bool configure

Set to false to disable configuration

uint32 control

The control register

uint32 rxConfig

Serdes Rx config

uint32 txConfig

Serdes Tx config


The documentation for this struct was generated from the following file:
 All Data Structures Variables