IBL Configuration
|
Provide status on the boot operation. More...
#include <ibl.h>
Data Fields | |
uint32 | iblMagic |
uint32 | iblVersion |
uint32 | iblFail |
uint32 | i2cRetries |
uint32 | i2cDataRetries |
uint32 | spiRetries |
uint32 | spiDataRetries |
uint32 | magicRetries |
uint32 | mapSizeFail |
uint32 | mapRetries |
int32 | heartBeat |
int32 | activeBoot |
int32 | activeDevice |
int32 | activeFileFormat |
uint32 | autoDetectFailCnt |
uint32 | nameDetectFailCnt |
uint32 | invalidDataFormatSpec |
uint32 | exitAddress |
iblEthBootInfo_t | ethParams |
Provide status on the boot operation.
Run time status of the IBL is provided to aid in debugging
int32 activeBoot |
Describes the active boot mode Defines the boot modes supported by the IBL
int32 activeDevice |
Describes the active boot peripheral device IblActiveDevice
int32 activeFileFormat |
Describes the format being decoded
uint32 autoDetectFailCnt |
Counts the number of times an auto detect of the data format failed
Last ethernet boot attemp parameters
uint32 exitAddress |
If non-zero the IBL exited and branched to this address
int32 heartBeat |
An increasing value as long as the boot code is running
uint32 i2cDataRetries |
Number of retries while reading block data from the i2c
uint32 i2cRetries |
Count of I2C read retries
uint32 iblFail |
If non-zero the IBL has encountered a fatal error
uint32 iblMagic |
The ibl_MAGIC_VALUE is placed here to indicate the boot has begun
uint32 iblVersion |
The version number. MSB = major, SMSB = minor, SLSB = minor minor LSB= tiny
uint32 invalidDataFormatSpec |
Counts the number of times the main boot found an invalid boot format request
uint32 magicRetries |
Count of I2C/SPI re-reads because the magic number was incorrect
uint32 mapRetries |
Number of times the checksum failed on the read of the i2c/spi map
uint32 mapSizeFail |
Number of times an invalid map table size was read from the i2c/spi
uint32 nameDetectFailCnt |
Counts the number of times an name detect of the data format failed
uint32 spiDataRetries |
Number of retries while reading block data from the spi
uint32 spiRetries |
Count of SPI read retries