#ifndef __TIBOOT_H__ #define __TIBOOT_H__ /****************************************************************************** * FILE PURPOSE: Define Structures, MACROs and etc for TI Shared ROM Boot ****************************************************************************** * FILE NAME: tiboot.h * * DESCRIPTION: Define structures, macros and etc for the TI Shared ROM boot * process. * * TABS: NONE * * $Id: $ * * REVISION HISTORY: * * $Log: $ * * (C) Copyright 2004 TELOGY Networks, Inc. ******************************************************************************/ #include "types.h" /******************************************************************************* * Utility Macro definitions ******************************************************************************/ #define HEX_DIGIT(digit) ((digit) + '0') #define BOOT_BIT_TO_MASK(bit) (1 << (bit)) /******************************************************************************* * Data Definition: Error Handling relatBOOT_ENTRY_POINT_ADDRed definition: ******************************************************************************* * Description: Define Handling related macros, constants * ******************************************************************************/ /* Define Module IDs */ #define BOOT_MODULE_ID_MAIN 0 #define BOOT_MODULE_ID_BTBL 1 #define BOOT_MODULE_ID_BETH 2 #define BOOT_MODULE_ID_I2C 3 #define BOOT_MODULE_ID_CHIP 4 #define BOOT_MODULE_ID_HW 5 /* Boot error codes */ enum { BOOT_NOERR = 0, BOOT_ERROR = 1, /* General error */ BOOT_INVALID_BOOT_MODE = 2, BOOT_INVALID_I2C_DEV_ADDR = 3, BOOT_INVALID_CHECKSUM = 4, /* Invalid checksum of the boot parameters */ BOOT_INVALID_PARAMS_SIZE = 5, /* the size of boot parameters is too big */ BOOT_RX_ETH_QUEUE_FULL = 6, /* ethmain.c, hw_rxPacket */ BOOT_CACHE_INIT_FAIL = 7, /* rmain.c, cache init failed */ BOOT_CACHE_DISABLE_FAIL = 8, /* rmain.c, cache disable failed */ BOOT_INVALID_CPPI_SIZE = 9, /* ethmain.c, invalid compile sizes */ BOOT_INVALID_CORE_ID = 10, /* Invalid core ID in cold boot */ BOOT_INVALID_MAC_ADDR = 11, /* Invalid MAC address (all 0's) */ BOOT_ETH_TX_SCRATCH = 12, /* tx scratch size invalid */ BOOT_ETH_TX_PACKET = 13, /* tx packet formation failure */ BOOT_ETH_MAC_INIT = 14 /* ethmain.c - mac init failed */ }; /* Error tracking prototypes (functions in rmain.c)*/ void bootException (UINT16 errorCode); void bootError (UINT16 errorCode); /* Error code = (module ID * 100) + module specific error */ #define BOOT_ERROR_CODE(id, code) ((UINT16)((id<<8) + code)) #define BOOT_EXCEPTION(error_code) bootException(error_code) #define BOOT_ERROR(error_code) bootError(error_code) /******************************************************************************* * Begin Boot Parameter definitions ******************************************************************************/ /******************************************************************************* * Boot Parameter Common ******************************************************************************/ typedef struct boot_params_common_s{ UINT16 length; /* size of the entire boot parameters in bytes */ UINT16 checksum; /* non-zero: 1's complement checksum of the boot * parameters * zero: checksum is not applicable */ UINT16 boot_mode; /* * Specify the boot mode * bit 02-00: Standard Boot Mode * bit 15-03: Extended Boot Mode */ } BOOT_PARAMS_COMMON_T; typedef struct boot_params_ethernet_s{ /* common portion of the Boot parameters */ UINT16 length; UINT16 checksum; UINT16 boot_mode; /* Etherent specific portion of the Boot Parameters */ UINT16 options; /* * Ethernet Specific Options * Bit 0: GE: * 0 - 10/100 Mb * 1 - 1 Gb * Bit 2: HD: * 0 - Full Duplex * 1 - Half Duplex * Bit 3: SKIP TX * 0 - Send the Ethernet Ready Frame * 1 - Skip sending the Ethernet Ready Frame * Bit 4: SKIP INIT * 0 - Initialize the Ethernet MAC peripheral * 1 - Skip initializing the Ethernet MAC peripheral * Bit 5: FC * 0 - Disable Flow Control * 1 - Enable Flow Control * Other bits: Reserved */ #define BOOT_PARAMS_ETH_OPTIONS_GE 0x0001 #define BOOT_PARAMS_ETH_OPTIONS_HD 0x0004 #define BOOT_PARAMS_ETH_OPTIONS_SKIP_TX 0x0008 #define BOOT_PARAMS_ETH_OPTIONS_SKIP_INIT 0x0010 #define BOOT_PARAMS_ETH_OPTIONS_FC 0x0020 /* * he device MAC address to be used for Boot: * All zero mac address indicates that the device E-fuse address should * be used. */ UINT16 mac_addr_h; UINT16 mac_addr_m; UINT16 mac_addr_l; /* * The multicast or broadcast MAC address which should be accepted as * a destination MAC address for boot table frames */ UINT16 mmac_addr_h; UINT16 mmac_addr_m; UINT16 mmac_addr_l; UINT16 src_port; /* Source UDP port number to be used during boot process */ /* 0: allow any SRC UDP port */ UINT16 dest_port; /* Destination UDP port number to be used during boot process */ /* The Device ID to be included in the boot ready announcement frame */ UINT16 device_id_12; UINT16 device_id_34; #define BOOT_PARAMS_DEVICE_ID_HIGH_MASK 0xFF00 #define BOOT_PARAMS_DEVICE_ID_HIGH_SHIFT 8 #define BOOT_PARAMS_DEVICE_ID_LOW_MASK 0x00FF #define BOOT_PARAMS_DEVICE_ID_LOW_SHIFT 0 #define BOOT_PARAMS_GET_DEVICE_ID_13(device_id) \ (((device_id) & BOOT_PARAMS_DEVICE_ID_HIGH_MASK) > BOOT_PARAMS_DEVICE_ID_HIGH_SHIFT) #define BOOT_PARAMS_GET_DEVICE_ID_24(device_id) \ (((device_id) & BOOT_PARAMS_DEVICE_ID_LOW_MASK) > BOOT_PARAMS_DEVICE_ID_LOW_SHIFT) /* * The destination MAC address used for the boot ready announce frame */ UINT16 hmac_addr_h; UINT16 hmac_addr_m; UINT16 hmac_addr_l; } BOOT_PARAMS_ETHERNET_T; typedef struct boot_params_i2c_s{ /* common portion of the Boot parameters */ UINT16 length; UINT16 checksum; UINT16 boot_mode; /* I2C specific portion of the Boot Parameters */ UINT16 options; /* * I2C Specific Options * Bit 01-00: BT: * 00 - Boot Parameter Mode * 01 - Boot Table Mode * 10 - Boot Config mode * 11 - Slave receive boot config * Bit 04-02: EETYPE: EEPROM type * Other bits: Reserved */ #define BOOT_PARAMS_I2C_OPTIONS_BP 0x0000 #define BOOT_PARAMS_I2C_OPTIONS_BT 0x0001 #define BOOT_PARAMS_I2C_OPTIONS_BC 0x0002 #define BOOT_PARAMS_I2C_OPTIONS_SLVOPT 0x0003 #define BOOT_PARAMS_I2C_OPTIONS_MASK 0x0003 #define BOOT_PARAMS_I2C_OPTIONS_SHIFT 0 #define BOOT_PARAMS_I2C_OPTIONS_EETYPE_MASK 0x001C #define BOOT_PARAMS_I2C_OPTIONS_EETYPE_SHIFT 2 #define BOOT_PARAMS_I2C_IS_BOOTTBL_MODE(options) \ (((options) & BOOT_PARAMS_I2C_OPTIONS_MASK) == BOOT_PARAMS_I2C_OPTIONS_BT) #define BOOT_PARAMS_I2C_IS_BOOTCONFIG_MODE(options) \ (((options) & BOOT_PARAMS_I2C_OPTIONS_MASK) == BOOT_PARAMS_I2C_OPTIONS_BC) #define BOOT_PARAMS_I2C_IS_SLAVE_RCV_OPTIONS_MODE(options) \ (((options) & BOOT_PARAMS_I2C_OPTIONS_MASK) == BOOT_PARAMS_I2C_OPTIONS_SLVOPT) #define BOOT_PARAMS_I2C_SET_BOOTTBL_MODE(options, mode) \ (options) = ((options) & ~BOOT_PARAMS_I2C_OPTIONS_MASK) | \ (((mode) & BOOT_PARAMS_I2C_OPTIONS_MASK) << \ BOOT_PARAMS_I2C_OPTIONS_SHIFT) #define BOOT_PARAMS_I2C_GET_EETYPE(options) \ (((options) & BOOT_PARAMS_I2C_OPTIONS_EETYPE_MASK) >> BOOT_PARAMS_I2C_OPTIONS_EETYPE_SHIFT) #define BOOT_PARAMS_I2C_SET_EETYPE(options, ee_type) \ (options) = (((options) & ~BOOT_PARAMS_I2C_OPTIONS_EETYPE_MASK) | \ (((ee_type) << BOOT_PARAMS_I2C_OPTIONS_EETYPE_SHIFT) & BOOT_PARAMS_I2C_OPTIONS_EETYPE_MASK)) /* The device address to be used for Boot */ UINT16 dev_addr; /* 16-bit device address (low) */ UINT16 dev_addr_ext; /* 16-bit extended device address (high) * set to zero if not used * Note: some I2C device requires 32-bit * address */ UINT16 multi_i2c_id; /* Multi device master write boot ID */ UINT16 my_i2c_id; /* This parts I2C address */ UINT16 core_freq_mhz; /* Core frequency, MHz */ UINT16 i2c_clk_freq_khz; /* Desired I2C clock frequency, kHz */ UINT16 next_dev_addr; /* Used only for the boot config mode. */ UINT16 next_dev_addr_ext; /* Copied into dev_addr* after config complete */ UINT16 address_delay; /* Rough number of cycles delay between address write * and read to the i2c eeprom */ } BOOT_PARAMS_I2C_T; /* * UNION of boot parameter structures in all modes * Note: We need to make sure that the structures genertaed by the C-compiler * match with the boot parameter table data format i.e. a set of 16-bit * data array. */ #define BOOT_PARAMS_SIZE_IN_BYTES 256 typedef union { BOOT_PARAMS_COMMON_T common; BOOT_PARAMS_ETHERNET_T eth; BOOT_PARAMS_I2C_T i2c; UINT16 parameter[BOOT_PARAMS_SIZE_IN_BYTES/2]; } BOOT_PARAMS_T; /******************************************************************************* * Definition: The time stamp and version number are placed into the stats. * This will be two characters packed per 16bits . The length * value must be 32 bit divisible *******************************************************************************/ #define BOOT_VERSION_LEN_UINT16 32 typedef struct BOOT_VERSION_S { UINT16 vstring[BOOT_VERSION_LEN_UINT16]; } BOOT_VERSION_T; extern BOOT_VERSION_T bootVersion; /******************************************************************************* * Definition: Runs time stats that are not initialized on cold boot entry * !!!!!! boot.s assumes that the nonInit stats are at the top of the structure * !!!!!! and that stage is the first element *******************************************************************************/ typedef struct BOOT_STATS_NONINIT_S { UINT16 stage; /* Record the SharedROM code execution stage */ #define BOOT_STAGE_ASM_START_UP 1 #define BOOT_STAGE_INIT_CACHE 2 #define BOOT_STAGE_CHCHE_INITED 3 #define BOOT_STAGE_ENTER_WARMBOOT 4 #define BOOT_STAGE_INIT_CPGMAC 5 #define BOOT_STAGE_SEND_ERA_FRAME 6 #define BOOT_STAGE_ETH_MAIN_LOOP 7 #define BOOT_STAGE_I2C_BOOTTBL_LOOP 8 #define BOOT_STAGE_I2C_BOOTPARAM_LOOP 9 #define BOOT_STAGE_DISABLE_CACHE 10 #define BOOT_STAGE_CHCHE_DISABLED 11 #define BOOT_STAGE_EXIT 12 #define BOOT_STAGE_ERROR_LOOP 13 #define BOOT_STAGE_I2C_BOOTCONFIG_LOOP 14 #define BOOT_STAGE_I2C_SLV_RCV_OPTIONS_LOOP 15 UINT16 coldBootEntries; } BOOT_STATS_NONINIT_T; /******************************************************************************* * Definition: Run time statistics and error counts. These stats are * initialized on cold boot entry. ******************************************************************************/ typedef struct BOOT_STATS_MAIN_S { UINT16 errorCode; /* (module ID <<8 ) + module specific error */ /* I2C operation related statistics */ UINT16 numI2Cpkts; /* number of I2C boot table packets processed */ UINT16 numI2CchksumError;/* number of I2C checksum errors */ UINT16 numI2CotherError; /* number of I2C section with invalid length and etc */ UINT16 numI2Cretrys; /* number of I2C retrys due to read access errors */ UINT16 numI2cWrites; /* number of I2C master writes to passive devices */ UINT16 numI2cWriteError; /* number of I2C master write errors */ UINT16 warmBootEntry; /* Count of entries into warm boot routine */ } BOOT_STATS_MAIN_T; /***************************************************************************** * Definition: I2C stats, Boot table and Ethernrt stats initialized * on cold boot entry *****************************************************************************/ typedef struct I2C_STATS_tag { UINT16 num_trans; UINT16 num_trys; UINT16 num_try_ok; UINT16 num_try_lost_arb; UINT16 num_try_idle_to; UINT16 num_try_no_ack; UINT16 num_try_other_err; UINT32 extra_idle_waits; UINT32 extra_clock_waits; UINT32 tx_bytes; UINT32 rx_bytes; UINT32 data_re_reads; } I2C_STATS_T; typedef struct BTBL_STATS_tag { UINT16 num_sections; /* number of boot table sections received */ UINT16 num_pdma_copies; /* number of PDMA copies performed */ } BTBL_STATS_T; typedef struct ETH_STATS_tag { /* MAC packets related statistics */ UINT16 uniMacPkts; /* Count of packets received with valid unicast mac address */ UINT16 multiMacPkts; /* Count of packets received with valid multicast or broadcast mac address */ UINT16 invalidMacPkts; /* Count of packets received with invalid mac address */ UINT16 invalidLLCPkts; /* Count of 802.3 packets with wrong LLC/SNAP header */ UINT16 nonIpPkts; /* Count of non-IP packets received with valid MAC address */ /* IP packets related statistics */ UINT16 nonIP4Pkts; /* Count of non-IP4 packets */ UINT16 ipfragments; /* Count of IP fragments received */ UINT16 ipTruncatedError; /* Count of truncated IP frame */ UINT16 nonUDPPkts; /* Count of IP packets with non-UDP paylaod */ /* UDP packets related statistics */ UINT16 udpSizeError; /* Count of UDP packet with invalid (odd) size */ UINT16 udpPortError; /* Count of UDP packets with invalid port number */ UINT16 udpChksumError; /* Count of UDP packets with checksum error */ /* Boot table packets related statistics */ UINT16 nonBtblPkts; /* Count of UDP packets with invalid boot table paylaod */ UINT16 outSeqPkts; /* Count of out of sequence boot table packets received i.e. packets with unexpected seq_num */ UINT16 expSeqNum; /* Expected Sequence Number */ UINT16 lastSeqNum; /* Last sequence number received */ /* Driver errors */ UINT16 sizeZeroPackets; /* Count of packets arriving with 0 size */ } ETH_STATS_T; typedef struct PCI_EEAI_STATS_tag { UINT16 pciI2cReads; /* Count of block reads of i2c eeprom */ UINT16 pciI2cRetries; /* Count of i2c read retries */ UINT16 pciChkSumErr; /* Count of block check sum errors */ UINT16 pciEeaiFail; /* Count of aborted pci attempts */ } PCI_EEAI_STATS_T; /* Rapid I/O stats */ typedef struct RAPIDIO_STATS_tag { UINT16 rapidIoFailReady; /* If set rapid I/O peripheral failed to report ready */ } RAPIDIO_STATS_T; /******************************************************************************* * Definition: The statistics * * !!!!!! boot.s assumes that the nonInit stats are at the top of the structure! *******************************************************************************/ typedef struct BOOT_STATS_S { BOOT_STATS_NONINIT_T nonInit; BOOT_STATS_MAIN_T main; ETH_STATS_T eth; I2C_STATS_T i2c; BTBL_STATS_T btbl; PCI_EEAI_STATS_T pci_eeai; RAPIDIO_STATS_T rapidIo; } BOOT_STATS_T; extern BOOT_STATS_T bootStats; /******************************************************************************* * Definition: The magic start address, known to all modules *******************************************************************************/ extern volatile UINT32 *p_boot_entry_addr; #endif /* __TIBOOT_H__ */ /* nothing past this point */