/************************************************************************************ * FILE PURPOSE: C6474 Device Specific functions ************************************************************************************ * FILE NAME: c6474.c * * DESCRIPTION: Implements the device specific functions for the IBL * * @file c6474.c * * @brief * This file implements the device specific functions for the IBL * ************************************************************************************/ #include "ibl.h" #include "device.h" #include "pllapi.h" #include "emif31api.h" #include "pscapi.h" #include "gpio.h" #include extern cregister unsigned int DNUM; /** * @brief The default boot configuration table is filled in * * @details * A default ibl configuraiton table is provided when one is not found * preloaded. */ void deviceLoadDefaultIblTable (void) { uint32 macA, macB; #if 0 /* This is really the default. Switching to a direct tftp boot until I have a bootp server * on a private lan for test */ ibl.ethConfig[0].ethPriority = ibl_LOWEST_PRIORITY; ibl.ethConfig[0].port = 0; ibl.ethConfig[0].doBootp = TRUE; ibl.ethConfig[0].bootFormat = ibl_BOOT_FORMAT_AUTO; memset (&ibl.ethConfig[0].ethInfo, 0, sizeof(ibl.ethConfig[0].ethInfo)); #endif /* This is the temporary code */ ibl.ethConfig[0].ethPriority = ibl_LOWEST_PRIORITY; ibl.ethConfig[0].port = 0; ibl.ethConfig[0].doBootp = FALSE; ibl.ethConfig[0].useBootpServerIp = FALSE; ibl.ethConfig[0].useBootpFileName = FALSE; ibl.ethConfig[0].bootFormat = ibl_BOOT_FORMAT_NAME; memset (&ibl.ethConfig[0].ethInfo, 0, sizeof(ibl.ethConfig[0].ethInfo)); ibl.ethConfig[0].ethInfo.ipAddr[0] = 10; ibl.ethConfig[0].ethInfo.ipAddr[1] = 218; ibl.ethConfig[0].ethInfo.ipAddr[2] = 109; ibl.ethConfig[0].ethInfo.ipAddr[3] = 21; ibl.ethConfig[0].ethInfo.serverIp[0] = 10; ibl.ethConfig[0].ethInfo.serverIp[1] = 218; ibl.ethConfig[0].ethInfo.serverIp[2] = 109; ibl.ethConfig[0].ethInfo.serverIp[3] = 196; ibl.ethConfig[0].ethInfo.gatewayIp[0] = 10; ibl.ethConfig[0].ethInfo.gatewayIp[1] = 218; ibl.ethConfig[0].ethInfo.gatewayIp[2] = 109; ibl.ethConfig[0].ethInfo.gatewayIp[3] = 1; /* Leave hw address as 0 */ strcpy (ibl.ethConfig[0].ethInfo.fileName, "test2_little.out"); ibl.ethConfig[0].blob.startAddress = 0x00200000; /* Base address of SL2 */ ibl.ethConfig[0].blob.sizeBytes = 0x000c0000; /* All of SL2 */ ibl.ethConfig[0].blob.branchAddress = 0x00200000; /* Base of SL2 */ macA = *((uint32 *)0x2a80700); macB = *((uint32 *)0x2a80704); ibl.ethConfig[0].ethInfo.hwAddress[0] = (macA >> 24) & 0xff; ibl.ethConfig[0].ethInfo.hwAddress[1] = (macA >> 16) & 0xff; ibl.ethConfig[0].ethInfo.hwAddress[2] = (macA >> 8) & 0xff; ibl.ethConfig[0].ethInfo.hwAddress[3] = (macA >> 0) & 0xff; ibl.ethConfig[0].ethInfo.hwAddress[4] = (macB >> 24) & 0xff; ibl.ethConfig[0].ethInfo.hwAddress[5] = (macB >> 16) & 0xff; ibl.ethConfig[1].ethPriority = ibl_DEVICE_NOBOOT; /* MDIO configuration */ ibl.mdioConfig.nMdioOps = 8; ibl.mdioConfig.mdioClkDiv = 0x20; ibl.mdioConfig.interDelay = 1400; /* ~2ms at 700 MHz */ ibl.mdioConfig.mdio[0] = (1 << 30) | (27 << 21) | (24 << 16) | 0x848b; ibl.mdioConfig.mdio[1] = (1 << 30) | (20 << 21) | (24 << 16) | 0x0ce0; ibl.mdioConfig.mdio[2] = (1 << 30) | (24 << 21) | (24 << 16) | 0x4101; ibl.mdioConfig.mdio[3] = (1 << 30) | ( 0 << 21) | (24 << 16) | 0x9140; ibl.mdioConfig.mdio[4] = (1 << 30) | (27 << 21) | (25 << 16) | 0x848b; ibl.mdioConfig.mdio[5] = (1 << 30) | (20 << 21) | (25 << 16) | 0x0ce0; ibl.mdioConfig.mdio[6] = (1 << 30) | (24 << 21) | (25 << 16) | 0x4101; ibl.mdioConfig.mdio[7] = (1 << 30) | ( 0 << 21) | (25 << 16) | 0x9140; /* Main Pll configuration */ ibl.pllConfig[ibl_MAIN_PLL].doEnable = TRUE; ibl.pllConfig[ibl_MAIN_PLL].prediv = 1; ibl.pllConfig[ibl_MAIN_PLL].mult = 28; ibl.pllConfig[ibl_MAIN_PLL].postdiv = 1; ibl.pllConfig[ibl_MAIN_PLL].pllOutFreqMhz = 500; /* The DDR PLL. The multipliers/dividers are fixed, so are really dont cares */ ibl.pllConfig[ibl_DDR_PLL].doEnable = TRUE; /* The network PLL. The multipliers/dividers are fixed */ ibl.pllConfig[ibl_NET_PLL].doEnable = TRUE; /* EMIF configuration */ ibl.ddrConfig.uEmif.emif3p1.sdcfg = 0x00538832; /* timing, 32bit wide */ ibl.ddrConfig.uEmif.emif3p1.sdrfc = 0x0000073B; /* Refresh 533Mhz */ ibl.ddrConfig.uEmif.emif3p1.sdtim1 = 0x47245BD2; /* Timing 1 */ ibl.ddrConfig.uEmif.emif3p1.sdtim2 = 0x0125DC44; /* Timing 2 */ ibl.ddrConfig.uEmif.emif3p1.dmcctl = 0x50001906; /* PHY read latency for CAS 5 is 5 + 2 - 1 */ /* NAND configuration for the MT29F1G08 flash */ ibl.nandConfig.nandPriority = ibl_HIGHEST_PRIORITY; ibl.nandConfig.bootFormat = ibl_BOOT_FORMAT_COFF; ibl.nandConfig.nandInfo.busWidthBits = 8; ibl.nandConfig.nandInfo.pageSizeBytes = 2048; ibl.nandConfig.nandInfo.pageEccBytes = 64; ibl.nandConfig.nandInfo.pagesPerBlock = 64; ibl.nandConfig.nandInfo.totalBlocks = 1024; ibl.nandConfig.nandInfo.addressBytes = 4; ibl.nandConfig.nandInfo.lsbFirst = TRUE; ibl.nandConfig.nandInfo.blockOffset = 22; ibl.nandConfig.nandInfo.pageOffset = 16; ibl.nandConfig.nandInfo.columnOffset = 0; ibl.nandConfig.nandInfo.resetCommand = 0xff; ibl.nandConfig.nandInfo.readCommandPre = 0; ibl.nandConfig.nandInfo.readCommandPost = 0x30; ibl.nandConfig.nandInfo.postCommand = TRUE; } /** * @brief Determine if an address is local * * @details * Examines an input address to determine if it is a local address */ bool address_is_local (Uint32 addr) { /* L2 */ if ((addr >= 0x00800000) && (addr < 0x00898000)) return (TRUE); /* L1P */ if ((addr >= 0x00e00000) && (addr < 0x00e08000)) return (TRUE); /* L2D */ if ((addr >= 0x00f00000) && (addr < 0x00f08000)) return (TRUE); return (FALSE); } /** * @brief Convert a local l1d, l1p or l2 address to a global address * * @details * The global address is formed. If the address is not local then * the input address is returned */ Uint32 deviceLocalAddrToGlobal (Uint32 addr) { if (address_is_local (addr)) addr = (1 << 28) | (DNUM << 24) | addr; return (addr); } /** * @brief Configure the PLLs * * @details * Only the main PLL can be configured here. The DDR pll is enabled by default, * and the network PLL is enabled through serdes configuration. * the multiplier and dividers. */ void devicePllConfig (void) { if (ibl.pllConfig[ibl_MAIN_PLL].doEnable == TRUE) hwPllSetPll (MAIN_PLL, ibl.pllConfig[ibl_MAIN_PLL].prediv, ibl.pllConfig[ibl_MAIN_PLL].mult, ibl.pllConfig[ibl_MAIN_PLL].postdiv); } /** * @brief * Enable the DDR * * @details * The DDR controller on the c6474 is an emif 3.1. The controller is * initialized directly with the supplied values */ void deviceDdrConfig (void) { if (ibl.ddrConfig.configDdr != 0) hwEmif3p1Enable (&ibl.ddrConfig.uEmif.emif3p1); } /** * @brief Power up a peripheral * * @details * Boot peripherals are powered up */ int32 devicePowerPeriph (int32 modNum) { /* If the input value is < 0 there is nothing to power up */ if (modNum < 0) return (0); if (modNum >= TARGET_PWR_MAX_MOD) return (-1); return ((int32)pscEnableModule(modNum)); } /** * @brief Enable the pass through version of the nand controller * * @details On the evm the nand controller is enabled by setting * gpio 14 high */ int32 deviceConfigureForNand(void) { hwGpioSetDirection(NAND_MODE_GPIO, GPIO_OUT); hwGpioSetOutput(NAND_MODE_GPIO); return (0); } /** * @brief * The e-fuse mac address is loaded */ void deviceLoadDefaultEthAddress (uint8 *maddr) { uint32 macA, macB; /* Read the e-fuse mac address */ macA = *((uint32 *)0x2880834); macB = *((uint32 *)0x2880838); maddr[0] = (macB >> 8) & 0xff; maddr[1] = (macB >> 0) & 0xff; maddr[2] = (macA >> 24) & 0xff; maddr[3] = (macA >> 16) & 0xff; maddr[4] = (macA >> 8) & 0xff; maddr[5] = (macA >> 0) & 0xff; }