/************************************************************************************ * FILE PURPOSE: C6474 Device Specific functions ************************************************************************************ * FILE NAME: c6474.c * * DESCRIPTION: Implements the device specific functions for the IBL * * @file c6474.c * * @brief * This file implements the device specific functions for the IBL * ************************************************************************************/ #include "ibl.h" #include "device.h" #include "pllapi.h" #include "emif31api.h" #include "pscapi.h" #include "gpio.h" #include extern cregister unsigned int DNUM; /** * @brief Determine if an address is local * * @details * Examines an input address to determine if it is a local address */ bool address_is_local (Uint32 addr) { /* L2 */ if ((addr >= 0x00800000) && (addr < 0x00898000)) return (TRUE); /* L1P */ if ((addr >= 0x00e00000) && (addr < 0x00e08000)) return (TRUE); /* L2D */ if ((addr >= 0x00f00000) && (addr < 0x00f08000)) return (TRUE); return (FALSE); } /** * @brief Convert a local l1d, l1p or l2 address to a global address * * @details * The global address is formed. If the address is not local then * the input address is returned */ Uint32 deviceLocalAddrToGlobal (Uint32 addr) { if (address_is_local (addr)) addr = (1 << 28) | (DNUM << 24) | addr; return (addr); } /** * @brief Configure the PLLs * * @details * Only the main PLL can be configured here. The DDR pll is enabled by default, * and the network PLL is enabled through serdes configuration. * the multiplier and dividers. */ void devicePllConfig (void) { if (ibl.pllConfig[ibl_MAIN_PLL].doEnable == TRUE) hwPllSetPll (MAIN_PLL, ibl.pllConfig[ibl_MAIN_PLL].prediv, ibl.pllConfig[ibl_MAIN_PLL].mult, ibl.pllConfig[ibl_MAIN_PLL].postdiv); } /** * @brief * Enable the DDR * * @details * The DDR controller on the c6474 is an emif 3.1. The controller is * initialized directly with the supplied values */ void deviceDdrConfig (void) { if (ibl.ddrConfig.configDdr != 0) hwEmif3p1Enable (&ibl.ddrConfig.uEmif.emif3p1); } /** * @brief Power up a peripheral * * @details * Boot peripherals are powered up */ int32 devicePowerPeriph (int32 modNum) { /* If the input value is < 0 there is nothing to power up */ if (modNum < 0) return (0); if (modNum >= TARGET_PWR_MAX_MOD) return (-1); return ((int32)pscEnableModule(modNum)); } /** * @brief Enable the pass through version of the nand controller * * @details On the evm the nand controller is enabled by setting * gpio 14 high */ #if 0 int32 deviceConfigureForNand(void) { hwGpioSetDirection(NAND_MODE_GPIO, GPIO_OUT); hwGpioSetOutput(NAND_MODE_GPIO); return (0); } #endif /** * @brief * The e-fuse mac address is loaded */ void deviceLoadDefaultEthAddress (uint8 *maddr) { uint32 macA, macB; /* Read the e-fuse mac address */ macA = *((uint32 *)0x2880834); macB = *((uint32 *)0x2880838); maddr[0] = (macB >> 8) & 0xff; maddr[1] = (macB >> 0) & 0xff; maddr[2] = (macA >> 24) & 0xff; maddr[3] = (macA >> 16) & 0xff; maddr[4] = (macA >> 8) & 0xff; maddr[5] = (macA >> 0) & 0xff; }