/* * * Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ /************************************************************************************ * FILE PURPOSE: C6474 Device Specific functions ************************************************************************************ * FILE NAME: c6474.c * * DESCRIPTION: Implements the device specific functions for the IBL * * @file c6474.c * * @brief * This file implements the device specific functions for the IBL * ************************************************************************************/ #include "ibl.h" #include "device.h" #include "pllapi.h" #include "emif31api.h" #include "pscapi.h" #include "gpio.h" #include "nandhwapi.h" #include extern cregister unsigned int DNUM; /** * @brief Determine if an address is local * * @details * Examines an input address to determine if it is a local address */ bool address_is_local (Uint32 addr) { /* L2 */ if ((addr >= 0x00800000) && (addr < 0x00898000)) return (TRUE); /* L1P */ if ((addr >= 0x00e00000) && (addr < 0x00e08000)) return (TRUE); /* L2D */ if ((addr >= 0x00f00000) && (addr < 0x00f08000)) return (TRUE); return (FALSE); } /** * @brief Convert a local l1d, l1p or l2 address to a global address * * @details * The global address is formed. If the address is not local then * the input address is returned */ Uint32 deviceLocalAddrToGlobal (Uint32 addr) { if (address_is_local (addr)) addr = (1 << 28) | (DNUM << 24) | addr; return (addr); } /** * @brief * Enable the DDR * * @details * The DDR controller on the c6474 is an emif 3.1. The controller is * initialized directly with the supplied values */ void deviceDdrConfig (void) { if (ibl.ddrConfig.configDdr != 0) hwEmif3p1Enable (&ibl.ddrConfig.uEmif.emif3p1); } /** * @brief Power up a peripheral * * @details * Boot peripherals are powered up */ int32 devicePowerPeriph (int32 modNum) { /* If the input value is < 0 there is nothing to power up */ if (modNum < 0) return (0); if (modNum >= TARGET_PWR_MAX_MOD) return (-1); return ((int32)pscEnableModule(modNum)); } unsigned int get_device_switch_setting() { volatile unsigned int w; unsigned int v; w = *((uint32 *)0x02880804); v = w & 0x40; v = v >> 6; return(v); } /** * @brief Enable the pass through version of the nand controller * * @details On the evm the nand controller is enabled by setting * gpio 14 high */ #ifndef EXCLUDE_NAND_GPIO int32 deviceConfigureForNand(void) { hwGpioSetDirection(NAND_MODE_GPIO, GPIO_OUT); hwGpioSetOutput(NAND_MODE_GPIO); return (0); } #endif /** * @brief * The e-fuse mac address is loaded */ void deviceLoadDefaultEthAddress (uint8 *maddr) { uint32 macA, macB; /* Read the e-fuse mac address */ macA = *((uint32 *)0x2880834); macB = *((uint32 *)0x2880838); maddr[0] = (macB >> 8) & 0xff; maddr[1] = (macB >> 0) & 0xff; maddr[2] = (macA >> 24) & 0xff; maddr[3] = (macA >> 16) & 0xff; maddr[4] = (macA >> 8) & 0xff; maddr[5] = (macA >> 0) & 0xff; } /** * @brief Return the NAND interface call table. Only GPIO is supported on c6474 */ #ifndef EXCLUDE_NAND_GPIO nandCtbl_t nandCtbl = { nandHwGpioDriverInit, nandHwGpioDriverReadBytes, nandHwGpioDriverReadPage, nandHwGpioDriverClose }; nandCtbl_t *deviceGetNandCtbl (int32 interface) { return (&nandCtbl); } #endif