/* * * Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ /************************************************************************** * FILE PURPOSE: Target specific definitions ************************************************************************** * FILE NAME: target.h * * DESCRIPTION: This file defines target specific values used by low level * drivers. * * @file target.h * * @brief * Low level target specific values are defined * ***************************************************************************/ #ifndef _TARGET_H #define _TARGET_H #include "types.h" /** * @brief * Device EMAC definitions */ /** * @brief * Device Timer definitions */ #define TIMER0_BASE 0x02200000u #define TIMER_INPUT_DIVIDER 6 /* Timer driven from cpu clock / 6 */ /** * @def MAIN_PLL */ #define MAIN_PLL 0 /**< The index to the main PLL */ /** * @def NET_PLL */ #define NET_PLL 1 /**< The index to the network PLL */ /** * @def DDR_PLL */ #define DDR_PLL 2 /**< The index to the DDR PLL */ /** * @brief * Device PLL definitions */ #define DEVICE_PLL_BASE(x) ((x) == MAIN_PLL ? 0x2310000 : ((x) == NET_PLL ? 0x2620338 : 0x2620330)) #define DEVICE_MAIN_PLL_CTL_0 0x2620328 #define DEVICE_MAIN_PLL_CTL_1 0x262032c /** * @brief * The c661x devices use a register external to the PLL controller for prediv configuration */ #define chipPllExternalPrediv(x) TRUE /** * @brief * Device PSC definitions */ #define DEVICE_PSC_BASE 0x02350000u /** * @brief * The SPI module base and module divider */ #define DEVICE_SPI_BASE(x) 0x20bf0000u #define DEVICE_SPI_MOD_DIVIDER 6 #define DEVICE_SPI_MAX_DIVIDER 0xff /** * @brief * The PSC number for the PA sub-system */ #define TARGET_PWR_PA 7 /** * @brief * The PSC number for the SGMII */ #define TARGET_PWR_ETH(x) 8 /** * @brief * The PSC numbers for EMIF16 and SPI vary between devices. The devices are run time * identified by reading the JTAG ID register */ #define DEVICE_C6616_JTAG_ID_VAL 0x9d02f #define DEVICE_C6618_JTAG_ID_VAL 0x9e02f #define DEVICE_JTAG_ID_REG 0x2620018 /** * @brief * The PSC number for NAND depends on the device */ #define TARGET_PWR_NAND deviceNandPscNum() #define TARGET_PWR_NAND_C6618 3 /* * @brief * The PSC number for SPI depends on the device */ #define TARGET_PWR_SPI deviceSpiPscNum() /** * @brief * Flag to indicate timer 0 power up requested. The time is always on in the 6472 */ #define TARGET_PWR_TIMER_0 -1 /** * @brief * Device DDR controller definitions */ #define DEVICE_EMIF4_BASE 0x21000000 #define targetEmifType() ibl_EMIF_TYPE_40 /** * @brief * Device EMIF 2.5 controller definitions */ #define DEVICE_EMIF25_BASE 0x20c00000 /** * @brief * NAND memory regions */ #define TARGET_MEM_NAND_CS_2 0x70000000 #define TARGET_MEM_NAND_CS_3 0x74000000 #define TARGET_MEM_NAND_CS_4 0x78000000 #define TARGET_MEM_NAND_CS_5 0x7c000000 uint32 deviceNandMemBase (int32 cs); #define TARGET_SHFL(x) _shfl(x) /* The shuffle intrinsic */ /** * @brief * The highest module number. The value for nyquist is used */ #define TARGET_PWR_MAX_MOD 30 /** * @brief * The base address of MDIO */ #define TARGET_MDIO_BASE 0x2090300 /** * @brief * The number of external ethernet ports */ #define TARGET_EMAC_N_PORTS 2 /** * @brief * The base address of the I2C peripheral, and the module divisor of the cpu clock */ #define DEVICE_I2C_BASE 0x02530000 #define DEVICE_I2C_MODULE_DIVISOR 6 /** * @brief * Prototypes for the PLL functions handled outside the main PLL registers */ SINT16 chipPllSetExternalPrediv(UINT16 pllNum, UINT32 predivRegVal); SINT16 chipPllExternalBwAdj (UINT16 pllNum, UINT16 mult); UINT32 chipPllExternalMult (UINT16 pllNum, UINT16 mult); /** * @brief * Hardware network subsystem support, ethernet switch */ #define DEVICE_CPSW #define DEVICE_CPSW_NUM_PORTS 3 /* 3 switch ports */ #define DEVICE_CPSW_BASE (0x02090800) #define targetGetSwitchCtl() CPSW_CTL_P0_ENABLE /* Enable port 0 */ #define targetGetSwitchMaxPktSize() 9000 #define DEVICE_QM #define DEVICE_QM_MANAGER_BASE 0x02a68000 #define DEVICE_QM_DESC_SETUP_BASE 0x02a6a000 #define DEVICE_QM_MANAGER_QUEUES_BASE 0x02a20000 #define DEVICE_QM_MANAGER_Q_PROXY_BASE 0x02a40000 #define DEVICE_QM_QUEUE_STATUS_BASE 0x02a00000 #define DEVICE_QM_NUM_LINKRAMS 2 #define DEVICE_QM_NUM_MEMREGIONS 20 void *targetGetQmConfig(void); void targetInitQs (void); #define chipLmbd(x,y) _lmbd(x,y) #define DEVICE_CPDMA #define DEVICE_PA_CDMA_GLOBAL_CFG_BASE 0x02004000 #define DEVICE_PA_CDMA_TX_CHAN_CFG_BASE 0x02004400 #define DEVICE_PA_CDMA_RX_CHAN_CFG_BASE 0x02004800 #define DEVICE_PA_CDMA_RX_FLOW_CFG_BASE 0x02005000 #define DEVICE_PA_CDMA_RX_NUM_CHANNELS 24 #define DEVICE_PA_CDMA_RX_NUM_FLOWS 32 #define DEVICE_PA_CDMA_TX_NUM_CHANNELS 9 #define DEVICE_QM_FREE_Q 910 #define DEVICE_QM_LNK_BUF_Q 911 #define DEVICE_QM_RCV_Q 912 #define DEVICE_QM_TX_Q 913 #define DEVICE_QM_PA_CFG_Q 640 #define DEVICE_QM_ETH_TX_Q 648 #define DEVICE_RX_CDMA_TIMEOUT_COUNT 1000 #define DEVICE_PA #define DEVICE_PA_BASE 0x02000000 #define DEVICE_PA_NUM_PDSPS 6 #define DEVICE_PA_RUN_CHECK_COUNT 100 /* Number of loops to verify PA firmware is running */ #define DEVICE_PA_PLL_BASE 0x02620338 #define chipLower8(x) ((x) & 0x00ff) #define TARGET_SGMII_EXTERNAL_SERDES #define TARGET_SGMII_TYPE_2 /* Use second sgmii setup sequence */ #define TARGET_SGMII_BASE_ADDRESSES { 0x02090100, 0x02090200 } #define TARGET_SGMII_SERDES_BASE 0x2620340 #define TARGET_SGMII_SERDES_STATUS_BASE 0x2620158 #define TARGET_SGMII_SOFT_RESET 0x04 #define TARGET_SGMII_CONTROL 0x10 #define TARGET_SGMII_MR_ADV_ABILITY 0x18 void targetSgmiiSerdesConfig (int32 port, void *cfg); #define chipKickOpenSerdes(x) *((uint32 *)0x2620038) = 0x83e70b13; *((uint32 *)0x262003c) = 0x95a4f1e0 #define chipKickClosedSerdes(x) ; /* never lock the registers */ #define TARGET_SERDES_LOCK_DELAY (1600*1000) #define DEVICE_EMACSL_BASE(x) (0x02090900 + (x)*0x040) #define DEVICE_N_GMACSL_PORTS 2 #define DEVICE_EMACSL_RESET_POLL_COUNT 100 Int32 targetMacSend (void *ptr_device, Uint8* buffer, int num_bytes); Int32 targetMacRcv (void *ptr_device, UINT8 *buffer); #define DEVICE_SS #define DEVICE_PSTREAM_CFG_REG_ADDR 0x2000604 #define DEVICE_PSTREAM_CFG_REG_VAL_ROUTE_PDSP0 0 #define hwConfigStreamingSwitch() DEVICE_REG32_W(DEVICE_PSTREAM_CFG_REG_ADDR, DEVICE_PSTREAM_CFG_REG_VAL_ROUTE_PDSP0); /** * @brief * Register access macros */ #define DEVICE_REG32_W(x,y) *(volatile unsigned int *)(x)=(y) #define DEVICE_REG32_R(x) (*(volatile unsigned int *)(x)) #define BOOTBITMASK(x,y) ( ( ( ((UINT32)1 << (((UINT32)x)-((UINT32)y)+(UINT32)1) ) - (UINT32)1 ) ) << ((UINT32)y) ) #define BOOT_READ_BITFIELD(z,x,y) (((UINT32)z) & BOOTBITMASK(x,y)) >> (y) #define BOOT_SET_BITFIELD(z,f,x,y) (((UINT32)z) & ~BOOTBITMASK(x,y)) | ( (((UINT32)f) << (y)) & BOOTBITMASK(x,y) ) /** * @brief * Mpax configuration registers */ #define DEVICE_REG_XMPAX_L(x) *((volatile unsigned int *)(0x08000000 + (8*(x)))) #define DEVICE_REG_XMPAX_H(x) *((volatile unsigned int *)(0x08000004 + (8*(x)))) /** * @brief * ROM boot loader boot modes and table locations */ #define BOOT_MODE_I2C 40 #define BOOT_MODE_SPI 50 #define ROM_BOOT_PARAMS_ADDR_C6618 0x873680 #define ROM_BOOT_PARAMS_ADDR_C6616 0x8f3680 #endif /* _TARGET_H */