/** * @file c665xinit.c * * @brief * c66x functions used during the initial stage of the ibl load * */ #include "ibl.h" #include "iblloc.h" #include "device.h" #include "pllapi.h" #include "spi_api.h" #include "spi_loc.h" #include "tiboot_c665x.h" /** * @brief Configure the PLLs * * @details * The three PLLs are enabled. Only the main PLL has the ability to configure * the multiplier and dividers. */ void devicePllConfig (void) { /* Unlock the chip registers and leave them unlocked */ *((Uint32 *)0x2620038) = 0x83e70b13; *((Uint32 *)0x262003c) = 0x95a4f1e0; if (ibl.pllConfig[ibl_MAIN_PLL].doEnable == TRUE) hwPllSetPll (MAIN_PLL, ibl.pllConfig[ibl_MAIN_PLL].prediv, ibl.pllConfig[ibl_MAIN_PLL].mult, ibl.pllConfig[ibl_MAIN_PLL].postdiv); if (ibl.pllConfig[ibl_DDR_PLL].doEnable == TRUE) hwPllSetCfg2Pll (DEVICE_PLL_BASE(DDR_PLL), ibl.pllConfig[ibl_DDR_PLL].prediv, ibl.pllConfig[ibl_DDR_PLL].mult, ibl.pllConfig[ibl_DDR_PLL].postdiv, ibl.pllConfig[ibl_MAIN_PLL].pllOutFreqMhz, ibl.pllConfig[ibl_DDR_PLL].pllOutFreqMhz); } /** * @brief * Return the endian status of the device * * @details * Returns true if the device is executing in little endian mode */ extern cregister volatile unsigned int CSR; bool deviceIsLittleEndian (void) { if ((CSR & (1 << 8)) == 0) return (FALSE); return (TRUE); } /** * @brief * Return the device used for the second stage program load. * For SPI NAND a second stage loader is required and this * function must be changed to locate that fingerprint. */ int32 deviceReadBootDevice (void) { uint32 v; int32 w; BOOT_PARAMS_COMMON_T *params; #if (defined(EXCLUDE_NOR_SPI) && defined(EXCLUDE_NAND_SPI) && !defined(EXCLUDE_I2C)) return (BOOT_DEVICE_I2C); #elif (defined(EXCLUDE_NOR_SPI) && !defined(EXCLUDE_NAND_SPI) && defined(EXCLUDE_I2C)) return (BOOT_DEVICE_NAND_SPI); #elif (!defined(EXCLUDE_NOR_SPI) && defined(EXCLUDE_NAND_SPI) && defined(EXCLUDE_I2C)) return (BOOT_DEVICE_NOR_SPI); #endif v = *((Uint32 *)DEVICE_JTAG_ID_REG); v &= DEVICE_JTAG_ID_MASK; if (v == DEVICE_C6657_JTAG_ID_VAL) params = (BOOT_PARAMS_COMMON_T *)ROM_BOOT_PARAMS_ADDR_C6657; switch (params->boot_mode) { #ifndef EXCLUDE_I2C case BOOT_MODE_I2C: w = BOOT_DEVICE_I2C; break; #endif #ifndef EXCLUDE_NOR_SPI case BOOT_MODE_SPI: w = BOOT_DEVICE_SPI_NOR; break; #endif default: w = BOOT_DEVICE_INVALID; break; } return (w); } #define L1PEDCMD 0x01846408 #define L2EDCEN 0x01846030 #define L2EDCMD 0x01846008 #define SMEDCC 0x0BC00010 /** * @brief * Enable the EDC for the local memory */ void iblEnableEDC () { /* Enable L1P EDC */ *(volatile unsigned int *)(L1PEDCMD) = 0x1; //Set EN(bit0)=1 /* Enable EDC L2EDCEN, set DL2CEN(bit0),PL2CEN(bit1),DL2SEN(bit2),PL2SEN(bit3),SDMAEN(bit4)=1 */ *(volatile unsigned int *)(L2EDCEN) |= 0x1F; /* Enalble L2 EDC */ *(volatile unsigned int *)(L2EDCMD) = 0x1; /* Enalbe MSMC EDC */ *(volatile unsigned int *)(SMEDCC) &= 0x7FFFFFFF; //Clear SEN(bit31)=0 *(volatile unsigned int *)(SMEDCC) |= 0x40000000; //Set ECM(bit30)=1 } #ifdef IBL_ENABLE_PCIE_WORKAROUND /* undocumented register in data manual * Bit 0 of this register is supposed to give the status of PCIe PLL lock*/ #define PCIE_STS_REG 0x262015C /* Workaround for PCIe boot mode support for C6678/C6670 */ /* This is a temporary workaround should be removed once fixed in RBL */ /* PCIe Config register base on C6678/C6670 */ #define PCIE_BASE_ADDR 0x21800000 /* PCIe Application registers */ #define PCIE_APP_CMD_STATUS 0x4 #define PCIE_APP_OB_SIZE 0x30 #define PCIE_APP_SERDES_CFG0 0x390 #define PCIE_APP_SERDES_CFG1 0x394 /* PCIe Local Configuration registers */ #define PCIE_VENDER_DEVICE_ID 0x1000 #define PCIE_STATUS_CMD 0x1004 #define PCIE_CLASSCODE_REVID 0x1008 #define PCIE_BAR0 0x1010 #define PCIE_BAR1 0x1014 #define PCIE_BAR2 0x1018 #define PCIE_BAR3 0x101c #define PCIE_DEVICE_CAP 0x1074 #define PCIE_DEV_STAT_CTRL 0x1078 #define PCIE_LINK_STAT_CTRL 0x1080 #define PCIE_ACCR 0x1118 #define PCIE_DEBUG0 0x1728 #define PCIE_PL_GEN2 0x180C /* SERDES Configuration registers */ #define PCIE_SERDES_CFG_PLL 0x2620358 void waitForBoot(UINT32 MAGIC_ADDR) { void (*exit)(); UINT32 i, entry_addr; while(1) { entry_addr = DEVICE_REG32_R(MAGIC_ADDR); if (entry_addr != 0) { /* jump to the exit point, which will be the entry point for the full IBL */ exit = (void (*)())entry_addr; (*exit)(); } for (i=0; i < 100; i++) asm("nop"); } } void iblPCIeWorkaround() { UINT32 v, flag_6678 = 0, flag_6670 = 0, flag_6657 = 0, MAGIC_ADDR; UINT32 i; /* Power up PCIe */ devicePowerPeriph (TARGET_PWR_PCIE); for(i=0; i<1000; i++) asm (" NOP"); DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_APP_SERDES_CFG0), 0x00062320); /* ss clock */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_APP_SERDES_CFG1), 0x00022320); /* ss clock */ /* Wait for PCIe PLL lock */ while(!(DEVICE_REG32_R(PCIE_STS_REG) & 1)); /* Determine 6670 or 6678 */ v = *((Uint32 *)DEVICE_JTAG_ID_REG); v &= DEVICE_JTAG_ID_MASK; if (v == DEVICE_C6678_JTAG_ID_VAL) { MAGIC_ADDR = 0x87fffc; flag_6678 = 1; } if (v == DEVICE_C6670_JTAG_ID_VAL) { MAGIC_ADDR = 0x8ffffc; flag_6670 = 1; } if (v == DEVICE_C6657_JTAG_ID_VAL) { MAGIC_ADDR = 0x8ffffc; flag_6657 = 1; } DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_CLASSCODE_REVID), 0x04800001); /* class 0x04, sub-class 0x80, Prog I/F 0x00, Other multimedia device */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_LINK_STAT_CTRL), 0x10110080); /* extended sync, slot_clk_cfg = 1 */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_VENDER_DEVICE_ID), 0xb005104c); /* Vendor and Device ID */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_DEVICE_CAP), 0x288701); /* L0 = 4, L1 = 3 */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_APP_OB_SIZE), 0x00000003); /* OB_SIZE = 8M */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_PL_GEN2), 0x0000000F); /* num_fts = 0xF*/ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_APP_CMD_STATUS), 0x0020); /* Set dbi_cs2 to allow access to the BAR registers */ if (flag_6678) { /* 6678 */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR0), 0x00000FFF); /* 4K */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR1), 0x0007FFFF); /* 512K */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR2), 0x003FFFFF); /* 4M */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR3), 0x00FFFFFF); /* 16M */ } if (flag_6670) { /* 6670 */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR0), 0x00000FFF); /* 4K */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR1), 0x000FFFFF); /* 1M */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR2), 0x001FFFFF); /* 2M */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR3), 0x00FFFFFF); /* 16M */ } if (flag_6657) { /* 6657 */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR0), 0x00000FFF); /* 4K */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR1), 0x000FFFFF); /* 1M */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR2), 0x001FFFFF); /* 2M */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR3), 0x00FFFFFF); /* 16M */ } DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_APP_CMD_STATUS), 0x0); /* dbi_cs2=0 */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_STATUS_CMD), 0x00100146); /* ENABLE mem access */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_DEV_STAT_CTRL), 0x0000281F); /* Error control */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_ACCR), 0x000001E0); /* Error control */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_BAR0), 0); /* non-prefetch, 32-bit, mem bar */ DEVICE_REG32_W ((PCIE_BASE_ADDR + PCIE_APP_CMD_STATUS), 0x0000007); /* enable LTSSM, IN, OB */ while((DEVICE_REG32_R(PCIE_BASE_ADDR + PCIE_DEBUG0) & 0x11)!=0x11); /* Wait for training to complete */ /* Wait for the Boot from Host */ DEVICE_REG32_W(MAGIC_ADDR, 0); waitForBoot(MAGIC_ADDR); /* Will never reach here */ return; } #endif #define FPGA_BM_GPI_STATUS_LO_REG 4 /* Boot Mode GPI Status (07-00 Low Byte) Register */ #define FPGA_BM_GPI_STATUS_HI_REG 5 /* Boot Mode GPI Status (15-08 High Byte) Register */ #define FPGA_ICS557_SEL_CTRL_REG 0x50 /* ICS 557 Clock Selection Control Register*/ #define FPGA_READ_REG_CMD(x) ((x | 0x80) << 8) #define FPGA_WRITE_REG_CMD(addr,byte) (((addr & 0x7f) << 8) | (byte & 0xff)) /** * @brief * Enter the ROM boot loader if the FPGA boot register * indicates it was not I2C address 0x51 boot, this is necessary * to apply the PLL workaround for non-I2C boot modes */ void iblEnterRom () { uint32 v, dev_stat, bm_lo, bm_hi; void (*exit)(); /* Reset SPI */ DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIGCR0, SPI_REG_VAL_SPIGCR0_RESET); /* Release Reset */ DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIGCR0, SPI_REG_VAL_SPIGCR0_ENABLE); /* CS1, CLK, in and out are functional pins, FPGA uses SPI CS1 */ DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIPC0, 0xe02); /* prescale=7, char len=16 */ DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIFMT(0), 0x710); /* C2TDELAY=0x6, T2CDELAY=0x3 */ DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIDELAY, 0x6030000); /* Clear the SPIDAT0 */ //DEVICE_REG32_R (DEVICE_SPI_BASE(0) + SPI_REG_SPIDAT0); /* Master mode, enable SPI */ DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIGCR1, 0x01000003); /* Read the BM status lo register */ DEVICE_REG32_W(DEVICE_SPI_BASE(0) + SPI_REG_SPIDAT0, FPGA_READ_REG_CMD(FPGA_BM_GPI_STATUS_LO_REG)); chipDelay32(10000); v = DEVICE_REG32_R(DEVICE_SPI_BASE(0) + SPI_REG_SPIFLG); if ( v & 0x100) { bm_lo = DEVICE_REG32_R(DEVICE_SPI_BASE(0) + SPI_REG_SPIBUF) & 0xff; } else { return; } /* Read the BM status hi register */ DEVICE_REG32_W(DEVICE_SPI_BASE(0) + SPI_REG_SPIDAT0, FPGA_READ_REG_CMD(FPGA_BM_GPI_STATUS_HI_REG)); chipDelay32(10000); v = DEVICE_REG32_R(DEVICE_SPI_BASE(0) + SPI_REG_SPIFLG); if ( v & 0x100) { bm_hi = DEVICE_REG32_R(DEVICE_SPI_BASE(0) + SPI_REG_SPIBUF) & 0xff; } else { return; } if ( (BOOT_READ_BITFIELD(bm_lo,3,1) != 0x5) || (BOOT_READ_BITFIELD(bm_hi,3,3) == 0x0) ) { /* Not i2c boot or i2c boot with address 0x50 */ /* Update the DEVSTAT to v1 */ dev_stat = DEVICE_REG32_R(DEVICE_REG_DEVSTAT ); dev_stat &= ~(0x0000080E); dev_stat |= ((bm_hi << 8) | bm_lo); /* Update the DEVSTAT register for the intended Boot Device and i2c Addr */ DEVICE_REG32_W (DEVICE_REG_DEVSTAT, dev_stat); #ifdef IBL_ENABLE_PCIE_WORKAROUND #define BOOT_DEVICE_MASK 0xE #define DEVSTAT_BOOTDEVICE_SHIFT 1 #define PCI_BOOT_MODE 0x4 if (((dev_stat & BOOT_DEVICE_MASK)>>DEVSTAT_BOOTDEVICE_SHIFT) == PCI_BOOT_MODE) { /* Write ICS 557 Clock Selection Control Register in the FPGA */ /* 1 : FPGA_ICS557_SEL s driven high */ DEVICE_REG32_W(DEVICE_SPI_BASE(0) + SPI_REG_SPIDAT0, FPGA_WRITE_REG_CMD(FPGA_ICS557_SEL_CTRL_REG,1)); chipDelay32(10000); /* Reset SPI */ DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIGCR0, SPI_REG_VAL_SPIGCR0_RESET); iblPCIeWorkaround(); /* Will never reach here */ } #endif /* Reset SPI */ DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIGCR0, SPI_REG_VAL_SPIGCR0_RESET); exit = (void (*)())BOOT_ROM_ENTER_ADDRESS; (*exit)(); } else { /* Update the DEVSTAT register for the actual boot configuration */ DEVICE_REG32_W (DEVICE_REG_DEVSTAT, ((bm_hi << 8) | bm_lo)); } /* Reset SPI */ DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIGCR0, SPI_REG_VAL_SPIGCR0_RESET); } #if (!defined(EXCLUDE_NOR_SPI) || !defined(EXCLUDE_NAND_SPI)) /** * @brief * Return the default hardware configuration for SPI. If this information * is available in the boot ROM it is used, otherwise defaults are used. */ void deviceLoadInitSpiConfig (void *vcfg) { uint32 v; spiConfig_t *cfg = (spiConfig_t *)vcfg; BOOT_PARAMS_COMMON_T *params; BOOT_PARAMS_SPI_T *spip; v = *((Uint32 *)DEVICE_JTAG_ID_REG); v &= DEVICE_JTAG_ID_MASK; if (v == DEVICE_C6657_JTAG_ID_VAL) params = (BOOT_PARAMS_COMMON_T *)ROM_BOOT_PARAMS_ADDR_C6657; /* SPI_ROM is a constant defined during make which enables the use of the * parameters from the ROM boot loader */ if ((SPI_ROM == 1) && (params->boot_mode == BOOT_MODE_SPI)) { spip = (BOOT_PARAMS_SPI_T *)params; cfg->port = 0; cfg->mode = spip->mode; cfg->addrWidth = spip->addrWidth; cfg->npin = spip->nPins; cfg->csel = spip->csel; cfg->c2tdelay = spip->c2tdelay; /* TODO:cpufreqMhz need update */ v = (UINT32)spip->cpuFreqMhz * 1000; /* CPU frequency in kHz */ v = v / (DEVICE_SPI_MOD_DIVIDER * (((UINT32)(spip->busFreqMhz) * 1000) + spip->busFreqKhz)); if (v > DEVICE_SPI_MAX_DIVIDER) v = DEVICE_SPI_MAX_DIVIDER; cfg->clkdiv = v; } else { cfg->port = 0; cfg->mode = SPI_MODE; cfg->addrWidth = SPI_ADDR_WIDTH; cfg->npin = SPI_NPIN; cfg->csel = SPI_CSEL; cfg->c2tdelay = SPI_C2TDEL; cfg->clkdiv = SPI_CLKDIV; } } #endif