/* * * Copyright (C) 2010-2012 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ /************************************************************************************ * FILE PURPOSE: C66xK2x Device Specific functions ************************************************************************************ * FILE NAME: c66xk2x.c * * DESCRIPTION: Implements the device specific functions for the IBL * * @file c66xk2x.c * * @brief * This file implements the device specific functions for the IBL * ************************************************************************************/ #include "ibl.h" #include "iblloc.h" #include "iblcfg.h" #include "device.h" #include "pllapi.h" #include "emif31api.h" #include "pscapi.h" #include "gpio.h" #include "qm_api.h" #include "cpdma_api.h" #include "pa_api.h" #include "serdes_api.h" #include "net.h" #include "nandhwapi.h" #include "nor_api.h" #include "spi_api.h" #include #include #include "target.h" #include "uart.h" #define PLL_DDR_INIT_LOOPMAX 10 #define IBL_RESULT_CODE_STR_LEN 20 #define IBL_RESULT_CODE_LOC 17 extern cregister unsigned int DNUM; /** * @brief Determine if an address is local * * @details * Examines an input address to determine if it is a local address. Using the largest * L2 size on the c66xk2x. */ bool address_is_local (Uint32 addr) { /* L2 */ if ((addr >= 0x00800000) && (addr < 0x00900000)) return (TRUE); /* L1P */ if ((addr >= 0x00e00000) && (addr < 0x00e08000)) return (TRUE); /* L2D */ if ((addr >= 0x00f00000) && (addr < 0x00f08000)) return (TRUE); return (FALSE); } /** * @brief Convert a local l1d, l1p or l2 address to a global address * * @details * The global address is formed. If the address is not local then * the input address is returned */ Uint32 deviceLocalAddrToGlobal (Uint32 addr) { if (address_is_local (addr)) addr = (1 << 28) | (DNUM << 24) | addr; return (addr); } /** * @brief * Enable the DDR * * @details * The DDR controller on the c66x is an emif 4.0. The controller is * initialized directly with the supplied values */ void deviceDdrConfig (void) { uint32 loopcount=0; int8 ddr_result_code_str[IBL_RESULT_CODE_STR_LEN] = "IBL Result code 0"; /* The emif registers must be made visible. MPAX mapping 2 is used */ DEVICE_REG_XMPAX_L(2) = 0x10000000 | 0xff; /* replacement addr + perm*/ DEVICE_REG_XMPAX_H(2) = 0x2100000B; /* base addr + seg size (64KB)*/ if (ibl.ddrConfig.configDdr != 0) hwEmif4p0Enable (&ibl.ddrConfig.uEmif.emif4p0); #ifdef PLL_REINIT_WORKAROUND for (loopcount = 0; loopcount < PLL_DDR_INIT_LOOPMAX; loopcount++) { /* Calling MAIN, PA, DDR PLL init */ if (ibl.pllConfig[ibl_MAIN_PLL].doEnable == TRUE) hwPllSetPll (MAIN_PLL, ibl.pllConfig[ibl_MAIN_PLL].prediv, ibl.pllConfig[ibl_MAIN_PLL].mult, ibl.pllConfig[ibl_MAIN_PLL].postdiv); if (ibl.pllConfig[ibl_NET_PLL].doEnable == TRUE) hwPllSetCfgPll (DEVICE_PLL_BASE(NET_PLL), ibl.pllConfig[ibl_NET_PLL].prediv, ibl.pllConfig[ibl_NET_PLL].mult, ibl.pllConfig[ibl_NET_PLL].postdiv, ibl.pllConfig[ibl_MAIN_PLL].pllOutFreqMhz, ibl.pllConfig[ibl_NET_PLL].pllOutFreqMhz); if (ibl.pllConfig[ibl_DDR_PLL].doEnable == TRUE) hwPllSetCfg2Pll (DEVICE_PLL_BASE(DDR_PLL), ibl.pllConfig[ibl_DDR_PLL].prediv, ibl.pllConfig[ibl_DDR_PLL].mult, ibl.pllConfig[ibl_DDR_PLL].postdiv, ibl.pllConfig[ibl_MAIN_PLL].pllOutFreqMhz, ibl.pllConfig[ibl_DDR_PLL].pllOutFreqMhz); if (ibl.ddrConfig.configDdr != 0) hwEmif4p0Enable (&ibl.ddrConfig.uEmif.emif4p0); if (ddr3_memory_test() == 0) { break; } } /* Init UART again because we are re-initializing the PLL's */ uart_init(); if (loopcount < 10) { ddr_result_code_str[IBL_RESULT_CODE_LOC] = loopcount + '0'; } else if ((loopcount >= 10) && (loopcount < 35)) { ddr_result_code_str[IBL_RESULT_CODE_LOC] = loopcount + 'A'; } else { ddr_result_code_str[IBL_RESULT_CODE_LOC] = loopcount + 'Z'; } if (loopcount == PLL_DDR_INIT_LOOPMAX) { uart_write_string("IBL: DDR INITIALIZATION FAILED",0); } else { uart_write_string("IBL: PLL and DDR Initialization Complete",0); } uart_write_string(ddr_result_code_str,0); #endif } /** * @brief Enable EMIF25 or SPI interface to the NAND * */ int32 deviceConfigureForNand(void) { return (0); } /** * @brief * Return the base memory address for emif25 in a given chip select space */ uint32 deviceEmif25MemBase (int32 cs) { switch (cs) { case 2: return (TARGET_MEM_NAND_CS_2); case 3: return (TARGET_MEM_NAND_CS_3); case 4: return (TARGET_MEM_NAND_CS_4); case 5: return (TARGET_MEM_NAND_CS_5); } return (0xffffffff); } /** * @brief * Return the PSC number for NAND/NOR through emif. Only 6678 has the emif */ Int32 deviceEmifPscNum (void) { Uint32 v; v = *((Uint32 *)DEVICE_JTAG_ID_REG); v &= DEVICE_JTAG_ID_MASK; if (v == DEVICE_TCI6636K2H_JTAG_ID_VAL) return (TARGET_PWR_EMIF_TCI6634K2K); /* Return a negative number to indicate no PSC module is associated with NAND */ return (-1); } /** * @brief * The e-fuse mac address is loaded */ void deviceLoadDefaultEthAddress (uint8 *maddr) { uint32 macA, macB; /* Read the e-fuse mac address */ macA = *((uint32 *)0x2620110); macB = *((uint32 *)0x2620114); maddr[0] = (macB >> 8) & 0xff; maddr[1] = (macB >> 0) & 0xff; maddr[2] = (macA >> 24) & 0xff; maddr[3] = (macA >> 16) & 0xff; maddr[4] = (macA >> 8) & 0xff; maddr[5] = (macA >> 0) & 0xff; } /** * @brief * Compile time queue manager information */ #define DEVICE_NUM_RX_CPPIS 1 #define DEVICE_NUM_TX_CPPIS 1 #define DEVICE_NUM_CPPIS (DEVICE_NUM_RX_CPPIS + DEVICE_NUM_TX_CPPIS) /* The linking RAM */ #pragma DATA_SECTION(qm_linkram_buf, ".linkram") #pragma DATA_ALIGN(qm_linkram_buf, 16) uint8 qm_linkram_buf[DEVICE_NUM_CPPIS * 2 * (sizeof(uint32)/sizeof(uint8))]; /* The CPPI RAM */ #pragma DATA_SECTION(qm_cppi_buf, ".cppi") #pragma DATA_ALIGN(qm_cppi_buf, 16) uint8 qm_cppi_buf[QM_DESC_SIZE_BYTES * DEVICE_NUM_CPPIS]; /* The rx data buffers */ #pragma DATA_SECTION(qm_buffer, ".mac_buffer") #pragma DATA_ALIGN(qm_buffer, 16) uint8 qm_buffer[MAX_SIZE_STREAM_BUFFER * DEVICE_NUM_RX_CPPIS]; const qmConfig_t qmConfig = { (UINT32) qm_linkram_buf, sizeof (qm_cppi_buf), (UINT32) qm_cppi_buf, DEVICE_NUM_CPPIS, DEVICE_QM_FREE_Q }; /** * @brief * Return the queue manager memory configuration information */ void *targetGetQmConfig (void) { return ((void *)&qmConfig); } /** * @brief * Attach a packet buffer to each descriptor and push onto the linked buffer queue */ void targetInitQs (void) { int32 i; qmHostDesc_t *hd; for (i = 0; i < DEVICE_NUM_RX_CPPIS; i++) { hd = hwQmQueuePop (DEVICE_QM_FREE_Q); hd->buffLen = sizeof (qm_buffer) / DEVICE_NUM_CPPIS; hd->buffPtr = (UINT32) &(qm_buffer[MAX_SIZE_STREAM_BUFFER * i]); hd->nextBDPtr = 0; hd->origBufferLen = MAX_SIZE_STREAM_BUFFER; hd->origBuffPtr = hd->buffPtr; hwQmQueuePush (hd, DEVICE_QM_LNK_BUF_Q, QM_DESC_SIZE_BYTES); } for (i = 0; i < DEVICE_NUM_TX_CPPIS; i++) { hd = hwQmQueuePop (DEVICE_QM_FREE_Q); hd->buffLen = 0; hd->buffPtr = 0; hd->nextBDPtr = 0; hd->origBufferLen = 0; hd->origBuffPtr = 0; hwQmQueuePush (hd, DEVICE_QM_TX_Q, QM_DESC_SIZE_BYTES); } } const cpdmaRxCfg_t cpdmaEthRxCfg = { DEVICE_PA_CDMA_RX_CHAN_CFG_BASE, /* Base address of PA CPDMA rx config registers */ DEVICE_PA_CDMA_RX_NUM_CHANNELS, /* Number of rx channels */ DEVICE_PA_CDMA_RX_FLOW_CFG_BASE, /* Base address of PA CPDMA rx flow registers */ DEVICE_PA_CDMA_RX_NUM_FLOWS, /* Number of rx flows */ 0, /* Queue manager for descriptor / buffer for received packets */ DEVICE_QM_LNK_BUF_Q, /* Queue of descriptors /buffers for received packets */ 0, /* Queue manager for received packets */ DEVICE_QM_RCV_Q, /* Queue for received packets (overridden by PA) */ DEVICE_RX_CDMA_TIMEOUT_COUNT /* Teardown maximum loop wait */ }; /** * @brief * Return the cpdma configuration information */ void *targetGetCpdmaRxConfig (void) { return ((void *)&cpdmaEthRxCfg); } const cpdmaTxCfg_t cpdmaEthTxCfg = { DEVICE_PA_CDMA_GLOBAL_CFG_BASE, /* Base address of global config registers */ DEVICE_PA_CDMA_TX_CHAN_CFG_BASE, /* Base address of PA CPDMA tx config registers */ DEVICE_PA_CDMA_TX_NUM_CHANNELS /* Number of tx channels */ }; /** * @brief * return the tx cpdma configuration information */ void *targetGetCpdmaTxConfig (void) { return ((void *)&cpdmaEthTxCfg); } /** * @brief * Configure the PA */ void targetPaConfig (uint8 *macAddr) { paConfig_t paCfg; qmHostDesc_t *hd; SINT16 ret; /* Filter everything except the desired mac address and the broadcast mac */ paCfg.mac0ms = ((uint32)macAddr[0] << 24) | ((uint32)macAddr[1] << 16) | ((uint32)macAddr[2] << 8) | (uint32)(macAddr[3]); paCfg.mac0ls = ((uint32)macAddr[4] << 24) | ((uint32)macAddr[5] << 16); paCfg.mac1ms = 0xffffffff; paCfg.mac1ls = 0xffff0000; paCfg.rxQnum = DEVICE_QM_RCV_Q; /* Form the configuration command in a buffer linked to a descriptor */ hd = hwQmQueuePop (DEVICE_QM_LNK_BUF_Q); paCfg.cmdBuf = (uint8 *)hd->origBuffPtr; ret = hwPaEnable (&paCfg); if (ret != 0) { iblStatus.iblFail = ibl_FAIL_CODE_PA; return; } /* Send the command to the PA through the QM */ hd->softwareInfo0 = PA_MAGIC_ID; hd->buffLen = 16; QM_DESC_DESCINFO_SET_PKT_LEN(hd->descInfo, 16); /* Set the return Queue */ QM_DESC_PINFO_SET_QM (hd->packetInfo, 0); QM_DESC_PINFO_SET_QUEUE (hd->packetInfo, DEVICE_QM_LNK_BUF_Q); hwQmQueuePush (hd, DEVICE_QM_PA_CFG_Q, QM_DESC_SIZE_BYTES); } /** * @brief * Chip level SGMII serdes configuration * * @details * Both lanes are always setup, regardless of the port value */ void targetSgmiiSerdesConfig (int32 port, void *viblSgmii) { serdesConfig_t scfg; iblSgmii_t *sgmii = (iblSgmii_t *)viblSgmii; scfg.cfg = sgmii->auxConfig; scfg.nLanes = 2; scfg.rxCfg[0] = scfg.rxCfg[1] = sgmii->rxConfig; scfg.txCfg[0] = scfg.txCfg[1] = sgmii->txConfig; #if 0 /* TBD */ hwSerdesConfig (TARGET_SGMII_SERDES_BASE, &scfg); hwSerdesWaitLock (TARGET_SGMII_SERDES_STATUS_BASE); #endif } Int32 targetMacSend (void *vptr_device, Uint8* buffer, int num_bytes) { qmHostDesc_t *hd; NET_DRV_DEVICE *ptr_device = (NET_DRV_DEVICE *)vptr_device; int i; /* Must always setup the descriptor to have the minimum packet length */ if (num_bytes < 64) num_bytes = 64; for (i = 0, hd = NULL; hd == NULL; i++, chipDelay32 (1000)) hd = hwQmQueuePop (DEVICE_QM_TX_Q); if (hd == NULL) return (-1); QM_DESC_DESCINFO_SET_PKT_LEN(hd->descInfo, num_bytes); hd->buffLen = num_bytes; hd->origBufferLen = num_bytes; hd->buffPtr = deviceLocalAddrToGlobal((UINT32)buffer); hd->origBuffPtr = deviceLocalAddrToGlobal((UINT32)buffer); /* Return the descriptor back to the transmit queue */ QM_DESC_PINFO_SET_QM(hd->packetInfo, 0); QM_DESC_PINFO_SET_QUEUE(hd->packetInfo, DEVICE_QM_TX_Q); hwQmQueuePush (hd, DEVICE_QM_ETH_TX_Q, QM_DESC_SIZE_BYTES); return (0); } Int32 targetMacRcv (void *vptr_device, UINT8 *buffer) { Int32 pktSizeBytes; qmHostDesc_t *hd; NET_DRV_DEVICE *ptr_device = (NET_DRV_DEVICE *)vptr_device; hd = hwQmQueuePop (DEVICE_QM_RCV_Q); if (hd == NULL) return (0); pktSizeBytes = QM_DESC_DESCINFO_GET_PKT_LEN(hd->descInfo); iblMemcpy ((void *)buffer, (void *)hd->buffPtr, pktSizeBytes); hd->buffLen = hd->origBufferLen; hd->buffPtr = hd->origBuffPtr; hwQmQueuePush (hd, DEVICE_QM_LNK_BUF_Q, QM_DESC_SIZE_BYTES); return (pktSizeBytes); } void targetFreeQs (void) { qmHostDesc_t *hd; do { hd = hwQmQueuePop (DEVICE_QM_FREE_Q); } while (hd != NULL); do { hd = hwQmQueuePop (DEVICE_QM_LNK_BUF_Q); } while (hd != NULL); do { hd = hwQmQueuePop (DEVICE_QM_RCV_Q); } while (hd != NULL); do { hd = hwQmQueuePop (DEVICE_QM_TX_Q); } while (hd != NULL); } extern nandCtbl_t nandEmifCtbl; /** * @brief Return the NAND interface (GPIO, EMIF25 or SPI) used based on the value * of interface */ #ifndef EXCLUDE_NAND_GPIO nandCtbl_t nandGpioCtbl = { nandHwGpioDriverInit, nandHwGpioDriverReadBytes, nandHwGpioDriverReadPage, nandHwGpioDriverClose }; #endif #ifndef EXCLUDE_NAND_EMIF extern Int32 nandHwEmifDriverInit (int32 cs, void *vdevInfo); extern Int32 nandHwEmifDriverReadBytes (Uint32 block, Uint32 page, Uint32 byte, Uint32 nbytes, Uint8 *data); extern Int32 nandHwEmifDriverReadPage (Uint32 block, Uint32 page, Uint8 *data); extern Int32 nandHwEmifDriverClose (void); nandCtbl_t nandEmifCtbl = { nandHwEmifDriverInit, nandHwEmifDriverReadBytes, nandHwEmifDriverReadPage, nandHwEmifDriverClose }; #endif #ifndef EXCLUDE_NAND_SPI nandCtbl_t nandSpiCtbl = { nandHwSpiDriverInit, nandHwSpiDriverReadBytes, nandHwSpiDriverReadPage, nandHwSpiDriverClose }; #endif nandCtbl_t *deviceGetNandCtbl (int32 interface) { #ifndef EXCLUDE_NAND_GPIO if (interface == ibl_PMEM_IF_GPIO) return (&nandGpioCtbl); #endif #ifndef EXCLUDE_NAND_SPI if (interface == ibl_PMEM_IF_SPI) return (&nandSpiCtbl); #endif #ifndef EXCLUDE_NAND_EMIF if ((interface >= ibl_PMEM_IF_CHIPSEL_2) && (interface <= ibl_PMEM_IF_CHIPSEL_5)) return (&nandEmifCtbl); #endif return (NULL); } /** * @brief * Get the nor call table for the specified nor interface */ #ifndef EXCLUDE_NOR_EMIF norCtbl_t norEmifCtbl = { norHwEmifDriverInit, norHwEmifDriverReadBytes, norHwEmifDriverClose }; #endif #ifndef EXCLUDE_NOR_SPI norCtbl_t norSpiCtbl = { norHwSpiDriverInit, norHwSpiDriverReadBytes, norHwSpiDriverClose }; #endif norCtbl_t *deviceGetNorCtbl (int32 interface) { #ifndef EXCLUDE_NOR_SPI if (interface == ibl_PMEM_IF_SPI) return (&norSpiCtbl); #endif #ifndef EXCLUDE_NOR_EMIF if ((interface >= ibl_PMEM_IF_CHIPSEL_2) && (interface <= ibl_PMEM_IF_CHIPSEL_5)) return (&norEmifCtbl); #endif return (NULL); }