/** * @file tftp.c * * @brief * The file implements the NET Module TFTP functionality. * * \par * NOTE: * (C) Copyright 2008, Texas Instruments, Inc. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * * \par */ #include "types.h" #include "iblloc.h" #include "net.h" #include "netif.h" #include "timer.h" #include "stream.h" #include #include "net_osal.h" /********************************************************************** *************************** LOCAL Structures ************************* **********************************************************************/ /** * @brief * The structure describes the TFTP State * * @details * The TFTP client can be in one of the following states which are * described in this structure. */ typedef enum TFTP_STATE { /** * @brief This is the initial state of the TFTP client during startup * In this state the TFTP client has sent out the READ Request and has * not yet received a data packet in acknowledgment. */ READ_REQUEST = 0x1, /** * @brief This is the data receive state of the TFTP client in which * the TFTP client is receiving data packets from the TFTP server. */ DATA_RECEIVE }TFTP_STATE; /** * @brief * The structure describes the TFTP Master Control Block. * * @details * The TFTP Master control block stores information used by the * TFTP module. */ typedef struct TFTP_MCB { /** * @brief This describes the state of the TFTP client. */ TFTP_STATE state; /** * @brief This is the IP Address of the server from where the file * is downloaded. */ IPN server_ip; /** * @brief This is the TFTP socket which is used to communicate * with the UDP module. */ Int32 sock; /** * @brief This is the TFTP Timer handle which is used to handle * retransmissions of the READ REQUEST. */ Int32 timer; /** * @brief This is the name of the file which is being downloaded. * File Names are typically exchanged through the BOOTP protocol * where the max file name length is 64. */ Uint8 filename[64]; /** * @brief This is the block number we expect. */ Uint16 block_num; /** * @brief This is a generic buffer used by the TFTP module, */ Uint8 buffer[TFTP_DATA_SIZE + TFTPHEADER_SIZE]; /** * @brief Number of retransmission done. */ Uint32 num_retransmits; }TFTP_MCB; /********************************************************************** *************************** GLOBAL Variables ************************* **********************************************************************/ /** * @brief This is the global master control block for the TFTP * module and keeps track of all the information regarding TFTP. */ TFTP_MCB tftpmcb; /********************************************************************** **************************** TFTP Functions ************************** **********************************************************************/ /** * @b Description * @n * The function cleans up the TFTP Client. This can be called * on an ERROR or SUCCESSFUL exit. * * @retval * Not Applicable. */ static void tftp_cleanup (void) { /* Close any open timers. */ timer_delete (tftpmcb.timer); tftpmcb.timer = -1; /* Close the UDP Sockets. */ udp_sock_close (tftpmcb.sock); /* Close the STREAM module */ stream_close (); return; } /** * @b Description * @n * The function creates the TFTP read request and populates it * in the internal TFTP buffer. * * @retval * Size of the TFTP Read Request. */ static Int32 tftp_create_read_req (Uint8* filename) { Uint16* ptr_op; Int32 index = 0; /* Create the Read Request: Populate the Request op type */ ptr_op = (Uint16 *)&tftpmcb.buffer[0]; *ptr_op = htons(TFTP_OPCODE_RRQ); /* Copy the file name */ index = 0; while (filename[index] != 0) { tftpmcb.buffer[index + 2] = filename[index]; index++; } /* Null Terminate the file name. */ tftpmcb.buffer[index + 2] = 0; index = index + 3; /* Copy the transfer mode. */ tftpmcb.buffer[index++] = (Uint8)'o'; tftpmcb.buffer[index++] = (Uint8)'c'; tftpmcb.buffer[index++] = (Uint8)'t'; tftpmcb.buffer[index++] = (Uint8)'e'; tftpmcb.buffer[index++] = (Uint8)'t'; tftpmcb.buffer[index++] = (Uint8)0; /* Return the size of the read request */ return index; } /** * @b Description * @n * The function is used to send an ACK back to TFTP Server. * * @retval * Not Applicable */ static void tftp_send_ack(void) { TFTPHDR* ptr_tftphdr; /* Initialize the data buffer. */ netMemset ((void *)&tftpmcb.buffer[0], 0, TFTP_DATA_SIZE + TFTPHEADER_SIZE); /* Create an ACK packet which is to be sent out. Get the pointer to the * TFTP Header. */ ptr_tftphdr = (TFTPHDR *)&tftpmcb.buffer[0]; ptr_tftphdr->opcode = htons (TFTP_OPCODE_ACK); ptr_tftphdr->block = htons (tftpmcb.block_num); /* The packet has been populated; send it to the server; this transfer is now done * over the data socket. */ udp_sock_send (tftpmcb.sock, (Uint8 *)ptr_tftphdr, TFTPHEADER_SIZE); /* Increment the block number. */ tftpmcb.block_num++; return; } /** * @b Description * @n * The function is the timer expiration for TFTP. * * @retval * Not Applicable */ static void tftp_timer_expiry (void) { Int32 len; /* Determine the state of the TFTP. */ if (tftpmcb.state == READ_REQUEST) { /* We were sending out READ Request and have not received a response * Increment the number of retransmissions which have been done. */ tftpmcb.num_retransmits++; /* Check if we have exceeded the max allowed? */ if (tftpmcb.num_retransmits > MAX_TFTP_RETRANSMITS) { /* FATAL Error: We need to close the TFTP Client and signal Error to the NET Boot Module. */ mprintf ("Error: TFTP READ REQ Retransmissions have exceeded\n"); tftp_cleanup (); net_set_error(); return; } /* Create the TFTP Read Request */ len = tftp_create_read_req (&tftpmcb.filename[0]); /* Send out the READ Request again. */ udp_sock_send (tftpmcb.sock, (Uint8 *)&tftpmcb.buffer[0], len); } else { /* We were receiving data from the TFTP Server and there was a timeout. This can * happen only if we have not received any data from the TFTP server. */ mprintf ("Error: TFTP server is down; no packet received.\n"); tftp_cleanup(); net_set_error(); return; } return; } /** * @b Description * @n * This is a call back function registered with the UDP module to * be invoked when a TFTP packet is received. * * @param[in] sock * This is the socket handle on which packet was received. * @param[in] ptr_data * This is the pointer to the TFTP data payload. * @param[in] num_bytes * This is the number of bytes of TFTP data received. * * @retval * Success - 0 * @retval * Error - <0 */ static Int32 tftp_receive (Int32 sock, Uint8* ptr_data, Int32 num_bytes) { TFTPHDR* ptr_tftphdr; UDPHDR* ptr_udphdr; Uint16 src_port; SOCKET socket; /* Get the pointer to the TFTP Header. */ ptr_tftphdr = (TFTPHDR *)ptr_data; /* Process the received packet depending on the type of packet received */ switch (ntohs(ptr_tftphdr->opcode)) { case TFTP_OPCODE_DATA: { /* Is this the first data packet we have received? */ if (tftpmcb.state == READ_REQUEST) { /* YES. In this case the socket on which the request was sent has completed * its job. Lets shut it down and open another one for the data transfers. */ udp_sock_close (sock); /* We need to get the source port from where the data was received. * This information is present in the UDP layer. This is required to * open the data socket. */ ptr_udphdr = (UDPHDR *)(ptr_data - sizeof(UDPHDR)); src_port = ntohs(ptr_udphdr->SrcPort); /* Populate the socket structure and register this with the UDP module. */ socket.local_port = 1234; socket.remote_port = src_port; socket.remote_address = tftpmcb.server_ip; socket.app_fn = tftp_receive; /* Move to the DATA State. */ tftpmcb.state = DATA_RECEIVE; tftpmcb.num_retransmits = 0; /* Close the timer. */ timer_delete (tftpmcb.timer); tftpmcb.timer = -1; /* Open the TFTP data socket. */ tftpmcb.sock = udp_sock_open (&socket); if (tftpmcb.sock < 0) { /* Error: Data Socket open failed. */ mprintf ("Error: TFTP Data Socket Open Failed\n"); tftp_cleanup(); net_set_error(); return -1; } } /* We are in the DATA State: Start the TFTP Server Keep Alive Timer. This timer * keeps track of the TFTP Server and ensures it does not die behind us. This will * help detect that error. */ timer_delete (tftpmcb.timer); tftpmcb.timer = timer_add (TFTP_SERVER_TIMEOUT, tftp_timer_expiry); if (tftpmcb.timer < 0) { /* Timer creation failed. */ mprintf ("Error: TFTP Timer creation failed\n"); tftp_cleanup(); net_set_error(); return -1; } /* Received a data block. Ensure that the block number matches what we expect! */ if (ntohs(ptr_tftphdr->block) != tftpmcb.block_num) { /* There is a block number mismatch. This could occur if the ACK we sent was lost. * Increment the number of retransmissions. */ tftpmcb.num_retransmits++; if (tftpmcb.num_retransmits > MAX_TFTP_RETRANSMITS) { /* OK; we resent the ACK multiple times & the server still kept sending the * same packet back. We just give up now. */ mprintf ("Error: TFTP ACK Retransmits Exceeded\n"); tftp_cleanup(); net_set_error(); return -1; } /* We need to send out the ACK for the previous 'block' */ tftpmcb.block_num = tftpmcb.block_num - 1; /* Send the ACK out again. */ tftp_send_ack (); /* We dont need to process this packet since we had already picked it up. */ return 0; } /* The packet looks good. Reset the number of retransmissions. */ tftpmcb.num_retransmits = 0; /* Pass the received data packet to the STREAM Module. * We need to skip the TFTP Header. */ if (stream_write ((ptr_data + TFTPHEADER_SIZE), (num_bytes - TFTPHEADER_SIZE)) == 0) { /* Packet has been copied successfully into the STREAM Buffer. */ tftp_send_ack(); } else { /* Packet could not be copied; let the server retransmit the packet * because we did not send the ACK. */ } /* Determine if the TFTP file transfer is complete or not? * If the received number of bytes is less than the TFTP Data Size this * indicates that the transfer is successfully completed. */ if (num_bytes < (TFTP_DATA_SIZE + TFTPHEADER_SIZE)) { /* Successfully downloaded the file */ tftp_cleanup(); } break; } default: { /* Control comes here for ERROR, ACK and WRQ which are all indicate * failure. ERROR packet is the only expected failure which is mentioned * in the RFC. All other packets are violation of the RFC. Both these * cases are handled similarly. */ mprintf ("Error: TFTP Error Packet Received\n"); tftp_cleanup(); net_set_error(); /* Return Error. */ return -1; } } return 0; } /** * @b Description * @n * The function gets a file from the TFTP Server. The function * simply initiates the transfer. Successful completion of this * API does not gurantee that the file was downloaded. * * @param[in] server_ip * TFTP Server IP address from where the file is downloaded. * @param[in] filename * Name of the file to be downloaded. * * @retval * Success - 0 * @retval * Error - <0 */ Int32 tftp_get_file (IPN server_ip, Int8* filename) { SOCKET socket; Int32 index = 0; /* Basic Validations: Ensure the parameters passed are correct. */ if ((server_ip == 0) || (filename == NULL)) { /* Error: Invalid parameters passed. Stop the network boot module. */ net_set_error(); return -1; } /* Open the stream module. */ if (stream_open (TFTP_DATA_SIZE) < 0) { /* Error: Unable to open the stream device. */ net_set_error(); return -1; } /* Initialize the TFTP MCB at this stage... */ netMemset ((void *)&tftpmcb, 0, sizeof(TFTP_MCB)); /* Populate the socket structure and register this with the UDP module. */ socket.local_port = 1234; socket.remote_port = TFTP_SERVER_PORT; socket.remote_address = server_ip; socket.app_fn = tftp_receive; /* Open the TFTP Control socket. */ tftpmcb.sock = udp_sock_open (&socket); if (tftpmcb.sock < 0) { /* ERROR: UDP Socket could not be opened. */ stream_close(); net_set_error(); return -1; } /* Remember the parameters passed to the TFTP. */ tftpmcb.server_ip = server_ip; /* Copy the file name over... */ while (filename[index] != 0) { tftpmcb.filename[index] = filename[index]; index++; } /* Initialize the block number expected. */ tftpmcb.block_num = 1; /* Create the TFTP Read Request. */ index = tftp_create_read_req ((Uint8 *)filename); /* Initialize the TFTP Client state */ tftpmcb.state = READ_REQUEST; /* Initialize the TFTP Timer. */ tftpmcb.timer = timer_add (TFTP_TIMEOUT, tftp_timer_expiry); if (tftpmcb.timer < 0) { /* Error: TFTP Timer Creation Failed. TFTP is not operational. */ mprintf ("Error: TFTP Timer Creation Failed\n"); tftp_cleanup (); net_set_error(); return -1; } /* The packet has been populated; send it to the server. */ udp_sock_send (tftpmcb.sock, (Uint8 *)&tftpmcb.buffer[0], index); /* Send out the TFTP Read request. */ return 0; }