/** * @file stream.c * * @brief * The file implements the STREAM module. * * \par * NOTE: * (C) Copyright 2008, Texas Instruments, Inc. * * \par */ /********************************************************************** ************************** Local Structures ************************** **********************************************************************/ #include "types.h" #include "iblcfg.h" #include /** * @brief * The structure describes the Stream Master Control block. * * @details * The structure stores information about the stream module * internal buffers and state information. */ typedef struct STREAM_MCB { /** * @brief Flag which indicates if the stream buffer is open or not? */ Bool is_open; /** * @brief This is the *internal* stream buffer. */ Uint8 buffer[MAX_SIZE_STREAM_BUFFER]; /** * @brief This is the read index from where data is read. */ Int32 read_idx; /** * @brief This is the write index to which data is written. */ Int32 write_idx; /** * @brief This is the free size available in the internal buffer. */ Int32 free_size; }STREAM_MCB; /********************************************************************** ************************** Global Variables ************************** **********************************************************************/ /** * @brief This is the STREAM Master control block which keeps track * of all the stream module information. */ STREAM_MCB stream_mcb; /********************************************************************** ************************** Stream Functions ************************** **********************************************************************/ /** * @b Description * @n * The function is called to open the stream module * * @param[in] chunk_size * Maximum amount of data that can be received at any * instant by the boot module. * * @retval * Success - 0 * @retval * Error - <0 */ Int32 stream_open (Uint32 chunk_size) { /* Basic Validations: Ensure that the chunk size is not greater * than the internal buffer size. */ if (chunk_size > MAX_SIZE_STREAM_BUFFER) return -1; /* Initialize the Master control block. */ stream_mcb.is_open = TRUE; stream_mcb.read_idx = 0; stream_mcb.write_idx = 0; stream_mcb.free_size = MAX_SIZE_STREAM_BUFFER; /* Module has been initialized. */ return 0; } /** * @b Description * @n * The function is called to read data from the stream module. * * @param[in] ptr_data * Pointer to the data buffer where the data will be copied to. * @param[in] num_bytes * Number of bytes to be read. * * @retval * Success - Number of bytes actually read * @retval * Error - <0 */ Int32 stream_read (Uint8* ptr_data, Int32 num_bytes) { Int32 index; Int32 num_bytes_to_read; /* Determine the number of bytes which can be read. */ if (num_bytes > (MAX_SIZE_STREAM_BUFFER - stream_mcb.free_size)) { /* User has requested more data than what is available. In this case we * can return only what we have. */ num_bytes_to_read = (MAX_SIZE_STREAM_BUFFER - stream_mcb.free_size); } else { /* User has requested less data than what is available. In this case we * return only what the user wants. */ num_bytes_to_read = num_bytes; } /* There is data available copy it from the internal to the user supplied buffer. */ for (index = 0; index < num_bytes_to_read; index++) { /* Copy the data to the "write" index. */ *(ptr_data + index) = *(stream_mcb.buffer + stream_mcb.read_idx); /* Increment the read index. */ stream_mcb.read_idx = (stream_mcb.read_idx + 1) % MAX_SIZE_STREAM_BUFFER; } /* Once data has been copied; increment the free size accordingly */ stream_mcb.free_size = stream_mcb.free_size + num_bytes_to_read; /* Return the number of bytes read. */ return num_bytes_to_read; } /** * @b Description * @n * The function is called to write data to the stream * module. * * @param[in] ptr_data * Pointer to the data buffer which contains the data to be copied. * @param[in] num_bytes * Number of bytes being written * * @retval * Success - 0 * @retval * Error - <0 */ Int32 stream_write (Uint8* ptr_data, Int32 num_bytes) { Int32 index; /* Basic Validations: Ensure there is sufficient space to copy the data. */ if (num_bytes > stream_mcb.free_size) return -1; /* Basic Validations: Make sure the pointers are valid. */ if (ptr_data == NULL) return -1; /* There was sufficient space to copy the data lets do so but we copy byte by byte * since the internal buffer is circular and we can wrap around... */ for (index = 0; index < num_bytes; index++) { /* Copy the data to the "write" index. */ *(stream_mcb.buffer + stream_mcb.write_idx) = *(ptr_data + index); /* Increment the write index. */ stream_mcb.write_idx = (stream_mcb.write_idx + 1) % MAX_SIZE_STREAM_BUFFER; } /* Once data has been copied; decrement the free size accordingly */ stream_mcb.free_size = stream_mcb.free_size - num_bytes; return 0; } /** * @b Description * @n * The function is used to check if the stream buffers are empty or * not? * * @retval * Empty - TRUE * @retval * Not Empty - FALSE */ Bool stream_isempty (void) { /* Check the number of free bytes available? */ if (stream_mcb.free_size == MAX_SIZE_STREAM_BUFFER) return TRUE; /* There is data in the stream buffer; so its not empty. */ return FALSE; } /** * @b Description * @n * The function closes the stream module. * * @retval * Not Applicable. */ void stream_close (void) { /* The stream module is no longer open... */ stream_mcb.is_open = FALSE; return; } /** * @b Description * @n * The function initializes the stream module. * * @retval * Not Applicable. */ void stream_init (void) { /* Reset the memory contents. */ memset ((void *)&stream_mcb, 0, sizeof(STREAM_MCB)); /* Make sure we initialize the free size correctly. */ stream_mcb.free_size = MAX_SIZE_STREAM_BUFFER; return; }