/** * @file timer.c * * @brief * The file implements the TIMER module. * * \par * NOTE: * (C) Copyright 2008, Texas Instruments, Inc. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * * \par */ #include "types.h" #include "iblloc.h" #include "timer.h" #include "devtimer.h" #include "iblcfg.h" #include "timer_osal.h" #include /********************************************************************** *************************** LOCAL Structures ************************* **********************************************************************/ /** * @brief * The structure describes the Timer blocks. * * @details * Each timer in the system is associated with a timer * block. */ typedef struct TIMER_BLOCK { /** * @brief Expiration Routine which is called once the timer * expires. */ void (*expiry)(void); /** * @brief This is the original expiration time in milli-seconds. */ Uint32 org_timeout; /** * @brief This is the expiration time in milli-seconds. This is * decremented by the timer module. */ Uint32 timeout; }TIMER_BLOCK; /** * @brief * The structure describes the Timer Master Control Block. * * @details * The structure contains information about the Timer Master Control * block which stores information about the Timer Module. */ typedef struct TIMER_MCB { /** * @brief This keeps track of all timers which can exist in the * System. */ TIMER_BLOCK timer[MAX_TIMER_BLOCKS]; /** * @brief This is the number of active timers in the system. */ Uint32 num_active_timers; }TIMER_MCB; /********************************************************************** *************************** GLOBAL Variables ************************* **********************************************************************/ /** * @brief This global variable keeps track of all the timer which are * currently active in the system. */ TIMER_MCB timermcb; /********************************************************************** *************************** TIMER Functions ************************** **********************************************************************/ /** * @b Description * @n * The function initializes the Timer module. * * @retval * Not Applicable. */ void timer_init (void) { /* Initialize the Timer Master Control Block. */ timerMemset (&timermcb, 0, sizeof(TIMER_MCB)); return; } /** * @b Description * @n * The function creates a timer. * * @param[in] timeout * This is the timeout specified in milli-seconds after which the timer * will expire. * @param[in] expiry * Expiration routine which is called to indicate that the timer block * has expired. * * @retval * Success - Handle to the timer block * @retval * Error - <0 */ Int32 timer_add (Uint32 timeout, void (*expiry)(void)) { Uint16 index; /* Basic Validations: Ensure parameters passed are valid. */ if ((timeout == 0) || (expiry == NULL)) return -1; /* Cycle through and find a free timer block. */ for (index = 0; index < MAX_TIMER_BLOCKS; index++) { /* Free timers can be identified using the expiry routine. NULL indicates * that the timer block is free. */ if (timermcb.timer[index].expiry == NULL) { /* Found a free slot. Is this the first timer being created? */ if (timermcb.num_active_timers == 0) { /* YES. We need to start the device timer. */ if (dev_create_timer() < 0) { /* Device layer timer creation failed. We will not be able * to get the timers operational without this API. So we * might as well fail also. */ return -1; } } /* Populate the timer block structure. */ timermcb.timer[index].expiry = expiry; timermcb.timer[index].timeout = timeout; timermcb.timer[index].org_timeout = timeout; /* Increment the number of timers in the system */ timermcb.num_active_timers++; /* Return the handle to the timer block. */ return index; } } /* Control comes here indicating that there were no free timer slots. */ return -1; } /** * @b Description * @n * The function deletes a timer which was previously created. * * @param[in] handle * This is the handle to the timer block to be deleted. * * @retval * Not Applicable. */ void timer_delete (Int32 handle) { /* Basic Validations: Ensure paramter is valid. */ if ((handle < 0) || (handle > MAX_TIMER_BLOCKS)) return; /* Make sure there is at least one timer which is active; */ if (timermcb.num_active_timers > 0) { /* Simply reset the memory contents */ timerMemset ((void *)&timermcb.timer[handle], 0, sizeof(TIMER_BLOCK)); /* Decrement the number of active timers in the system */ timermcb.num_active_timers--; /* Check if there are any active timers in the system? */ if (timermcb.num_active_timers == 0) { /* No more active timers; we can delete the timer in the device layer. */ dev_delete_timer (); } } return; } /** * @b Description * @n * The function runs the timer scheduler. This API is required to be * called by the boot modules and this in turn will decrement the various * timer registered in the system and will call the appropriate * expiration routines. If the boot modules fail to call this API then * the timers will never expire. * * @retval * Not Applicable. */ void timer_run (void) { Uint16 index; /* Check if there are any active timers in the System or not? * If none are present; then we dont need to run the scheduler. */ if (timermcb.num_active_timers == 0) return; /* Check if the device timer has expired or not? * If the timer has not expired there is no management to be done. */ if (dev_check_timer() == FALSE) return; /* Cycle through all the timer blocks and update them. */ for (index = 0; index < MAX_TIMER_BLOCKS; index++) { /* Is this an active timer? */ if (timermcb.timer[index].expiry != NULL) { /* YES. Decrement the timeout. */ timermcb.timer[index].timeout = timermcb.timer[index].timeout - 100; /* Has the timer expired? */ if (timermcb.timer[index].timeout == 0) { /* Reset the timeouts */ timermcb.timer[index].timeout = timermcb.timer[index].org_timeout; /* Call the expiration routine. */ timermcb.timer[index].expiry(); } } } return; }