/****************************************************************************** * Copyright (c) 2010 Texas Instruments Incorporated - http://www.ti.com * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * *****************************************************************************/ /****************************************************************************** * * File Name: ecc.c * * Description: This file implements ECC algorithm used on micron NAND flash * * History: * SEP/4/2009, Amit Solanki, Created the file * *****************************************************************************/ /**************** * Include Files ****************/ #include "types.h" #include "ecc.h" /********************************* * Defines and Macros and globals *********************************/ // Pre-calculated 256-way 1 byte column parity static const Uint8 nand_ecc_precalc_table[] = { 0x00, 0x55, 0x56, 0x03, 0x59, 0x0c, 0x0f, 0x5a, 0x5a, 0x0f, 0x0c, 0x59, 0x03, 0x56, 0x55, 0x00, 0x65, 0x30, 0x33, 0x66, 0x3c, 0x69, 0x6a, 0x3f, 0x3f, 0x6a, 0x69, 0x3c, 0x66, 0x33, 0x30, 0x65, 0x66, 0x33, 0x30, 0x65, 0x3f, 0x6a, 0x69, 0x3c, 0x3c, 0x69, 0x6a, 0x3f, 0x65, 0x30, 0x33, 0x66, 0x03, 0x56, 0x55, 0x00, 0x5a, 0x0f, 0x0c, 0x59, 0x59, 0x0c, 0x0f, 0x5a, 0x00, 0x55, 0x56, 0x03, 0x69, 0x3c, 0x3f, 0x6a, 0x30, 0x65, 0x66, 0x33, 0x33, 0x66, 0x65, 0x30, 0x6a, 0x3f, 0x3c, 0x69, 0x0c, 0x59, 0x5a, 0x0f, 0x55, 0x00, 0x03, 0x56, 0x56, 0x03, 0x00, 0x55, 0x0f, 0x5a, 0x59, 0x0c, 0x0f, 0x5a, 0x59, 0x0c, 0x56, 0x03, 0x00, 0x55, 0x55, 0x00, 0x03, 0x56, 0x0c, 0x59, 0x5a, 0x0f, 0x6a, 0x3f, 0x3c, 0x69, 0x33, 0x66, 0x65, 0x30, 0x30, 0x65, 0x66, 0x33, 0x69, 0x3c, 0x3f, 0x6a, 0x6a, 0x3f, 0x3c, 0x69, 0x33, 0x66, 0x65, 0x30, 0x30, 0x65, 0x66, 0x33, 0x69, 0x3c, 0x3f, 0x6a, 0x0f, 0x5a, 0x59, 0x0c, 0x56, 0x03, 0x00, 0x55, 0x55, 0x00, 0x03, 0x56, 0x0c, 0x59, 0x5a, 0x0f, 0x0c, 0x59, 0x5a, 0x0f, 0x55, 0x00, 0x03, 0x56, 0x56, 0x03, 0x00, 0x55, 0x0f, 0x5a, 0x59, 0x0c, 0x69, 0x3c, 0x3f, 0x6a, 0x30, 0x65, 0x66, 0x33, 0x33, 0x66, 0x65, 0x30, 0x6a, 0x3f, 0x3c, 0x69, 0x03, 0x56, 0x55, 0x00, 0x5a, 0x0f, 0x0c, 0x59, 0x59, 0x0c, 0x0f, 0x5a, 0x00, 0x55, 0x56, 0x03, 0x66, 0x33, 0x30, 0x65, 0x3f, 0x6a, 0x69, 0x3c, 0x3c, 0x69, 0x6a, 0x3f, 0x65, 0x30, 0x33, 0x66, 0x65, 0x30, 0x33, 0x66, 0x3c, 0x69, 0x6a, 0x3f, 0x3f, 0x6a, 0x69, 0x3c, 0x66, 0x33, 0x30, 0x65, 0x00, 0x55, 0x56, 0x03, 0x59, 0x0c, 0x0f, 0x5a, 0x5a, 0x0f, 0x0c, 0x59, 0x03, 0x56, 0x55, 0x00 }; /****************************************************************************** * * Function: nandTransResult * * Description: Creates non-inverted ECC code from line parity * * Parameters: Uint8 uchReg2 - line parity reg 2 * Uint8 uchReg3 - line parity reg 3 * Uint8 *puchEccCode - ecc * * Return Value: void ******************************************************************************/ static void nandTransResult(Uint8 uchReg2, Uint8 uchReg3, Uint8 *puchEccCode) { Uint8 a, b, i, tmp1, tmp2; /* Initialize variables */ a = b = 0x80; tmp1 = tmp2 = 0; /* Calculate first ECC byte */ for (i = 0; i < 4; i++) { if (uchReg3 & a) /* LP15,13,11,9 --> ecc_code[0] */ tmp1 |= b; b >>= 1; if (uchReg2 & a) /* LP14,12,10,8 --> ecc_code[0] */ tmp1 |= b; b >>= 1; a >>= 1; } /* Calculate second ECC byte */ b = 0x80; for (i = 0; i < 4; i++) { if (uchReg3 & a) /* LP7,5,3,1 --> ecc_code[1] */ tmp2 |= b; b >>= 1; if (uchReg2 & a) /* LP6,4,2,0 --> ecc_code[1] */ tmp2 |= b; b >>= 1; a >>= 1; } /* Store two of the ECC bytes */ puchEccCode[0] = tmp1; puchEccCode[1] = tmp2; } /****************************************************************************** * * Function: eccComputeECC * * Description: Compute 3 byte ECC code for 256 byte block * * Parameters: Uint8* puchData - pointer to raw data * Uint8 *puchEccCode - pointer to ECC buffer * * Return Value: status ******************************************************************************/ Int32 eccComputeECC(const Uint8 *puchData, Uint8 *puchEccCode) { Uint8 uchIndex, uchReg1, uchReg2, uchReg3; int j; if(puchData == NULL || puchEccCode == NULL) return ECC_FAIL; /* Initialize variables */ uchReg1 = uchReg2 = uchReg3 = 0; puchEccCode[0] = puchEccCode[1] = puchEccCode[2] = 0; /* Build up column parity */ for(j = 0; j < 256; j++) { /* Get CP0 - CP5 from table */ uchIndex = nand_ecc_precalc_table[puchData[j]]; uchReg1 ^= (uchIndex & 0x3f); /* All bit XOR = 1 ? */ if (uchIndex & 0x40) { uchReg3 ^= (Uint8) j; uchReg2 ^= ~((Uint8) j); } } /* Create non-inverted ECC code from line parity */ nandTransResult(uchReg2, uchReg3, puchEccCode); /* Calculate final ECC code */ puchEccCode[0] = ~puchEccCode[0]; puchEccCode[1] = ~puchEccCode[1]; puchEccCode[2] = ((~uchReg1) << 2) | 0x03; return ECC_SUCCESS; } /****************************************************************************** * * Function: eccCorrectData * * Description: Detect and correct a 1 bit error for 256 byte block * * Parameters: Uint8* puchData - Raw data read from the chip * Uint8 *puchEccRead - ECC from the chip * Uint8 *puchEccCalc - ECC calculated from raw data * * Return Value: status ******************************************************************************/ Int32 eccCorrectData(Uint8 *puchData, Uint8 *puchEccRead, Uint8 *puchEccCalc) { Uint8 a, b, c, d1, d2, d3, add, bit, i; if(puchData == NULL || puchEccRead == NULL || puchEccCalc == NULL) return ECC_FAIL; /* Do error detection */ d1 = puchEccCalc[0] ^ puchEccRead[0]; d2 = puchEccCalc[1] ^ puchEccRead[1]; d3 = puchEccCalc[2] ^ puchEccRead[2]; if ((d1 | d2 | d3) == 0) { /* No errors */ return ECC_SUCCESS; } else { a = (d1 ^ (d1 >> 1)) & 0x55; b = (d2 ^ (d2 >> 1)) & 0x55; c = (d3 ^ (d3 >> 1)) & 0x54; /* Found and will correct single bit error in the data */ if ((a == 0x55) && (b == 0x55) && (c == 0x54)) { c = 0x80; add = 0; a = 0x80; for (i=0; i<4; i++) { if (d1 & c) add |= a; c >>= 2; a >>= 1; } c = 0x80; for (i=0; i<4; i++) { if (d2 & c) add |= a; c >>= 2; a >>= 1; } bit = 0; b = 0x04; c = 0x80; for (i=0; i<3; i++) { if (d3 & c) bit |= b; c >>= 2; b >>= 1; } b = 0x01; a = puchData[add]; a ^= (b << bit); puchData[add] = a; return ECC_SUCCESS; } else { i = 0; while (d1) { if (d1 & 0x01) ++i; d1 >>= 1; } while (d2) { if (d2 & 0x01) ++i; d2 >>= 1; } while (d3) { if (d3 & 0x01) ++i; d3 >>= 1; } if (i == 1) { /* ECC Code Error Correction */ puchEccRead[0] = puchEccCalc[0]; puchEccRead[1] = puchEccCalc[1]; puchEccRead[2] = puchEccCalc[2]; return ECC_SUCCESS; } else { /* Uncorrectable Error */ return ECC_FAIL; } } } } /* The number of bytes required for ecc */ Int32 eccNumBytes(void) { return (3); } /* The number of bytes each ECC covers */ Int32 eccBytesPerBlock (void) { return (256); }