/****************************************************************************** * Copyright (c) 2010 Texas Instruments Incorporated - http://www.ti.com * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * *****************************************************************************/ /****************************************************************************** * * File Name: gpio.c * * Description: This file contains the lower level function to access GPIO * * History: * JUL/22/2009, Amit Solanki, Created the file * SEP/01/2009, Amit Solanki, Updated the documentation * *****************************************************************************/ /**************** * Include Files ****************/ #include "types.h" #include "gpio.h" #include "target.h" /****************************************************************************** * * Function: hwGpioSetDirection * * Description: This function configures the specified GPIO's direction * * Parameters: uiNumber - GPIO number to configure * direction - GPIO_OUT or GPIO_IN * * Return Value: void * *****************************************************************************/ void hwGpioSetDirection( Uint32 uiNumber, GpioDirection direction ) { Uint32* puiGpioDir = ( Uint32*)GPIO_DIR_REG; if ( direction == GPIO_OUT ) *puiGpioDir = *puiGpioDir & ~(1 << uiNumber); // Set to OUTPUT else *puiGpioDir = *puiGpioDir | (1 << uiNumber); // Set to INTPUT } /****************************************************************************** * * Function: hwGpioSetDataBusDirection * * Description: This function configures the GPIO[7:0]'s direction * * Parameters: direction - GPIO_OUT or GPIO_IN * * Return Value: void * *****************************************************************************/ void hwGpioSetDataBusDirection( GpioDirection direction ) { Uint32* puiGpioDir = ( Uint32*)GPIO_DIR_REG; if ( direction == GPIO_OUT ) *puiGpioDir = *puiGpioDir & 0xffffff00; // Set to OUTPUT else *puiGpioDir = *puiGpioDir | 0x000000ff; // Set to INTPUT } /****************************************************************************** * * Function: hwGpioSetOutput * * Description: This function sets the specified GPIO's pin state to 1 * * Parameters: uiNumber - GPIO number to configure * * Return Value: void * * Pre-Condition: The specified GPIO should be configured as output * *****************************************************************************/ void hwGpioSetOutput( Uint32 uiNumber) { Uint32* puiGpioSet = (Uint32*) GPIO_SET_DATA_REG; *puiGpioSet = ( 1 << (uiNumber % 32) ); // Set to 1 } /****************************************************************************** * * Function: hwGpioClearOutput * * Description: This function Clears the specified GPIO's pin state to 0 * * Parameters: uiNumber - GPIO number to configure * * Return Value: void * * Pre-Condition: The specified GPIO should be configured as output * *****************************************************************************/ void hwGpioClearOutput( Uint32 uiNumber) { Uint32* puiGpioClear = (Uint32*) GPIO_CLEAR_DATA_REG; *puiGpioClear = ( 1 << (uiNumber % 32) ); // Clear to 0 } /****************************************************************************** * * Function: hwGpioReadInput * * Description: This function gets the specified GPIO's pin state * * Parameters: uiNumber - GPIO number to configure * * Return Value: Uint32 - Input state of GPIO if success * - else GPIO status * * Pre-Condition: The specified GPIO should be configured as input * *****************************************************************************/ Uint32 hwGpioReadInput( Uint32 uiNumber ) { Uint32* puiGpioInput = (Uint32*)GPIO_IN_DATA_REG; if(uiNumber > GPIO_MAX_NUMBER) return INVALID_GPIO_NUMBER; if( ( (*puiGpioInput >> uiNumber) & GPIO_HIGH) == GPIO_HIGH) return GPIO_HIGH; else return GPIO_LOW; } /****************************************************************************** * * Function: hwGpioWriteDataBus * * Description: This function sets the GPIO[7:0] pins state * * Parameters: uchValue - Value to set as output * * Return Value: void * * Pre-Condition: The GPIO[7:0] should be configured as output * *****************************************************************************/ void hwGpioWriteDataBus ( Uint8 uchValue ) { Uint32* puiGpioOutput = (Uint32*) GPIO_OUT_DATA_REG; *puiGpioOutput = ( (*puiGpioOutput & 0xffffff00) | uchValue ); } /****************************************************************************** * * Function: hwGpioClearDataBus * * Description: This function sets the value to the Clear data register * * Parameters: uchValue - Value to set as output * * Return Value: void * * Pre-Condition: None * *****************************************************************************/ void hwGpioClearDataBus(Uint8 uchValue) { Uint32* puiGpioOutput = (Uint32*) GPIO_CLEAR_DATA_REG; *puiGpioOutput = uchValue; } /****************************************************************************** * * Function: hwGpioSetDataBus * * Description: This function sets the value to the Set data register * * Parameters: uchValue - Value to set as output * * Return Value: void * * Pre-Condition: None * *****************************************************************************/ void hwGpioSetDataBus(Uint8 uchValue) { Uint32* puiGpioOutput = (Uint32*) GPIO_SET_DATA_REG; *puiGpioOutput = uchValue; } /****************************************************************************** * * Function: hwGpioReadDataBus * * Description: This function gets the GPIO[7:0] pins state * * Parameters: void * * Return Value: Uint8 - Input state of GPIO[7:0] * * Pre-Condition: The GPIO[7:0] should be configured as input * *****************************************************************************/ Uint8 hwGpioReadDataBus( void ) { Uint8* puchGpioInput = (Uint8*)GPIO_IN_DATA_REG; return *puchGpioInput; } /****************************************************************************** * * Function: hwGpioEnableGlobalInterrupt * * Description: This function Enables GPIO interrupts to CPU * * Parameters: void * * Return Value: void * *****************************************************************************/ void hwGpioEnableGlobalInterrupt( void ) { Uint32* puiGpioInterrupt = (Uint32*)GPIO_BINTEN_REG; *puiGpioInterrupt = 0x01; } /****************************************************************************** * * Function: hwGpioDisableGlobalInterrupt * * Description: This function Disables GPIO interrupts to CPU * * Parameters: void * * Return Value: void * *****************************************************************************/ void hwGpioDisableGlobalInterrupt( void ) { Uint32* puiGpioInterrupt = (Uint32*)GPIO_BINTEN_REG; *puiGpioInterrupt = 0x00; } /****************************************************************************** * * Function: hwGpioSetRisingEdgeInterrupt * * Description: This function sets specified GPIO's rising edge interrupt * * Parameters: uiNumber - GPIO number to configure * * Return Value: void * *****************************************************************************/ void hwGpioSetRisingEdgeInterrupt( Uint32 uiNumber ) { Uint32* puiGpioSetRisingEdge = (Uint32*)GPIO_SET_RIS_TRIG_REG; *puiGpioSetRisingEdge = (1 << uiNumber); } /****************************************************************************** * * Function: hwGpioClearRisingEdgeInterrupt * * Description: This function clears specified GPIO's rising edge interrupt * * Parameters: uiNumber - GPIO number to configure * * Return Value: void * *****************************************************************************/ void hwGpioClearRisingEdgeInterrupt( Uint32 uiNumber ) { Uint32* puiGpioClearRisingEdge = (Uint32*)GPIO_CLR_RIS_TRIG_REG; *puiGpioClearRisingEdge = (1 << uiNumber); } /****************************************************************************** * * Function: hwGpioSetFallingEdgeInterrupt * * Description: This function sets specified GPIO's falling edge interrupt * * Parameters: uiNumber - GPIO number to configure * * Return Value: void * *****************************************************************************/ void hwGpioSetFallingEdgeInterrupt( Uint32 uiNumber ) { Uint32* puiGpioSetFallingEdge = (Uint32*)GPIO_SET_FAL_TRIG_REG; *puiGpioSetFallingEdge = (1 << uiNumber); } /****************************************************************************** * * Function: hwGpioClearFallingEdgeInterrupt * * Description: This function clears specified GPIO's falling edge interrupt * * Parameters: uiNumber - GPIO number to configure * * Return Value: void * *****************************************************************************/ void hwGpioClearFallingEdgeInterrupt( Uint32 uiNumber ) { Uint32* puiGpioClearFallingEdge = (Uint32*)GPIO_CLR_FAL_TRIG_REG; *puiGpioClearFallingEdge = (1 << uiNumber); }