/******************************************************************************************************** * FILE PURPOSE: Config level PLL driver ******************************************************************************************************** * FILE NAME: cfgpll.c * * DESCRIPTION: The boot driver for PLLs that dont have a pll controller, but are controlled * by registers in config space. * *********************************************************************************************************/ #include "types.h" #include "target.h" #include "pllapi.h" #define DEVICE_REG32_W(x,y) *(volatile unsigned int *)(x)=(y) #define DEVICE_REG32_R(x) (*(volatile unsigned int *)(x)) #define BOOTBITMASK(x,y) ( ( ( ((UINT32)1 << (((UINT32)x)-((UINT32)y)+(UINT32)1) ) - (UINT32)1 ) ) << ((UINT32)y) ) #define BOOT_READ_BITFIELD(z,x,y) (((UINT32)z) & BOOTBITMASK(x,y)) >> (y) #define BOOT_SET_BITFIELD(z,f,x,y) (((UINT32)z) & ~BOOTBITMASK(x,y)) | ( (((UINT32)f) << (y)) & BOOTBITMASK(x,y) ) void pass_pll_delay (UINT32 del) { UINT32 i; volatile UINT32 j; for (i = j = 0; i < del; i++) asm (" nop "); } /********************************************************************************************************* * FUNCTION PURPOSE: Configure and enable a pll ********************************************************************************************************* * DESCRIPTION: The PLL is configured. If the existing configuration matches the requested one no * register write is made. *********************************************************************************************************/ SINT16 hwPllSetCfgPll (UINT32 base, UINT32 prediv, UINT32 mult, UINT32 postdiv, UINT32 chipFreqMhz, UINT32 pllFreqMhz) { UINT32 reg; UINT32 regb; UINT32 bwAdj; UINT16 currentPrediv; UINT16 currentMult; UINT16 currentPostdiv; UINT16 currentBypass; UINT16 currentBwAdj; UINT16 currentEnable; UINT16 currentClkOut; reg = DEVICE_REG32_R (base); regb = DEVICE_REG32_R (base + 4); currentPrediv = 1 + BOOT_READ_BITFIELD (reg, 5, 0); currentMult = 1 + BOOT_READ_BITFIELD (reg, 18, 6); currentPostdiv = 1 + BOOT_READ_BITFIELD (reg, 22, 19); currentBypass = BOOT_READ_BITFIELD (reg, 23, 23); currentBwAdj = 1 + BOOT_READ_BITFIELD (reg, 31, 24) + ((BOOT_READ_BITFIELD (regb, 3, 0)) << 8); currentEnable = BOOT_READ_BITFIELD(regb, 14, 14); currentClkOut = BOOT_READ_BITFIELD(regb, 13, 13); /* The PLL is currently enabled and connected if bypass == 0, enable == 1, clkout == 1 */ if ( (currentBypass == 0) && (currentPrediv == prediv) && (currentMult == mult) && (currentPostdiv == postdiv) && (currentEnable == 0) && (currentClkOut == 1) && (currentBwAdj == (mult >> 1)) ) return (0); /* bwAdj is based only on the mult value */ bwAdj = (mult >> 1) - 1; /* Write to the ENSAT bit */ regb = BOOT_SET_BITFIELD(regb, 1, 6, 6); DEVICE_REG32_W (base + 4, regb); /* Setup the PLL. Assert bypass */ reg = BOOT_SET_BITFIELD (reg, 1, 23, 23); /* Bypass must be enabled */ DEVICE_REG32_W (base, reg); /* Set bit 14 in register 1 to disable the PLL (assert reset) */ regb = BOOT_SET_BITFIELD(regb, 1, 14, 14); DEVICE_REG32_W (base + 4, regb); reg = BOOT_SET_BITFIELD (reg, prediv - 1, 5, 0); reg = BOOT_SET_BITFIELD (reg, mult - 1, 18, 6); reg = BOOT_SET_BITFIELD (reg, (bwAdj & 0xff), 31, 24); DEVICE_REG32_W (base, reg); /* The 4 MS Bits of bwadj */ regb = BOOT_SET_BITFIELD (regb, (bwAdj >> 8), 3, 0); DEVICE_REG32_W (base + 4, regb); /* Reset must be asserted for at least 5us */ pass_pll_delay(7000); /* Clear bit 14 in register 1 to re-enable the pll */ regb = BOOT_SET_BITFIELD(regb, 0, 14, 14); DEVICE_REG32_W (base + 4, regb); /* Wait for atleast 500 * REFCLK cycles * (PLLD+1) */ pass_pll_delay(70000); /* Disable the bypass */ reg = BOOT_SET_BITFIELD (reg, 0, 23, 23); /* The value 0 disables the bypass */ DEVICE_REG32_W (base, reg); return (0); } /* hwPllSetCfgPll */