/************************************************************************************* * FILE PURPOSE: Provide PLL control functions ************************************************************************************* * FILE NAME: pll.c * * DESCRIPTION: Provides functions to control the pll * *************************************************************************************/ #include "types.h" #include "ibl.h" #include "pllloc.h" #include "pllapi.h" #include "target.h" #define DEVICE_REG32_W(x,y) *(volatile unsigned int *)(x)=(y) #define DEVICE_REG32_R(x) (*(volatile unsigned int *)(x)) #define BOOTBITMASK(x,y) ( ( ( ((UINT32)1 << (((UINT32)x)-((UINT32)y)+(UINT32)1) ) - (UINT32)1 ) ) << ((UINT32)y) ) #define BOOT_READ_BITFIELD(z,x,y) (((UINT32)z) & BOOTBITMASK(x,y)) >> (y) #define BOOT_SET_BITFIELD(z,f,x,y) (((UINT32)z) & ~BOOTBITMASK(x,y)) | ( (((UINT32)f) << (y)) & BOOTBITMASK(x,y) ) typedef enum { HW_PLL_DO_NOT_ENABLE_PLL, HW_PLL_ENABLE_PLL } hwPllEnable_t; /********************************************************************************* * FUNCTION PURPOSE: Provide a delay loop ********************************************************************************* * DESCRIPTION: Generates a delay, units of cycles *********************************************************************************/ void hw_pll_delay (UINT32 del) { UINT32 i; volatile UINT32 j; for (i = j = 0; i < del; i++) asm (" nop "); } /* hw_pll_delay */ /********************************************************************************** * FUNCTION PURPOSE: Enables the pll to the specified multiplier ********************************************************************************** * DESCRIPTION: Sets up the pll **********************************************************************************/ SINT16 hwPllSetPll (UINT32 pllNum, UINT32 prediv, UINT32 mult, UINT32 postdiv) { UINT32 ctl, reg; UINT32 secctl; UINT32 status; UINT32 alnctl; UINT32 pmult; UINT32 pdiv; UINT32 pllBase; UINT32 i; SINT16 ret = 0; UINT32 pllm_min = 10, plld_min =0, outputdiv = 9; UINT32 div2=3, div5=5, div8=64; /* Mutliplier/divider values of 0 are invalid */ if (prediv == 0) prediv = 1; if (mult == 0) mult = 1; if (postdiv == 0) postdiv = 1; /* Get the base address of the pll */ pllBase = (UINT32) DEVICE_PLL_BASE(pllNum); /* Wait for Stabilization time (min 100 us) */ /* assuming max device speed, 1.4GHz, 1 cycle = 0.714 ns * * so, 100 us = 100000 ns = 140056 cycles */ hw_pll_delay (140056); /* Program pllen=0 (pll bypass), pllrst=1 (reset pll), pllsrc = 0 */ ctl = DEVICE_REG32_R (pllBase + PLL_REG_CTL); /* Check if PLL BYPASS is turned off previously */ secctl = DEVICE_REG32_R (pllBase + PLL_REG_SECCTL); if ( (secctl & PLL_REG_SECCTL_FIELD_BYPASS) != 0 ) { /* PLL BYPASS is turned on */ /* Set the ENSAT Bit */ /* Usage Note 9: For optimal PLL operation, the ENSAT bit in the PLL control * registers for the Main PLL, DDR3 PLL, and PA PLL should be set to 1. * The PLL initialization sequence in the silicon sets this bit to 0 and * could lead to non-optimal PLL operation. Software can set the bit to the * optimal value of 1 after boot */ reg = DEVICE_REG32_R (DEVICE_MAIN_PLL_CTL_1); reg = reg | (1 << 6); DEVICE_REG32_W (DEVICE_MAIN_PLL_CTL_1, reg); /* Clear the PLLENSRC bit */ ctl = ctl & ~(PLL_REG_CTL_FIELD_PLLENSRC); DEVICE_REG32_W (pllBase + PLL_REG_CTL, ctl); /* Clear the PLLEN bit */ ctl = ctl & ~(PLL_REG_CTL_FIELD_PLLEN); DEVICE_REG32_W (pllBase + PLL_REG_CTL, ctl); /* Wait for 4 Ref clocks */ /* The slowest clock can be at 25MHz, so min:160ns delay */ hw_pll_delay(225); /* Put the PLL in Bypass mode to perform the power down mode */ secctl = secctl | PLL_REG_SECCTL_FIELD_BYPASS; DEVICE_REG32_W (pllBase + PLL_REG_SECCTL, secctl); /* Advisory 8: Multiple PLLs May Not Lock After Power-on Reset Issue * In order to ensure proper PLL startup, the PLL power_down pin needs to be * toggled. This is accomplished by toggling the PLLPWRDN bit in the PLLCTL * register. This needs to be done before the main PLL initialization * sequence */ ctl = ctl | 2; DEVICE_REG32_W (pllBase + PLL_REG_CTL, ctl); /* Stay in a loop such that the bit is set for 5 µs (minimum) and * then clear the bit. */ hw_pll_delay (14005); /* waiting 10 us */ /* Power up the PLL */ ctl = ctl & ~2; DEVICE_REG32_W (pllBase + PLL_REG_CTL, ctl); } /* Assert PLL Reset */ ctl = ctl | (PLL_REG_CTL_FIELD_PLLRST); DEVICE_REG32_W (pllBase + PLL_REG_CTL, ctl); /* Program the necessary multipliers/dividers and BW adjustments * This routine will subtract 1 from the mult value */ pmult = chipPllExternalMult(pllNum, mult); pmult = pmult & PLL_REG_PLLM_FIELD_MULTm1; DEVICE_REG32_W (pllBase + PLL_REG_PLLM, pmult); /* set the BWADJ */ chipPllExternalBwAdj (pllNum, mult); /* Set the PLL Divider */ chipPllSetExternalPrediv(pllNum, prediv - 1); /* set the output divide */ secctl = BOOT_SET_BITFIELD(secctl, 1 & 0x000f, 22, 19); DEVICE_REG32_W (pllBase + PLL_REG_SECCTL, secctl); /* wait for the GOSTAT, but don't trap if lock is never read */ for (i = 0; i < 100; i++) { hw_pll_delay (300); status = DEVICE_REG32_R (pllBase + PLL_REG_PLLSTAT); if ( (status & PLL_REG_STATUS_FIELD_GOSTAT) == 0 ) break; } /* Enable the pll even if the lock failed. Return a warning. */ if (i == 100) ret = -1; /* Set PLL dividers if needed */ reg = 0x8000 | (div2 -1); DEVICE_REG32_W (pllBase + PLL_REG_DIV2, reg); reg = 0x8000 | (div5 -1); DEVICE_REG32_W (pllBase + PLL_REG_DIV5, reg); reg = 0x8000 | (div8 -1); DEVICE_REG32_W (pllBase + PLL_REG_DIV8, reg); /* Program ALNCTLn registers */ alnctl = DEVICE_REG32_R (pllBase + PLL_REG_ALNCTL); alnctl = alnctl | ((1 << 1) | (1 << 4) | (1 << 7)); DEVICE_REG32_W (pllBase + PLL_REG_ALNCTL, alnctl); /* Set GOSET bit in PLLCMD to initiate the GO operation to change the divide * * values and align the SYSCLKs as programmed */ reg = DEVICE_REG32_R (pllBase + PLL_REG_CMD); reg = reg | 1; DEVICE_REG32_W (pllBase + PLL_REG_CMD, reg); /* wait for the GOSTAT, but don't trap if lock is never read */ for (i = 0; i < 100; i++) { hw_pll_delay (300); status = DEVICE_REG32_R (pllBase + PLL_REG_PLLSTAT); if ( (status & PLL_REG_STATUS_FIELD_GOSTAT) == 0 ) break; } if (i == 100) ret = -1; /* Wait for a minimum of 7 us*/ hw_pll_delay (14006); /* Release PLL from Reset */ ctl = ctl & ~(PLL_REG_CTL_FIELD_PLLRST); DEVICE_REG32_W (pllBase + PLL_REG_CTL, ctl); /* Wait for PLL Lock time (min 50 us) */ hw_pll_delay (140056 >> 1); /* Clear the secondary controller bypass bit */ secctl = secctl & ~PLL_REG_SECCTL_FIELD_BYPASS; DEVICE_REG32_W (pllBase + PLL_REG_SECCTL, secctl); /* Set pllen to 1 to enable pll mode */ ctl = ctl | PLL_REG_CTL_FIELD_PLLEN; DEVICE_REG32_W (pllBase + PLL_REG_CTL, ctl); return (ret); } /* hwPllSetPll */