/****************************************************************************** * FILE PURPOSE: Boot TaBLe (btbl) processing file ****************************************************************************** * FILE NAME: btblpr.c * * DESCRIPTION: This file contains the main boot table processing state machine. * * For reference here is the Boot table format: * * (32-bit) Entry point byte address : Code Execution start address * (32-bit) Number of I/O Registers, delay and etc. * (32-bit) 1st Word for I/O Register configuration(optional) * ... * (32-bit) Nth Word for I/O Register configuration(optional) * (32-bit) Words for added delay in CPU cycles (optional) * (32-bit) Words for Core Start Vector (optional) * (32-bit) 1st code section byte count * (32-bit) 1st code section starting address in bytes * 1st section code byte * ... * (32-bit) Nth code section byte count * (32-bit) Nth code section starting address in bytes * Nth section code byte * ... * Last word of Nth section code type * (32-bit) Zero byte count * * Note1: Core start vector and added delay are special format of I/O Registers * 0xFFFF: NOP execution * 0xFFFE: core start vector * * Note2: There will be a padded byte added if the code section contains odd * number of bytes * * FUNCTION DESCRIPTION * -------- ----------- * * btblpr.c: * boot_init_boot_tbl_inst() Initialize the boot table control instance * boot_proc_boot_tbl() Boot Table main processing routine * boot_proc_boot_tbl_xxx() Boot Table procssing routine in xxx state * * (C) Copyright 2004, TELOGY Networks, Inc. *****************************************************************************/ /* types.h must be included before stdlib.h for splint to work */ #include "types.h" /* Ansi header files */ #include #include /* For memset() */ #include "btblwrap.h" #if 0 /* System utility files */ #include "tiboot.h" /* Main level */ #include "rmain.h" /* Device utilities */ #include "device.h" #endif /* Module specific file */ #include "btbl.h" #include "btblloc.h" /* Build specific Configuration */ #include "iblcfg.h" /******************************************************************************* * Private prototypes ******************************************************************************/ /* boot table processing state machine functions */ void boot_proc_boot_tbl_init(BOOT_TBL_CB_T* p_inst); void boot_proc_boot_tbl_io_cnt(BOOT_TBL_CB_T* p_inst); void boot_proc_boot_tbl_io_regs(BOOT_TBL_CB_T* p_inst); void boot_proc_boot_tbl_size(BOOT_TBL_CB_T* p_inst); void boot_proc_boot_tbl_addr(BOOT_TBL_CB_T* p_inst); void boot_proc_boot_tbl_data(BOOT_TBL_CB_T* p_inst); void boot_proc_boot_tbl_flush(BOOT_TBL_CB_T* p_inst); void boot_proc_boot_tbl_pad(BOOT_TBL_CB_T* p_inst); /******************************************************************************* * Local variables ******************************************************************************/ BOOT_TBL_CB_T btbl_inst; /* Boot table Control Instance */ /******************************************************************************* * DATA DEFINITION: Boot Table Processing State Machine ******************************************************************************/ BootTblProcFcn_t btbl_st_proc_fcn[BOOT_TBL_NUM_STATES]; /******************************************************************************* * FUNCTION PURPOSE: Process the boot table in Init State ******************************************************************************* * DESCRIPTION: Process the boot table in Init State * Record the entry point * * void boot_proc_boot_tbl_init ( * BOOT_TBL_CB_T *p_inst) - A pointer to Boot Table Control instance * *****************************************************************************/ void boot_proc_boot_tbl_init(BOOT_TBL_CB_T* p_inst) { if(p_inst->f_wait_lsw) { /* Process the entry point LSW */ p_inst->code_start_addr += (*p_inst->p_data & 0xFFFF); /* C55x boot tables contain an I/O space config. C6x boot tables * do not */ #ifdef BOOTCONFIG_NO_BTBL_IO p_inst->state = BOOT_TBL_STATE_SIZE; #else p_inst->state = BOOT_TBL_STATE_IO_CNT; #endif p_inst->f_wait_lsw = FALSE; } else { /* Process the entry point MSW */ p_inst->code_start_addr = ((UINT32)(*p_inst->p_data & 0xFFFF)) << 16; p_inst->f_wait_lsw = (bool)TRUE; } /* Update data buffer and counter */ p_inst->p_data++; p_inst->data_size_uint16--; } /******************************************************************************* * FUNCTION PURPOSE: Process the boot table in IO_CNT State ******************************************************************************* * DESCRIPTION: Process the boot table in IO_CNT State * Record the number of IO Registers * * void boot_proc_boot_tbl_io_cnt ( * BOOT_TBL_CB_T *p_inst) - A pointer to Boot Table Control instance * *****************************************************************************/ #ifndef BOOTCONFIG_NO_BTBL_IO void boot_proc_boot_tbl_io_cnt(BOOT_TBL_CB_T* p_inst) { if(p_inst->f_wait_lsw) { /* LSW processing */ p_inst->num_io_regs += (*p_inst->p_data & 0xFFFF); p_inst->f_wait_lsw = FALSE; if(p_inst->num_io_regs) { p_inst->state = BOOT_TBL_STATE_IO_REGS; } else { p_inst->state = BOOT_TBL_STATE_SIZE; } } else { /* MSW processing */ p_inst->num_io_regs = ((UINT32)(*p_inst->p_data & 0xFFFF)) << 16; p_inst->f_wait_lsw = TRUE; } /* Update data buffer and counter */ p_inst->p_data++; p_inst->data_size_uint16--; } #endif /******************************************************************************* * FUNCTION PURPOSE: Process the boot table in IO_REGS State ******************************************************************************* * DESCRIPTION: Process the boot table in IO_REG State * Process IO Register configuration * * void boot_proc_boot_tbl_io_regs ( * BOOT_TBL_CB_T *p_inst) - A pointer to Boot Table Control instance * *****************************************************************************/ #ifndef BOOTCONFIG_NO_BTBL_IO void boot_proc_boot_tbl_io_regs(BOOT_TBL_CB_T* p_inst) { UINT16 data; if(p_inst->f_wait_lsw) { /* LSW processing */ data = *p_inst->p_data; /* proess the IO register configuration based on its address (opcode) */ switch(p_inst->io_addr) { case BOOT_TBL_IO_CFG_DELAY: /* perform the delay loop requested */ chipDelay(data); break; case BOOT_TBL_IO_CFG_START_CORE: /* Verify whether the start_vector is valid */ if(data >= (BOOT_BIT_TO_MASK(chipReadNumCores()))) { BOOT_EXCEPTION(BOOT_ERROR_CODE(BOOT_MODULE_ID_BTBL, BTBL_ERR_INVALID_START_VECTOR)); } /* record the core start vector */ p_inst->core_start_vector = data; break; default: /* IO Configuration */ chipIoWrite(p_inst->io_addr, data); break; } p_inst->f_wait_lsw = FALSE; /* Is it the last IO Register to be configured */ if((--p_inst->num_io_regs) == 0) { p_inst->state = BOOT_TBL_STATE_SIZE; } } else { /* MSW processing */ p_inst->io_addr = *p_inst->p_data; p_inst->f_wait_lsw = TRUE; } /* Update data buffer and counter */ p_inst->p_data++; p_inst->data_size_uint16--; } #endif /******************************************************************************* * FUNCTION PURPOSE: Process the boot table in SIZE State ******************************************************************************* * DESCRIPTION: Process the boot table in SIZE State * Record the size of the new code section * perform end of table processing if size = 0 * * void boot_proc_boot_tbl_size ( * BOOT_TBL_CB_T *p_inst) - A pointer to Boot Table Control instance * *****************************************************************************/ void boot_proc_boot_tbl_size(BOOT_TBL_CB_T* p_inst) { if(p_inst->f_wait_lsw) { /* LSW processing */ p_inst->section_size_bytes += (*p_inst->p_data & 0xFFFF); /* Is it the end of the boot table */ if(p_inst->section_size_bytes == 0) { chipStartCore(p_inst->code_start_addr, (UINT32)p_boot_entry_addr, p_inst->core_start_vector); /* End of Boot table:Clear the instance */ p_inst->state = BOOT_TBL_STATE_FLUSH; p_inst->f_wait_lsw = FALSE; return; } p_inst->state = BOOT_TBL_STATE_ADDR; p_inst->f_wait_lsw = FALSE; /* Update statistics */ bootStats.btbl.num_sections++; } else { /* MSW processing */ p_inst->section_size_bytes = ((UINT32)(*p_inst->p_data & 0xFFFF)) << 16; p_inst->f_wait_lsw = (bool)TRUE; } /* Update data buffer and counter */ p_inst->p_data++; p_inst->data_size_uint16--; } /******************************************************************************* * FUNCTION PURPOSE: Process the boot table in ADDR State ******************************************************************************* * DESCRIPTION: Process the boot table in ADDR State * Record the start address of the new code section * * void boot_proc_boot_tbl_addr ( * BOOT_TBL_CB_T *p_inst) - A pointer to Boot Table Control instance * *****************************************************************************/ void boot_proc_boot_tbl_addr(BOOT_TBL_CB_T* p_inst) { if(p_inst->f_wait_lsw) { /* LSW processing */ p_inst->section_addr += (*p_inst->p_data & 0xFFFF); p_inst->state = BOOT_TBL_STATE_DATA; p_inst->f_wait_lsw = FALSE; } else { /* MSW processing */ p_inst->section_addr = ((UINT32)(*p_inst->p_data & 0xFFFF)) << 16; p_inst->f_wait_lsw = (bool)TRUE; } /* Update data buffer and counter */ p_inst->p_data++; p_inst->data_size_uint16--; } /******************************************************************************* * FUNCTION PURPOSE: Process the boot table in the PAD state ******************************************************************************* * DESCRIPTION: Toss data bytes to advance to the next section *******************************************************************************/ #define MIN(a,b) (a)<(b) ? (a) : (b) void boot_proc_boot_tbl_pad(BOOT_TBL_CB_T* p_inst) { UINT32 num_bytes; UINT32 num_uint16_words; num_bytes = MIN (p_inst->section_size_bytes, CHIP_UINT16_TO_BYTES(p_inst->data_size_uint16)); num_uint16_words = CHIP_BYTES_TO_UINT16(num_bytes); /* Update instance variables for the next code section */ p_inst->data_size_uint16 -= num_uint16_words; p_inst->p_data += num_uint16_words; p_inst->section_addr += num_bytes; p_inst->section_size_bytes -= num_bytes; if(p_inst->section_size_bytes == 0) { p_inst->state = BOOT_TBL_STATE_SIZE; /* Chip specific post block handling. Can be defined to an empty statement */ chipBtblBlockDone(); } } /******************************************************************************* * FUNCTION PURPOSE: Process the boot table in DATA State ******************************************************************************* * DESCRIPTION: Process the boot table in DATA State * Copy the received section data to the destination memory * locations * * void boot_proc_boot_tbl_data ( * BOOT_TBL_CB_T *p_inst) - A pointer to Boot Table Control instance * *****************************************************************************/ void boot_proc_boot_tbl_data(BOOT_TBL_CB_T* p_inst) { UINT32 num_bytes; /* number of bytes to be copy */ UINT32 num_uint16_words; /* number of 16 bit words to copy */ UINT32 num_uint16_words_pad; /* number of 16 bit words, rounded up to a multiple of 4 bytes */ UINT32 pad_uint16; /* The amount of pad present */ UINT16 error; num_bytes = MIN (p_inst->section_size_bytes, CHIP_UINT16_TO_BYTES(p_inst->data_size_uint16)); num_uint16_words = CHIP_BYTES_TO_UINT16(num_bytes); /* Some processors add padding to the memwidth used in the rom (created by tools) */ num_uint16_words_pad = chipAddBtblUint16Pad (num_uint16_words); pad_uint16 = num_uint16_words_pad - num_uint16_words; /* * Record the last UINT16 word and copy the data to the destination * locations */ if((error = coreCopyData(p_inst->section_addr, p_inst->p_data, num_bytes, p_inst->core_start_vector)) != CORE_NOERR) { /* Error Processing */ BOOT_EXCEPTION(BOOT_ERROR_CODE(BOOT_MODULE_ID_CHIP, error)); } /* Update instance variables for the next code section */ p_inst->data_size_uint16 -= num_uint16_words; p_inst->p_data += num_uint16_words; p_inst->section_addr += num_bytes; p_inst->section_size_bytes -= num_bytes; if(p_inst->section_size_bytes == 0) { if (pad_uint16) { p_inst->state = BOOT_TBL_STATE_PAD; p_inst->section_size_bytes = CHIP_UINT16_TO_BYTES(pad_uint16); } else { p_inst->state = BOOT_TBL_STATE_SIZE; /* Chip specific post block handling. Can be defined to an empty statement */ chipBtblBlockDone(); } } /* update statistics */ bootStats.btbl.num_pdma_copies++; } /******************************************************************************* * FUNCTION PURPOSE: Process the boot table in Flush State ******************************************************************************* * DESCRIPTION: Process the boot table in Flush State * We will enter this state when the end of table or error * condition occurs * set data_size to 0, i.e. ignore the reamining data * * void boot_proc_boot_tbl_error ( * BOOT_TBL_CB_T *p_inst) - A pointer to Boot Table Control instance * *****************************************************************************/ void boot_proc_boot_tbl_flush(BOOT_TBL_CB_T* p_inst) { p_inst->data_size_uint16 = 0; } /* ------------------- PUBLIC FUNCTIONS START HERE ----------------------- */ /******************************************************************************* * FUNCTION PURPOSE: Initialize the boot table control instance ******************************************************************************* * DESCRIPTION: Initialize and allocate the boot table control instance * Initialize all the variables to zero * Set the state to Init * * void boot_init_boot_tbl_inst ( void ) * * Note: only one instance is used at this moment * a free instance function will be needed when multiple instances are * supported * *****************************************************************************/ void boot_init_boot_tbl_inst(BOOT_TBL_CB_T *p_btbl_inst) { memset(p_btbl_inst, 0, sizeof(BOOT_TBL_CB_T)); p_btbl_inst->state = BOOT_TBL_STATE_INIT; /* * Set the core start vector to start core A only as its default value * in case the boot table does not contain the setting of the core * start vector. */ p_btbl_inst->core_start_vector = 1; /* Initialize the toot table processing function table */ btbl_st_proc_fcn[BOOT_TBL_STATE_INIT] = boot_proc_boot_tbl_init; #ifndef BOOTCONFIG_NO_BTBL_IO btbl_st_proc_fcn[BOOT_TBL_STATE_IO_CNT] = boot_proc_boot_tbl_io_cnt; btbl_st_proc_fcn[BOOT_TBL_STATE_IO_REGS] = boot_proc_boot_tbl_io_regs; #endif btbl_st_proc_fcn[BOOT_TBL_STATE_SIZE] = boot_proc_boot_tbl_size; btbl_st_proc_fcn[BOOT_TBL_STATE_ADDR] = boot_proc_boot_tbl_addr; btbl_st_proc_fcn[BOOT_TBL_STATE_DATA] = boot_proc_boot_tbl_data; btbl_st_proc_fcn[BOOT_TBL_STATE_PAD] = boot_proc_boot_tbl_pad; btbl_st_proc_fcn[BOOT_TBL_STATE_FLUSH] = boot_proc_boot_tbl_flush; } /* end of boot_init_boot_tbl_inst() */ /******************************************************************************* * FUNCTION PURPOSE: Process the boot table ******************************************************************************* * DESCRIPTION: Process the whole or partial boot table received by going * through the boot table processing state machine until all * the UINT16 words are processed or the end of table condition * (section size == 0) is satisfied. * * void boot_proc_boot_tbl ( * UINT16 *p_data, - 16-bit boot table content to be processed * UINT16 size) - number of 16-bit words * * * Note: It is up to the caller to reserve 4 16-bit word space in front of the * input buffer since the data may be moved to achieve 32-bit alignment * requirement for PDMA transfer *****************************************************************************/ void boot_proc_boot_tbl(BOOT_TBL_CB_T *p_btbl_inst, UINT16* p_data, UINT32 size) { /* Record the input data buffer and size */ p_btbl_inst->p_data = p_data; p_btbl_inst->data_size_uint16 = size; /* Optional: verify the inst state is valid */ if(p_btbl_inst->state > BOOT_TBL_LAST_STATE) { /* Error Processing */ BOOT_EXCEPTION(BOOT_ERROR_CODE(BOOT_MODULE_ID_BTBL, BTBL_ERR_INVALID_STATE)); } /* * Invoke the Boot table processing state machine until all the input * data are processed or the end of table condition is satified */ while (p_btbl_inst->data_size_uint16 != 0) { btbl_st_proc_fcn[p_btbl_inst->state](p_btbl_inst); } } /* end of boot_proc_boot_tbl() */