/************************************************************************************ * FILE PURPOSE: Wrapper for the TI boot table processor ************************************************************************************ * FILE NAME: btblwrap.c * * DESCRIPTION: The IBL wrapper for the boot table processor. * ************************************************************************************/ #include "types.h" #include "ibl.h" #include "iblloc.h" #include "btblwrap.h" #include "btbl.h" #include "btblloc.h" #include "iblbtbl.h" #include #include /* Globals used by the TI boot table processor */ BOOT_TBL_CB_T tiBootTable; bootStats_t bootStats; Uint32 btblEcode; Int32 btblWrapEcode; #define MIN(a,b) ((a) < (b)) ? (a) : (b) /************************************************************************************ * FUNCTION PURPOSE: The main boot wrapper for the TI boot table processor ************************************************************************************ * DESCRIPTION: Interfaces the IBL to the TI boot table driver. * The TI boot table driver operates in a push data mode, the * IBL operates in a pull data mode. This function pulls data * from the interface and pushes is to the TI driver. To do this * the internal state of the TI boot table driver is used * to determine how much data to pull. ************************************************************************************/ void iblBootBtbl (BOOT_MODULE_FXN_TABLE *bootFxn, Uint32 *entry_point) { Uint32 readSize; Uint32 blockSize; Uint32 blockSize16; Uint8 *data; Uint16 *data16; Uint16 t16; Int32 i, j; *entry_point = 0; btblEcode = 0; btblWrapEcode = 0; /* Initialize stats and btbl state */ memset (&bootStats, 0, sizeof(bootStats_t)); boot_init_boot_tbl_inst (&tiBootTable); data = malloc (TI_BTBL_BLOCK_SIZE); if (data == NULL) { btblWrapEcode = BTBL_WRAP_ECODE_MALLOC_FAIL; return; } data16 = (Uint16 *)data; while ((tiBootTable.state != BOOT_TBL_STATE_FLUSH) && (btblEcode == 0)) { switch (tiBootTable.state) { case BOOT_TBL_STATE_INIT: case BOOT_TBL_STATE_SIZE: case BOOT_TBL_STATE_ADDR: readSize = 4; break; case BOOT_TBL_STATE_DATA: readSize = tiBootTable.section_size_bytes; break; } while (readSize > 0) { blockSize = MIN(readSize, TI_BTBL_BLOCK_SIZE); blockSize16 = (blockSize + 1) >> 1; /* No recovery on block read failure */ if ((*bootFxn->read)(data, blockSize) < 0) { btblWrapEcode = BTBL_WRAP_ECODE_READ_FAIL; free (data); return; } /* The data has been read as a byte stream. This data must * be re-formatted as a 16 bit word stream */ for (j = i = 0; j < blockSize16; j++, i += 2) { t16 = (data[i+0] << 8) | data[i+1]; data16[j] = t16; } /* Process the block */ boot_proc_boot_tbl (&tiBootTable, data16, blockSize16); readSize = readSize - blockSize; } } if (btblEcode == 0) *entry_point = tiBootTable.code_start_addr; free (data); } /*********************************************************************************** * FUNCTION PURPOSE: Handle a fatal error from the boot table processor *********************************************************************************** * DESCRIPTION: The error code is stored. Processing is terminated * through the global ecode value. ***********************************************************************************/ void btblBootException (UINT32 ecode) { btblEcode = ecode; btblWrapEcode = BTBL_WRAP_ECODE_BTBL_FAIL; }