#ifndef BTBLWRAP_H #define BTBLWRAP_H /******************************************************************************** * FILE PURPOSE: Define the IBL wrapper for the TI boot table processor ******************************************************************************** * FILE NAM:E btblwrap.h * * DESCRIPTION: Definitions required for the IBL wrapper of the TI boot table * processor * ********************************************************************************/ /* chipStartCore does nothing, since multiple core start is not supported */ #define chipStartCore(x,y,z) /* A minimal boot stats structure */ typedef struct bootTblStats_s { UINT32 num_sections; UINT32 num_pdma_copies; } bootTblStats_t; typedef struct bootStats_s { bootTblStats_t btbl; } bootStats_t; extern bootStats_t bootStats; /**************************************************************************** * Definition: The c64x boot table tools will always pad boot table * entries to 32 bit elements. The boot table works in 16 bit * element sizes. If the size is not an even number of 16 bit * elements, add one word of padding. ****************************************************************************/ #define chipAddBtblUint16Pad(x) (((x)+1) & 0xfffffffe) /* Return values */ #define CORE_NOERR 0 /* Module number */ #define BOOT_MODULE_ID_CHIP 0 #define BOOT_MODULE_ID_BTBL 1 /* Error code creation */ #define BOOT_ERROR_CODE(modnum,errnum) (((modnum) << 16) | (errnum)) /* Fatal error handling */ #define BOOT_EXCEPTION btblBootException /* Macros */ #define CHIP_UINT16_TO_BYTES(x) ((x) << 1) #define CHIP_BYTES_TO_UINT16(x) (((x) + 1) >> 1) /* No interblock processing required */ #define chipBtblBlockDone() /* No tracing dummy function */ #define chipDummy(x) /* gem.c prototypes */ UINT16 coreCopyData (UINT32 dest_addr, UINT16 *p_data, UINT32 sizeBytes, UINT16 start_vector); /* btblwrap.c prototypes */ void btblBootException (UINT32 ecode); /* The block size allocated through malloc. Chosen to match the value defined * for the coff loader. malloc is used so the same heap section can be used. */ #define TI_BTBL_BLOCK_SIZE 0x4000 /* Read/Write 32bit values */ #define chipStoreWord(x,y) *(x) = (y) #define chipReadWord(x) *(x) /* Boot table wrapper error codes */ #define BTBL_WRAP_ECODE_MALLOC_FAIL 100 #define BTBL_WRAP_ECODE_READ_FAIL 101 #define BTBL_WRAP_ECODE_BTBL_FAIL 102 #define btblMemset iblMemset #endif /* BTBLWRAP_H */