/*************************************************************************** * FILENAME: cload.c * VERSION: 2.6 5/2/96 13:11:03 * SCCS ID: "@(#)cload.c 2.6 5/2/96" ***************************************************************************/ /******************************************************************************/ /* CLOAD.C - Generic COFF Loader Version 6.00 4/96 */ /******************************************************************************/ /* */ /* This module contains functions to read in and load a COFF object file. */ /* The following routines are defined here: */ /* */ /* cload() - Main driver for COFF loader. */ /* cload_headers() - Read in the various headers of the COFF file. */ /* cload_data() - Read in the raw data and load it into memory. */ /* cload_sect_data() - Read, relocate, and write out one section. */ /* cload_cinit() - Process one buffer of C initialization records. */ /* cload_symbols() - Read in the symbol table. */ /* cload_strings() - Read in the string table. */ /* str_free() - Free a string table. */ /* sym_read() - Read and relocate a symbol and its aux entry. */ /* sym_name() - Return a pointer to the name of a symbol. */ /* sym_add_name() - Add a symbol name to the string table. */ /* reloc_add() - Add a symbol to the relocation symbol table. */ /* relocate() - Perform a single relocation. */ /* reloc_read() - Read in and swap one relocation entry. */ /* reloc_size() - Return the field size of a relocation type. */ /* reloc_offset() - Return the field offset of a relocation type. */ /* reloc_stop() - Return the number of bits to read for a reloc type. */ /* sym_reloc_amount()- Return relocation amount for a relocation entry. */ /* unpack() - Extract a relocation field from object bytes. */ /* repack() - Encode a relocated field into object bytes. */ /* cload_lineno() - Read in & swap line number entries. */ /* swap4byte() - Swap the order of bytes in a int. */ /* swap2byte() - Swap the order of bytes in a short. */ /* */ /* The loader calls the following external functions to perform application */ /* specific tasks: */ /* */ /* set_reloc_amount() - Define relocation amounts for each section. */ /* mem_write() - Load a buffer of data into memory. */ /* lookup_sym() - Look up a symbol in an external symbol table. */ /* load_syms() - Build the symbol table for the application. */ /* load_msg() - Write diagnostic messages during loading. */ /* */ /******************************************************************************/ #include "header.h" #include "coff_trg.h" #if ((FILE_BASED) && !defined(FILE)) #include #endif /*----------------------------------------------------------------------------*/ /* CONSTANTS, MACROS, VARIABLES, AND STRUCTURES FOR THE LOADER. */ /*----------------------------------------------------------------------------*/ #define TRUE 1 #define FALSE 0 #define WORDSZ sizeof(T_DATA) /* SIZE OF DATA UNITS IN OBJ FILE */ #ifdef TMS320C60 extern int target_coff (unsigned short flags); #endif /*----------------------------------------------------------------------------*/ /* APPLICATION VARIABLES */ /*----------------------------------------------------------------------------*/ #if (FILE_BASED) FILE *fin; /* INPUT FILE */ #else extern unsigned char gRxBuffer[0x400040]; #endif int need_data = TRUE; /* APPLICATION NEEDS RAW DATA */ int need_symbols = FALSE; /* APPLICATION NEEDS SYMBOL TABLE */ int clear_bss = FALSE; /* CLEAR BSS SECTION */ /*----------------------------------------------------------------------------*/ /* FILL VALUES TO BE USED BY LOADERS */ /*----------------------------------------------------------------------------*/ #if defined(OTIS) extern int fill_bss; extern int fill_bss_value; #else #define fill_bss 0 #define fill_bss_value 0 #endif /*----------------------------------------------------------------------------*/ /* LOADER VARIABLES */ /*----------------------------------------------------------------------------*/ FILHDR file_hdr; /* FILE HEADER STRUCTURE */ int coff_version; /* COFF VERSION USED IN FILE */ AOUTHDR o_filehdr; /* OPTIONAL (A.OUT) FILE HEADER */ T_ADDR entry_point; /* ENTRY POINT OF MODULE */ T_ADDR *reloc_amount = NULL; /* AMOUNT OF RELOCATION PER SECTION */ char *sect_hdrs = NULL; /* ARRAY OF SECTION HEADERS */ char *o_sect_hdrs = NULL; /* ARRAY OF OLD COFF SECTION HEADERS */ int n_sections; /* NUMBER OF SECTIONS IN THE FILE */ int big_e_target; /* TARGET DATA IN BIG-ENDIAN FORMAT */ int byte_swapped; /* BYTE ORDERING OPPOSITE OF HOST */ int curr_sect; /* SECTION NUMBER CURRENTLY LOADING */ int load_err; /* ERROR CODE RETURNED IF LOADER FAILS*/ struct strtab *str_head = NULL; /* LIST OF STRING TABLE BUFFERS */ static T_SIZE init_size = 0; /* CURRENT SIZE OF C INITIALIZATION */ static int need_reloc; /* RELOCATION REQUIRED */ #if TMS320C60 int big_e_config = TRG_DEF_BIG_E; /* ENDIANNESS CONFIGURATION */ #else int big_e_config = DONTCARE; /* ENDIANNESS CONFIGURATION */ #endif /*----------------------------------------------------------------------------*/ /* THIS STRUCTURE IS USED TO STORE THE RELOCATION AMOUNTS FOR SYMBOLS. */ /* EACH RELOCATABLE SYMBOL HAS A CORRESPONDING ENTRY IN THIS TABLE. */ /* THE TABLE IS SORTED BY SYMBOL INDEX; LOOKUP USES A BINARY SEARCH. */ /*----------------------------------------------------------------------------*/ typedef struct { int rt_index; /* INDEX OF SYMBOL IN SYMBOL TABLE */ int rt_disp; /* AMOUNT OF RELOCATION */ } RELOC_TAB; /*----------------------------------------------------------------------------*/ /* THE RELOCATION SYMBOL TABLE IS ALLOCATED DYNAMICALLY, AND REALLOCATED */ /* AS MORE SPACE IS NEEDED. */ /*----------------------------------------------------------------------------*/ #define RELOC_TAB_START 128 /* STARTING SIZE OF TABLE */ #define RELOC_GROW_SIZE 128 /* REALLOC AMOUNT FOR TABLE */ static RELOC_TAB *reloc_tab = NULL; /* RELOCATION SYMBOL TABLE */ static int reloc_tab_size; /* CURRENT ALLOCATED AMOUNT */ static int reloc_sym_index; /* CURRENT SIZE OF TABLE */ /*----------------------------------------------------------------------------*/ /* RUN-TIME RELOCATION (AS OPPOSED TO LOAD-TIME) RELOCATION IS DETERMINED */ /* AS FOLLOWS: IF THE SECTION'S RUNTIME ADDRESS == LOADTIME ADDRESS, USE */ /* LOADTIME RELOCATION. OTHERWISE, ASSUME LOADTIME RELOC ONLY (RUNTIME RELOC */ /* == 0). */ /*----------------------------------------------------------------------------*/ #define RUN_RELOC_AMOUNT(i) ((SECT_HDR(i)->s_paddr == SECT_HDR(i)->s_vaddr) ? \ reloc_amount[i] : 0) /*----------------------------------------------------------------------------*/ /* DEFINE A STRUCTURE FOR STRING TABLE BUFFERS. THESE BUFFERS ARE STORED */ /* AS A LINKED LIST OF MEMORY PACKETS, EACH CONTAINING UP TO 64K OF THE */ /* STRING TABLE. */ /*----------------------------------------------------------------------------*/ typedef struct strtab { unsigned int size; /* SIZE OF THIS PACKET */ unsigned int offset; /* STARTING OFFSET OF THIS PACKET */ unsigned int index; /* AMOUNT CURRENTLY FILLED */ struct strtab *next; /* NEXT BUFFER */ char buf[1]; /* STRING DATA (EXPAND AS ALLOCATED) */ } STRTAB; #define MAX_STRING_ALLOC (unsigned int)(0xffff-sizeof(STRTAB)+1) /* MAX STRING BUFFER: 64K (SMALL HOSTS)*/ #define MIN_STRING_ALLOC 0x0400 /* MIN STRING BUFFER: 1K */ unsigned int unpack(); #define reloc_read(x) TRUE /* extern void mem_copy(unsigned char* dst, unsigned char* src, int nbytes); - defined in osal.h */ /******************************************************************************/ /* */ /* CLOAD() - Main driver for COFF loader. */ /* */ /******************************************************************************/ int cload() { int result; load_err = 0; result = cload_headers() && cload_data(); if (reloc_tab) free(reloc_tab); reloc_tab = NULL; if(result == TRUE) return 0; else return -1; } /******************************************************************************/ /* */ /* CLOAD_HEADERS() - Read in the various headers of the COFF file. */ /* */ /******************************************************************************/ int cload_headers() { int i; byte_swapped = FALSE; need_reloc = FALSE; #if FILE_BASED if (fseek(fin, 0L, 0) != 0 || !fread(&file_hdr, FILHSZ, 1, fin)) { load_err = E_FILE; return FALSE; } #else mem_copy((void*)&file_hdr, gRxBuffer, FILHSZ); #endif /*-------------------------------------------------------------------------*/ /* MAKE SURE THIS IS REALLY A COFF FILE. CHECK FOR SWAPPED FILES. */ /* DETERMINE BYTE ORDERING OF OBJECT DATA. */ /*-------------------------------------------------------------------------*/ if (!ISCOFF(file_hdr.f_magic)) { swap2byte(&file_hdr.f_magic); if (!ISCOFF(file_hdr.f_magic)) { load_err = E_MAGIC; return FALSE; } byte_swapped = TRUE; swap2byte(&file_hdr.f_nscns); swap4byte(&file_hdr.f_timdat); swap4byte(&file_hdr.f_symptr); swap4byte(&file_hdr.f_nsyms); swap2byte(&file_hdr.f_opthdr); swap2byte(&file_hdr.f_flags); #if COFF_VERSION_1 || COFF_VERSION_2 swap2byte(&file_hdr.f_target_id); #endif } /*-------------------------------------------------------------------------*/ /* DETERMINE THE ENDIANNESS OF THE COFF FILE, AND ENSURE THE ENDIANNESS OF */ /* THE FILE IS THE SAME AS THE TARGET, IF THERE IS A TARGET. */ /*-------------------------------------------------------------------------*/ big_e_target = ((file_hdr.f_flags & F_BIG) != 0); if (big_e_config != DONTCARE && big_e_target != big_e_config) { load_err = E_ENDIAN; return FALSE; } /*-------------------------------------------------------------------------*/ /* DETERMINE VERSION OF COFF BEING USED, CHECK TARGET ID IF NEEDED. */ /*-------------------------------------------------------------------------*/ if (ISCOFF_1(file_hdr.f_magic) || ISCOFF_2(file_hdr.f_magic)) { if (!ISMAGIC(file_hdr.f_target_id)) { load_err = E_MAGIC; return FALSE; } coff_version = file_hdr.f_magic; } else coff_version = COFF_MAGIC_0; #ifdef TMS320C60 /*-------------------------------------------------------------------------*/ /* DETERMINE WHETHER THE RIGHT COFF IS BEING LOADED */ /*-------------------------------------------------------------------------*/ if ( !target_coff( file_hdr.f_flags) ) { load_err = E_FILE; return FALSE; } #endif /*-------------------------------------------------------------------------*/ /* READ IN OPTIONAL HEADER, IF THERE IS ONE, AND SWAP IF NEEDED. */ /*-------------------------------------------------------------------------*/ if (file_hdr.f_opthdr == AOUTSZ) { #if FILE_BASED fseek(fin, (int)FILHSZ_IN(coff_version), 0); if (fread(&o_filehdr, file_hdr.f_opthdr, 1, fin) != 1) { load_err = E_FILE; return FALSE; } #else mem_copy((void*)&o_filehdr, &gRxBuffer[(int)FILHSZ_IN(coff_version)], file_hdr.f_opthdr); #endif if (byte_swapped) { swap2byte(&o_filehdr.magic); swap2byte(&o_filehdr.vstamp); swap4byte(&o_filehdr.tsize); swap4byte(&o_filehdr.dsize); swap4byte(&o_filehdr.bsize); swap4byte(&o_filehdr.entrypt); swap4byte(&o_filehdr.text_start); swap4byte(&o_filehdr.data_start); } entry_point = o_filehdr.entrypt; } /*-------------------------------------------------------------------------*/ /* Read in string table so that we can see long section names, if needed. */ /* This used tobe read right before the symbol table was read, but now the */ /* section headers use "flexname" method to specify section names and so */ /* might need access to a string table entry. */ /*-------------------------------------------------------------------------*/ //if (!cload_strings()) return FALSE; /*-------------------------------------------------------------------------*/ /* READ IN SECTION HEADERS. */ /*-------------------------------------------------------------------------*/ if (sect_hdrs) { free(sect_hdrs); sect_hdrs = NULL; } if (o_sect_hdrs) { free(o_sect_hdrs); o_sect_hdrs = NULL; } if (!(sect_hdrs = (char *)malloc((n_sections = file_hdr.f_nscns) * SCNHSZ))) { load_err = E_ALLOC; return FALSE; } #if FILE_BASED fseek(fin, (int)FILHSZ_IN(coff_version) + file_hdr.f_opthdr, 0); #endif /*-------------------------------------------------------------------------*/ /* Depending on which version of COFF we are reading, set up the section */ /* headers or s copy that we can translate into the new version. */ /*-------------------------------------------------------------------------*/ if (ISCOFF_2(coff_version)) { #if FILE_BASED if (fread(sect_hdrs,SCNHSZ_IN(coff_version),n_sections,fin) != n_sections) { load_err = E_FILE; return FALSE; } #else mem_copy((void*)sect_hdrs, &gRxBuffer[(int)FILHSZ_IN(coff_version) + file_hdr.f_opthdr], SCNHSZ_IN(coff_version)*n_sections ); #endif } else { if (!(o_sect_hdrs = (char *)malloc(n_sections * SCNHSZ_IN(coff_version)))) { load_err = E_ALLOC; return FALSE; } #if FILE_BASED if (fread(o_sect_hdrs,SCNHSZ_IN(coff_version),n_sections,fin)!=n_sections) { load_err = E_FILE; return FALSE; } #else mem_copy((void*)o_sect_hdrs, &gRxBuffer[(int)FILHSZ_IN(coff_version) + file_hdr.f_opthdr], SCNHSZ_IN(coff_version)*n_sections ); #endif } if (reloc_amount) free(reloc_amount); if (!(reloc_amount = (T_ADDR*)malloc(n_sections * sizeof(T_ADDR)))) { load_err = E_ALLOC; return FALSE; } /*-------------------------------------------------------------------------*/ /* SWAP SECTION HEADERS IF REQUIRED. */ /*-------------------------------------------------------------------------*/ for (i = 0; i < n_sections; i++) { SCNHDR *sptr = SECT_HDR(i); O_SCNHDR *tptr = O_SECT_HDR(i); if (byte_swapped) { /*-----------------------------------------------------------------*/ /* Swap sections according to native COFF version. */ /*-----------------------------------------------------------------*/ if (ISCOFF_2(coff_version)) { if (sptr->s_zeroes == 0L) swap4byte(&sptr->s_offset); swap4byte(&sptr->s_paddr); swap4byte(&sptr->s_vaddr); swap4byte(&sptr->s_size); swap4byte(&sptr->s_scnptr); swap4byte(&sptr->s_relptr); swap4byte(&sptr->s_lnnoptr); swap4byte(&sptr->s_nreloc); swap4byte(&sptr->s_nlnno); swap4byte(&sptr->s_flags); /* s_mwidth - single byte */ /* s_reserved - single byte */ swap2byte(&sptr->s_page); } else { swap4byte(&tptr->os_paddr); swap4byte(&tptr->os_vaddr); swap4byte(&tptr->os_size); swap4byte(&tptr->os_scnptr); swap4byte(&tptr->os_relptr); swap4byte(&tptr->os_lnnoptr); swap2byte(&tptr->os_nreloc); swap2byte(&tptr->os_nlnno); swap2byte(&tptr->os_flags); /* os_reserved - one byte */ /* os_page - one byte */ } } /*---------------------------------------------------------------------*/ /* Old COFF version section headers are now ready to be transferred. */ /*---------------------------------------------------------------------*/ if (!ISCOFF_2(coff_version)) { strn_copy(sptr->s_name, tptr->os_name, SYMNMLEN); sptr->s_paddr = tptr->os_paddr; sptr->s_vaddr = tptr->os_vaddr; sptr->s_size = tptr->os_size; sptr->s_scnptr = tptr->os_scnptr; sptr->s_relptr = tptr->os_relptr; sptr->s_lnnoptr = tptr->os_lnnoptr; sptr->s_nreloc = tptr->os_nreloc; sptr->s_nlnno = tptr->os_nlnno; sptr->s_flags = tptr->os_flags; sptr->s_page = tptr->os_page; } reloc_amount[i] = 0; #if 0 // not to search the string table /*---------------------------------------------------------------------*/ /* Fix up section name if it is a pointer into the string table. */ /*---------------------------------------------------------------------*/ if (sptr->s_zeroes == 0L) { STRTAB *packet = str_head; if (packet == NULL) { return -1; } if (str_head->offset > sptr->s_offset) { return -1; } while (sptr->s_offset < (int)packet->offset) packet = packet->next; sptr->s_nptr = packet->buf + (sptr->s_offset - packet->offset); } #endif } // for ends /*-------------------------------------------------------------------------*/ /* CALL AN EXTERNAL ROUTINE TO DETERMINE THE RELOCATION AMOUNTS FOR */ /* EACH SECTION. */ /*-------------------------------------------------------------------------*/ if (!set_reloc_amount()) { load_err = E_SETRELOC; return FALSE; } for (i = 0; i < n_sections; i++) need_reloc |= (reloc_amount[i] != 0); if (!need_data) need_reloc = FALSE; if (need_reloc && (file_hdr.f_flags & F_RELFLG)) { load_err = E_RELOC; return FALSE; } return TRUE; } /******************************************************************************/ /* */ /* CLOAD_DATA() - Read in the raw data and load it into memory. */ /* */ /******************************************************************************/ int cload_data() { int ok = TRUE; if (!need_data) return TRUE; /*-------------------------------------------------------------------------*/ /* LOOP THROUGH THE SECTIONS AND LOAD THEM ONE AT A TIME. */ /*-------------------------------------------------------------------------*/ for (curr_sect = 0; curr_sect < n_sections && ok; curr_sect++) { SCNHDR *sptr = SECT_HDR(curr_sect); char *sname = (sptr->s_zeroes == 0L) ? sptr->s_nptr : SNAMECPY(sptr->s_name); /*----------------------------------------------------------------------*/ /* IF THIS IS THE TEXT SECTION, RELOCATE THE ENTRY POINT. */ /*----------------------------------------------------------------------*/ if ((sptr->s_flags & STYP_TEXT) && !str_comp(sname, ".text")) entry_point += RUN_RELOC_AMOUNT(curr_sect); /*----------------------------------------------------------------------*/ /* IGNORE EMPTY SECTIONS OR SECTIONS WHOSE FLAGS INDICATE THE */ /* SECTION IS NOT TO BE LOADED. IF THE CLEAR_BSS FLAG IS SET, BSS */ /* IS "LOADED" EVEN THOUGH IT HAS NO DATA, AND DEFER THE CINIT */ /* SECTION UNTIL LATER TO ENSURE BSS IS LOADED FIRST. */ /*----------------------------------------------------------------------*/ if ((sptr->s_scnptr || ((clear_bss || fill_bss) && IS_BSS(sptr))) && (sptr->s_size) && !(sptr->s_flags & (STYP_DSECT | STYP_COPY | STYP_NOLOAD))) ok &= cload_sect_data(sptr); } /*-------------------------------------------------------------------------*/ /* WE DEFERRED CINIT, LOAD IT/THEM NOW. */ /*-------------------------------------------------------------------------*/ for (curr_sect = 0; curr_sect < n_sections && ok; curr_sect++) { SCNHDR *sptr = SECT_HDR(curr_sect); char *sname = (sptr->s_zeroes == 0L) ? sptr->s_nptr : SNAMECPY(sptr->s_name); if (IS_CINIT(sptr)) { ok &= cload_sect_data(sptr); } } return ok; } /******************************************************************************/ /* */ /* CLOAD_SECT_DATA() - Read, relocate, and write out the data for one section.*/ /* */ /******************************************************************************/ int cload_sect_data(SCNHDR *sptr) { T_ADDR addr = sptr->s_vaddr; /* CURRENT ADDRESS IN SECTION */ unsigned int nbytes; /* BYTE COUNT WITHIN SECTION */ int packet_size = 0; /* SIZE OF CURRENT DATA BUFFER */ int excess = 0; /* BYTES LEFT FROM PREVIOUS BUFFER */ unsigned int n_reloc = 0; /* COUNTER FOR RELOCATION ENTRIES */ RELOC reloc; /* RELOCATION ENTRY */ int relsz = RELSZ_IN(coff_version); unsigned char *packet = NULL; /* LOAD BUFFER */ unsigned int section_length = (unsigned int)LOCTOBYTE(sptr->s_size); unsigned int buffer_size = LOADBUFSIZE; #if defined (UNBUFFERED) && UNBUFFERED /*-------------------------------------------------------------------------*/ /* IF UNBUFFERED, THEN SET SIZE TO SECTION LENGTH ROUNDED UP TO MULTIPLE */ /* 32 BYTES. WE MAINTAIN A MINIMIUM OF LOADBUFSIZE IN THE EVENT SOMEONE */ /* CONTINUES TO USE THAT MACRO AS A SIZE LIMIT. */ /*-------------------------------------------------------------------------*/ buffer_size = MAX(buffer_size, (section_length + 32) & ~31ul); #endif /*-------------------------------------------------------------------------*/ /* ENSURE LOADBUFSIZE IS A MULTIPLE OF 2 */ /*-------------------------------------------------------------------------*/ if (LOADBUFSIZE % 2) { return -1; } /*-------------------------------------------------------------------------*/ /* READ THE FIRST RELOCATION ENTRY, IF THERE ARE ANY. */ /* IF THIS IS A BSS SECTION, CLEAR THE LOAD BUFFER. */ /*-------------------------------------------------------------------------*/ #if FILE_BASED if (need_reloc && sptr->s_nreloc && (fseek(fin, sptr->s_relptr, 0) != 0 || !reloc_read(&reloc))) { load_err = E_FILE; return FALSE; } #else // need_reloc is not used.... if (need_reloc && sptr->s_nreloc && !reloc_read(&reloc, sptr->s_relptr)) { load_err = E_FILE; return FALSE; } #endif /*-------------------------------------------------------------------------*/ /* ALLOCATE THE PACKET BUFFER */ /*-------------------------------------------------------------------------*/ packet = (unsigned char *) malloc(buffer_size); if (!packet) { load_err = E_ALLOC; return FALSE; } #ifdef OTIS if (IS_BSS(sptr)) { TRG_MVAL filval = fill_bss_value; free (packet); if (!mem_fill(filval, LOCTOBYTE(sptr->s_size), addr, sptr->s_page)) { load_err = E_MEMWRITE; return FALSE; } return TRUE; } #else /*-------------------------------------------------------------------------*/ /* Always want to clear memory for cases where memsize is not a multiple */ /* of the data size being written out. If we do not clear the array, the */ /* last byte or so can be corrupted with data from the last buffer read. */ /*-------------------------------------------------------------------------*/ for (nbytes = 0; nbytes < buffer_size; ++nbytes) packet[nbytes] = 0; #endif /*-------------------------------------------------------------------------*/ /* COPY ALL THE DATA IN THE SECTION. */ /*-------------------------------------------------------------------------*/ for (nbytes = 0; nbytes < section_length; nbytes += packet_size) { int j; /*----------------------------------------------------------------------*/ /* READ IN A BUFFER OF DATA. IF THE PREVIOUS RELOCATION SPANNED */ /* ACROSS THE END OF THE LAST BUFFER, COPY THE LEFTOVER BYTES INTO */ /* THE BEGINNING OF THE NEW BUFFER. */ /*----------------------------------------------------------------------*/ for (j = 0; j < excess; ++j) packet[j] = packet[packet_size + j]; packet_size = (int)MIN(LOCTOBYTE(sptr->s_size) - nbytes, buffer_size); if (sptr->s_scnptr) #if FILE_BASED if ((fseek(fin, sptr->s_scnptr + (int)(nbytes + excess), 0) != 0) || (fread(packet + excess, packet_size - excess, 1, fin) != 1)) { load_err = E_FILE; free (packet); return FALSE; } #else mem_copy((void*)(packet + excess), (void*)&gRxBuffer[sptr->s_scnptr + (int)(nbytes + excess)], packet_size - excess); #endif excess = 0; /*----------------------------------------------------------------------*/ /* Clear out end of packet in case we write padding. */ /*----------------------------------------------------------------------*/ if (excess + packet_size < buffer_size) for(j = excess + packet_size; j < buffer_size; j++) packet[j] = 0; /*----------------------------------------------------------------------*/ /* READ AND PROCESS ALL THE RELOCATION ENTRIES THAT AFFECT DATA */ /* CURRENTLY IN THE BUFFER. */ /*----------------------------------------------------------------------*/ if (need_reloc) while (n_reloc < sptr->s_nreloc && (T_ADDR)reloc.r_vaddr < addr + BYTETOLOC(packet_size)) { int i = (int)LOCTOBYTE(reloc.r_vaddr - addr); /* BYTE NDX */ int fieldsz = reloc_size(reloc.r_type); /* IN BITS */ int wordsz = MAX(fieldsz, reloc_stop(reloc.r_type)); /* IN BITS */ /*----------------------------------------------------------------*/ /* IF THIS RELOCATION SPANS PAST THE END OF THE BUFFER, */ /* SET 'EXCESS' TO THE NUMBER OF REMAINING BYTES AND FLUSH THE */ /* BUFFER. AT THE NEXT FILL, THESE BYTES WILL BE COPIED FROM */ /* THE END OF THE BUFFER TO THE BEGINNING AND THEN RELOCATED. */ /*----------------------------------------------------------------*/ if (i + (wordsz >> 3) > packet_size) { i -= i % LOADWORDSIZE; /* DON'T BREAK WITHIN A WORD */ excess = packet_size - i; packet_size = i; break; } /*----------------------------------------------------------------*/ /* PERFORM THE RELOCATION AND READ IN THE NEXT RELOCATION ENTRY. */ /*----------------------------------------------------------------*/ #if 0 if (!relocate(&reloc, packet + i, curr_sect)) { free (packet); return FALSE; } #endif #if FILE_BASED if (n_reloc++ < sptr->s_nreloc && (fseek(fin, sptr->s_relptr + ((int)n_reloc * relsz), 0) != 0 || !reloc_read(&reloc))) #else if (n_reloc++ < sptr->s_nreloc && !reloc_read(&reloc, sptr->s_relptr + ((int)n_reloc * relsz))); #endif { load_err = E_FILE; free (packet); return FALSE; } } /*----------------------------------------------------------------------*/ /* WRITE OUT THE RELOCATED DATA TO THE TARGET DEVICE. IF THIS IS A */ /* CINIT SECTION, CALL A SPECIAL FUNCTION TO HANDLE IT. */ /*----------------------------------------------------------------------*/ if (!(IS_CINIT(sptr) ? cload_cinit(packet, &packet_size, &excess) : (int) mem_write(packet, packet_size, addr + reloc_amount[curr_sect], sptr->s_page))) { load_err = E_MEMWRITE; free (packet); return FALSE; } /*----------------------------------------------------------------------*/ /* KEEP TRACK OF THE ADDRESS WITHIN THE SECTION. */ /*----------------------------------------------------------------------*/ addr += BYTETOLOC(packet_size); } free (packet); return TRUE; } /******************************************************************************/ /* */ /* CLOAD_CINIT() - Process one buffer of C initialization records. */ /* */ /******************************************************************************/ int cload_cinit(unsigned char *packet, int *packet_size, int *excess) { int i; /* BYTE COUNTER */ int init_packet_size; /* SIZE OF CURRENT INITIALIZATION */ static T_ADDR init_addr; /* ADDRESS OF CURRENT INITIALIZATION */ int bss_page = 0; /* BSS SECTION PAGE NUMBER */ /*-------------------------------------------------------------------------*/ /* FIND THE BSS SECTION ASSOCIATED WITH THE THE CINIT SECTION CURRENTLY */ /* BEING LOADED. */ /*-------------------------------------------------------------------------*/ for (i = 0; i < n_sections; ++i) if (IS_BSS(SECT_HDR(i))) { bss_page = SECT_HDR(i)->s_page; break; } /*-------------------------------------------------------------------------*/ /* PROCESS ALL THE INITIALIZATION RECORDS IN THE BUFFER. */ /*-------------------------------------------------------------------------*/ for (i = 0; i < *packet_size; i += init_packet_size) { /*----------------------------------------------------------------------*/ /* IF STARTING A NEW INITIALIZATION, READ THE SIZE AND ADDRESS FROM */ /* THE TABLE. */ /*----------------------------------------------------------------------*/ if (init_size == 0) { T_SIZE temp; int align; /*-------------------------------------------------------------------*/ /* POSITION THE BYTE INDEX ON THE NEXT INIT RECORD. */ /*-------------------------------------------------------------------*/ if (align = (i % INIT_ALIGN)) i += (INIT_ALIGN - align); /*-------------------------------------------------------------------*/ /* IF THE SIZE AND ADDRESS ARE NOT FULLY CONTAINED IN THIS BUFFER, */ /* STOP HERE. SET THE 'EXCESS' COUNTER TO THE NUMBER OF UNPROCESSED */ /* BYTES - THESE WILL BE COPIED TO THE HEAD OF THE NEXT BUFFER. */ /*-------------------------------------------------------------------*/ if ((int)(i + sizeof(T_SIZE)) > *packet_size) { *excess += *packet_size - i; *packet_size = i; break; } /*-------------------------------------------------------------------*/ /* IF THE NEXT SIZE FIELD IS ZERO, BREAK. */ /*-------------------------------------------------------------------*/ temp = unpack(packet + i, sizeof(T_SIZE)*8, sizeof(T_SIZE)*8, 0); if (temp == 0) break; /*-------------------------------------------------------------------*/ /* READ THE ADDRESS FIELD ,IF IT'S ALL HERE. */ /*-------------------------------------------------------------------*/ if ((int)(i + sizeof(T_SIZE) + sizeof(T_IADDR)) > *packet_size) { *excess += *packet_size - i; *packet_size = i; break; } i += sizeof(T_SIZE); init_size = temp; init_addr = unpack(packet+i,sizeof(T_IADDR)*8,sizeof(T_IADDR)*8,0); i += sizeof(T_IADDR); } /*----------------------------------------------------------------------*/ /* WRITE OUT THE CURRENT PACKET, UP TO THE END OF THE BUFFER. */ /*----------------------------------------------------------------------*/ if (init_packet_size = MIN(*packet_size-i, (int)(init_size * INIT_WSIZE))) { if (!mem_write(packet + i, init_packet_size, init_addr, bss_page)) return FALSE; init_addr += BYTETOLOC(init_packet_size); init_size -= init_packet_size / INIT_WSIZE; } } return TRUE; } #if 0 /******************************************************************************/ /* */ /* CLOAD_SYMBOLS() - Read in the symbol table. */ /* */ /******************************************************************************/ int cload_symbols() { SYMENT sym; AUXENT aux; int first, next; if (file_hdr.f_nsyms == 0 || (!need_symbols && !need_reloc)) return TRUE; /*------------------------------------------------------------------------*/ /* ALLOCATE THE RELOCATION SYMBOL TABLE. */ /*------------------------------------------------------------------------*/ if (need_reloc) { reloc_sym_index = 0; reloc_tab_size = MIN(RELOC_TAB_START, (int)file_hdr.f_nsyms); if (!(reloc_tab = (RELOC_TAB *)malloc(reloc_tab_size*sizeof(RELOC_TAB)))) { load_err = E_ALLOC; return FALSE; } } /*------------------------------------------------------------------------*/ /* IF THE APPLICATION NEEDS THE SYMBOL TABLE, LET IT READ IT IN. */ /* PASS NEED_RELOC TO THE APPLICATION SO THAT IT CAN CALL RELOC_ADD(). */ /*------------------------------------------------------------------------*/ if (need_symbols) { if (load_syms(need_reloc)) return TRUE; else { load_err = E_SYM; return FALSE; } } /*------------------------------------------------------------------------*/ /* READ THE SYMBOL TABLE AND BUILD THE RELOCATION SYMBOL TABLE */ /* FOR SYMBOLS THAT CAN BE USED IN RELCOATION, STORE THEM IN A */ /* SPECIAL SYMBOL TABLE THAT CAN BE SEARCHED QUICKLY DURING */ /* RELOCATION. */ /*------------------------------------------------------------------------*/ for (first = 0; first < file_hdr.f_nsyms; first = next) { if (!(next = sym_read(first, &sym, &aux))) { load_err = E_FILE; return FALSE; } if (sym.n_sclass == C_EXT || sym.n_sclass == C_EXTREF || sym.n_sclass == C_STAT || sym.n_sclass == C_LABEL || sym.n_sclass == C_SYSTEM || sym.n_sclass == C_BLOCK || sym.n_sclass == C_FCN || sym.n_sclass == C_STATLAB || sym.n_sclass == C_EXTLAB) if (!reloc_add(first, &sym)) return FALSE; } return TRUE; } /******************************************************************************/ /* */ /* CLOAD_STRINGS() - Read in the string table. */ /* */ /******************************************************************************/ int cload_strings() { unsigned int str_size; /* SIZE OF STRING TABLE */ unsigned int bufsize; /* SIZE OF CURRENT BUFFER */ unsigned int ntoread; /* AMOUNT TO READ FROM FILE */ int excess; /* AMOUNT LEFT OVER FROM LAST BUFFER */ STRTAB *packet; /* STRING TABLE BUFFER PACKET */ unsigned int i = 0; /*----------------------------------------------------------------------*/ /* Do not load if not loading/saving the symbol tables. */ /* This is because the string table is an extension of the symbol table */ /* and if you free and rebuild it, the symbol table's str_head will be */ /* incorrect. */ /*----------------------------------------------------------------------*/ if (!need_symbols) return TRUE; /*------------------------------------------------------------------------*/ /* FREE ANY PREVIOUS STRING BUFFERS */ /*------------------------------------------------------------------------*/ str_free(str_head); str_head = NULL; /*------------------------------------------------------------------------*/ /* SEEK TO THE END OF THE SYMBOL TABLE AND READ IN THE SIZE OF THE STRING */ /* TABLE. */ /*------------------------------------------------------------------------*/ #if FILE_BASED if ((file_hdr.f_nsyms == 0) || fseek(fin, file_hdr.f_symptr + (file_hdr.f_nsyms * SYMESZ), 0) != 0 || fread(&str_size, sizeof(int), 1, fin) != 1) return TRUE; #else mem_copy(&str_size, &gRxBuffer[file_hdr.f_symptr + (file_hdr.f_nsyms * SYMESZ)], sizeof(int)); if ((file_hdr.f_nsyms == 0)) return TRUE; #endif if (byte_swapped) swap4byte(&str_size); /*------------------------------------------------------------------------*/ /* THE STRING TABLE IS READ IN AS A LINKED LIST OF BUFFERS. TO */ /* PREVENT NAMES FROM BEING SPLIT ACROSS MULTIPLE BUFFERS, ANY PARTIAL */ /* NAME AT THE END OF A BUFFER IS COPIED INTO THE BEGINNING OF THE */ /* NEXT BUFFER. THE VARIABLE 'EXCESS' KEEPS TRACK OF HOW MUCH NEEDS */ /* TO BE COPIED FROM THE PREVIOUS BUFFER. */ /*------------------------------------------------------------------------*/ str_size -= 4; /* SUBTRACT OFF 4 BYTES ALREADY READ */ excess = 0; /* INITIALIZE LAST-BUFFER OVERFLOW */ /*------------------------------------------------------------------------*/ /* READ STRING BUFFERS UNTIL THE WHOLE STRING TABLE IS READ. */ /*------------------------------------------------------------------------*/ while (str_size) { /*---------------------------------------------------------------------*/ /* ALLOCATE A NEW BUFFER. ON 16-BIT MACHINES, RESTRICT THE */ /* BUFFER SIZE TO THE MAXIMUM THAT CAN BE ALLOCATED AT ONCE. */ /*---------------------------------------------------------------------*/ bufsize = str_size + excess; if (sizeof(int) < 4 && bufsize > MAX_STRING_ALLOC) bufsize = MAX_STRING_ALLOC; if (!(packet = (struct strtab *)malloc(sizeof(STRTAB) + (unsigned int)bufsize - 1))) { load_err = E_ALLOC; return FALSE; } /*---------------------------------------------------------------------*/ /* COPY ANY PARTIAL STRING FROM THE LAST BUFFER INTO THIS ONE. */ /* THEN FILL THE REST OF THE BUFFER BY READING FROM THE FILE. */ /*---------------------------------------------------------------------*/ if (excess) strn_copy(packet->buf, str_head->buf + str_head->size, excess); ntoread = (unsigned int)(bufsize - excess); #if FILE_BASED if (fread(packet->buf + excess, ntoread, 1, fin) != 1) { load_err = E_FILE; return FALSE; } #else mem_copy(packet->buf + excess, &gRxBuffer[file_hdr.f_symptr + (file_hdr.f_nsyms * SYMESZ) +sizeof(int)+ i++*ntoread], ntoread); #endif str_size -= ntoread; /*---------------------------------------------------------------------*/ /* IF THE BUFFER ENDS IN A PARTIAL STRING (DOESN'T END IN NULL), */ /* KEEP TRACK OF HOW MANY CHARACTERS ARE IN THE PARTIAL STRING */ /* SO THEY CAN BE COPIED INTO THE NEXT BUFFER. */ /*---------------------------------------------------------------------*/ for (excess = 0; packet->buf[bufsize - 1]; --bufsize, ++excess) ; /*---------------------------------------------------------------------*/ /* LINK THE NEW BUFFER INTO THE HEAD OF THE LIST. */ /*---------------------------------------------------------------------*/ packet->size = packet->index = bufsize; packet->next = str_head; packet->offset = str_head ? (str_head->offset + str_head->size) : 4; str_head = packet; } return TRUE; } /******************************************************************************/ /* */ /* STR_FREE() - Free the list of string table buffers. */ /* */ /******************************************************************************/ void str_free(STRTAB *head) { STRTAB *this_one, *next; for (this_one = head; this_one; this_one = next) { next = this_one->next; free(this_one); } } /******************************************************************************/ /* */ /* SYM_READ() - Read and relocate a symbol and its aux entry. Return the */ /* index of the next symbol. */ /* */ /******************************************************************************/ int sym_read(int index, SYMENT *sym, AUXENT *aux) { /*------------------------------------------------------------------------*/ /* READ IN A SYMBOL AND ITS AUX ENTRY. */ /*------------------------------------------------------------------------*/ #if FILE_BASED if (fseek(fin, file_hdr.f_symptr + (index * SYMESZ), 0) != 0 || fread(sym, SYMESZ, 1, fin) != 1 || (sym->n_numaux && fread(aux, SYMESZ, 1, fin) != 1)) { load_err = E_FILE; return FALSE; } #else mem_copy((void*)sym, (void*)&gRxBuffer[file_hdr.f_symptr + (index * SYMESZ)], SYMESZ); if (sym->n_numaux) { mem_copy((void*)aux, (void*)&gRxBuffer[file_hdr.f_symptr + ( (index+1) * SYMESZ)], SYMESZ); load_err = E_FILE; return FALSE; } #endif if (byte_swapped) { /*--------------------------------------------------------------------*/ /* SWAP THE SYMBOL TABLE ENTRY. */ /*--------------------------------------------------------------------*/ if (sym->n_zeroes == 0) swap4byte(&sym->n_offset); swap4byte(&sym->n_value); swap2byte(&sym->n_scnum); swap2byte(&sym->n_type); /*--------------------------------------------------------------------*/ /* SWAP THE AUX ENTRY, BASED ON THE STORAGE CLASS. */ /*--------------------------------------------------------------------*/ if (sym->n_numaux) switch(sym->n_sclass) { case C_FILE : break; case C_STRTAG : case C_UNTAG : case C_ENTAG : swap4byte(&aux->x_tag.x_fsize); swap4byte(&aux->x_tag.x_endndx); break; case C_FCN : if (!str_comp(sym->n_name, ".bf")) { swap2byte(&aux->x_block.x_lcnt); swap4byte(&aux->x_block.x_regmask); swap4byte(&aux->x_block.x_framesize); } case C_BLOCK : swap2byte(&aux->x_block.x_lnno); swap4byte(&aux->x_block.x_endndx); break; case C_EOS : swap4byte(&aux->x_eos.x_fsize); swap4byte(&aux->x_eos.x_tagndx); break; default : /*-------------------------------------------------*/ /* HANDLE FUNCTION DEFINITION SYMBOL */ /*-------------------------------------------------*/ if (((sym->n_type >> 4) & 3) == DCT_FCN) { swap4byte(&aux->x_func.x_tagndx); swap4byte(&aux->x_func.x_fsize); swap4byte(&aux->x_func.x_lnnoptr); swap4byte(&aux->x_func.x_endndx); } /*-------------------------------------------------*/ /* HANDLE ARRAYS. */ /*-------------------------------------------------*/ else if (((sym->n_type >> 4) & 3) == DCT_ARY) { swap4byte(&aux->x_array.x_tagndx); swap4byte(&aux->x_array.x_fsize); swap2byte(&aux->x_array.x_dimen[0]); swap2byte(&aux->x_array.x_dimen[1]); swap2byte(&aux->x_array.x_dimen[2]); swap2byte(&aux->x_array.x_dimen[3]); } /*-------------------------------------------------*/ /* HANDLE SECTION DEFINITIONS */ /*-------------------------------------------------*/ else if (sym->n_type == 0) { swap4byte(&aux->x_scn.x_scnlen); swap2byte(&aux->x_scn.x_nreloc); swap2byte(&aux->x_scn.x_nlinno); } /*-------------------------------------------------*/ /* HANDLE MISC SYMBOL RECORD */ /*-------------------------------------------------*/ else { swap4byte(&aux->x_sym.x_fsize); swap4byte(&aux->x_sym.x_tagndx); } } } /*------------------------------------------------------------------------*/ /* RELOCATE THE SYMBOL, BASED ON ITS STORAGE CLASS. */ /*------------------------------------------------------------------------*/ switch(sym->n_sclass) { case C_SYSTEM : case C_EXT : case C_EXTREF : case C_STAT : case C_LABEL : case C_BLOCK : case C_FCN : case C_STATLAB : case C_EXTLAB : /*------------------------------------------------------------------*/ /* IF THE SYMBOL IS UNDEFINED, CALL AN APPLICATION ROUTINE TO LOOK */ /* IT UP IN AN EXTERNAL SYMBOL TABLE. IF THE SYMBOL IS DEFINED, */ /* RELOCATE IT ACCORDING TO THE SECTION IT IS DEFINED IN. */ /*------------------------------------------------------------------*/ if (sym->n_scnum == 0) lookup_sym((short)index, sym, aux); else if (sym->n_scnum > 0) { if (sym->n_sclass == C_STATLAB || sym->n_sclass == C_EXTLAB) sym->n_value += reloc_amount[sym->n_scnum - 1]; else sym->n_value += RUN_RELOC_AMOUNT(sym->n_scnum - 1); } } return (index + sym->n_numaux + 1); } /******************************************************************************/ /* */ /* SYM_NAME() - Return a pointer to the name of a symbol in either the symbol */ /* entry or the string table. */ /* */ /******************************************************************************/ char *sym_name(SYMENT *symptr) { static char temp[9]; if (symptr->n_zeroes == 0) { STRTAB *packet = str_head; /*---------------------------------------------------------------------*/ /* Return the empty string if this symbol has no name (offset == 0) */ /*---------------------------------------------------------------------*/ if (symptr->n_offset < 4) /* Anything below 4 isn't valid */ { temp[0] = 0; return temp; } /*---------------------------------------------------------------------*/ /* Otherwise, return the string in the string table. */ /*---------------------------------------------------------------------*/ while (packet && symptr->n_offset < (int)packet->offset) packet = packet->next; /*---------------------------------------------------------------------*/ /* Return the empty string if packet NULL (invalid offset) */ /*---------------------------------------------------------------------*/ if (!packet) { temp[0] = 0; return temp; } return packet->buf + (symptr->n_offset - packet->offset); } strn_copy(temp, symptr->n_name, 8); temp[8] = 0; return temp; } /******************************************************************************/ /* */ /* SYM_ADD_NAME() - Given a symbol table entry, return a pointer to the */ /* symbol's name in the string table. Add the name to the */ /* table if it's not already there. */ /* */ /******************************************************************************/ char *sym_add_name(SYMENT *symptr) { char *dest; char *result; int i; /*------------------------------------------------------------------------*/ /* IF THE SYMBOL'S NAME WAS IN THE COFF STRING TABLE, LOOK THROUGH THE */ /* LIST OF STRING TABLE BUFFERS UNTIL FINDING THE ONE THE NAME IS IN, */ /* AND SIMPLY POINT INTO THE BUFFER. */ /*------------------------------------------------------------------------*/ if (symptr->n_zeroes == 0) return sym_name(symptr); /*------------------------------------------------------------------------*/ /* OTHERWISE ADD THE STRING TO THE STRING TABLE. */ /* ALLOCATE AND LINK IN A NEW PACKET IF NECESSARY. NEW PACKETS ARE */ /* LINKED TO THE HEAD OF THE LIST TO EASE ADDING NEW SYMBOLS. */ /*------------------------------------------------------------------------*/ if (!str_head || str_head->index + SYMNMLEN + 1 > str_head->size) { STRTAB *packet; if (!(packet = (STRTAB *)malloc(sizeof(STRTAB) + MIN_STRING_ALLOC - 1))) { load_err = E_ALLOC; return NULL; } packet->size = MIN_STRING_ALLOC; packet->index = 0; packet->next = str_head; packet->offset = str_head ? (str_head->offset + str_head->size) : 4; str_head = packet; } /*------------------------------------------------------------------------*/ /* COPY THE NAME INTO THE STRING TABLE. */ /*------------------------------------------------------------------------*/ result = dest = str_head->buf + str_head->index; for (i = 0; *dest++ = symptr->n_name[i++]; ) if (i == SYMNMLEN) { *dest++ = '\0'; ++i; break; } symptr->n_zeroes = 0; symptr->n_offset = str_head->offset + str_head->index; str_head->index += i; return result; } #endif #if 0 /******************************************************************************/ /* */ /* RELOC_ADD() - Add an entry to the relocation symbol table. This table */ /* stores relocation information for each relocatable symbol. */ /* */ /******************************************************************************/ int reloc_add(int index, SYMENT *sym) { int disp; /* RELOCATION AMOUNT FOR THIS SYMBOL */ if (!need_reloc) return TRUE; /*-------------------------------------------------------------------------*/ /* USE THE SYMBOL VALUE TO CALCULATE THE RELOCATION AMOUNT: */ /* 1) IF THE SYMBOL WAS UNDEFINED (DEFINED IN SECTION 0), USE THE */ /* SYMBOL'S VALUE. */ /* 2) IF THE SYMBOL HAS A POSITIVE SECTION NUMBER, USE THE RELOCATION */ /* AMOUNT FOR THE SECTION IN WHICH THE SYMBOL IS DEFINED. */ /* 3) OTHERWISE, THE SYMBOL IS ABSOLUTE, SO THE RELOCATION AMOUNT IS 0. */ /*-------------------------------------------------------------------------*/ if (sym->n_scnum == 0) disp = sym->n_value; else if (sym->n_scnum > 0) { if (sym->n_sclass == C_STATLAB || sym->n_sclass == C_EXTLAB) disp = reloc_amount[sym->n_scnum - 1]; else disp = RUN_RELOC_AMOUNT(sym->n_scnum - 1); } else disp = 0; /*-------------------------------------------------------------------------*/ /* IF THERE IS A NON-ZERO RELOCATION AMOUNT, ADD THE SYMBOL TO THE TABLE. */ /*-------------------------------------------------------------------------*/ if (disp == 0) return TRUE; if (reloc_sym_index >= reloc_tab_size) { reloc_tab_size += RELOC_GROW_SIZE; reloc_tab = (RELOC_TAB *)realloc((char *)reloc_tab, reloc_tab_size*sizeof(RELOC_TAB)); if (!reloc_tab) { load_err = E_ALLOC; return FALSE; } } reloc_tab[reloc_sym_index ].rt_index = index; reloc_tab[reloc_sym_index++].rt_disp = disp; return TRUE; } /******************************************************************************/ /* */ /* RELOCATE() - Perform a single relocation by patching the raw data. */ /* */ /******************************************************************************/ int relocate(RELOC *rp, unsigned char *data, int s) { /* RELOC *rp; RELOCATION ENTRY */ /* unsigned char *data; DATA BUFFER */ /* int s; INDEX OF CURRENT SECTION */ int fieldsz = reloc_size(rp->r_type); /* SIZE OF ACTUAL PATCH VALUE */ int offset = reloc_offset(rp->r_type); /* OFFSET OF ACTUAL PATCH VALUE */ int wordsz = MAX(fieldsz, reloc_stop(rp->r_type)); /* SIZE CONTAINING FLD */ int objval; /* FIELD TO BE PATCHED */ int reloc_amt; /* AMOUNT OF RELOCATION */ int pp_shift_cnt = 0; int pp_local = FALSE; if (rp->r_type == R_ABS) return TRUE; /* NOTHING TO DO */ /*-------------------------------------------------------------------------*/ /* DETERMINE THE RELOCATION AMOUNT FROM THE RELOCATION SYMBOL TABLE. */ /*-------------------------------------------------------------------------*/ reloc_amt = (rp->r_symndx == -1) ? RUN_RELOC_AMOUNT(s) : sym_reloc_amount(rp); /*-------------------------------------------------------------------------*/ /* EXTRACT THE RELOCATABLE FIELD FROM THE OBJECT DATA. */ /*-------------------------------------------------------------------------*/ objval = unpack(data, fieldsz, wordsz, offset + BIT_OFFSET(rp->r_vaddr)); /*-------------------------------------------------------------------------*/ /* MODIFY THE FIELD BASED ON THE RELOCATION TYPE. */ /*-------------------------------------------------------------------------*/ switch (rp->r_type) { /*----------------------------------------------------------------------*/ /* NORMAL RELOCATIONS: ADD IN THE RELOCATION AMOUNT. */ /*----------------------------------------------------------------------*/ case R_RELBYTE: case R_RELWORD: case R_REL24: case R_RELLONG: case R_DIR32: case R_PARTLS16: objval += reloc_amt; break; /*--------------------------------------------------------------------*/ /* ADD IN THE RELOCATION AMOUNT, BUT MAKE SURE WE'RE STILL IN THE */ /* 370'S REGISTER FILE. */ /*--------------------------------------------------------------------*/ case R_RRNREG: case R_RRRELREG: if (rp->r_type == R_RRNREG) objval = ((char)objval + reloc_amt); else objval += reloc_amt; if (objval & ((-1L >> 8*fieldsz) << 8*fieldsz)) { /* ERROR */ } break; /*--------------------------------------------------------------------*/ /* PP UNSCALED 15-BIT OFFSET RELOCATION. */ /*--------------------------------------------------------------------*/ case R_PP15 : case R_PPL15 : case R_PPN15 : case R_PPLN15 : { int bit; char *sname = (SECT_HDR(s)->s_zeroes == 0L) ? SECT_HDR(s)->s_nptr : SNAMECPY(SECT_HDR(s)->s_name); pp_local = (rp->r_type == R_PPL15) || (rp->r_type == R_PPLN15); /*--------------------------------------------------------------*/ /* IF NEGATIVE RELOC TYPE, THEN TREAT CONST OFFSET AS A NEGATIVE*/ /*--------------------------------------------------------------*/ if (rp->r_type == R_PPN15 || rp->r_type == R_PPLN15) { objval = -objval; rp->r_type -= 010; /* CHANGE TYPE TO NON NEG. */ } objval += reloc_amt; /*--------------------------------------------------------------*/ /* IF THE ADDRESS STILL FALLS WITHIN AN APPROPRIATE RANGE */ /*--------------------------------------------------------------*/ if ((objval >= 0x00000000 && objval <= 0x00007fff) || (objval >= 0x01000000 && objval <= 0x010007ff) ) break; /*--------------------------------------------------------------*/ /* IF THE ADDRESS FALLS OUTSIDE AN APPROPRIATE RANGE, BUT CAN */ /* BE SCALED BY SIZE TO GET BACK INTO RANGE, THEN READ THE UPPER*/ /* BIT OF THE SIZE FIELD. IF IT IS A 1, THEN WE CAN SCALE THIS */ /* OFFSET BY 4, IF IT IS 0, THEN WE CAN SCALE THIS OFFSET BY 2. */ /*--------------------------------------------------------------*/ bit = unpack(data, 1, 64, pp_local ? 30 : 8); /*--------------------------------------------------------------*/ /* DETERMINE IF THE OFFSET IS ALIGNED FOR SCALING. IF SO, */ /* THEN PACK THE SCALED OFFSET INTO INSTRUCTION, CHANGE THE */ /* RELOC TYPE TO SCALED, AND TURN ON SCALE BIT IN INSTRUCT. */ /*--------------------------------------------------------------*/ if (!(objval & ((2<>= (bit+1)) >= 0 && objval <= 0x7fff) { rp->r_type = pp_local ? (bit ? R_PPL15W : R_PPL15H) : (bit ? R_PP15W : R_PP15H); repack(1, data, 1, 64, pp_local ? 28 : 6); break; } /*--------------------------------------------------------------*/ /* ERROR, THE OFFSET WILL NOT FIT SCALED OR UNSCALED. */ /*--------------------------------------------------------------*/ load_err = E_RELOCENT; return FALSE; } /*--------------------------------------------------------------------*/ /* PP SCALED 15-BIT OFFSET RELOCATION. FOR R_PP15W THE RELOC_AMT IS */ /* DIVIDED BY 4. FOR R_PP15H THE RELOC_AMT IS DIVIDED BY 2. */ /*--------------------------------------------------------------------*/ case R_PP15W : case R_PPL15W : case R_PPN15W : case R_PPLN15W : pp_shift_cnt++; /* FALL THROUGH */ case R_PP15H : case R_PPL15H : case R_PPN15H : case R_PPLN15H : pp_shift_cnt++; /* FALL THROUGH */ { int obj_addr_x; char *sname = (SECT_HDR(s)->s_zeroes == 0) ? SECT_HDR(s)->s_nptr : SNAMECPY(SECT_HDR(s)->s_name); /*--------------------------------------------------------------*/ /* NOTE THAT THIS IS DEPENDENT ON THE NUMBERING OF THESE RELOC */ /* VALUES. */ /*--------------------------------------------------------------*/ pp_local = (rp->r_type & 4); /*--------------------------------------------------------------*/ /* IF NEGATIVE RELOC TYPE, THEN TREAT CONST OFFSET AS NEGATIVE */ /*--------------------------------------------------------------*/ if (rp->r_type >= R_PPN15) { objval = -objval; rp->r_type -= 010; /* CHANGE TYPE TO NON NEG. */ } obj_addr_x = (objval << pp_shift_cnt) + reloc_amt; /*--------------------------------------------------------------*/ /* LINK TIME ADDRESS VIOLATES THE SCALING FACTOR WE ARE USING */ /* FOR THIS OPERAND. UNSCALE THE VALUE IF IT WILL FIT IN 15 BITS*/ /* BY CHANGING RELOC TYPE TO UNSCALED, AND CHANGING SCALE BIT */ /* IN THE INSTRUCTION. */ /*--------------------------------------------------------------*/ if (pp_shift_cnt && (reloc_amt & ((1<r_type = (pp_local ? R_PPL15 : R_PP15); repack(0, data, 1, 64, pp_local ? 28 : 6); } else objval = obj_addr_x >> pp_shift_cnt; /*--------------------------------------------------------------*/ /* IF THE ADDRESS STILL FALLS WITHIN AN APPROPRIATE RANGE */ /*--------------------------------------------------------------*/ if ((objval >= 0x00000000 && objval <= 0x00007fff) || (obj_addr_x >= 0x01000000 && obj_addr_x <= 0x010007ff) ) break; /*--------------------------------------------------------------*/ /* ERROR, THE OFFSET WILL NOT FIT SCALED OR UNSCALED. */ /*--------------------------------------------------------------*/ load_err = E_RELOCENT; return FALSE; } /*--------------------------------------------------------------------*/ /* PP 16-bit byte offset relocation. For R_PP16B the lower 15-bits */ /* are handled just like R_PP15, and the upper bit is placed in the */ /* scale indicator bit of the field. */ /*--------------------------------------------------------------------*/ case R_PP16B : case R_PPL16B : case R_PPN16B : case R_PPLN16B : { char *sname = (SECT_HDR(s)->s_zeroes == 0) ? SECT_HDR(s)->s_nptr : SNAMECPY(SECT_HDR(s)->s_name); pp_local = (rp->r_type == R_PPL16B) || (rp->r_type == R_PPLN16B); /*--------------------------------------------------------------*/ /* READ THE SCALE BIT (16th BIT) AND CREATE 16 BIT CONSTANT OFF */ /*--------------------------------------------------------------*/ objval |= (unpack(data, 1, 64, pp_local ? 28 : 6) << 15); /*--------------------------------------------------------------*/ /* IF NEGATIVE RELOC TYPE, THEN TREAT CONST OFFSET AS NEGATIVE */ /*--------------------------------------------------------------*/ if (rp->r_type == R_PPN16B || rp->r_type == R_PPLN16B) { objval = - objval; rp->r_type -= 010; /* CHANGE THE TYPE TO A NON NEG TYPE. */ } objval += reloc_amt; /*--------------------------------------------------------------*/ /* IF THE ADDRESS STILL FALLS WITHIN AN APPROPRIATE RANGE */ /*--------------------------------------------------------------*/ if ((objval >= 0x00000000 && objval <= 0x0000ffff) || (objval >= 0x01000000 && objval <= 0x010007ff) ) { /*-----------------------------------------------------------*/ /* RELOCATE THE 16TH BIT OF THE ADDRESS. */ /*-----------------------------------------------------------*/ repack(((objval&0x8000) >> 15), data, 1, 64, pp_local ? 28 : 6); break; } /*--------------------------------------------------------------*/ /* ADDRESS IS OUT OF RANGE. */ /*--------------------------------------------------------------*/ load_err = E_RELOCENT; return FALSE; } /*--------------------------------------------------------------------*/ /* PP BASE ADDRESS RELOCATION. BIT 0 IS 0 IF IN DATA RAM, 1 IF IN */ /* PARAMETER RAM. THIS CODE ASSUMES THAT WE DO NOT RELOCATE FROM */ /* PRAM TO DRAM OR FROM DRAM TO PRAM AT LOAD TIME. */ /*--------------------------------------------------------------------*/ case R_PPLBASE: pp_local = TRUE; case R_PPBASE: { /*---------------------------------------------------------------*/ /* IF WAS DRAM AND RELOC_AMT IS GREAT ENOUGH TO MOVE INTO PRAM, */ /* CHANGE TO PRAM */ /*---------------------------------------------------------------*/ if (!objval && reloc_amt > (int)(0x01000000 - 0xC000)) objval = 1; /*---------------------------------------------------------------*/ /* IF WAS PRAM AND RELOC_AMT IS NEGATIVE AND CAN MOVE INTO DRAM, */ /* CHANGE TO DRAM */ /*---------------------------------------------------------------*/ else if (objval && (-reloc_amt) > (int)(0x01000000 - 0xC000)) objval = 0; break; } /*----------------------------------------------------------------------*/ /* 34010 ONE'S COMPLEMENT RELOCATION. SUBTRACT INSTEAD OF ADD. */ /*----------------------------------------------------------------------*/ case R_OCRLONG: objval -= reloc_amt; break; /*----------------------------------------------------------------------*/ /* 34020 WORD-SWAPPED RELOCATION. SWAP BEFORE RELOCATING. */ /*----------------------------------------------------------------------*/ case R_GSPOPR32: case R_OCBD32: objval = ((objval >> 16) & 0xFFFF) | (objval << 16); objval += (rp->r_type == R_GSPOPR32) ? reloc_amt : -reloc_amt; objval = ((objval >> 16) & 0xFFFF) | (objval << 16); break; /*----------------------------------------------------------------------*/ /* PC-RELATIVE RELOCATIONS. IN THIS CASE THE RELOCATION AMOUNT */ /* IS ADJUSTED BY THE PC DIFFERENCE. IF THIS IS AN INTERNAL */ /* RELOCATION TO THE CURRENT SECTION, NO ADJUSTMENT IS NEEDED. */ /*----------------------------------------------------------------------*/ case R_PCRBYTE: case R_PCRWORD: case R_GSPPCR16: case R_GSPPCA16: case R_PCRLONG: case R_PCR24: case R_ANKPCR16: case R_ANKPCR8: { int shift = 8 * (4 - fieldsz); unsigned int pcdif = RUN_RELOC_AMOUNT(s); /*----------------------------------------------------------------*/ /* HANDLE SPECIAL CASES OF JUMPING FROM ABSOLUTE SECTIONS (SPECIAL*/ /* RELOC TYPE) OR TO ABSOLUTE DESTINATION (SYMNDX == -1). IN */ /* EITHER CASE, SET THE APPROPRIATE RELOCATION AMOUNT TO 0. */ /*----------------------------------------------------------------*/ if( rp->r_symndx == -1 ) reloc_amt = 0; if( rp->r_type == R_GSPPCA16) pcdif = 0; /*----------------------------------------------------------------*/ /* Handle ankoor's offset where upper 14 (PCR8) and upper 6(PCR16)*/ /* bits of 22 bit address is held in r_disp field of reloc entry */ /*----------------------------------------------------------------*/ if(rp->r_type == R_ANKPCR8 || rp->r_type == R_ANKPCR16) { shift = 10; objval |= rp->r_disp << ((rp->r_type == R_ANKPCR8) ? 8 : 16); } reloc_amt -= pcdif; if (rp->r_type == R_GSPPCR16 || rp->r_type == R_GSPPCA16) reloc_amt >>= 4; /* BITS TO WORDS */ objval = (int)(objval << shift) >> shift; /* SIGN EXTEND */ objval += reloc_amt; break; } /*--------------------------------------------------------------------*/ /* Ankoor page-addressing. Calculate address from the 22-bit */ /* value in the relocation field plus the relocation amount. Shift */ /* out the lower 16 bits. */ /*--------------------------------------------------------------------*/ case R_PARTMS6: objval = (objval & 0xC0) | (((rp->r_disp += reloc_amt) >> 16) & 0x3F); break; /*----------------------------------------------------------------------*/ /* 320C30 PAGE-ADDRESSING RELOCATION. CALCULATE THE ADDRESS FROM */ /* THE 8-BIT PAGE VALUE IN THE FIELD, THE 16-BIT OFFSET IN THE RELOC */ /* ENTRY, AND THE RELOCATION AMOUNT. THEN, STORE THE 8-BIT PAGE */ /* VALUE OF THE RESULT BACK IN THE FIELD. */ /*----------------------------------------------------------------------*/ case R_PARTMS8: objval = (int)((objval << 16) + rp->r_disp + reloc_amt) >> 16; break; /*----------------------------------------------------------------------*/ /* DSP(320) PAGE-ADDRESSING. CALCULATE ADDRESS FROM THE 16-BIT */ /* VALUE IN THE RELOCATION FIELD PLUS THE RELOCATION AMOUNT. OR THE */ /* TOP 9 BITS OF THIS RESULT INTO THE RELOCATION FIELD. */ /*----------------------------------------------------------------------*/ case R_PARTMS9: objval = (objval & 0xFE00) | (((int)(rp->r_disp + reloc_amt) >> 7) & 0x1FF); break; /*----------------------------------------------------------------------*/ /* DSP(320) PAGE-ADDRESSING. CALCULATE ADDRESS AS ABOVE, AND OR THE */ /* 7-BIT DISPLACEMENT INTO THE FIELD. */ /*----------------------------------------------------------------------*/ case R_PARTLS7: objval = (objval & 0x80) | ((rp->r_disp + reloc_amt) & 0x7F); break; /*--------------------------------------------------------------------*/ /* Ankoor page-addressing. Calculate address from the 22-bit */ /* value in the relocation field plus the relocation amount. Mask off */ /* bits [21:16] and [5:0] to extract a data page within a 64K page */ /*--------------------------------------------------------------------*/ case R_PARTMID10: objval = (objval & 0xFC00) | (((rp->r_disp += reloc_amt) >> 6) & 0x3FF); break; /*--------------------------------------------------------------------*/ /* RR(370) MSB RELOCATION. CALCULATE ADDRESS FROM THE 16-BIT VALUE */ /* IN THE RELOCATION ENTRY PLUS THE RELOCATION AMOUNT. PATCH THE */ /* MSB OF THE RESULT INTO THE RELOCATION FIELD. */ /*--------------------------------------------------------------------*/ case R_HIWORD: objval += (rp->r_disp += (unsigned short)reloc_amt) >> 8; break; /*--------------------------------------------------------------------*/ /* C8+ High byte of 24-bit address. Calculate address from 24-bit */ /* value in the relocation entry plus the relocation amount. Patch */ /* the MSB of the result into the relocation field. */ /*--------------------------------------------------------------------*/ case R_C8PHIBYTE: objval = (int)((objval << 16) + rp->r_disp + reloc_amt) >> 16; break; /*--------------------------------------------------------------------*/ /* C8+ Middle byte of 24-bit address. Calculate address from 24-bit */ /* value in the relocation entry plus the relocation amount. Patch */ /* the middle byte of the result into the relocation field. */ /*--------------------------------------------------------------------*/ case R_C8PMIDBYTE: objval = (int)((objval << 16) + rp->r_disp + reloc_amt) >> 8; break; /*--------------------------------------------------------------------*/ /* C8+ Vector Address. Calculate address from 24-bit value in the */ /* relocation entry plus the relocation amount. MSB must be 0xFF */ /* since interrupt and trap handlers must be programmed in the top- */ /* most segment of memory. Patch bottom 16-bits of the result into */ /* the relocation field. */ /*--------------------------------------------------------------------*/ case R_C8PVECADR: objval += reloc_amt; if ((objval & 0xFF0000) != 0xFF0000) { /* ERROR */ } objval &= 0xFFFF; break; /*----------------------------------------------------------------------*/ /* C8+ 24-bit Address. The byte ordering for 24-bit addresses on the */ /* C8+ is reversed (low, middle, high). Needs to be unordered, add */ /* in reloc_amt, then re-ordered. */ /*----------------------------------------------------------------------*/ case R_C8PADR24: objval = ((objval>>16) | (objval&0xff00) | ((objval&0xff)<<16)); objval += reloc_amt; objval = ((objval>>16) | (objval&0xff00) | ((objval&0xff)<<16)); break; /*----------------------------------------------------------------------*/ /* DSP(320) 13-BIT CONSTANT. RELOCATE ONLY THE LOWER 13 BITS OF THE */ /* FIELD. */ /*----------------------------------------------------------------------*/ case R_REL13: objval = (objval & 0xE000) | ((objval + reloc_amt) & 0x1FFF); break; /*--------------------------------------------------------------------*/ /* ANKOOR 22-bit extended address. Calculate address by masking */ /* off the opcode and OR in the lower 16-bit constant + the */ /* amount. */ /*--------------------------------------------------------------------*/ case R_REL22: { unsigned int obj_hi = unpack(data , 16, 16, 0); unsigned int obj_lo = unpack(data+2, 16, 16, 0); /*--------------------------------------------------------------*/ /* BUILD THE OFFSET TO BE RELOCATED. */ /*--------------------------------------------------------------*/ objval = ((obj_hi & 0x003F) << 16) | (obj_lo & 0xFFFF); /*--------------------------------------------------------------*/ /* Calculate displacement */ /*--------------------------------------------------------------*/ objval += reloc_amt; /*--------------------------------------------------------------*/ /* REPACK THE RELOCATED VALUE BACK IN THE OBJECT VALUE. */ /*--------------------------------------------------------------*/ obj_hi = (obj_hi & 0xFFC0) | ((objval & 0x3F0000) >> 16); obj_lo = objval & 0xFFFF; repack(obj_hi, data , 16, 16, 0); repack(obj_lo, data+2, 16, 16, 0); return TRUE; } /*--------------------------------------------------------------------*/ /* DSP, LEAD 23-bit extended address. Calculate address by masking */ /* off the opcode and OR in the lower 16-bit constant + the */ /* amount. */ /*--------------------------------------------------------------------*/ case R_REL23: { unsigned int obj_hi = unpack(data , 16, 16, 0); unsigned int obj_lo = unpack(data+2, 16, 16, 0); /*--------------------------------------------------------------*/ /* BUILD THE OFFSET TO BE RELOCATED. */ /*--------------------------------------------------------------*/ objval = ((obj_hi & 0x007F) << 16) | (obj_lo & 0xFFFF); /*--------------------------------------------------------------*/ /* Calculate displacement */ /*--------------------------------------------------------------*/ objval += reloc_amt; /*--------------------------------------------------------------*/ /* REPACK THE RELOCATED VALUE BACK IN THE OBJECT VALUE. */ /*--------------------------------------------------------------*/ obj_hi = (obj_hi & 0xFF80) | ((objval & 0x7F0000) >> 16); obj_lo = objval & 0xFFFF; repack(obj_hi, data , 16, 16, 0); repack(obj_lo, data+2, 16, 16, 0); return TRUE; } /*----------------------------------------------------------------------*/ /* PRISM (370/16) code label relocation. Convert word address to byte */ /* address, add in relocation, convert back to word address. */ /*----------------------------------------------------------------------*/ case R_LABCOD: objval = ((objval << 1) + reloc_amt) >> 1; break; } /*-------------------------------------------------------------------------*/ /* PACK THE RELOCATED FIELD BACK INTO THE OBJECT DATA. */ /*-------------------------------------------------------------------------*/ repack(objval, data, fieldsz, wordsz, offset + BIT_OFFSET(rp->r_vaddr)); return TRUE; } /******************************************************************************/ /* */ /* RELOC_READ() - Read a single relocation entry. */ /* */ /******************************************************************************/ #if FILE_BASED int reloc_read(RELOC *rptr) #else int reloc_read(RELOC *rptr, unsigned int offset) #endif { #if COFF_VERSION_1 || COFF_VERSION_2 /*------------------------------------------------------------------------*/ /* THE FOLLOWING UNION IS USED TO READ IN VERSION 0 OR 1 RELOC ENTRIES */ /*------------------------------------------------------------------------*/ /* THE FORMAT OF RELOCATION ENTRIES CHANGED BETWEEN COFF VERSIONS 0 AND 1.*/ /* VERSION 0 HAS A 16 BIT SYMBOL INDEX, WHILE VERSION 1 HAS A 32 BIT INDX.*/ /*------------------------------------------------------------------------*/ union { RELOC new_c; RELOC_OLD old; } input_entry; #if FILE_BASED if (fread(&input_entry, RELSZ_IN(coff_version), 1, fin) != 1) { load_err = E_FILE; return FALSE; } #else mem_copy((void*)&input_entry, (void*)&gRxBuffer[offset], RELSZ_IN(coff_version)); #endif /*------------------------------------------------------------------------*/ /* IF LOADING A VERSION 0 FILE, TRANSLATE ENTRY TO VERSION 1 FORMAT. */ /* (THIS COULD BE SIMPLER - ALL THE SWAPS EXCEPT FOR THE SYMBOL INDEX */ /* COULD BE DONE AFTER THE TRANSLATION - BUT THIS SEEMS TO BE CLEARER) */ /*------------------------------------------------------------------------*/ if (ISCOFF_0(coff_version)) { if (byte_swapped) { swap4byte(&input_entry.old.r_vaddr); swap2byte(&input_entry.old.r_type); /* if a field reloc, fields are chars, so don't swap */ if (!isfldrel(input_entry.old.r_type)) { swap2byte(&input_entry.old.r_symndx); swap2byte(&input_entry.old.r_disp); } } rptr->r_vaddr = input_entry.old.r_vaddr; rptr->r_symndx = input_entry.old.r_symndx; rptr->r_disp = input_entry.old.r_disp; rptr->r_type = input_entry.old.r_type; } else { *rptr = input_entry.new_c; if (byte_swapped) { swap4byte(&rptr->r_vaddr); swap2byte(&rptr->r_type); /* Again, if a field reloc, fields are chars, so don't swap */ if (!isfldrel(rptr->r_type)) { swap4byte(&rptr->r_symndx); swap2byte(&rptr->r_disp); } } } #else /*-------------------------------------------------------------------------*/ /* READ IN AND BYTE SWAP AN VERSION 0 RELOC ENTRY */ /*-------------------------------------------------------------------------*/ if (fread(rptr, RELSZ, 1, fin) != 1) { load_err = E_FILE; return FALSE; } if (byte_swapped) { swap4byte(&rptr->r_vaddr); swap2byte(&rptr->r_type); /* If a field reloc, fields are chars, so don't swap */ if (!isfldrel(rptr->r_type)) { swap2byte(&rptr->r_symndx); swap2byte(&rptr->r_disp); } } #endif return TRUE; } #endif /*************************************************************************/ /* */ /* RELOC_SIZE()- */ /* Return the field size of a relocation type. */ /* */ /*************************************************************************/ int reloc_size(int type) { switch (type) { case R_PPBASE: case R_PPLBASE: return 1; case R_HIWORD: case R_C8PHIBYTE: case R_C8PMIDBYTE: case R_RELBYTE: case R_PCRBYTE: case R_RRNREG: case R_RRRELREG: case R_ANKPCR8: case R_PARTLS6: case R_PARTMS6: case R_PARTLS7: return 8; case R_PP15: case R_PP15W: case R_PP15H: case R_PP16B: case R_PPN15: case R_PPN15W: case R_PPN15H: case R_PPN16B: case R_PPL15: case R_PPL15W: case R_PPL15H: case R_PPL16B: case R_PPLN15: case R_PPLN15W: case R_PPLN15H: case R_PPLN16B: return 15; case R_LABCOD: case R_RELWORD: case R_PCRWORD: case R_ANKPCR16: case R_GSPPCR16: case R_GSPPCA16: case R_PARTLS16: case R_PARTMS8: case R_PARTMS9: case R_PARTMID10: case R_PARTMS16: case R_REL22: case R_REL13: case R_C8PVECADR: return 16; case R_REL24: case R_PCR24: case R_PCR24W: case R_C8PADR24: return 24; case R_MPPCR: case R_GSPOPR32: case R_RELLONG: case R_PCRLONG: case R_OCBD32: case R_OCRLONG: case R_DIR32: return 32; default: return 0; } } /*************************************************************************/ /* */ /* RELOC_OFFSET()- */ /* Return the offset of a relocation type field. The value of */ /* offset should be the bit offset of the LSB of the field in */ /* little-endian mode. */ /* */ /*************************************************************************/ int reloc_offset(int type) { switch (type) { case R_PP15 : case R_PP15W : case R_PP15H : case R_PP16B : case R_PPN15 : case R_PPN15W : case R_PPN15H : case R_PPN16B : case R_PPLBASE : return 22; case R_PPL15 : case R_PPL15W : case R_PPL15H : case R_PPL16B : case R_PPLN15 : case R_PPLN15W : case R_PPLN15H : case R_PPLN16B : case R_PPBASE : return 0; default : return 0; } } /*************************************************************************/ /* */ /* RELOC_STOP() - */ /* Return the number of bits to read for a relocation type. */ /* */ /*************************************************************************/ int reloc_stop(int type) { switch (type) { case R_PPBASE : case R_PPLBASE : case R_PP15 : case R_PP15W : case R_PP15H : case R_PP16B : case R_PPL15 : case R_PPL15W : case R_PPL15H : case R_PPL16B : case R_PPN15 : case R_PPN15W : case R_PPN15H : case R_PPN16B : case R_PPLN15 : case R_PPLN15W : case R_PPLN15H : case R_PPLN16B : return 64; default : return WORDSZ * 8; } } #if 0 /******************************************************************************/ /* */ /* SYM_RELOC_AMOUNT() - Determine the amount of relocation for a particular */ /* relocation entry. Search the relocation symbol table */ /* for the referenced symbol, and return the amount from */ /* the table. */ /* */ /******************************************************************************/ int sym_reloc_amount(RELOC *rp) { int index = rp->r_symndx; int i = 0, j = reloc_sym_index - 1; /*-------------------------------------------------------------------------*/ /* THIS IS A SIMPLE BINARY SEARCH (THE RELOC TABLE IS ALWAYS SORTED). */ /*-------------------------------------------------------------------------*/ while (i <= j) { int m = (i + j) / 2; if (reloc_tab[m].rt_index < index) i = m + 1; else if (reloc_tab[m].rt_index > index) j = m - 1; else return reloc_tab[m].rt_disp; /* FOUND */ } /*-------------------------------------------------------------------------*/ /* IF NOT FOUND, SYMBOL WAS NOT RELOCATED. */ /*-------------------------------------------------------------------------*/ return 0; } #endif /******************************************************************************/ /* */ /* UNPACK() - Extract a relocation field from object bytes and convert into */ /* a int so it can be relocated. */ /* */ /******************************************************************************/ unsigned int unpack(unsigned char *data, int fieldsz, int wordsz, int bit_offset) { register int i; unsigned int objval; int start; /* MS byte with reloc data */ int stop; /* LS byte with reloc data */ int r = bit_offset & 7; /* num unused LS bits in stop */ int l = 8 - r; /* num used MS bits in stop */ int tr = ((bit_offset+fieldsz-1) & 7)+1; /* # LS bits in strt*/ int tl = 8 - tr; /* num unused MS bits in start */ start = (big_e_target ? (wordsz-fieldsz-bit_offset) : (bit_offset+fieldsz-1)) >>3; stop = (big_e_target ? (wordsz-bit_offset-1) : bit_offset) >>3; if (start == stop) return (data[stop] >> r) & ((0x1 << fieldsz) - 0x1); objval = (unsigned)((data[start] << tl) & 0xFF) >> tl; if (big_e_target) for (i=start+1; istop; --i) objval = (objval << 8) | data[i]; return (objval << l) | (data[stop] >> r); } /******************************************************************************/ /* */ /* REPACK() - Encode a binary relocated field back into the object data. */ /* */ /******************************************************************************/ void repack(unsigned int objval, unsigned char *data, int fieldsz, int wordsz, int bit_offset) { register int i; int start; /* MS byte with reloc data */ int stop; /* LS byte with reloc data */ int r = bit_offset & 7; /* num unused LS bits in stop */ int l = 8 - r; /* num used MS bits in stop */ int tr = ((bit_offset+fieldsz-1) & 7)+1; /* # LS bits in strt */ unsigned int mask = (1ul << fieldsz) - 1ul; if (fieldsz < sizeof(objval)) objval &= mask; start = (big_e_target ? (wordsz-fieldsz-bit_offset) : (bit_offset+fieldsz-1)) >>3; stop = (big_e_target ? (wordsz-bit_offset-1) : bit_offset) >>3; if (start == stop) { data[stop] &= ~(mask << r); data[stop] |= (objval << r); return; } data[start] &= ~((1<>= l; if (big_e_target) for (i = stop - 1; i > start; objval >>= 8) data[i--] = objval; else for (i = stop + 1; i < start; objval >>= 8) data[i++] = objval; data[start] |= objval; } /******************************************************************************/ /* */ /* CLOAD_LINENO() - Read in, swap, and relocate line number entries. This */ /* function is not called directly by the loader, but by the */ /* application when it needs to read in line number entries. */ /* */ /******************************************************************************/ int cload_lineno(int filptr, int count, LINENO *lptr, int scnum) { /* int filptr; WHERE TO READ FROM */ /* int count; HOW MANY TO READ */ /* LINENO *lptr; WHERE TO PUT THEM */ /* int scnum; SECTION NUMBER OF THESE ENTRIES */ int i; /*------------------------------------------------------------------------*/ /* READ IN THE REQUESTED NUMBER OF LINE NUMBER ENTRIES AS A BLOCK. */ /*------------------------------------------------------------------------*/ #if FILE_BASED if (fseek(fin, filptr, 0) != 0) { load_err = E_FILE; return FALSE; } for (i = 0; i < count; i++) if (fread(lptr + i, 1, LINESZ, fin) != LINESZ) { load_err = E_FILE; return FALSE; } #else for (i = 0; i < count; i++) mem_copy((void*)(lptr+i), (void*)&gRxBuffer[filptr + i*LINESZ], LINESZ); #endif /*------------------------------------------------------------------------*/ /* SWAP AND RELOCATE EACH ENTRY, AS NECESSARY. */ /*------------------------------------------------------------------------*/ if (byte_swapped || RUN_RELOC_AMOUNT(scnum - 1)) for (i = 0; i < count; i++, lptr++) { if (byte_swapped) { swap2byte(&lptr->l_lnno); swap4byte(&lptr->l_addr.l_paddr); } if (lptr->l_lnno != 0) lptr->l_addr.l_paddr += RUN_RELOC_AMOUNT(scnum - 1); } return TRUE; } /******************************************************************************/ /* */ /* SWAP4BYTE() - Swap the order of bytes in a int. */ /* */ /******************************************************************************/ void swap4byte(void *addr) { unsigned int *value = (unsigned int *)addr; unsigned int temp1, temp2, temp3, temp4; temp1 = (*value) & 0xFF; temp2 = (*value >> 8) & 0xFF; temp3 = (*value >> 16) & 0xFF; temp4 = (*value >> 24) & 0xFF; *value = (temp1 << 24) | (temp2 << 16) | (temp3 << 8) | temp4; } /******************************************************************************/ /* */ /* SWAP2BYTE() - Swap the order of bytes in a short. */ /* */ /******************************************************************************/ void swap2byte(void *addr) { unsigned short *value = (unsigned short *)addr; unsigned short temp1,temp2; temp1 = temp2 = *value; *value = ((temp2 & 0xFF) << 8) | ((temp1 >> 8) & 0xFF); }