/* * * Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ /** * @file iblinit.c * * @brief * This file contains code which runs prior to loading the full IBL * * @details * The IBL loads itself in a two stage process. The ROM boot loader * loads this first stage IBL first. This entire program must be * endian independent in execution. * * This first loader reads the IBL parameters, and will endian * switch them if required. The PLL is configured if indicated * by the parameters. * * The I2C block which contains the I2C EEPROM address for both * the big and little endian images is then read. Based on the * endianness of the device the rest of the IBL is read from * the I2C EEPROM, and execution is transferred to the full * IBL. * * The subsequent reads are allowed to cross 16 bit i2c EEPROM * addresses. When the boundary is crossed the i2c address * field is incremented. * */ #include "ibl.h" #include "iblloc.h" #include "iblcfg.h" #include "device.h" #include "iblbtbl.h" #include "iblinit.h" #include /** * @brief * Data structures shared between the 1st and 2nd stage IBL load * are declared in a single header file, included in both stages */ #include "iblStage.h" /** * @brief * The boot table processing status is declared in the boot table wrapper, * and used here in the main status fields. */ extern Int32 btblWrapEcode; /** * @brief * The malloc function used for both boot stages of the ibl */ void *iblMalloc (Uint32 size) { return (malloc (size)); } /** * @brief * The free function used for both stages of the ibl */ void iblFree (void *mem) { free (mem); } /** * @brief * The memset function used for both stages of the ibl */ void *iblMemset (void *mem, Int32 ch, Uint32 n) { return (memset (mem, ch, n)); } /** * @brief * The memcpy function used for both stages of the ibl */ void *iblMemcpy (void *s1, const void *s2, Uint32 n) { return (memcpy (s1, s2, n)); } /** * @brief * Ones complement addition */ inline uint16 onesComplementAdd (uint16 value1, uint16 value2) { uint32 result; result = (uint32)value1 + (uint32)value2; result = (result >> 16) + (result & 0xFFFF); /* add in carry */ result += (result >> 16); /* maybe one more */ return ((uint16)result); } /** * @brief * Ones complement checksum computation */ uint16 onesComplementChksum (uint16 * restrict p_data, uint16 len) { uint16 chksum = 0; while (len > 0) { chksum = onesComplementAdd(chksum, *p_data); p_data++; len--; } return (chksum); } /** * @brief * Do a 4 byte endian swap */ uint32 swap32val (uint32 v) { v = (((v >> 24) & 0xff) << 0) | (((v >> 16) & 0xff) << 8) | (((v >> 8) & 0xff) << 16) | (((v >> 0) & 0xff) << 24); return (v); } /** * @brief * Do a 2 byte endian swap */ uint16 swap16val (uint16 v) { v = (((v >> 8) & 0xff) << 0) | (((v >> 0) & 0xff) << 8); return (v); } /** * @brief * Do an endian swap on the ibl structure */ void iblSwap (void) { int i, j, k; ibl.iblMagic = swap32val (ibl.iblMagic); for (i = 0; i < ibl_N_PLL_CFGS; i++) { ibl.pllConfig[i].doEnable = swap16val (ibl.pllConfig[i].doEnable); ibl.pllConfig[i].prediv = swap32val (ibl.pllConfig[i].prediv); ibl.pllConfig[i].mult = swap32val (ibl.pllConfig[i].mult); ibl.pllConfig[i].postdiv = swap32val (ibl.pllConfig[i].postdiv); ibl.pllConfig[i].pllOutFreqMhz = swap32val (ibl.pllConfig[i].pllOutFreqMhz); } ibl.ddrConfig.configDdr = swap16val (ibl.ddrConfig.configDdr); if (targetEmifType() == ibl_EMIF_TYPE_31) { ibl.ddrConfig.uEmif.emif3p1.sdcfg = swap32val(ibl.ddrConfig.uEmif.emif3p1.sdcfg); ibl.ddrConfig.uEmif.emif3p1.sdrfc = swap32val(ibl.ddrConfig.uEmif.emif3p1.sdrfc); ibl.ddrConfig.uEmif.emif3p1.sdtim1 = swap32val(ibl.ddrConfig.uEmif.emif3p1.sdtim1); ibl.ddrConfig.uEmif.emif3p1.sdtim2 = swap32val(ibl.ddrConfig.uEmif.emif3p1.sdtim2); ibl.ddrConfig.uEmif.emif3p1.dmcctl = swap32val(ibl.ddrConfig.uEmif.emif3p1.dmcctl); } else if (targetEmifType() == ibl_EMIF_TYPE_40) { ibl.ddrConfig.uEmif.emif4p0.registerMask = swap32val(ibl.ddrConfig.uEmif.emif4p0.registerMask); ibl.ddrConfig.uEmif.emif4p0.sdRamConfig = swap32val(ibl.ddrConfig.uEmif.emif4p0.sdRamConfig); ibl.ddrConfig.uEmif.emif4p0.sdRamConfig2 = swap32val(ibl.ddrConfig.uEmif.emif4p0.sdRamConfig2); ibl.ddrConfig.uEmif.emif4p0.sdRamRefreshCtl = swap32val(ibl.ddrConfig.uEmif.emif4p0.sdRamRefreshCtl); ibl.ddrConfig.uEmif.emif4p0.sdRamTiming1 = swap32val(ibl.ddrConfig.uEmif.emif4p0.sdRamTiming1); ibl.ddrConfig.uEmif.emif4p0.sdRamTiming2 = swap32val(ibl.ddrConfig.uEmif.emif4p0.sdRamTiming2); ibl.ddrConfig.uEmif.emif4p0.sdRamTiming3 = swap32val(ibl.ddrConfig.uEmif.emif4p0.sdRamTiming3); ibl.ddrConfig.uEmif.emif4p0.lpDdrNvmTiming = swap32val(ibl.ddrConfig.uEmif.emif4p0.lpDdrNvmTiming); ibl.ddrConfig.uEmif.emif4p0.powerManageCtl = swap32val(ibl.ddrConfig.uEmif.emif4p0.powerManageCtl); ibl.ddrConfig.uEmif.emif4p0.iODFTTestLogic = swap32val(ibl.ddrConfig.uEmif.emif4p0.iODFTTestLogic); ibl.ddrConfig.uEmif.emif4p0.performCountCfg = swap32val(ibl.ddrConfig.uEmif.emif4p0.performCountCfg); ibl.ddrConfig.uEmif.emif4p0.performCountMstRegSel = swap32val(ibl.ddrConfig.uEmif.emif4p0.performCountMstRegSel); ibl.ddrConfig.uEmif.emif4p0.readIdleCtl = swap32val(ibl.ddrConfig.uEmif.emif4p0.readIdleCtl); ibl.ddrConfig.uEmif.emif4p0.sysVbusmIntEnSet = swap32val(ibl.ddrConfig.uEmif.emif4p0.sysVbusmIntEnSet); ibl.ddrConfig.uEmif.emif4p0.sdRamOutImpdedCalCfg = swap32val(ibl.ddrConfig.uEmif.emif4p0.sdRamOutImpdedCalCfg); ibl.ddrConfig.uEmif.emif4p0.tempAlterCfg = swap32val(ibl.ddrConfig.uEmif.emif4p0.tempAlterCfg); ibl.ddrConfig.uEmif.emif4p0.ddrPhyCtl1 = swap32val(ibl.ddrConfig.uEmif.emif4p0.ddrPhyCtl1); ibl.ddrConfig.uEmif.emif4p0.ddrPhyCtl2 = swap32val(ibl.ddrConfig.uEmif.emif4p0.ddrPhyCtl2); ibl.ddrConfig.uEmif.emif4p0.priClassSvceMap = swap32val(ibl.ddrConfig.uEmif.emif4p0.priClassSvceMap); ibl.ddrConfig.uEmif.emif4p0.mstId2ClsSvce1Map = swap32val(ibl.ddrConfig.uEmif.emif4p0.mstId2ClsSvce1Map); ibl.ddrConfig.uEmif.emif4p0.mstId2ClsSvce2Map = swap32val(ibl.ddrConfig.uEmif.emif4p0.mstId2ClsSvce2Map); ibl.ddrConfig.uEmif.emif4p0.eccCtl = swap32val(ibl.ddrConfig.uEmif.emif4p0.eccCtl); ibl.ddrConfig.uEmif.emif4p0.eccRange1 = swap32val(ibl.ddrConfig.uEmif.emif4p0.eccRange1); ibl.ddrConfig.uEmif.emif4p0.eccRange2 = swap32val(ibl.ddrConfig.uEmif.emif4p0.eccRange2); ibl.ddrConfig.uEmif.emif4p0.rdWrtExcThresh = swap32val(ibl.ddrConfig.uEmif.emif4p0.rdWrtExcThresh); } for (i = 0; i < ibl_N_ETH_PORTS; i++) { ibl.sgmiiConfig[i].configure = swap16val(ibl.sgmiiConfig[i].configure); ibl.sgmiiConfig[i].adviseAbility = swap32val(ibl.sgmiiConfig[i].adviseAbility); ibl.sgmiiConfig[i].control = swap32val(ibl.sgmiiConfig[i].control); ibl.sgmiiConfig[i].txConfig = swap32val(ibl.sgmiiConfig[i].txConfig); ibl.sgmiiConfig[i].rxConfig = swap32val(ibl.sgmiiConfig[i].rxConfig); ibl.sgmiiConfig[i].auxConfig = swap32val(ibl.sgmiiConfig[i].auxConfig); } ibl.mdioConfig.nMdioOps = swap16val (ibl.mdioConfig.nMdioOps); ibl.mdioConfig.mdioClkDiv = swap16val (ibl.mdioConfig.mdioClkDiv); ibl.mdioConfig.interDelay = swap32val (ibl.mdioConfig.interDelay); for (i = 0; i < ibl_N_MDIO_CFGS; i++) ibl.mdioConfig.mdio[i] = swap32val (ibl.mdioConfig.mdio[i]); ibl.spiConfig.addrWidth = swap16val(ibl.spiConfig.addrWidth); ibl.spiConfig.nPins = swap16val(ibl.spiConfig.nPins); ibl.spiConfig.mode = swap16val(ibl.spiConfig.mode); ibl.spiConfig.csel = swap16val(ibl.spiConfig.csel); ibl.spiConfig.c2tdelay = swap16val(ibl.spiConfig.c2tdelay); ibl.spiConfig.busFreqMHz = swap16val(ibl.spiConfig.busFreqMHz); for (i = 0; i < ibl_MAX_EMIF_PMEM; i++) { ibl.emifConfig[i].csSpace = swap16val(ibl.emifConfig[i].csSpace); ibl.emifConfig[i].busWidth = swap16val(ibl.emifConfig[i].busWidth); ibl.emifConfig[i].waitEnable = swap16val(ibl.emifConfig[i].waitEnable); } for (i = 0; i < ibl_N_BOOT_MODES; i++) { ibl.bootModes[i].bootMode = swap32val(ibl.bootModes[i].bootMode); ibl.bootModes[i].priority = swap32val(ibl.bootModes[i].priority); ibl.bootModes[i].port = swap32val(ibl.bootModes[i].port); if (ibl.bootModes[i].bootMode == ibl_BOOT_MODE_TFTP) { ibl.bootModes[i].u.ethBoot.doBootp = swap16val(ibl.bootModes[i].u.ethBoot.doBootp); ibl.bootModes[i].u.ethBoot.useBootpServerIp = swap16val(ibl.bootModes[i].u.ethBoot.useBootpServerIp); ibl.bootModes[i].u.ethBoot.useBootpFileName = swap16val(ibl.bootModes[i].u.ethBoot.useBootpFileName); ibl.bootModes[i].u.ethBoot.bootFormat = swap32val(ibl.bootModes[i].u.ethBoot.bootFormat); ibl.bootModes[i].u.ethBoot.blob.startAddress = swap32val(ibl.bootModes[i].u.ethBoot.blob.startAddress); ibl.bootModes[i].u.ethBoot.blob.sizeBytes = swap32val(ibl.bootModes[i].u.ethBoot.blob.sizeBytes); ibl.bootModes[i].u.ethBoot.blob.branchAddress = swap32val(ibl.bootModes[i].u.ethBoot.blob.branchAddress); } else if (ibl.bootModes[i].bootMode == ibl_BOOT_MODE_NAND) { ibl.bootModes[i].u.nandBoot.bootFormat = swap32val(ibl.bootModes[i].u.nandBoot.bootFormat); for (j = 0; j < ibl_N_ENDIANS; j++) { for (k = 0; k < ibl_N_IMAGES; k++) { ibl.bootModes[i].u.nandBoot.bootAddress[j][k] = swap32val(ibl.bootModes[i].u.nandBoot.bootAddress[j][k]); } } ibl.bootModes[i].u.nandBoot.interface = swap32val(ibl.bootModes[i].u.nandBoot.interface); for (j = 0; j < ibl_N_ENDIANS; j++) { for (k = 0; k < ibl_N_IMAGES; k++) { ibl.bootModes[i].u.nandBoot.blob[j][k].startAddress = swap32val(ibl.bootModes[i].u.nandBoot.blob[j][k].startAddress); ibl.bootModes[i].u.nandBoot.blob[j][k].sizeBytes = swap32val(ibl.bootModes[i].u.nandBoot.blob[j][k].sizeBytes); ibl.bootModes[i].u.nandBoot.blob[j][k].branchAddress = swap32val(ibl.bootModes[i].u.nandBoot.blob[j][k].branchAddress); } } ibl.bootModes[i].u.nandBoot.nandInfo.busWidthBits = swap32val(ibl.bootModes[i].u.nandBoot.nandInfo.busWidthBits); ibl.bootModes[i].u.nandBoot.nandInfo.pageSizeBytes = swap32val(ibl.bootModes[i].u.nandBoot.nandInfo.pageSizeBytes); ibl.bootModes[i].u.nandBoot.nandInfo.pageEccBytes = swap32val(ibl.bootModes[i].u.nandBoot.nandInfo.pageEccBytes); ibl.bootModes[i].u.nandBoot.nandInfo.pagesPerBlock = swap32val(ibl.bootModes[i].u.nandBoot.nandInfo.pagesPerBlock); ibl.bootModes[i].u.nandBoot.nandInfo.totalBlocks = swap32val(ibl.bootModes[i].u.nandBoot.nandInfo.totalBlocks); ibl.bootModes[i].u.nandBoot.nandInfo.addressBytes = swap32val(ibl.bootModes[i].u.nandBoot.nandInfo.addressBytes); ibl.bootModes[i].u.nandBoot.nandInfo.lsbFirst = swap16val(ibl.bootModes[i].u.nandBoot.nandInfo.lsbFirst); ibl.bootModes[i].u.nandBoot.nandInfo.blockOffset = swap32val(ibl.bootModes[i].u.nandBoot.nandInfo.blockOffset); ibl.bootModes[i].u.nandBoot.nandInfo.pageOffset = swap32val(ibl.bootModes[i].u.nandBoot.nandInfo.pageOffset); ibl.bootModes[i].u.nandBoot.nandInfo.columnOffset = swap32val(ibl.bootModes[i].u.nandBoot.nandInfo.columnOffset); /*for (j = 0; j < ibl_N_ECC_BYTES; j++) { ibl.bootModes[i].u.nandBoot.nandInfo.eccBytesIdx[j] = swap32val(ibl.bootModes[i].u.nandBoot.nandInfo.eccBytesIdx[j]); } for (j = 0; j < ibl_N_BAD_BLOCK_PAGE; j++) { ibl.bootModes[i].u.nandBoot.nandInfo.badBlkMarkIdx[j] = swap32val(ibl.bootModes[i].u.nandBoot.nandInfo.badBlkMarkIdx[j]); } ibl.bootModes[i].u.nandBoot.nandInfo.postCommand = swap16val(ibl.bootModes[i].u.nandBoot.nandInfo.postCommand);*/ } else if (ibl.bootModes[i].bootMode == ibl_BOOT_MODE_NOR) { ibl.bootModes[i].u.norBoot.bootFormat = swap32val(ibl.bootModes[i].u.norBoot.bootFormat); for (j = 0; j < ibl_N_ENDIANS; j++) { for (k = 0; k < ibl_N_IMAGES; k++) { ibl.bootModes[i].u.norBoot.bootAddress[j][k] = swap32val(ibl.bootModes[i].u.norBoot.bootAddress[j][k]); } } ibl.bootModes[i].u.norBoot.interface = swap32val(ibl.bootModes[i].u.norBoot.interface); for (j = 0; j < ibl_N_ENDIANS; j++) { for (k = 0; k < ibl_N_IMAGES; k++) { ibl.bootModes[i].u.norBoot.blob[j][k].startAddress = swap32val(ibl.bootModes[i].u.norBoot.blob[j][k].startAddress); ibl.bootModes[i].u.norBoot.blob[j][k].sizeBytes = swap32val(ibl.bootModes[i].u.norBoot.blob[j][k].sizeBytes); ibl.bootModes[i].u.norBoot.blob[j][k].branchAddress = swap32val(ibl.bootModes[i].u.norBoot.blob[j][k].branchAddress); } } } } ibl.chkSum = swap16val (ibl.chkSum); } /** * @brief * The init load context consists of the address of the next block * to read, and a simple fifo-ish structure holding any existing data. * * A full fifo is not defined here. The individual init load blocks * (I2C, SPI NOR, SPI NAND) will poke the structure values directly * to minimize the compiled code size. Most notably is the absence * of the write function. This fifo will always be completely emptied * before any writes are done, so writes are always done from the top. */ uint32 iFifoIn = 0; uint32 iFifoOut = 0; uint8 iData[I_MAX_BLOCK_SIZE]; /** * @brief * Checkum calculation. 16 bit values constructed from received bytes * always in big endian format, regardless of the endianness of the device */ uint16 iSum[I_MAX_BLOCK_SIZE >> 1]; /** * @brief * Return the number of elements in the fifo */ Uint32 iFifoCount (void) { Int32 count; if (iFifoIn >= iFifoOut) count = iFifoIn - iFifoOut; else count = iFifoIn + I_MAX_BLOCK_SIZE - iFifoOut; return (count); } /** * @brief * Read a byte from the fifo */ Uint8 iFifoRead(void) { Uint8 v; v = iData[iFifoOut]; iFifoOut += 1; if (iFifoOut == iFifoIn) iFifoOut = iFifoIn = 0; if (iFifoOut >= I_MAX_BLOCK_SIZE) iFifoOut = 0; return (v); } #define iblBITMASK(x,y) ( ( ( ((UINT32)1 << (((UINT32)x)-((UINT32)y)+(UINT32)1) ) - (UINT32)1 ) ) << ((UINT32)y) ) #define iblREAD_BITFIELD(z,x,y) (((UINT32)z) & iblBITMASK(x,y)) >> (y) /** * @brief * Return the lower 16 bits of a 32 bit value. A function is used (with cross-function optomization off) * which results in an endian independent version */ uint16 readLower16 (uint32 v) { return (iblREAD_BITFIELD(v,15,0)); } /** * @brief * Return the upper 16 bits of a 32 bit value. A function is used to force an endian independent version */ uint16 readUpper16 (uint32 v) { return (iblREAD_BITFIELD(v,31,16)); } /** * @brief * The main function * * @details * The ibl configuration parameters are read from the i2c, * followed by the i2c mapping information. The second stage * of the IBL is then loaded, and execution transferred * to the second stage. */ void main (void) { int32 bootDevice; uint32 entry; void (*exit)(); BOOT_MODULE_FXN_TABLE *bFxnTbl; memset (&iblStatus, 0, sizeof(iblStatus_t)); iblStatus.iblMagic = ibl_MAGIC_VALUE; iblStatus.iblVersion = ibl_VERSION; iblStatus.activeDevice = ibl_ACTIVE_DEVICE_I2C; /* Determine the boot device to read from */ bootDevice = deviceReadBootDevice(); switch (bootDevice) { #ifndef EXCLUDE_I2C case BOOT_DEVICE_I2C: bFxnTbl = iblInitI2c (); break; #endif #ifndef EXCLUDE_NOR_SPI case BOOT_DEVICE_SPI_NOR: bFxnTbl = iblInitSpiNor (); break; #endif default: iblStatus.iblFail = ibl_FAIL_CODE_INVALID_INIT_DEVICE; for (;;); } /* Pll configuration is device specific */ devicePllConfig (); /* Enable the EDC for local memory */ if (IBL_ENABLE_EDC) { iblEnableEDC (); } /* Check if need to enter Rom boot loader again */ if (IBL_ENTER_ROM) { iblEnterRom (); } /* Pass control to the boot table processor */ iblBootBtbl (bFxnTbl, &entry); if (btblWrapEcode != 0) { iblStatus.iblFail = ibl_FAIL_CODE_BTBL_FAIL; for (;;); } /* jump to the exit point, which will be the entry point for the full IBL */ exit = (void (*)())entry; (*exit)(); }