/** * @file iblinit.c * * @brief * This file contains code which runs prior to loading the full IBL * * @details * The IBL loads itself in a two stage process. The ROM boot loader * loads this first stage IBL first. This entire program must be * endian independent in execution. * * This first loader reads the IBL parameters, and will endian * switch them if required. The PLL is configured if indicated * by the parameters. * * The I2C block which contains the I2C EEPROM address for both * the big and little endian images is then read. Based on the * endianness of the device the rest of the IBL is read from * the I2C EEPROM, and execution is transferred to the full * IBL. * * The subsequent reads are allowed to cross 16 bit i2c EEPROM * addresses. When the boundary is crossed the i2c address * field is incremented. * */ #include "ibl.h" #include "iblloc.h" #include "iblcfg.h" #include "device.h" #include "iblbtbl.h" #include "i2c.h" #include /** * @brief * Data structures shared between the 1st and 2nd stage IBL load * are declared in a single header file, included in both stages */ #include "iblStage.h" /** * @brief * byte swapping of i2c data must be done when in little endian mode */ bool littleEndian; /** * @brief * The boot table processing status is declared in the boot table wrapper, * and used here in the main status fields. */ extern Int32 btblWrapEcode; /** * @brief * The malloc function used for both boot stages of the ibl */ void *iblMalloc (Uint32 size) { return (malloc (size)); } /** * @brief * The free function used for both stages of the ibl */ void iblFree (void *mem) { free (mem); } /** * @brief * The memset function used for both stages of the ibl */ void *iblMemset (void *mem, Int32 ch, Uint32 n) { return (memset (mem, ch, n)); } /** * @brief * The memcpy function used for both stages of the ibl */ void *iblMemcpy (void *s1, const void *s2, Uint32 n) { return (memcpy (s1, s2, n)); } /** * @brief * Ones complement addition */ inline uint16 onesComplementAdd (uint16 value1, uint16 value2) { uint32 result; result = (uint32)value1 + (uint32)value2; result = (result >> 16) + (result & 0xFFFF); /* add in carry */ result += (result >> 16); /* maybe one more */ return ((uint16)result); } /** * @brief * Ones complement checksum computation */ uint16 onesComplementChksum (uint16 * restrict p_data, uint16 len) { uint16 chksum = 0; while (len > 0) { chksum = onesComplementAdd(chksum, *p_data); p_data++; len--; } return (chksum); } /** * @brief * Do a 4 byte endian swap */ uint32 swap32val (uint32 v) { v = (((v >> 24) & 0xff) << 0) | (((v >> 16) & 0xff) << 8) | (((v >> 8) & 0xff) << 16) | (((v >> 0) & 0xff) << 24); return (v); } /** * @brief * Do a 2 byte endian swap */ uint16 swap16val (uint16 v) { v = (((v >> 8) & 0xff) << 0) | (((v >> 0) & 0xff) << 8); return (v); } /** * @brief * Do an endian swap on the ibl structure */ void iblSwap (void) { int i; ibl.iblMagic = swap32val (ibl.iblMagic); for (i = 0; i < ibl_N_PLL_CFGS; i++) { ibl.pllConfig[i].doEnable = swap16val (ibl.pllConfig[i].doEnable); ibl.pllConfig[i].prediv = swap32val (ibl.pllConfig[i].prediv); ibl.pllConfig[i].mult = swap32val (ibl.pllConfig[i].mult); ibl.pllConfig[i].postdiv = swap32val (ibl.pllConfig[i].postdiv); ibl.pllConfig[i].pllOutFreqMhz = swap32val (ibl.pllConfig[i].pllOutFreqMhz); } ibl.ddrConfig.configDdr = swap16val (ibl.ddrConfig.configDdr); ibl.ddrConfig.uEmif.emif3p1.sdcfg = swap32val(ibl.ddrConfig.uEmif.emif3p1.sdcfg); ibl.ddrConfig.uEmif.emif3p1.sdrfc = swap32val(ibl.ddrConfig.uEmif.emif3p1.sdrfc); ibl.ddrConfig.uEmif.emif3p1.sdtim1 = swap32val(ibl.ddrConfig.uEmif.emif3p1.sdtim1); ibl.ddrConfig.uEmif.emif3p1.sdtim2 = swap32val(ibl.ddrConfig.uEmif.emif3p1.sdtim2); ibl.ddrConfig.uEmif.emif3p1.dmcctl = swap32val(ibl.ddrConfig.uEmif.emif3p1.dmcctl); for (i = 0; i < ibl_N_ETH_PORTS; i++) { ibl.ethConfig[i].ethPriority = swap32val (ibl.ethConfig[i].ethPriority); ibl.ethConfig[i].port = swap32val (ibl.ethConfig[i].port); ibl.ethConfig[i].doBootp = swap16val (ibl.ethConfig[i].doBootp); ibl.ethConfig[i].useBootpServerIp = swap16val (ibl.ethConfig[i].useBootpServerIp); ibl.ethConfig[i].useBootpFileName = swap16val (ibl.ethConfig[i].useBootpFileName); ibl.ethConfig[i].bootFormat = swap32val (ibl.ethConfig[i].bootFormat); ibl.ethConfig[i].blob.startAddress = swap32val (ibl.ethConfig[i].blob.startAddress); ibl.ethConfig[i].blob.sizeBytes = swap32val (ibl.ethConfig[i].blob.sizeBytes); ibl.ethConfig[i].blob.branchAddress = swap32val (ibl.ethConfig[i].blob.branchAddress); ibl.sgmiiConfig[i].adviseAbility = swap32val (ibl.sgmiiConfig[i].adviseAbility); ibl.sgmiiConfig[i].control = swap32val (ibl.sgmiiConfig[i].control); ibl.sgmiiConfig[i].txConfig = swap32val (ibl.sgmiiConfig[i].txConfig); ibl.sgmiiConfig[i].rxConfig = swap32val (ibl.sgmiiConfig[i].rxConfig); ibl.sgmiiConfig[i].auxConfig = swap32val (ibl.sgmiiConfig[i].auxConfig); } ibl.mdioConfig.nMdioOps = swap16val (ibl.mdioConfig.nMdioOps); ibl.mdioConfig.mdioClkDiv = swap16val (ibl.mdioConfig.mdioClkDiv); ibl.mdioConfig.interDelay = swap32val (ibl.mdioConfig.interDelay); for (i = 0; i < ibl_N_MDIO_CFGS; i++) ibl.mdioConfig.mdio[i] = swap32val (ibl.mdioConfig.mdio[i]); ibl.nandConfig.nandPriority = swap32val (ibl.nandConfig.nandPriority); ibl.nandConfig.bootFormat = swap32val (ibl.nandConfig.bootFormat); ibl.nandConfig.blob.startAddress = swap32val (ibl.nandConfig.blob.startAddress); ibl.nandConfig.blob.sizeBytes = swap32val (ibl.nandConfig.blob.sizeBytes); ibl.nandConfig.blob.branchAddress = swap32val (ibl.nandConfig.blob.branchAddress); ibl.nandConfig.nandInfo.busWidthBits = swap32val (ibl.nandConfig.nandInfo.busWidthBits); ibl.nandConfig.nandInfo.pageSizeBytes = swap32val (ibl.nandConfig.nandInfo.pageSizeBytes); ibl.nandConfig.nandInfo.pageEccBytes = swap32val (ibl.nandConfig.nandInfo.pageEccBytes); ibl.nandConfig.nandInfo.pagesPerBlock = swap32val (ibl.nandConfig.nandInfo.pagesPerBlock); ibl.nandConfig.nandInfo.totalBlocks = swap32val (ibl.nandConfig.nandInfo.totalBlocks); ibl.nandConfig.nandInfo.addressBytes = swap32val (ibl.nandConfig.nandInfo.addressBytes); ibl.nandConfig.nandInfo.lsbFirst = swap16val (ibl.nandConfig.nandInfo.lsbFirst); ibl.nandConfig.nandInfo.blockOffset = swap32val (ibl.nandConfig.nandInfo.blockOffset); ibl.nandConfig.nandInfo.pageOffset = swap32val (ibl.nandConfig.nandInfo.pageOffset); ibl.nandConfig.nandInfo.columnOffset = swap32val (ibl.nandConfig.nandInfo.columnOffset); ibl.nandConfig.nandInfo.postCommand = swap16val (ibl.nandConfig.nandInfo.postCommand); ibl.chkSum = swap16val (ibl.chkSum); } /** * @brief * The i2c load context consists of the address of the next block * to read, and a simple fifo holding any existing data. */ #define I2C_MAX_BLOCK_SIZE 0x80 uint32 i2cReadAddress; uint32 i2cFifoIn = 0; uint32 i2cFifoOut = 0; uint8 i2cData[I2C_MAX_BLOCK_SIZE]; uint16 i2cSum[I2C_MAX_BLOCK_SIZE >> 1]; /** * @brief * Return the number of elements in the fifo */ Uint32 i2cFifoCount (void) { Int32 count; if (i2cFifoIn >= i2cFifoOut) count = i2cFifoIn - i2cFifoOut; else count = i2cFifoIn + I2C_MAX_BLOCK_SIZE - i2cFifoOut; return (count); } /** * @brief * Read a byte from the fifo */ Uint8 i2cFifoRead(void) { Uint8 v; v = i2cData[i2cFifoOut]; i2cFifoOut += 1; if (i2cFifoOut == i2cFifoIn) i2cFifoOut = i2cFifoIn = 0; if (i2cFifoOut >= I2C_MAX_BLOCK_SIZE) i2cFifoOut = 0; return (v); } /** * @brief * Read a block of data from the I2C eeprom and put it in the fifo */ void i2cReadBlock (void) { uint16 len; int32 i, j; uint32 v; for (;;) { while (hwI2cMasterRead (i2cReadAddress & 0xffff, /* The address on the eeprom of the table */ 4, /* The number of bytes to read */ i2cData, /* Where to store the bytes */ i2cReadAddress >> 16, /* The bus address of the eeprom */ IBL_I2C_CFG_ADDR_DELAY) /* The delay between sending the address and reading data */ != I2C_RET_OK) { iblStatus.i2cDataRetries += 1; } /* Form the length. The received bytes are always in big endian format */ len = (i2cData[0] << 8) | i2cData[1]; if (len > I2C_MAX_BLOCK_SIZE) continue; while (hwI2cMasterRead (i2cReadAddress & 0xffff, /* The address on the eeprom of the table */ len, /* The number of bytes to read */ i2cData, /* Where to store the bytes */ i2cReadAddress >> 16, /* The bus address of the eeprom */ IBL_I2C_CFG_ADDR_DELAY) /* The delay between sending the address and reading data */ != I2C_RET_OK) { iblStatus.i2cDataRetries += 1; } /* Must do endian conversion to verify the checksum */ for (i = j = 0; i < len; i += 2, j += 1) i2cSum[j] = (i2cData[i+0] << 8) | i2cData[i+1]; v = onesComplementChksum (i2cSum, j); if ((v == 0) || (v == 0xffff)) break; iblStatus.i2cDataRetries += 1; } i2cReadAddress += len; i2cFifoIn = len; i2cFifoOut = 4; /* The i2c header is effectively removed */ } /** * @brief * Read data from the I2C to pass to the interpreter */ Int32 iblI2cRead (Uint8 *buf, Uint32 num_bytes) { int i; for (i = 0; i < num_bytes; i++) { if (i2cFifoCount() == 0) i2cReadBlock (); buf[i] = i2cFifoRead(); } return (0); } #define iblBITMASK(x,y) ( ( ( ((UINT32)1 << (((UINT32)x)-((UINT32)y)+(UINT32)1) ) - (UINT32)1 ) ) << ((UINT32)y) ) #define iblREAD_BITFIELD(z,x,y) (((UINT32)z) & iblBITMASK(x,y)) >> (y) /** * @brief * Return the lower 16 bits of a 32 bit value. A function is used (with cross-function optomization off) * which results in an endian independent version */ uint16 readLower16 (uint32 v) { return (iblREAD_BITFIELD(v,15,0)); } /** * @brief * Return the upper 16 bits of a 32 bit value. A function is used to force an endian independent version */ uint16 readUpper16 (uint32 v) { return (iblREAD_BITFIELD(v,31,16)); } /** * @brief * The module function table used for boot from i2c */ BOOT_MODULE_FXN_TABLE i2cinit_boot_module = { NULL, /* Open API */ NULL, /* Close API */ iblI2cRead, /* Read API */ NULL, /* Write API */ NULL, /* Peek API */ NULL, /* Seek API */ NULL /* Query API */ }; /** * @brief * The main function * * @details * The ibl configuration parameters are read from the i2c, * followed by the i2c mapping information. The second stage * of the IBL is then loaded, and execution transferred * to the second stage. */ void main (void) { uint16 v; uint16 configAddrLsw; uint16 configAddrMsw; uint32 entry; void (*exit)(); iblI2cMap_t map; memset (&iblStatus, 0, sizeof(iblStatus_t)); iblStatus.iblMagic = ibl_MAGIC_VALUE; /* Read the endianness setting of the device */ littleEndian = deviceIsLittleEndian(); /* Load the default configuration table from the i2c. The actual speed of the device * isn't really known here, since it is part of the table, so a compile time * value is used (the pll may have been configured during the initial load) */ hwI2Cinit (IBL_I2C_DEV_FREQ_MHZ, /* The CPU frequency during I2C data load */ DEVICE_I2C_MODULE_DIVISOR, /* The divide down of CPU that drives the i2c */ IBL_I2C_CLK_FREQ_KHZ, /* The I2C data rate used during table load */ IBL_I2C_OWN_ADDR); /* The address used by this device on the i2c bus */ /* Read the I2C mapping information from the eeprom */ for (;;) { if (hwI2cMasterRead (IBL_I2C_MAP_TABLE_DATA_ADDR, /* The address on the eeprom of the data mapping */ sizeof(iblI2cMap_t), /* The number of bytes to read */ (UINT8 *)&map, /* Where to store the bytes */ IBL_I2C_MAP_TABLE_DATA_BUS_ADDR, /* The bus address of the eeprom */ IBL_I2C_CFG_ADDR_DELAY) /* The delay between sending the address and reading data */ == I2C_RET_OK) { /* On the I2C EEPROM the table is always formatted with the most significant * byte first. So if the device is running little endain the endian must be * swapped */ if (littleEndian == TRUE) { map.length = swap16val (map.length); map.chkSum = swap16val (map.chkSum); map.addrLe = swap32val (map.addrLe); map.configLe = swap32val (map.configLe); map.addrBe = swap32val (map.addrBe); map.configBe = swap32val (map.configBe); configAddrLsw = readLower16 (map.configLe); configAddrMsw = readUpper16 (map.configLe); } else { configAddrLsw = readLower16 (map.configBe); configAddrMsw = readUpper16 (map.configLe); } if (map.length != sizeof(iblI2cMap_t)) { iblStatus.mapSizeFail += 1; continue; } if (map.chkSum != 0) { v = onesComplementChksum ((UINT16 *)&map, sizeof(iblI2cMap_t)); if ((v != 0) && (v != 0xffff)) { iblStatus.mapRetries += 1; continue; } } break; } iblStatus.mapRetries += 1; } /* Read the i2c configuration tables until the checksum passes and the magic number * matches. The checksum must be verified before the endian re-ordering is done */ for (;;) { if (hwI2cMasterRead (configAddrLsw, /* The address on the eeprom of the table */ sizeof(ibl_t), /* The number of bytes to read */ (UINT8 *)&ibl, /* Where to store the bytes */ configAddrMsw, /* The bus address of the eeprom */ IBL_I2C_CFG_ADDR_DELAY) /* The delay between sending the address and reading data */ == I2C_RET_OK) { if (ibl.chkSum != 0) { v = onesComplementChksum ((UINT16 *)&ibl, sizeof(ibl_t) / sizeof(UINT16)); if ((v != 0) && (v != 0xffff)) { iblStatus.i2cRetries += 1; continue; } } if (ibl.iblMagic == ibl_MAGIC_VALUE) break; if (swap32val (ibl.iblMagic) == ibl_MAGIC_VALUE) { iblSwap (); break; } iblStatus.magicRetries += 1; } iblStatus.i2cRetries += 1; } /* Pll configuration is device specific */ devicePllConfig (); /* The rest of the IBL is in boot table format. Read and process the data */ if (littleEndian == TRUE) i2cReadAddress = map.addrLe; else i2cReadAddress = map.addrBe; if (i2cReadAddress == 0xffffffff) { iblStatus.iblFail = ibl_FAIL_CODE_INVALID_I2C_ADDRESS; for (;;); } /* Pass control to the boot table processor */ iblBootBtbl (&i2cinit_boot_module, &entry); if (btblWrapEcode != 0) { iblStatus.iblFail = ibl_FAIL_CODE_BTBL_FAIL; for (;;); } /* jump to the exit point, which will be the entry point for the full IBL */ exit = (void (*)())entry; (*exit)(); }