/* * * Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ #include "ibl.h" #include "iblloc.h" #include "iblcfg.h" #include "device.h" #include "iblbtbl.h" #include "spi_api.h" #include "iblinit.h" #include #if (!defined(EXCLUDE_NOR_SPI) || !defined(EXCLUDE_NAND_SPI)) /** * @brief * The next read address on the SPI flash is stored in a global for * access through the boot call chain. */ uint32 spiReadAddress; /** * @brief * Read a block of data from the SPI eeprom and put it in the fifo */ void spiReadBlock (void) { uint16 len; int32 i, j; uint32 v; for (;;) { while (hwSpiRead (spiReadAddress, /* The address on the eeprom of the table */ 4, /* The number of bytes to read */ iData) /* Where to store the bytes */ != 0) { iblStatus.spiDataRetries += 1; } /* Form the length. The received bytes are always in big endian format */ len = (iData[0] << 8) | iData[1]; if (len > I_MAX_BLOCK_SIZE) continue; while (hwSpiRead (spiReadAddress, /* The address on the eeprom of the table */ len, /* The number of bytes to read */ iData) /* Where to store the bytes */ != 0) { iblStatus.spiDataRetries += 1; } /* Must do endian conversion to verify the checksum */ for (i = j = 0; i < len; i += 2, j += 1) iSum[j] = (iData[i+0] << 8) | iData[i+1]; v = onesComplementChksum (iSum, j); if ((v == 0) || (v == 0xffff)) break; iblStatus.spiDataRetries += 1; } spiReadAddress += len; iFifoIn = len; iFifoOut = 4; /* The spi header is effectively removed */ } /** * @brief * Read data from the SPI to pass to the interpreter */ Int32 iblSpiRead (Uint8 *buf, Uint32 num_bytes) { int i; for (i = 0; i < num_bytes; i++) { if (iFifoCount() == 0) spiReadBlock (); buf[i] = iFifoRead(); } return (0); } /** * @brief * The module function table used for boot from spi */ BOOT_MODULE_FXN_TABLE spiinit_boot_module = { NULL, /* Open API */ NULL, /* Close API */ iblSpiRead, /* Read API */ NULL, /* Write API */ NULL, /* Peek API */ NULL, /* Seek API */ NULL /* Query API */ }; /** * @brief * Configure the SPI, then read the parameters from the SPI and * pass them to the second stage boot */ BOOT_MODULE_FXN_TABLE *iblInitSpiNor (void) { iblBootMap_t map; spiConfig_t cfg; uint32 configAddr; bool littleEndian; uint16 v; /* Read the endianness of the device */ littleEndian = deviceIsLittleEndian(); /* Load the default configuration table from the SPI. The actual speed of * the device isn't really known here, since it is part of the table, so a * compile time value is used (the pll may have been configured during the initial load) */ deviceLoadInitSpiConfig ((void *)&cfg); if (hwSpiConfig (&cfg) != 0) { iblStatus.iblFail = ibl_FAIL_CODE_SPI_PARAMS; for (;;); } /* Read the SPI mapping information from the nor flash */ for (;;) { if (hwSpiRead (IBL_CFG_SPI_MAP_TABLE_DATA_ADDR, /* The address on the flash of the data mapping */ sizeof(iblBootMap_t), /* The number of bytes to read */ (UINT8 *)&map) /* Where to store the data */ == 0) { /* On the flash the table is always formatted with the most significant * byte first. So if the device is running little endian, the endian * must be swapped */ if (littleEndian == TRUE) { map.length = swap16val (map.length); map.chkSum = swap16val (map.chkSum); map.addrLe = swap32val (map.addrLe); map.configLe = swap32val (map.configLe); map.addrBe = swap32val (map.addrBe); map.configBe = swap32val (map.configBe); configAddr = map.configLe; spiReadAddress = map.addrLe; } else { configAddr = map.configBe; spiReadAddress = map.addrBe; } if (map.length != sizeof(iblBootMap_t)) { iblStatus.mapSizeFail += 1; continue; } if (map.chkSum != 0) { v = onesComplementChksum ((UINT16 *)&map, sizeof(iblBootMap_t)); if ((v != 0) && (v != 0xffff)) { iblStatus.mapRetries += 1; continue; } } break; } iblStatus.mapRetries += 1; } /* Read the SPI configuration tables until the checksum passes and the magic * number matches. The checksum must be verified before the endian re-ordering */ for (;;) { if (hwSpiRead (configAddr, /* The address on the flash of the table */ sizeof(ibl_t), /* The number of bytes to read */ (UINT8 *)&ibl) /* Where to store the bytes */ == 0) { if (ibl.chkSum != 0) { v = onesComplementChksum ((UINT16 *)&ibl, sizeof(ibl_t) / sizeof(UINT16)); if ((v != 0) && (v != 0xffff)) { iblStatus.spiRetries += 1; continue; } } if (ibl.iblMagic == ibl_MAGIC_VALUE) break; if (swap32val (ibl.iblMagic) == ibl_MAGIC_VALUE) { iblSwap (); break; } iblStatus.magicRetries += 1; } iblStatus.spiRetries += 1; } /* the rest of the IBL is in boot table format. Read and process the data */ if (spiReadAddress == 0xffffffff) { iblStatus.iblFail = ibl_FAIL_CODE_INVALID_SPI_ADDRESS; for (;;); } return (&spiinit_boot_module); } #endif /* (!defined(EXCLUDE_NOR_SPI) || !defined(EXCLUDE_NAND_SPI)) */