/* * * Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ /***************************************************************************************** * FILE PURPOSE: Perform the top level boot ***************************************************************************************** * FILE NAME: iblmain.c * * DESCRIPTION: The top level boot examines the boot configuration and performs boot * based on this configuration * * @file iblmain.c * * @brief * This file is used to launch a boot based on the boot configuration structure * *****************************************************************************************/ #include "ibl.h" #include "iblloc.h" #include "iblcfg.h" #include "device.h" #include "ethboot.h" #include "nandboot.h" #include "norboot.h" #include "bis.h" #include "coffwrap.h" #include "iblbtbl.h" #include "iblblob.h" #include "timer.h" #include "i2c.h" #include "spi_api.h" #include "ibl_elf.h" #include extern cregister unsigned int IER; uint32 iblEndianIdx = 0; uint32 iblImageIdx = 0; /** * @brief * Data structures shared between the 1st and 2nd stage IBL load * are declared in a single header file, included in both stages */ #include "iblStage.h" /* Eat printfs */ void mprintf(char *x, ...) { } /** * @b Description * @n * * Returns TRUE if the input priority is valid and enabled */ BOOL iblPriorityIsValid (uint32 priority) { if ( (priority >= ibl_HIGHEST_PRIORITY) && (priority <= ibl_LOWEST_PRIORITY) ) return (TRUE); return (FALSE); } /** * @b Description * @n * * Returns TRUE if the mac address is 0 */ BOOL iblMacAddrIsZero (uint8 *maddr) { int32 i; for (i = 0; i < 6; i++) if (maddr[i] != 0) return (FALSE); return (TRUE); } /** * @b Description * @n * * For NAND and NOR boots, configure the specified peripheral or memory interface */ void iblPmemCfg (int32 interface, int32 port, bool enableNand) { int32 ret; switch (interface) { #if (!defined(EXCLUDE_NAND_GPIO)) case ibl_PMEM_IF_GPIO: ret = devicePowerPeriph (TARGET_PWR_GPIO); break; #endif #if (!defined(EXCLUDE_NOR_SPI) && !defined(EXCLUDE_NAND_SPI)) case ibl_PMEM_IF_SPI: { Uint32 v; spiConfig_t cfg; ret = devicePowerPeriph (TARGET_PWR_SPI); if (ret != 0) break; cfg.port = port; cfg.mode = ibl.spiConfig.mode; cfg.addrWidth = ibl.spiConfig.addrWidth; cfg.npin = ibl.spiConfig.nPins; cfg.csel = ibl.spiConfig.csel; cfg.c2tdelay = ibl.spiConfig.c2tdelay; /* On c661x devices the PLL module has a built in divide by 6, and the SPI * has a maximum clock divider value of 0xff */ v = ibl.pllConfig[ibl_MAIN_PLL].pllOutFreqMhz / (DEVICE_SPI_MOD_DIVIDER * ibl.spiConfig.busFreqMHz); if (v > 0xff) v = 0xff; cfg.clkdiv = (UINT16) v; ret = hwSpiConfig (&cfg); if (ret != 0) { iblStatus.iblFail = ibl_FAIL_CODE_SPI_PARAMS; return; } } break; #endif #if (!defined(EXCLUDE_NOR_EMIF) || !defined(EXCLUDE_NAND_EMIF)) case ibl_PMEM_IF_CHIPSEL_2: case ibl_PMEM_IF_CHIPSEL_3: case ibl_PMEM_IF_CHIPSEL_4: case ibl_PMEM_IF_CHIPSEL_5: { int i; /* Locate the configuration corresponding to this chip select space */ for (i = 0; i < ibl_MAX_EMIF_PMEM; i++) if (ibl.emifConfig[i].csSpace == interface) break; if (i == ibl_MAX_EMIF_PMEM) { iblStatus.iblFail = ibl_FAIL_CODE_NO_EMIF_CFG; return; } ret = devicePowerPeriph (TARGET_PWR_EMIF); if (ret != 0) break; if (hwEmif25Init (interface, ibl.emifConfig[i].busWidth, ibl.emifConfig[i].waitEnable, enableNand) != 0) iblStatus.iblFail = ibl_FAIL_CODE_EMIF_CFG_FAIL; } break; #endif default: iblStatus.iblFail = ibl_FAIL_CODE_INVALID_NAND_PERIPH; return; } if (ret != 0) { iblStatus.iblFail = ibl_FAIL_CODE_PERIPH_POWER_UP; return; } } /** * @b Description * @n * * The main function kicks off the boot. If it does not find the magic value in the * configuration array then default values are loaded. This default load * is done only once at the start of boot. * * @retval * None */ void main (void) { int32 i, j; UINT32 v, boot_mode_idx, boot_para_idx; /* Initialize the status structure */ iblMemset (&iblStatus, 0, sizeof(iblStatus_t)); iblStatus.iblMagic = ibl_MAGIC_VALUE; iblStatus.iblVersion = ibl_VERSION; /* Power up the timer */ devicePowerPeriph (TARGET_PWR_TIMER_0); /* Initialize the system timer (software tracking of the hardware timer state) */ timer_init (); /* Load default mac addresses for ethernet boot if requested */ for (i = 0; i < ibl_N_BOOT_MODES; i++) { if (ibl.bootModes[i].bootMode == ibl_BOOT_MODE_TFTP) { if (iblMacAddrIsZero (ibl.bootModes[i].u.ethBoot.ethInfo.hwAddress)) deviceLoadDefaultEthAddress (ibl.bootModes[i].u.ethBoot.ethInfo.hwAddress); } } /* DDR configuration is device specific */ deviceDdrConfig (); /* Try booting forever */ for (;;) { #ifndef EXCLUDE_MULTI_BOOT v = DEVICE_REG32_R(DEVICE_JTAG_ID_REG); if ( (v == DEVICE_C6618_JTAG_ID_VAL) || (v == DEVICE_C6616_JTAG_ID_VAL) ) { IER = 0; /* For C66x devices, check the DEVSTAT register to find which image on which device to boot. */ v = DEVICE_REG32_R(DEVICE_REG_DEVSTAT); /* Get the Endianness */ if (ibl_N_ENDIANS == 1) { iblEndianIdx = 0; } else { if (v & ibl_ENDIAN_LITTLE) { iblEndianIdx = 0; } else { iblEndianIdx = 1; } } /* Get the boot mode index */ boot_para_idx = BOOT_READ_BITFIELD(v,8,4); /* Only 1 image supported for TFTP boot */ if (boot_para_idx > (ibl_N_IMAGES*(ibl_N_BOOT_MODES-1))) { /* boot parameter index not supported */ continue; } boot_mode_idx = boot_para_idx/ibl_N_IMAGES; /* Get the boot image index */ iblImageIdx == boot_para_idx & (ibl_N_IMAGES - 1); iblStatus.activeBoot = ibl.bootModes[boot_mode_idx].bootMode; #endif switch (ibl.bootModes[boot_mode_idx].bootMode) { #ifndef EXCLUDE_ETH case ibl_BOOT_MODE_TFTP: iblStatus.activeDevice = ibl_ACTIVE_DEVICE_ETH; iblMemcpy (&iblStatus.ethParams, &ibl.bootModes[boot_mode_idx].u.ethBoot.ethInfo, sizeof(iblEthBootInfo_t)); iblEthBoot (boot_mode_idx); break; #endif #if ((!defined(EXCLUDE_NAND_EMIF)) ) case ibl_BOOT_MODE_NAND: iblPmemCfg (ibl.bootModes[boot_mode_idx].u.nandBoot.interface, ibl.bootModes[boot_mode_idx].port, TRUE); memset ((void *)0x80000000, 0, 0x20000000); iblNandBoot (boot_mode_idx); break; #endif #if (!defined(EXCLUDE_NOR_EMIF) && !defined(EXCLUDE_NOR_SPI)) case ibl_BOOT_MODE_NOR: iblPmemCfg (ibl.bootModes[boot_mode_idx].u.norBoot.interface, ibl.bootModes[boot_mode_idx].port, TRUE); iblNorBoot (boot_mode_idx); break; #endif } iblStatus.heartBeat += 1; } else { /* For C64x devices, loop through the boot modes to find the one with the highest priority * value, and try to boot it. */ for (i = ibl_HIGHEST_PRIORITY; i < ibl_LOWEST_PRIORITY; i++) { for (j = 0; j < ibl_N_BOOT_MODES; j++) { if (ibl.bootModes[j].priority == i) { iblStatus.activeBoot = ibl.bootModes[j].bootMode; switch (ibl.bootModes[j].bootMode) { #ifndef EXCLUDE_ETH case ibl_BOOT_MODE_TFTP: iblStatus.activeDevice = ibl_ACTIVE_DEVICE_ETH; iblMemcpy (&iblStatus.ethParams, &ibl.bootModes[j].u.ethBoot.ethInfo, sizeof(iblEthBootInfo_t)); iblEthBoot (j); break; #endif #if ((!defined(EXCLUDE_NAND_EMIF)) ) case ibl_BOOT_MODE_NAND: iblPmemCfg (ibl.bootModes[j].u.nandBoot.interface, ibl.bootModes[j].port, TRUE); iblNandBoot (j); break; #endif #if (!defined(EXCLUDE_NOR_EMIF) && !defined(EXCLUDE_NOR_SPI)) case ibl_BOOT_MODE_NOR: iblPmemCfg (ibl.bootModes[j].u.norBoot.interface, ibl.bootModes[j].port, TRUE); iblNorBoot (j); break; #endif } } iblStatus.heartBeat += 1; } } } } } /* main */ /** * @b Description * @n * * The ibl boot function links a device to a data format. The data format * parser pulls data from the boot device * * @param[in] bootFxn The structure containing the boot device functions * * @retval * None */ Uint32 iblBoot (BOOT_MODULE_FXN_TABLE *bootFxn, Int32 dataFormat, void *formatParams) { Uint32 entry = 0; Uint32 value32; Uint8 dataBuf[4]; Uint16 value16; /* Determine the data format if required */ if (dataFormat == ibl_BOOT_FORMAT_AUTO) { (*bootFxn->peek)(dataBuf, sizeof(dataBuf)); value32 = (dataBuf[0] << 24) | (dataBuf[1] << 16) | (dataBuf[2] << 8) | (dataBuf[3] << 0); value16 = (dataBuf[0] << 8) | (dataBuf[1] << 0); /* BIS */ #ifndef EXCLUDE_BIS if (value32 == BIS_MAGIC_NUMBER) dataFormat = ibl_BOOT_FORMAT_BIS; #endif #ifndef EXCLUDE_COFF if (iblIsCoff (value16)) dataFormat = ibl_BOOT_FORMAT_COFF; #endif #ifndef EXCLUDE_ELF if (iblIsElf (dataBuf)) dataFormat = ibl_BOOT_FORMAT_ELF; #endif if (dataFormat == ibl_BOOT_FORMAT_AUTO) { iblStatus.autoDetectFailCnt += 1; return (0); } } iblStatus.activeFileFormat = dataFormat; /* Invoke the parser */ switch (dataFormat) { #ifndef EXCLUDE_BIS case ibl_BOOT_FORMAT_BIS: iblBootBis (bootFxn, &entry); break; #endif #ifndef EXCLUDE_COFF case ibl_BOOT_FORMAT_COFF: iblBootCoff (bootFxn, &entry); break; #endif case ibl_BOOT_FORMAT_BTBL: iblBootBtbl (bootFxn, &entry); break; #ifndef EXCLUDE_BLOB case ibl_BOOT_FORMAT_BBLOB: iblBootBlob (bootFxn, &entry, formatParams); break; #endif #ifndef EXCLUDE_ELF case ibl_BOOT_FORMAT_ELF: iblBootElf (bootFxn, &entry); break; #endif default: iblStatus.invalidDataFormatSpec += 1; break; } return (entry); }