/* * * Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ /* Append a boot table section to the end of a boot table * usage: bfaddsect infile addr byte1 [bytes2 [byte3 [...]]] * The output is to stdout * * All values are taken to be btye values */ #include #include int asciiByte (unsigned char c) { if ((c >= '0') && (c <= '9')) return (1); if ((c >= 'A') && (c <= 'F')) return (1); return (0); } int toNum (unsigned char c) { if ((c >= '0') && (c <= '9')) return (c - '0'); return (c - 'A' + 10); } /* Copy a line from s to stdout */ void lineCpy (FILE *s) { char iline[132]; fgets (iline, 131, s); fputs (iline, stdout); } /* Read a .b file. */ int readBFile (FILE *s, unsigned char *data, unsigned maxSize) { unsigned char x, y; int byteCount = 0; for (;;) { /* read the 1st ascii char */ do { x = fgetc (s); if (x == (unsigned char)EOF) return (byteCount); } while (!asciiByte(x)); /* Read the next ascii char */ y = fgetc (s); if (y == (unsigned char)EOF) return (byteCount); if (asciiByte(y)) data[byteCount++] = (toNum(x) << 4) | toNum (y); if (byteCount >= maxSize) { fprintf (stderr, "Max input array size exceeded\n"); return (-1); } } } unsigned dwordConvert (unsigned char *data) { unsigned value; unsigned char c[4]; int i; c[0] = c[1] = c[2] = c[3] = 0; for (i = 0; i < 4; i++) { c[i] = data[i]; } value = c[3] | (c[2] << 8) | (c[1] << 16) | (c[0] << 24); return (value); } #define SIZE 0x100000 /* max number of bytes in the array */ #define MAX_BYTES 64 /* max size of the boot table */ int main (int argc, char *argv[]) { FILE *strin; unsigned char *dataSet; unsigned int addr; unsigned int secsize; unsigned char newchars[MAX_BYTES]; int i; int nbytes; int asize; int p; /* get the args */ if (argc < 4) { fprintf (stderr, "usage: %s infile hex_addr byte1 [byte2 [byte3 [ ...byte64]]]\n", argv[0]); return (-1); } /* input file */ strin = fopen (argv[1], "r"); if (strin == NULL) { fprintf (stderr, "%s: Could not open file %s\n", argv[0], argv[1]); return (-1); } /* Address */ sscanf (argv[2], "%x", &addr); /* Number of bytes */ nbytes = argc - 3; for (i = 0; i < nbytes; i++) sscanf (argv[i+3], "%x", &newchars[i]); /* Allocate memory for the data set */ dataSet = malloc (SIZE * sizeof (unsigned char)); if (dataSet == NULL) { fprintf (stderr, "%s: malloc failure\n", argv[0]); return (-1); } /* Copy the first two lines of the input file to stdout */ lineCpy (strin); lineCpy (strin); /* Read the data into the byte stream */ asize = readBFile (strin, dataSet, SIZE); fclose (strin); /* Parse the input file. Prepend the new section at the end */ /* Just skip the entry address */ p = 4; do { secsize = dwordConvert (&dataSet[p]); secsize = (secsize + 3) & 0xfffffffc; /* segment pad */ p = p + secsize + 8; /* 4 bytes length, 4 bytes address */ } while (secsize); /* back up to the zero section size */ p = p - 8; /* p now points to the 0 length entry. Put the new data here */ /* The section size */ dataSet[p++] = (nbytes >> 24) & 0xff; dataSet[p++] = (nbytes >> 16) & 0xff; dataSet[p++] = (nbytes >> 8) & 0xff; dataSet[p++] = (nbytes >> 0) & 0xff; /* Put the section address */ dataSet[p++] = (addr >> 24) & 0xff; dataSet[p++] = (addr >> 16) & 0xff; dataSet[p++] = (addr >> 8) & 0xff; dataSet[p++] = (addr >> 0) & 0xff; /* Put the data */ for (i = 0; i < nbytes; i++) dataSet[p++] = newchars[i]; while (p % 4) dataSet[p++] = 0; /* Add the 0 length section */ for (i = 0; i < 4; i++) dataSet[p++] = 0; /* Write out the data */ for (i = 0; i < p; i++) { fprintf (stdout, "%02X", dataSet[i]); if ( ((i+1) % 24) ) fprintf (stdout, " "); else fprintf (stdout, "\n"); } /* Write the trailing character */ fprintf (stdout, "\n%c",3); free (dataSet); return (0); }