/* Combine two boot tables. * usage bfmerge file1 file2 [file3 [file4 [...]]] * The output is to stdout * * */ #include #include int asciiByte (unsigned char c) { if ((c >= '0') && (c <= '9')) return (1); if ((c >= 'A') && (c <= 'F')) return (1); return (0); } int toNum (unsigned char c) { if ((c >= '0') && (c <= '9')) return (c - '0'); return (c - 'A' + 10); } /* Copy a line from s to stdout */ void lineCpy (FILE *s) { char iline[132]; fgets (iline, 131, s); fputs (iline, stdout); } /* Toss a line */ void lineToss (FILE *s) { char iline[132]; fgets (iline, 131, s); } /* Read a .b file. */ int readBFile (FILE *s, unsigned char *data, unsigned maxSize) { unsigned char x, y; int byteCount = 0; for (;;) { /* read the 1st ascii char */ do { x = fgetc (s); if (x == (unsigned char)EOF) return (byteCount); } while (!asciiByte(x)); /* Read the next ascii char */ y = fgetc (s); if (y == (unsigned char)EOF) return (byteCount); if (asciiByte(y)) data[byteCount++] = (toNum(x) << 4) | toNum (y); if (byteCount >= maxSize) { fprintf (stderr, "Max input array size exceeded\n"); return (-1); } } } unsigned dwordConvert (unsigned char *data) { unsigned value; unsigned char c[4]; int i; c[0] = c[1] = c[2] = c[3] = 0; for (i = 0; i < 4; i++) { c[i] = data[i]; } value = c[3] | (c[2] << 8) | (c[1] << 16) | (c[0] << 24); return (value); } int bparse (unsigned char *dataSet, int l) { unsigned int secsize; do { secsize = dwordConvert (&dataSet[l]); secsize = (secsize + 3) & 0xfffffffc; /* segment pad */ l = l + secsize + 8; /* 4 bytes length, 4 bytes address */ } while (secsize); /* Back up to the zero section size */ l = l - 8; return (l); } #define SIZE 1000000 #define APPEND 100000 int main (int argc, char *argv[]) { FILE *strin; unsigned char *dataSet; unsigned char *appSet; unsigned int addr; unsigned int secsize; int asize; int i, j; int nbytes; int p; /* Must have at least two input files */ if (argc < 3) { fprintf (stderr, "usage: %s file1 file2 [file3 [file4 [...]]]\n", argv[0]); return (-1); } /* Allocate memory for the data set */ dataSet = malloc (SIZE * sizeof (unsigned char)); if (dataSet == NULL) { fprintf (stderr, "%s: malloc failure\n", argv[0]); return (-1); } appSet = malloc (APPEND * sizeof (unsigned char )); if (appSet == NULL) { fprintf (stderr, "%s malloc failure\n", argv[0]); return (-1); } /* The first data file is handled seperately */ strin = fopen (argv[1], "r"); if (strin == NULL) { fprintf (stderr, "%s: Could not open file %s\n", argv[0], argv[1]); free (dataSet); return (-1); } /* Copy the first two lines of the input file to stdout */ lineCpy (strin); lineCpy (strin); /* Read in the first data set */ asize = readBFile (strin, dataSet, SIZE); fclose (strin); /* Parse the file, skipping the entry symbol */ p = 4; p = bparse (dataSet, p); /* Add the remaining data sets */ for (i = 2; i < argc; i++) { strin = fopen (argv[i], "r"); if (strin == NULL) { fprintf (stderr, "%s: Could not open file %s\n", argv[0], argv[i]); free (dataSet); return (-1); } /* Toss the first two lines */ lineToss (strin); lineToss (strin); asize = readBFile (strin, appSet, APPEND); fclose (strin); /* Append the new data set, skip the 4 bytes of entry symbol */ for (j = 0; j < asize-4; j++) dataSet[p+j] = appSet[j+4]; /* reparse from the current point */ p = bparse (dataSet, p); } /* Add the 0 section size */ for (i = 0; i < 4; i++) dataSet[p++] = 0; /* Write out the data */ for (i = 0; i < p; i++) { fprintf (stdout, "%02X", dataSet[i]); if ( ((i+1) % 24) ) fprintf (stdout, " "); else fprintf (stdout, "\n"); } /* Write the trailing character */ fprintf (stdout, "\n%c",3); free (dataSet); return (0); }