#define TRUE 1 #define FALSE 0 #define ibl_MAGIC_VALUE 0xCEC11EBB #define ibl_HIGHEST_PRIORITY 1 #define ibl_LOWEST_PRIORITY 10 #define ibl_DEVICE_NOBOOT 20 #define SETIP(array,i0,i1,i2,i3) array[0]=(i0); \ array[1]=(i1); \ array[2]=(i2); \ array[3]=(i3) #define ibl_BOOT_FORMAT_AUTO 0 #define ibl_BOOT_FORMAT_NAME 1 #define ibl_BOOT_FORMAT_BIS 2 #define ibl_BOOT_FORMAT_COFF 3 #define ibl_BOOT_FORMAT_ELF 4 #define ibl_BOOT_FORMAT_BBLOB 5 #define ibl_BOOT_FORMAT_BTBL 6 #define ibl_MAIN_PLL 0 #define ibl_DDR_PLL 1 #define ibl_NET_PLL 2 menuitem "EVM c6472 IBL"; hotmenu setConfig_c6472() { ibl.iblMagic = ibl_MAGIC_VALUE; ibl.pllConfig[ibl_MAIN_PLL].doEnable = TRUE; ibl.pllConfig[ibl_MAIN_PLL].prediv = 1; ibl.pllConfig[ibl_MAIN_PLL].mult = 28; ibl.pllConfig[ibl_MAIN_PLL].postdiv = 1; ibl.pllConfig[ibl_MAIN_PLL].pllOutFreqMhz = 700; /* The DDR PLL. The multipliers/dividers are fixed, so are really dont cares */ ibl.pllConfig[ibl_DDR_PLL].doEnable = TRUE; /* The network PLL. The multipliers/dividers are fixed */ ibl.pllConfig[ibl_NET_PLL].doEnable = TRUE; /* EMIF configuration. The values are for DDR at 533 MHz */ ibl.ddrConfig.configDdr = TRUE; ibl.ddrConfig.uEmif.emif3p1.sdcfg = 0x00538832; /* timing, 32bit wide */ ibl.ddrConfig.uEmif.emif3p1.sdrfc = 0x0000073B; /* Refresh 533Mhz */ ibl.ddrConfig.uEmif.emif3p1.sdtim1 = 0x47245BD2; /* Timing 1 */ ibl.ddrConfig.uEmif.emif3p1.sdtim2 = 0x0125DC44; /* Timing 2 */ ibl.ddrConfig.uEmif.emif3p1.dmcctl = 0x50001906; /* PHY read latency for CAS 5 is 5 + 2 - 1 */ /* Ethernet configuration for port 0 */ ibl.ethConfig[0].ethPriority = ibl_HIGHEST_PRIORITY; ibl.ethConfig[0].port = 0; /* Bootp is disabled. The server and file name are provided here */ ibl.ethConfig[0].doBootp = FALSE; ibl.ethConfig[0].useBootpServerIp = FALSE; ibl.ethConfig[0].useBootpFileName = FALSE; ibl.ethConfig[0].bootFormat = ibl_BOOT_FORMAT_BBLOB; SETIP(ibl.ethConfig[0].ethInfo.ipAddr, 158,218,100,113); SETIP(ibl.ethConfig[0].ethInfo.serverIp, 158,218,100,25); SETIP(ibl.ethConfig[0].ethInfo.gatewayIp, 158,218,100,2); SETIP(ibl.ethConfig[0].ethInfo.netmask, 255,255,255,0); /* Leave the hardware address as 0 so the e-fuse value will be used */ ibl.ethConfig[0].ethInfo.fileName[0] = 'c'; ibl.ethConfig[0].ethInfo.fileName[1] = '6'; ibl.ethConfig[0].ethInfo.fileName[2] = '4'; ibl.ethConfig[0].ethInfo.fileName[3] = '7'; ibl.ethConfig[0].ethInfo.fileName[4] = '2'; ibl.ethConfig[0].ethInfo.fileName[5] = '-'; ibl.ethConfig[0].ethInfo.fileName[6] = 'l'; ibl.ethConfig[0].ethInfo.fileName[7] = 'e'; ibl.ethConfig[0].ethInfo.fileName[8] = '.'; ibl.ethConfig[0].ethInfo.fileName[9] = 'b'; ibl.ethConfig[0].ethInfo.fileName[10] = 'i'; ibl.ethConfig[0].ethInfo.fileName[11] = 'n'; ibl.ethConfig[0].ethInfo.fileName[12] = '\0'; ibl.ethConfig[0].ethInfo.fileName[13] = '\0'; ibl.ethConfig[0].ethInfo.fileName[14] = '\0'; /* Even though the entire range of DDR2 is chosen, the load will * stop when the ftp reaches the end of the file */ ibl.ethConfig[0].blob.startAddress = 0xe0000000; /* Base address of DDR2 */ ibl.ethConfig[0].blob.sizeBytes = 0x20000000; /* All of DDR2 */ ibl.ethConfig[0].blob.branchAddress = 0xe0000000; /* Base of DDR2 */ /* For port 1 use bootp */ /* Ethernet configuration for port 0 */ ibl.ethConfig[1].ethPriority = ibl_HIGHEST_PRIORITY + 1; ibl.ethConfig[1].port = 1; /* Bootp is disabled. The server and file name are provided here */ ibl.ethConfig[1].doBootp = TRUE; ibl.ethConfig[1].useBootpServerIp = TRUE; ibl.ethConfig[1].useBootpFileName = TRUE; ibl.ethConfig[1].bootFormat = ibl_BOOT_FORMAT_BBLOB; /* SGMII not present */ ibl.sgmiiConfig[0].adviseAbility = 0; ibl.sgmiiConfig[0].control = 0; ibl.sgmiiConfig[0].txConfig = 0; ibl.sgmiiConfig[0].rxConfig = 0; ibl.sgmiiConfig[0].auxConfig = 0; ibl.sgmiiConfig[1].adviseAbility = 0; ibl.sgmiiConfig[1].control = 0; ibl.sgmiiConfig[1].txConfig = 0; ibl.sgmiiConfig[1].rxConfig = 0; ibl.sgmiiConfig[1].auxConfig = 0; /* Leave the hardware address as 0 so the e-fuse value will be used */ ibl.ethConfig[0].ethInfo.hwAddress[0] = 0; ibl.ethConfig[0].ethInfo.hwAddress[1] = 0; ibl.ethConfig[0].ethInfo.hwAddress[2] = 0; ibl.ethConfig[0].ethInfo.hwAddress[3] = 0; ibl.ethConfig[0].ethInfo.hwAddress[4] = 0; ibl.ethConfig[0].ethInfo.hwAddress[5] = 0; /* Leave all remaining fields as 0 since bootp will fill them in */ /* Even though the entire range of DDR2 is chosen, the load will */ /* stop when the ftp reaches the end of the file */ ibl.ethConfig[1].blob.startAddress = 0xe0000000; /* Base address of DDR2 */ ibl.ethConfig[1].blob.sizeBytes = 0x20000000; /* All of DDR2 */ ibl.ethConfig[1].blob.branchAddress = 0xe0000000; /* Base of DDR2 */ /* MDIO configuration */ ibl.mdioConfig.nMdioOps = 8; ibl.mdioConfig.mdioClkDiv = 0x20; ibl.mdioConfig.interDelay = 1400; /* ~2ms at 700 MHz */ ibl.mdioConfig.mdio[0] = (1 << 30) | (27 << 21) | (24 << 16) | 0x848b; ibl.mdioConfig.mdio[1] = (1 << 30) | (20 << 21) | (24 << 16) | 0x0ce0; ibl.mdioConfig.mdio[2] = (1 << 30) | (24 << 21) | (24 << 16) | 0x4101; ibl.mdioConfig.mdio[3] = (1 << 30) | ( 0 << 21) | (24 << 16) | 0x9140; ibl.mdioConfig.mdio[4] = (1 << 30) | (27 << 21) | (25 << 16) | 0x848b; ibl.mdioConfig.mdio[5] = (1 << 30) | (20 << 21) | (25 << 16) | 0x0ce0; ibl.mdioConfig.mdio[6] = (1 << 30) | (24 << 21) | (25 << 16) | 0x4101; ibl.mdioConfig.mdio[7] = (1 << 30) | ( 0 << 21) | (25 << 16) | 0x9140; /* Nand boot is disabled */ ibl.nandConfig.nandPriority = ibl_DEVICE_NOBOOT; } menuitem "EVM c6474 Mez IBL"; hotmenu setConfig_c6474() { ibl.iblMagic = ibl_MAGIC_VALUE; ibl.pllConfig[ibl_MAIN_PLL].doEnable = TRUE; ibl.pllConfig[ibl_MAIN_PLL].prediv = 1; ibl.pllConfig[ibl_MAIN_PLL].mult = 20; ibl.pllConfig[ibl_MAIN_PLL].postdiv = 1; ibl.pllConfig[ibl_MAIN_PLL].pllOutFreqMhz = 1000; /* The DDR PLL. The multipliers/dividers are fixed, so are really dont cares */ ibl.pllConfig[ibl_DDR_PLL].doEnable = TRUE; /* The network PLL. The multipliers/dividers are fixed */ ibl.pllConfig[ibl_NET_PLL].doEnable = TRUE; /* EMIF configuration. The values are for DDR at 533 MHz */ ibl.ddrConfig.configDdr = TRUE; ibl.ddrConfig.uEmif.emif3p1.sdcfg = 0x00d38a32; /* cas5, 8 banks, 10 bit column */ ibl.ddrConfig.uEmif.emif3p1.sdrfc = 0x00000a29; /* Refresh 333Mhz */ ibl.ddrConfig.uEmif.emif3p1.sdtim1 = 0x4d246c9a; /* Timing 1 */ ibl.ddrConfig.uEmif.emif3p1.sdtim2 = 0x00993c42; /* Timing 2 */ ibl.ddrConfig.uEmif.emif3p1.dmcctl = 0x50001906; /* PHY read latency for CAS 5 is 5 + 2 - 1 */ /* Ethernet configuration for port 0 */ ibl.ethConfig[0].ethPriority = ibl_HIGHEST_PRIORITY; ibl.ethConfig[0].port = 0; /* Bootp is disabled. The server and file name are provided here */ ibl.ethConfig[0].doBootp = FALSE; ibl.ethConfig[0].useBootpServerIp = FALSE; ibl.ethConfig[0].useBootpFileName = FALSE; ibl.ethConfig[0].bootFormat = ibl_BOOT_FORMAT_BBLOB; SETIP(ibl.ethConfig[0].ethInfo.ipAddr, 158,218,100,114); SETIP(ibl.ethConfig[0].ethInfo.serverIp, 158,218,100,25); SETIP(ibl.ethConfig[0].ethInfo.gatewayIp, 158,218,100,2); SETIP(ibl.ethConfig[0].ethInfo.netmask, 255,255,255,0); /* Set the hardware address as 0 so the e-fuse value will be used */ ibl.ethConfig[0].ethInfo.hwAddress[0] = 0; ibl.ethConfig[0].ethInfo.hwAddress[1] = 0; ibl.ethConfig[0].ethInfo.hwAddress[2] = 0; ibl.ethConfig[0].ethInfo.hwAddress[3] = 0; ibl.ethConfig[0].ethInfo.hwAddress[4] = 0; ibl.ethConfig[0].ethInfo.hwAddress[5] = 0; ibl.ethConfig[0].ethInfo.fileName[0] = 'c'; ibl.ethConfig[0].ethInfo.fileName[1] = '6'; ibl.ethConfig[0].ethInfo.fileName[2] = '4'; ibl.ethConfig[0].ethInfo.fileName[3] = '7'; ibl.ethConfig[0].ethInfo.fileName[4] = '4'; ibl.ethConfig[0].ethInfo.fileName[5] = '-'; ibl.ethConfig[0].ethInfo.fileName[6] = 'l'; ibl.ethConfig[0].ethInfo.fileName[7] = 'e'; ibl.ethConfig[0].ethInfo.fileName[8] = '.'; ibl.ethConfig[0].ethInfo.fileName[9] = 'b'; ibl.ethConfig[0].ethInfo.fileName[10] = 'i'; ibl.ethConfig[0].ethInfo.fileName[11] = 'n'; ibl.ethConfig[0].ethInfo.fileName[12] = '\0'; ibl.ethConfig[0].ethInfo.fileName[13] = '\0'; ibl.ethConfig[0].ethInfo.fileName[14] = '\0'; /* Even though the entire range of DDR2 is chosen, the load will * stop when the ftp reaches the end of the file */ ibl.ethConfig[0].blob.startAddress = 0x80000000; /* Base address of DDR2 */ ibl.ethConfig[0].blob.sizeBytes = 0x20000000; /* All of DDR2 */ ibl.ethConfig[0].blob.branchAddress = 0x80000000; /* Base of DDR2 */ /* There is no port 1 on the 6474 */ ibl.ethConfig[1].ethPriority = ibl_DEVICE_NOBOOT; /* SGMII is present */ ibl.sgmiiConfig[0].adviseAbility = 0; ibl.sgmiiConfig[0].control = 0; ibl.sgmiiConfig[0].txConfig = 0; ibl.sgmiiConfig[0].rxConfig = 0; ibl.sgmiiConfig[0].auxConfig = 0; /* MDIO configuration */ ibl.mdioConfig.nMdioOps = 8; ibl.mdioConfig.mdioClkDiv = 0x26; ibl.mdioConfig.interDelay = 2000; /* ~2ms at 1000 MHz */ ibl.mdioConfig.mdio[0] = (1 << 30) | ( 4 << 21) | (27 << 16) | 0x0081; ibl.mdioConfig.mdio[1] = (1 << 30) | (26 << 21) | (15 << 16) | 0x0047; ibl.mdioConfig.mdio[2] = (1 << 30) | (26 << 21) | (14 << 16) | 0x0047; ibl.mdioConfig.mdio[3] = (1 << 30) | ( 0 << 21) | (15 << 16) | 0x8140; ibl.mdioConfig.mdio[4] = (1 << 30) | ( 0 << 21) | (14 << 16) | 0x8140; ibl.mdioConfig.mdio[5] = (1 << 30) | ( 1 << 21) | (22 << 16) | 0x043e; ibl.mdioConfig.mdio[6] = (1 << 30) | ( 1 << 21) | (22 << 16) | 0x043e; ibl.mdioConfig.mdio[7] = (1 << 30) | ( 0 << 21) | ( 1 << 16) | 0xa100; /* Nand boot is disabled */ ibl.nandConfig.nandPriority = ibl_DEVICE_NOBOOT; } menuitem "EVM c6455 IBL"; hotmenu setConfig_c6455() { ibl.iblMagic = ibl_MAGIC_VALUE; ibl.pllConfig[ibl_MAIN_PLL].doEnable = TRUE; ibl.pllConfig[ibl_MAIN_PLL].prediv = 1; ibl.pllConfig[ibl_MAIN_PLL].mult = 20; ibl.pllConfig[ibl_MAIN_PLL].postdiv = 1; ibl.pllConfig[ibl_MAIN_PLL].pllOutFreqMhz = 1000; /* The DDR PLL. The multipliers/dividers are fixed, so are really dont cares */ ibl.pllConfig[ibl_DDR_PLL].doEnable = TRUE; /* The network PLL. The multipliers/dividers are fixed */ ibl.pllConfig[ibl_NET_PLL].doEnable = TRUE; /* EMIF configuration. The values are for DDR at 500 MHz */ ibl.ddrConfig.configDdr = TRUE; ibl.ddrConfig.uEmif.emif3p1.sdcfg = 0x00538822; /* timing, 32bit wide */ ibl.ddrConfig.uEmif.emif3p1.sdrfc = 0x000007a2; /* Refresh 500Mhz */ ibl.ddrConfig.uEmif.emif3p1.sdtim1 = 0x3edb4b91; /* Timing 1 */ ibl.ddrConfig.uEmif.emif3p1.sdtim2 = 0x00a2c722; /* Timing 2 */ ibl.ddrConfig.uEmif.emif3p1.dmcctl = 0x00000005; /* PHY read latency for CAS 4 is 4 + 2 - 1 */ /* Ethernet configuration for port 0 */ ibl.ethConfig[0].ethPriority = ibl_HIGHEST_PRIORITY; ibl.ethConfig[0].port = 0; /* Bootp is disabled. The server and file name are provided here */ ibl.ethConfig[0].doBootp = FALSE; ibl.ethConfig[0].useBootpServerIp = FALSE; ibl.ethConfig[0].useBootpFileName = FALSE; ibl.ethConfig[0].bootFormat = ibl_BOOT_FORMAT_BBLOB; SETIP(ibl.ethConfig[0].ethInfo.ipAddr, 158,218,100,118); SETIP(ibl.ethConfig[0].ethInfo.serverIp, 158,218,100,25); SETIP(ibl.ethConfig[0].ethInfo.gatewayIp, 158,218,100,2); SETIP(ibl.ethConfig[0].ethInfo.netmask, 255,255,255,0); /* There is no e-fuse mac address. A value must be assigned ibl.ethConfig[0].ethInfo.hwAddress[0] = 0x00; ibl.ethConfig[0].ethInfo.hwAddress[1] = 0xe0; ibl.ethConfig[0].ethInfo.hwAddress[2] = 0xa6; ibl.ethConfig[0].ethInfo.hwAddress[3] = 0x66; ibl.ethConfig[0].ethInfo.hwAddress[4] = 0x57; ibl.ethConfig[0].ethInfo.hwAddress[5] = 0x19; ibl.ethConfig[0].ethInfo.fileName[0] = 't'; ibl.ethConfig[0].ethInfo.fileName[1] = 'e'; ibl.ethConfig[0].ethInfo.fileName[2] = 's'; ibl.ethConfig[0].ethInfo.fileName[3] = 't'; ibl.ethConfig[0].ethInfo.fileName[4] = '.'; ibl.ethConfig[0].ethInfo.fileName[5] = 'b'; ibl.ethConfig[0].ethInfo.fileName[6] = 'l'; ibl.ethConfig[0].ethInfo.fileName[7] = 'o'; ibl.ethConfig[0].ethInfo.fileName[8] = 'b'; ibl.ethConfig[0].ethInfo.fileName[9] = '\0'; ibl.ethConfig[0].ethInfo.fileName[10] = '\0'; ibl.ethConfig[0].ethInfo.fileName[11] = '\0'; ibl.ethConfig[0].ethInfo.fileName[12] = '\0'; ibl.ethConfig[0].ethInfo.fileName[13] = '\0'; ibl.ethConfig[0].ethInfo.fileName[14] = '\0'; /* Even though the entire range of DDR2 is chosen, the load will * stop when the ftp reaches the end of the file */ ibl.ethConfig[0].blob.startAddress = 0xe0000000; /* Base address of DDR2 */ ibl.ethConfig[0].blob.sizeBytes = 0x20000000; /* All of DDR2 */ ibl.ethConfig[0].blob.branchAddress = 0xe0000000; /* Base of DDR2 */ /* There is no ethernet port 1 */ ibl.ethConfig[1].ethPriority = ibl_DEVICE_NOBOOT; /* SGMII not present */ ibl.sgmiiConfig[0].adviseAbility = 0; ibl.sgmiiConfig[0].control = 0; ibl.sgmiiConfig[0].txConfig = 0; ibl.sgmiiConfig[0].rxConfig = 0; ibl.sgmiiConfig[0].auxConfig = 0; ibl.sgmiiConfig[1].adviseAbility = 0; ibl.sgmiiConfig[1].control = 0; ibl.sgmiiConfig[1].txConfig = 0; ibl.sgmiiConfig[1].rxConfig = 0; ibl.sgmiiConfig[1].auxConfig = 0; /* MDIO configuration */ ibl.mdioConfig.nMdioOps = 0; ibl.mdioConfig.mdioClkDiv = 0x20; ibl.mdioConfig.interDelay = 2000; /* ~2ms at 1000 MHz */ ibl.mdioConfig.mdio[0] = (1 << 30) | (14 << 21) | (0 << 16) | 0xd5d0; /* Nand boot is disabled */ ibl.nandConfig.nandPriority = ibl_DEVICE_NOBOOT; }