/* * * Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ /******************************************************************************************************** * FILE PURPOSE: IBL configuration and control definitions ******************************************************************************************************** * FILE NAME: ibl.h * * DESCRIPTION: Defines the data structure used to handle initial configuration and control * of the ibl. This data structure resides at a fixed location in the device memory * map. It is initially populated either during the rom boot. The table can be * over-written during the ibl process to redirect the boot. For example the ibl * can initially load from an i2c which repopulates this table with parameters * for an ethernet boot. * * @file ibl.h * * @brief * This file defines the configuration and control of the IBL * * ********************************************************************************************************/ #ifndef IBL_H #define IBL_H #include "types.h" #define ibl_MAKE_VERSION(a,b,c,d) ((a << 24) | (b << 16) | (c << 8) | (d << 0)) /** * @brief * The version number, 1.0.0.11 */ #define ibl_VERSION ibl_MAKE_VERSION(1,0,0,11) #define SETIP(array,i0,i1,i2,i3) array[0]=(i0); \ array[1]=(i1); \ array[2]=(i2); \ array[3]=(i3) /** * @defgroup iblBootModes Defines the boot modes supported by the IBL * * @ingroup iblBootModes * @{ * * @def ibl_BOOT_MODE_TFTP */ #define ibl_BOOT_MODE_TFTP 10 /* Boot through a tftp interface */ /* @def ibl_BOOT_MODE_NAND */ #define ibl_BOOT_MODE_NAND 11 /* Boot through a nand interface */ /* @def ibl_BOOT_MODE_NOR */ #define ibl_BOOT_MODE_NOR 12 /* Boot through a nor (or flash) interface */ /* @def ibl_BOOT_MODE_NONE */ #define ibl_BOOT_MODE_NONE 13 /* Boot mode selection is inactive */ /* @} */ /** * @brief * Define the number of different boot modes which can be configured for * a single execution of the IBL. */ #define ibl_N_BOOT_MODES 3 /* Information used to make generate a bootp request */ /** * @brief * Defines parameters used for making a bootp request * * @details * The bootp request parameters are created from these fields */ typedef struct iblBootp_s { uint8 hwAddress[6]; /**< The hardware (mac) address of this device. If set to 0 the ibl will values from e-fuse */ uint8 ipDest[4]; /**< The IP address of this device. This is typically set to IP broadcast */ } iblBootp_t; /** * @brief * This structure contains information used for tftp boot. * * @details These fields are typically filled in by the bootp packet, but * can be provided if bootp will not be used. */ typedef struct iblEthBootInfo_s { uint8 ipAddr[4]; /**< The IP address of this device */ uint8 serverIp[4]; /**< The IP address of the tftp server */ uint8 gatewayIp[4]; /**< The IP address of the gateway */ uint8 netmask[4]; /**< The IP netmask */ uint8 hwAddress[6]; /**< The hardware (mac) address of this device */ char8 fileName[64]; /**< The file name to load */ } iblEthBootInfo_t; /** * @def ibl_ETH_PORT_FROM_RBL */ #define ibl_ETH_PORT_FROM_RBL -1 /**< The ethernet port used is the same one used during the ROM boot load process. */ /** * @def ibl_PORT_SWITCH_ALL */ #define ibl_PORT_SWITCH_ALL -2 /**< The ethernet subsystem is connected to a switch, and all ports on the subsystem should be configured */ /** * @defgroup iblBootFormats * * @ingroup iblBootFormats * @{ */ #define ibl_BOOT_FORMAT_AUTO 0 /**< Auto determine the boot format from the data */ #define ibl_BOOT_FORMAT_NAME 1 /**< Determines the boot format based on file name (bootp/tftp only) */ #define ibl_BOOT_FORMAT_BIS 2 /**< Boot TI AIS format */ #define ibl_BOOT_FORMAT_COFF 3 /**< Boot a COFF file */ #define ibl_BOOT_FORMAT_ELF 4 /**< Boot an ELF file */ #define ibl_BOOT_FORMAT_BBLOB 5 /**< Boot a binary blob */ #define ibl_BOOT_FORMAT_BTBL 6 /**< Boot a TI boot table file */ /* @} */ /** * @defgroup iblPeriphPriority Defines the boot sequence * * @ingroup iblPeriphPriority * @{ * @def ibl_LOWEST_PRIORITY */ #define ibl_LOWEST_PRIORITY 10 /**< The lowest priority assignable to a peripheral for boot */ /** * @def ibl_HIGHEST_PRIORITY */ #define ibl_HIGHEST_PRIORITY 1 /**< The highest priority assignable to a peripheral for boot */ /** * @def ibl_DEVICE_NOBOOT */ #define ibl_DEVICE_NOBOOT 20 /**< Indicates that the device is not to be used for boot */ /* @} */ /** * @brief * Emif controller 3.1 configuration * * @details * The paramters are directly placed into the emif controller */ typedef struct iblEmif3p1_s { uint32 sdcfg; /**< SD configuration register */ uint32 sdrfc; /**< Refresh timing register */ uint32 sdtim1; /**< DDR timing register 1 */ uint32 sdtim2; /**< DDR timing register 2 */ uint32 dmcctl; /**< CAS match timing */ } iblEmif3p1_t; /** * @brief * Emif controller 4.0 configuration * * @details * The parameters are placed directly into the emif controller */ typedef struct iblEmif4p0_s { uint32 registerMask; /**< Identifies which registers will be configured */ uint32 sdRamConfig; /**< SDRAM Config Register */ uint32 sdRamConfig2; /**< SDRAM Config2 Register */ uint32 sdRamRefreshCtl; /**< SDRAM Refresh Control Register */ uint32 sdRamTiming1; /**< SDRAM Timing 1 Register */ uint32 sdRamTiming2; /**< SDRAM Timing 2 Register */ uint32 sdRamTiming3; /**< SDRAM Timing 3 Register */ uint32 lpDdrNvmTiming; /**< LPDDR2-NVM Timing Register */ uint32 powerManageCtl; /**< Power Management Control Register */ uint32 iODFTTestLogic; /**< IODFT Test Logic Global Control Register */ uint32 performCountCfg; /**< Performance Counter Config Register */ uint32 performCountMstRegSel; /**< Performance Counter Master Region Select Register */ uint32 readIdleCtl; /**< Read Idle Control Register */ uint32 sysVbusmIntEnSet; /**< VBUSM Interrupt Enable Set Register */ uint32 sdRamOutImpdedCalCfg; /**< SDRAM Output Impedance Calibratin Config Register */ uint32 tempAlterCfg; /**< Temperature Alert Config Register */ uint32 ddrPhyCtl1; /**< DDR PHY Control 1 Register */ uint32 ddrPhyCtl2; /**< DDR PHY Control 2 Register */ uint32 priClassSvceMap; /**< DDR Priority to Class of Service Mapping Register */ uint32 mstId2ClsSvce1Map; /**< Master ID to Class of Service 1 Mapping Register */ uint32 mstId2ClsSvce2Map; /**< Master ID to Class of Service 2 Mapping Register */ uint32 eccCtl; /**< ECC Control Register */ uint32 eccRange1; /**< ECC Address Range 1 Register */ uint32 eccRange2; /**< ECC Address Range 2 Register */ uint32 rdWrtExcThresh; /**< Read Write Execution Threshold Register */ } iblEmif4p0_t; /** * @defgroup iblEmif4Select Defines the EMIF4 registers configured by IBL * * @ingroup iblEmif4Select * @{ * @def ibl_EMIF4_ENABLE_sdRamConfig */ #define ibl_EMIF4_ENABLE_sdRamConfig (1 << 0) /** @def ibl_EMIF4_ENABLE_sdRamConfig2 */ #define ibl_EMIF4_ENABLE_sdRamConfig2 (1 << 1) /** @def ibl_EMIF4_ENABLE_sdRamRefreshCtl */ #define ibl_EMIF4_ENABLE_sdRamRefreshCtl (1 << 2) /** @def ibl_EMIF4_ENABLE_sdRamTiming1 */ #define ibl_EMIF4_ENABLE_sdRamTiming1 (1 << 3) /** @def ibl_EMIF4_ENABLE_sdRamTiming2 */ #define ibl_EMIF4_ENABLE_sdRamTiming2 (1 << 4) /** @def ibl_EMIF4_ENABLE_sdRamTiming3 */ #define ibl_EMIF4_ENABLE_sdRamTiming3 (1 << 5) /** @def ibl_EMIF4_ENABLE_lpDdrNvmTiming */ #define ibl_EMIF4_ENABLE_lpDdrNvmTiming (1 << 6) /** @def ibl_EMIF4_ENABLE_powerManageCtl */ #define ibl_EMIF4_ENABLE_powerManageCtl (1 << 7) /** @def ibl_EMIF4_ENABLE_iODFTTestLogic */ #define ibl_EMIF4_ENABLE_iODFTTestLogic (1 << 8) /** @def ibl_EMIF4_ENABLE_performCountCfg */ #define ibl_EMIF4_ENABLE_performCountCfg (1 << 9) /** @def ibl_EMIF4_ENABLE_performCountMstRegSel */ #define ibl_EMIF4_ENABLE_performCountMstRegSel (1 << 10) /** @def ibl_EMIF4_ENABLE_readIdleCtl */ #define ibl_EMIF4_ENABLE_readIdleCtl (1 << 11) /** @def ibl_EMIF4_ENABLE_sysVbusmIntEnSet */ #define ibl_EMIF4_ENABLE_sysVbusmIntEnSet (1 << 12) /** @def ibl_EMIF4_ENABLE_sdRamOutImpdedCalCfg */ #define ibl_EMIF4_ENABLE_sdRamOutImpdedCalCfg (1 << 13) /** @def ibl_EMIF4_ENABLE_tempAlterCfg */ #define ibl_EMIF4_ENABLE_tempAlterCfg (1 << 14) /** @def ibl_EMIF4_ENABLE_ddrPhyCtl1 */ #define ibl_EMIF4_ENABLE_ddrPhyCtl1 (1 << 15) /** @def ibl_EMIF4_ENABLE_ddrPhyCtl2 */ #define ibl_EMIF4_ENABLE_ddrPhyCtl2 (1 << 16) /** @def ibl_EMIF4_ENABLE_priClassSvceMap */ #define ibl_EMIF4_ENABLE_priClassSvceMap (1 << 17) /** @def ibl_EMIF4_ENABLE_mstId2ClsSvce1Map */ #define ibl_EMIF4_ENABLE_mstId2ClsSvce1Map (1 << 18) /** @def ibl_EMIF4_ENABLE_mstId2ClsSvce2Map */ #define ibl_EMIF4_ENABLE_mstId2ClsSvce2Map (1 << 11) /** @def ibl_EMIF4_ENABLE_eccCtl */ #define ibl_EMIF4_ENABLE_eccCtl (1 << 19) /** @def ibl_EMIF4_ENABLE_eccRange1 */ #define ibl_EMIF4_ENABLE_eccRange1 (1 << 20) /** @def ibl_EMIF4_ENABLE_eccRange2 */ #define ibl_EMIF4_ENABLE_eccRange2 (1 << 21) /** @def ibl_EMIF4_ENABLE_rdWrtExcThresh */ #define ibl_EMIF4_ENABLE_rdWrtExcThresh (1 << 22) /** @def ibl_BOOT_EMIF4_ENABLE_ALL */ #define ibl_BOOT_EMIF4_ENABLE_ALL 0x007fffff /* @} */ /** * @defgroup iblEmifType Defines the EMIF4 type on a device * * @ingroup iblEmifType * @{ */ /** @def ibl_EMIF_TYPE_31 */ #define ibl_EMIF_TYPE_31 31 /** @def ibl_EMIF_TYPE_40 */ #define ibl_EMIF_TYPE_40 40 /* @} */ /** * @brief * This structure is used to configure the DDR interface * * @details * The DDR configuration parameters are setup * */ typedef struct idblDdr_s { bool configDdr; /**< Set to non-zero to enable EMIF configuration */ union { iblEmif3p1_t emif3p1; /**< Configuration of devices with emif controller version 3.1 */ iblEmif4p0_t emif4p0; /**< Configuration of devices with emif controller version 4.0 */ } uEmif; } iblDdr_t; /** * @brief * This structure is used to identify binary blob load parameters. * * @details * Since binary blob is formatless the start address, size and branch to address * can be specified. In the case of network boot, boot will terminate when no * more data is received (or timed out), even if the size is not reached. */ typedef struct iblBinBlob_s { uint32 startAddress; /**< Where the loaded data is placed */ uint32 sizeBytes; /**< How much data to load */ uint32 branchAddress; /**< Where to branch to when the load is complete */ } iblBinBlob_t; /** * @brief * This structure is used to control the operation of the ibl ethernet boot. * * @details * The ethernet port and bootp request are controlled through this structure. */ typedef struct iblEth_s { bool doBootp; /**< If true a bootp request is generated. If false the @ref iblEthBootInfo_t table must be populated before the ibl begins execution */ bool useBootpServerIp; /**< If TRUE then the server IP received from the bootp server is used, if FALSE the one in the ethInfo field is used */ bool useBootpFileName; /**< If TRUE then the file name received from the bootp server is used, if FALSE the one in the ethInfo field is used */ int32 bootFormat; /**< The format of the boot data file. @ref iblBootFormats */ iblBinBlob_t blob; /**< Used only if the format is ibl_BOOT_FORMAT_BBLOB */ iblEthBootInfo_t ethInfo; /**< Low level ethernet information */ } iblEth_t; /** * @brief * This structure is used to control the operation of the ibl sgmii ports * * @details * The physical register configuration is provided */ typedef struct iblSgmii_s { bool configure; /**< Set to false to disable configuration */ uint32 adviseAbility; /**< The advise ability register */ uint32 control; /**< The control register */ uint32 txConfig; /**< Serdes Tx config */ uint32 rxConfig; /**< Serdes Rx config */ uint32 auxConfig; /**< Serdes Aux config */ } iblSgmii_t; /** * @def ibl_N_ETH_PORTS */ #define ibl_N_ETH_PORTS 2 /**< The number of ethernet port configurations available */ /** * @def ibl_N_MDIO_CFGS */ #define ibl_N_MDIO_CFGS 16 /**< The maximum number of mdio configurations */ /** * @brief * This structure is used to configure phys through the mdio interface * * @details * Defines optional configuration through MDIO. * * The mdio transaction values are mapped as follows: * * /-------------------------------------------------------------\ * | 31 | 30 | 29 26 | 25 21 | 20 16 | 15 0| * | rsvd | write | rsvd | register | phy addr | data | * \-------------------------------------------------------------/ */ typedef struct iblMdio_s { int16 nMdioOps; /**< The number of mdio writes to perform */ uint16 mdioClkDiv; /**< The divide down of the mac clock which drives the mdio */ uint32 interDelay; /**< The number of cpu cycles to wait between mdio writes */ uint32 mdio[ibl_N_MDIO_CFGS]; /* The MDIO transactions */ } iblMdio_t; /** * @def ibl_N_ECC_BYTES */ #define ibl_N_ECC_BYTES 10 /**< The number of ECC bytes to be computed for each page */ /** * @def ibl_N_BAD_BLOCK_MARKER */ #define ibl_N_BAD_BLOCK_PAGE 2 /**< The number of pages in each block that has the bad block marker */ /** * @brief * This structure defines the physical parameters of the NAND device */ typedef struct nandDevInfo_s { uint32 busWidthBits; /**< 8 or 16 bit bus width */ uint32 pageSizeBytes; /**< The size of each page */ uint32 pageEccBytes; /**< Number of ecc bytes in each page */ uint32 pagesPerBlock; /**< The number of pages in each block */ uint32 totalBlocks; /**< The total number of blocks in a device */ uint32 addressBytes; /**< Number of bytes in the address */ bool lsbFirst; /**< Set to true if the LSB is output first, otherwise msb is first */ uint32 blockOffset; /**< Address bits which specify the block number */ uint32 pageOffset; /**< Address bits which specify the page number */ uint32 columnOffset; /**< Address bits which specify the column number */ uint8 eccBytesIdx[ibl_N_ECC_BYTES]; /**< Index of each ECC byte in each page data */ uint8 badBlkMarkIdx[ibl_N_BAD_BLOCK_PAGE]; /**< Index of bad block marker in each page data */ uint8 resetCommand; /**< The command to reset the flash */ uint8 readCommandPre; /**< The read command sent before the address */ uint8 readCommandPost; /**< The read command sent after the address */ bool postCommand; /**< If TRUE the post command is sent */ } nandDevInfo_t; /** * @def ibl_N_ENDIANS */ #define ibl_N_ENDIANS 2 /**< The number of endians supported */ #define ibl_ENDIAN_BIG 0 /**< Big endian */ #define ibl_ENDIAN_LITTLE 1 /**< Little endian */ /** * @def ibl_N_IMAGES */ #define ibl_N_IMAGES 2 /**< The number of boot images supported on the same device */ /** * @brief * This structure is used to control the operation of the NAND boot * */ typedef struct iblNand_s { int32 bootFormat; /**< The format of the boot data file. @ref iblBootFormats */ uint32 bootAddress[ibl_N_ENDIANS][ibl_N_IMAGES]; /**< The start address of each image for booting */ int32 interface; /**< The nand interface @ref iblPmemf */ iblBinBlob_t blob[ibl_N_ENDIANS][ibl_N_IMAGES]; /**< Used only if the format is ibl_BOOT_FORMAT_BBLOB */ nandDevInfo_t nandInfo; /** Low level device info */ } iblNand_t; /** * @brief * Nor boot configuration. */ typedef struct iblNor_s { int32 bootFormat; /**< The format of the boot data file. @ref iblBootFormats */ uint32 bootAddress[ibl_N_ENDIANS][ibl_N_IMAGES]; /**< The start address for booting */ int32 interface; /**< The nor interface. @ref iblPmemIf */ iblBinBlob_t blob[ibl_N_ENDIANS][ibl_N_IMAGES]; /**< Used only if the format is ibl_BOOT_FORMAT_BBLOB */ } iblNor_t; extern uint32 iblEndianIdx; extern uint32 iblImageIdx; /** * @defgroup iblPmemIf defines the interfaces used for NOR memory. Not all values are * valid for all devices * * @ingroup iblPmemIf * @{ */ /** @def ibl_PMEM_IF_GPIO - GPIO interface */ #define ibl_PMEM_IF_GPIO 0 /** @def ibl_PMEM_IF_CHIPSEL_2 */ #define ibl_PMEM_IF_CHIPSEL_2 2 /* EMIF interface using chip select 2, no wait enabled */ /** @def ibl_PMEM_IF_CHIPSEL_3 */ #define ibl_PMEM_IF_CHIPSEL_3 3 /* EMIF interface using chip select 3, no wait enabled */ /** @def ibl_PMEM_IF_CHIPSEL_4 */ #define ibl_PMEM_IF_CHIPSEL_4 4 /* EMIF interface using chip select 4 */ /** @def ibl_PMEM_IF_CHIPSEL_5 */ #define ibl_PMEM_IF_CHIPSEL_5 5 /* EMIF interface using chip select 5 */ /** @def ibl_PMEM_IF_SPI */ #define ibl_PMEM_IF_SPI 100 /* Interface through SPI */ /* @} */ /** * @brief * EMIF (nand/nor) configuration */ typedef struct iblEmif_s { int16 csSpace; /**< Chip select space, @ref iblPmemIf */ int16 busWidth; /**< Bus width, bits */ bool waitEnable; /**< Valid only for NOR devices */ } iblEmif_t; /** * @brief * The maximum number of chip select spaces for emif boot (not ddr) configuration */ #define ibl_MAX_EMIF_PMEM 2 /** * @brief * SPI configuration used for either NOR or NAND */ typedef struct iblSpi_s { int16 addrWidth; /**< 16 or 24 are the only valid values */ int16 nPins; /**< 4 or 5 are the only valid values */ int16 mode; /**< Clock / data polarities (valid values 0-3) */ int16 csel; /**< Chip select value (5 pin). Only 0b10 and 0b01 are valid */ uint16 c2tdelay; /**< Setup time between chip select and the transaction */ uint16 busFreqMHz; /**< Bus speed */ } iblSpi_t; /** * @brief * This structure is used to control the programming of the device PLL * * @details * The system PLLs are optionally configured */ typedef struct iblPll_s { bool doEnable; /**< If true the PLL is configured */ Uint32 prediv; /**< The pll pre-divisor */ Uint32 mult; /**< The pll multiplier */ Uint32 postdiv; /**< The pll post divider */ Uint32 pllOutFreqMhz; /**< The resulting output frequency, required for timer setup */ } iblPll_t; /** * @defgroup iblPllNum * * @ingroup iblPllNum * @{ * * @def ibl_MAIN_PLL */ #define ibl_MAIN_PLL 0 /**< The main cpu pll */ /** * @def ibl_DDR_PLL */ #define ibl_DDR_PLL 1 /**< The ddr pll */ /** * @def ibl_NET_PLL */ #define ibl_NET_PLL 2 /**< The network pll */ /** * @def the number of PLL configuration entries in the table */ #define ibl_N_PLL_CFGS (ibl_NET_PLL + 1) /* @} */ /** * @def iblBoot_t * Configures an ibl boot attempt * * @details * The ibl allows for the configuration for multiple boot attempts. This structure is * used to configure the ibl boot attempt. */ typedef struct iblBoot_s { int32 bootMode; /**< Identifies the boot mode @ref iblBootModes */ uint32 priority; /**< The boot priority. @ref iblPeriphPriority */ int32 port; /**< The port to use, or @ref ibl_PORT_FROM_RBL */ union { iblEth_t ethBoot; /**< Ethernet boot configuration. @ref iblEth_t */ iblNand_t nandBoot; /**< NAND boot configuration @ref iblNand_t */ iblNor_t norBoot; /**< NOR boot configuration @ref iblNor_t */ } u; } iblBoot_t; /** * @def ibl_MAGIC_VALUE */ #define ibl_MAGIC_VALUE 0xCEC11EBC /**< Indicates that the configuration table is valid */ /** * @def ibl_EVM_TYPE */ #define ibl_EVM_C6455L 0x10 /**< C6455 Low Cost EVM */ #define ibl_EVM_C6457L 0x20 /**< C6457 Low Cost EVM */ #define ibl_EVM_C6472L 0x30 /**< C6472 Low Cost EVM */ #define ibl_EVM_C6474L 0x40 /**< C6474 Low Cost EVM */ #define ibl_EVM_C6474M 0x41 /**< C6474 Mez EVM */ #define ibl_EVM_C6670L 0x50 /**< C6670 Low Cost EVM */ #define ibl_EVM_C6678L 0x60 /**< C6678 Low Cost EVM */ #define ibl_EVM_C6657L 0x70 /**< C6657 Low Cost EVM */ /** * @brief * The main configuration/control structure for the ibl * * @details * The operation of the ibl is configured/controlled based on the values in this structure. * This structure resides at a fixed location in the memory map. It can be changed during * the boot operation itself by loading new values into it, but these changes must occur * as part of the boot process itself (not through an asynchronous write through a master * peripheral). * * Each boot mode is assigned a priority, with lower values indicating a higher * priority. The lowest valid priority is @ref ibl_LOWEST_BOOT_PRIORITY, and the value * @ref ibl_DEVICE_NOBOOT indicates no boot will be attempted on that peripheral. */ typedef struct ibl_s { uint32 iblMagic; /**< @ref ibl_MAGIC_VALUE */ iblPll_t pllConfig[ibl_N_PLL_CFGS]; /**< PLL Configuration. @ref iblPll_t */ iblDdr_t ddrConfig; /**< DDR configuration @ref iblDdr_t */ iblSgmii_t sgmiiConfig[ibl_N_ETH_PORTS]; /**< SGMII boot configuration. @ref iblSgmii_t */ iblMdio_t mdioConfig; /**< MDIO configuration. @ref iblMdio_t */ iblSpi_t spiConfig; /**< SPI configuration @ref iblSpi_s */ iblEmif_t emifConfig[ibl_MAX_EMIF_PMEM]; /**< EMIF (nand/nor, not ddr) configuration. @ref iblEmif_t */ iblBoot_t bootModes[ibl_N_BOOT_MODES]; /**< Boot configuration */ uint16 iblEvmType; /**< @ref ibl_EVM_TYPE */ uint16 chkSum; /**< Ones complement checksum over the whole config structure */ } ibl_t; extern ibl_t ibl; /** * @defgroup iblActiveDevice * * @ingroup iblActiveDevice * @{ * @def ibl_ACTIVE_DEVICE_ETH */ #define ibl_ACTIVE_DEVICE_ETH 100 /**< Data received through an ethernet interface */ /** * @def ibl_ACTIVE_DEVICE_EMIF */ #define ibl_ACTIVE_DEVICE_EMIF 101 /**< Data read through an EMIF interface */ /** * @def ibl_ACTIVE_DEVICE_I2C */ #define ibl_ACTIVE_DEVICE_I2C 102 /**< Data read through an I2C interface */ /** * @def ibl_ACTIVE_DEVICE_SPI */ #define ibl_ACTIVE_DEVICE_SPI 103 /**< Data read through an SPI interface */ /* @} */ /** * @defgroup iblFailCode * * @ingroup iblFailCode * @{ * @def ibl_FAIL_CODE_INVALID_I2C_ADDRESS */ #define ibl_FAIL_CODE_INVALID_I2C_ADDRESS 700 /**< Invalid i2c eeprom address encountered */ /** * @def ibl_FAIL_CODE_BTBL_FAIL */ #define ibl_FAIL_CODE_BTBL_FAIL 701 /**< Boot table processing function error */ /** * @def ibl_FAIL_CODE_PA */ #define ibl_FAIL_CODE_PA 702 /**< Packet Accelerator setup failed */ /** * @def ibl_FAIL_CODE_SPI_PARAMS */ #define ibl_FAIL_CODE_SPI_PARAMS 703 /**< Invalid SPI configuration found */ /** * @def ibl_FAIL_CODE_INVALID_INIT_DEVICE */ #define ibl_FAIL_CODE_INVALID_INIT_DEVICE 704 /**< Second stage boot device specified is invalid */ /** * @def ibl_FAIL_CODE_INVALID_SPI_ADDRESS */ #define ibl_FAIL_CODE_INVALID_SPI_ADDRESS 705 /**< Invalid data address specified on SPI */ /** * @def ibl_FAIL_CODE_PERIPH_POWER_UP */ #define ibl_FAIL_CODE_PERIPH_POWER_UP 706 /**< Boot peripheral failed to power up */ /** * @def ibl_FAIL_CODE_INVALID_NAND_PERIPH */ #define ibl_FAIL_CODE_INVALID_NAND_PERIPH 707 /**< Invalid nand boot peripheral specified */ /** * @def ibl_FAIL_CODE_NO_EMIF_CFG */ #define ibl_FAIL_CODE_NO_EMIF_CFG 708 /**< No emif configuration found to match specified cs space */ /** * @def ibl_FAIL_CODE_EMIF_CFG_FAIL */ #define ibl_FAIL_CODE_EMIF_CFG_FAIL 709 /**< Hardware setup of emif failed */ /* @} */ /** * @brief * Provide status on the boot operation * * @details * Run time status of the IBL is provided to aid in debugging * */ typedef struct iblStatus_s { uint32 iblMagic; /**< The @ref ibl_MAGIC_VALUE is placed here to indicate the boot has begun */ uint32 iblVersion; /**< The version number. MSB = major, SMSB = minor, SLSB = minor minor LSB= tiny */ uint32 iblFail; /**< If non-zero the IBL has encountered a fatal error */ uint32 i2cRetries; /**< Count of I2C read retries */ uint32 i2cDataRetries; /**< Number of retries while reading block data from the i2c */ uint32 spiRetries; /**< Count of SPI read retries */ uint32 spiDataRetries; /**< Number of retries while reading block data from the spi */ uint32 magicRetries; /**< Count of I2C/SPI re-reads because the magic number was incorrect */ uint32 mapSizeFail; /**< Number of times an invalid map table size was read from the i2c/spi */ uint32 mapRetries; /**< Number of times the checksum failed on the read of the i2c/spi map */ int32 heartBeat; /**< An increasing value as long as the boot code is running */ int32 activeBoot; /**< Describes the active boot mode @ref iblBootModes */ int32 activeDevice; /**< Describes the active boot peripheral device @ref iblActiveDevice */ int32 activeFileFormat; /**< Describes the format being decoded */ uint32 autoDetectFailCnt; /**< Counts the number of times an auto detect of the data format failed */ uint32 nameDetectFailCnt; /**< Counts the number of times an name detect of the data format failed */ uint32 invalidDataFormatSpec; /**< Counts the number of times the main boot found an invalid boot format request */ uint32 exitAddress; /**< If non-zero the IBL exited and branched to this address */ iblEthBootInfo_t ethParams; /**< Last ethernet boot attemp parameters */ } iblStatus_t; extern iblStatus_t iblStatus; /** * @brief * The ibl boot map structure * * @details * The ibl boot device contains a structure which identifies the location of the big and little * endian ibl images on the external device. */ typedef struct iblBootMap_s { uint16 length; /**< Size of the structure in bytes */ uint16 chkSum; /**< Value which makes the ones complement checksum over the block equal to 0 or -0 */ uint32 addrLe; /**< Base address of the boot tables for the little endian image */ uint32 configLe; /**< Base address of the ibl structure for use with the little endian image */ uint32 addrBe; /**< Base address of the boot tables for the big endian image */ uint32 configBe; /**< Base address of the ibl structure for use with the big endian image */ } iblBootMap_t; ibl_t c6455_ibl_config(void); ibl_t c6474_ibl_config(void); ibl_t c6474l_ibl_config(void); ibl_t c6457_ibl_config(void); ibl_t c6472_ibl_config(void); ibl_t c6678_ibl_config(void); ibl_t c6670_ibl_config(void); ibl_t c6657_ibl_config(void); #endif /* IBL_H */