/************************************************************************************* * FILE PURPOSE: Create an I2C rom with multiple boot parameter sections and * programs ************************************************************************************* * FILE NAME: romparse.c * * DESCRIPTION: Creates a ccs hex file which contains the i2c eprom boot parameter * tables as well as any code. * *************************************************************************************/ #include #include #include #include "rparse.tab.h" #include "romparse.h" /************************************************************************************* * Definition: fixed i2c map locations *************************************************************************************/ #define PCI_PARAM_BASE (NUM_BOOT_PARAM_TABLES * 0x80) #define DATA_BASE (PCI_PARAM_BASE + PCI_EEAI_PARAM_SIZE) /************************************************************************************* * Declaration: The flex input file is assigned based on the command line *************************************************************************************/ extern FILE *yyin; /************************************************************************************* * Declaration: Keep track of lines in the parse *************************************************************************************/ int line = 1; /************************************************************************************* * Declaration: currentType identifies the current parse mode, either SECTION * or LAYOUT. *************************************************************************************/ int currentType; /************************************************************************************* * Declaration: The boot parameter tables. The current table is copied into position * when the section parse is complete. *************************************************************************************/ BOOT_PARAMS_T boot_params[NUM_BOOT_PARAM_TABLES]; BOOT_PARAMS_T current_table; int current_file; /* Identifies the program file in the current table */ int ctable_index = -1; /* Destination of current table */ int max_index = 0; /* maximum table index, used for compacting output */ /************************************************************************************ * Declaration: Layout tables. ************************************************************************************/ layout_t layouts[MAX_LAYOUTS]; /* Array of layout structures */ int currentLayout; /* Currently active layout */ /************************************************************************************ * Declaration: Pads ************************************************************************************/ pad_t pads[MAX_PADS]; /* Array of pad structures */ int currentPad; /* Currently active pad */ /************************************************************************************ * Declaration: The structure storing the program data files, and the number of * programs used. ************************************************************************************/ progFile_t progFile[NUM_BOOT_PARAM_TABLES]; int nProgFiles = 0; /************************************************************************************ * Declaration: The PCI parameter structure ************************************************************************************/ pciFile_t pciFile; int pciSet = 0; /************************************************************************************* * Declaration: The array that tracks the ordering of pad and layout structures *************************************************************************************/ padLayoutOrder_t padLayoutOrder[MAX_PADS+MAX_LAYOUTS]; int currentPL = 0; /************************************************************************************* * Declaration: The next free address in the ROM for general data usage. For the * start address there is room for the initial boot parameter tables, * plus room for the PCI eeai config. *************************************************************************************/ int romBase = DATA_BASE; /************************************************************************************* * Declaration: Args passed in from the command line *************************************************************************************/ char *inputFile; int compact = 0; /************************************************************************************* * FUNCTION PURPOSE: flex/bison required support functions. ************************************************************************************* * DESCRIPTION: yyerror and yywrap are required to support flex and/or bison parsing * of the parameter description file. yyerror directly reports the * error, yywrap is unused. *************************************************************************************/ void yyerror (char *s) { fprintf (stderr, "flex/bison error is %s at line %d\n", s, line); } /* yyerror */ void yywrap (void) { } /* yywrap */ /************************************************************************************* * FUNCTION PURPOSE: Initialize a boot table ************************************************************************************* * DESCRIPTION: Sets a boot parameter table to 0s *************************************************************************************/ void initTable (BOOT_PARAMS_T *current_table) { memset (current_table, 0, sizeof(BOOT_PARAMS_T)); } /************************************************************************************* * FUNCTION PURPOSE: Initialize the program data file table ************************************************************************************* * DESCRIPTION: The size and tags are all setup *************************************************************************************/ void initProgFile (void) { int i, j; for (i = 0; i < NUM_BOOT_PARAM_TABLES; i++) { progFile[i].sizeBytes = 0; progFile[i].align = 0; for (j = 0; j < NUM_BOOT_PARAM_TABLES; j++) progFile[i].tag[j] = -1; } } /************************************************************************************* * FUNCTION PURPOSE: Set the currently active parse type ************************************************************************************* * DESCRIPTION: Indicates if the subsequent parameters belong to a section or * a layout *************************************************************************************/ void rBegin (int blockType) { currentType = blockType; } /************************************************************************************* * FUNCTION PURPOSE: Initialize a layout structure ************************************************************************************* * DESCRIPTION: The layout is set to the initial state *************************************************************************************/ void initLayout (layout_t *cl) { cl->nFiles = 0; cl->dev_addr = 0x50; cl->address = 0; cl->align = 0; } /************************************************************************************* * FUNCTION PURPOSE: Complete a layout ************************************************************************************* * DESCRIPTION: The parser has found a complete layout specification. Complete * a layout structure *************************************************************************************/ void setLayout (void) { int i; int currentAlign; int newAlign; for (i = 0; i < layouts[currentLayout].nFiles; i++) { currentAlign = progFile[layouts[currentLayout].file[i]].align; newAlign = layouts[currentLayout].align; if (newAlign > currentAlign) progFile[layouts[currentLayout].file[i]].align = newAlign; } padLayoutOrder[currentPL].type = LAYOUT; padLayoutOrder[currentPL].index = currentLayout; currentPL += 1; currentLayout += 1; /* Advance to the next layout */ if (currentLayout < MAX_LAYOUTS) initLayout (&layouts[currentLayout]); } /************************************************************************************* * FUNCTION PURPOSE: Initialize a pad structure ************************************************************************************* * DESCRIPTION: A pad structure is set to the default state *************************************************************************************/ void initPad (pad_t *p) { p->address = 0; p->len = 0; } /************************************************************************************** * FUNCTION PURPOSE: Complete a pad ************************************************************************************** * DESCRIPTION: The parser has found a complete pad specification. Complete the pad * structure **************************************************************************************/ void setPad (void) { padLayoutOrder[currentPL].type = PAD; padLayoutOrder[currentPL].index = currentPad; currentPL += 1; currentPad += 1; if (currentPad < MAX_PADS) initPad (&pads[currentPad]); } /************************************************************************************* * FUNCTION PURPOSE: Complete a section ************************************************************************************* * DESCRIPTION: The parser has detected a complete section. Copy the section into * it's correct table location. *************************************************************************************/ void section (void) { int i; /* It's an error if no section value has been declared */ if (ctable_index == -1) { fprintf (stderr, "romparse: the section did not have a boot paramter index specified\n"); exit (-1); } /* Make sure the table is in range */ if (ctable_index >= NUM_BOOT_PARAM_TABLES) { fprintf (stderr, "romparse: The section index is too large (max %d)\n", NUM_BOOT_PARAM_TABLES-1); exit (-1); } /* The length must be set. Currently this program only supports I2C mode, so the * length is fixed */ current_table.common.length = 30; current_table.common.checksum = 0; /* Copy the table */ memcpy (&boot_params[ctable_index], ¤t_table, sizeof (BOOT_PARAMS_T)); initTable (¤t_table); /* Track the maximum table index */ if (ctable_index > max_index) max_index = ctable_index; /* If the section referenced a data file, link the data file back to this section */ if (current_file >= 0) { for (i = 0; i < NUM_BOOT_PARAM_TABLES; i++) { if (progFile[current_file].tag[i] < 0) progFile[current_file].tag[i] = ctable_index; break; } } ctable_index = -1; current_file = -1; } /* section */ /*************************************************************************************** * FUNCTION PURPOSE: Open a ccs hex file and read in the data. *************************************************************************************** * DESCRIPTION: Reads a ccs hex format data file, loads the file into the * next program file structure. Returns the index of the just loaded * table. ***************************************************************************************/ int openProgFile (char *fname) { FILE *str; int a, b, c, d, e; int i; char iline[132]; /* Store the file name */ strcpy (progFile[nProgFiles].fname, fname); /* Open the data file */ str = fopen (fname, "r"); if (str == NULL) { fprintf (stderr, "romparse: Could not open file %s\n", fname); exit (-1); } /* Read the one line ccs header. The length field in terms of lines */ fgets (iline, 132, str); sscanf (iline, "%x %x %x %x %x", &a, &b, &c, &d, &e); progFile[nProgFiles].sizeBytes = e * 4; /* Length was in 4 byte words */ /* Read in the data */ for (i = 0; i < e; i++) { fgets (iline, 132, str); sscanf (&(iline[2]), "%x", &((progFile[nProgFiles]).data[i])); } fclose (str); i = nProgFiles; nProgFiles += 1; return (i); } /* openProgFile */ /*************************************************************************************** * FUNCTION PURPOSE: Load the PCI paramter section *************************************************************************************** * DESCRIPTION: Loads the PCI parameter section and stores it in the rom. */ int setPciParams (char *fname) { FILE *str; int a, b, c, d, e; int i; char iline[132]; char *z; if (pciSet) { fprintf (stderr, "romparse: PCI parameters specified more then once\n"); exit (-1); } /* the input string still contains the quotes. Remove them here */ z = &fname[1]; *strchr (z, '"') = '\0'; /* Store the file name */ strcpy (pciFile.fname, z); /* Open the data file */ str = fopen (z, "r"); if (str == NULL) { fprintf (stderr, "romparse: Could not open pci file %s\n", fname); exit (-1); } /* The address of the pci params is currently fixed */ pciFile.addressBytes = PCI_PARAM_BASE; /* Read the one line ccs header. The length field is in terms of lines */ fgets (iline, 132, str); sscanf (iline, "%x %x %x %x %x", &a, &b, &c, &d, &e); pciFile.sizeBytes = e * 4; /* Convert length to bytes */ /* Read in the data */ for (i = 0; i < e; i++) { fgets (iline, 132, str); sscanf (&(iline[2]), "%x", &(pciFile.data[i])); } pciSet = 1; return (0); } /* setPciParams */ /*************************************************************************************** * FUNCTION PURPOSE: Store an assignment *************************************************************************************** * DESCRIPTION: Stores an assigned value into the current boot parameter table ***************************************************************************************/ void assignKeyVal (int field, int value) { switch (currentType) { case SECTION: switch (field) { case BOOT_MODE: current_table.common.boot_mode = value; break; case PARAM_INDEX: ctable_index = value; break; case OPTIONS: current_table.i2c.options = value; break; case MULTI_I2C_ID: current_table.i2c.multi_i2c_id = value; break; case MY_I2C_ID: current_table.i2c.my_i2c_id = value; break; case CORE_FREQ_MHZ: current_table.i2c.core_freq_mhz = value; break; case I2C_CLK_FREQ_KHZ: current_table.i2c.i2c_clk_freq_khz = value; break; case NEXT_DEV_ADDR: current_table.i2c.next_dev_addr = value; break; case NEXT_DEV_ADDR_EXT: current_table.i2c.next_dev_addr_ext = value; break; case ADDRESS_DELAY: current_table.i2c.address_delay = value; break; #ifndef c6455 case SWPLL: current_table.i2c.swPll = value; break; #endif case DEV_ADDR_EXT: current_table.i2c.dev_addr_ext = value; break; case DEV_ADDR: current_table.i2c.dev_addr = value; break; default: fprintf (stderr, "romparse: Invalid assignment in section specification (line %d)\n", line); break; } break; case LAYOUT: if (currentLayout >= MAX_LAYOUTS) { fprintf (stderr, "romparse: Too many layout sections (max = %d)\n", MAX_LAYOUTS); exit (-1); } switch (field) { case DEV_ADDR_EXT: layouts[currentLayout].dev_addr = value; break; case DEV_ADDR: layouts[currentLayout].address = value; break; case ALIGN: layouts[currentLayout].align = value; break; default: fprintf (stderr, "romparase: Invalid assignment in layout specification (line %d)\n", line); break; } break; case PAD: if (currentPad >= MAX_PADS) { fprintf (stderr, "romparse: Too many pad sections (max = %d)\n", MAX_PADS); exit (-1); } switch (field) { case DEV_ADDR: pads[currentPad].address = value; break; case LENGTH: pads[currentPad].len = value; break; default: fprintf (stderr, "romparse: Invalid assignment in pad specificaiton (line %d)\n", line); break; } break; } } /* assignKeyVal */ /******************************************************************************* * FUNCTION PURPOSE: Parse a string input. ******************************************************************************* * DESCRIPTION: Takes a string input. Currently only the i2c exe file name can be * assigned a string. *******************************************************************************/ void assignKeyStr (int value, char *y) { int i; char *z; /* the input string still contains the quotes. Remove them here */ z = &y[1]; *strchr (z, '"') = '\0'; /* Check if the file name is already open */ for (i = 0; i < nProgFiles; i++) { if (!strcmp (z, progFile[i].fname)) { /* Found a match */ if (currentType == SECTION) { current_file = i; if (current_table.i2c.dev_addr_ext == 0) current_table.i2c.dev_addr_ext = 0x50; /* hard coded to i2c rom slave address */ } else { /* LAYOUT */ if (currentLayout < MAX_LAYOUTS) layouts[currentLayout].file[layouts[currentLayout].nFiles++] = i; else fprintf (stderr, "romparse: Number of layout sections exceeded (max = %d)\n", MAX_LAYOUTS); } return; } } /* Open and read the ccs file, set the ROM address */ i = openProgFile (z); if (i >= 0) { if (currentType == SECTION) { current_file = i; if (current_table.i2c.dev_addr_ext == 0) current_table.i2c.dev_addr_ext = 0x50; } else { /* LAYOUT */ if (currentLayout < MAX_LAYOUTS) layouts[currentLayout].file[layouts[currentLayout].nFiles++] = i; else fprintf (stderr, "romparse: Number of layout sections exceeded (max = %d)\n", MAX_LAYOUTS); } } } /* assignKeyStr */ /************************************************************************************ * FUNCTION PURPOSE: Put a 32 bit value into the i2c image memory ************************************************************************************ * DESCRIPTION: The 32 bit value is placed in memory in big endian format. The * new offset is returned (4 bytes more then the input offset) ************************************************************************************/ unsigned int imageWord (unsigned int base, unsigned char *image, unsigned int value) { image[base+0] = (value >> 24) & 0xff; image[base+1] = (value >> 16) & 0xff; image[base+2] = (value >> 8) & 0xff; image[base+3] = (value >> 0) & 0xff; return (base + 4); } /************************************************************************************ * FUNCTION PURPOSE: Create a 32 bit value from the image array ************************************************************************************ * DESCRIPTION: A 32 bit word in big endian format is created ************************************************************************************/ unsigned int formWord (unsigned int p, unsigned char *image) { unsigned int v; v = (image[p+0] << 24) | (image[p+1] << 16) | (image[p+2] << 8) | (image[p+3] << 0) ; return (v); } /************************************************************************************ * FUNCTION PURPOSE: Pad the image array ************************************************************************************ * DESCRIPTION: Byte (value 0) are added to the image to reach the desired address * The desired address is returned. ************************************************************************************/ unsigned int imagePad (unsigned int base, unsigned char *image, unsigned int desired) { int i; if (desired < base) { fprintf (stderr, "romparse: Padd to %d requested, but current base (%d) is already past this point\n", desired, base); exit (-1); } for (i = base; i < desired; i++) image[i] = 0; return (desired); } /************************************************************************************ * FUNCTION PURPOSE: Opens and writes the output file ************************************************************************************ * DESCRIPTION: Creates the output file in ccs format. ************************************************************************************/ void createOutput (void) { FILE *str; int totalLenBytes; int i, j; int nTables, len; unsigned int value, v1, v2; unsigned int base, obase; unsigned char *image; str = fopen ("i2crom.ccs", "w"); if (str == NULL) { fprintf (stderr, "romparse: Could not open output file i2crom.ccs for writing\n"); exit (-1); } /* Compact the i2c eeprom to use the minimum memory possible */ base = PCI_PARAM_BASE; nTables = NUM_BOOT_PARAM_TABLES; if ((compact != 0) && (pciSet == 0)) { nTables = max_index + 1; base = nTables * 0x80; /* The number of parameter tables * size of a parameter table */ } if (pciSet) base = base + PCI_EEAI_PARAM_SIZE; /* Pad, layout tables */ for (i = 0; i < currentPL; i++) { j = padLayoutOrder[i].index; if (padLayoutOrder[i].type == LAYOUT) { /* Determine the size of the table. Four bytes for each file, plus the 4 byte header */ v1 = (layouts[j].nFiles * 4) + 4; v2 = (layouts[j].dev_addr << 16) + layouts[j].address; if (v2 == 0) base = base + v1; else { /* Mask out device address bits but extend past 64k */ v2 = v2 & I2C_ADDR_MASK; if (base > v2) { fprintf (stderr, "romparse: fatal error - layout block %d specified a start address of 0x%04x\n", j, layouts[j].address); fprintf (stderr, " but this conflicts with the base mapping (ends at 0x%04x)\n", base); exit (-1); } base = layouts[j].address + v1; } } else { /* Otherwise this is a pad */ if (base > pads[j].address) { fprintf (stderr, "romparse: fatal error - pad block %d specified a start address of 0x%04x\n", j, pads[j].address); fprintf (stderr, " but this conflicts with the base mapping (ends at 0x%04x)\n", base); exit (-1); } base = pads[j].address + pads[j].len; } } for (i = 0; i < NUM_BOOT_PARAM_TABLES; i++) { if (progFile[i].align > 0) base = ((base + progFile[i].align - 1) / progFile[i].align) * progFile[i].align; progFile[i].addressBytes = base + (0x50 << 16); /* For now hard code the base address */ base = base + progFile[i].sizeBytes; } /* Setup the base program file addresses. If a parameter set has * been tagged it means that this is an i2c program load */ for (i = 0; i < NUM_BOOT_PARAM_TABLES; i++) { for (j = 0; j < NUM_BOOT_PARAM_TABLES; j++) { if (progFile[i].tag[j] >= 0) boot_params[progFile[i].tag[j]].i2c.dev_addr = (progFile[i].addressBytes & 0xffff); } } /* Round up the size to a multiple of 4 bytes to fit into a ccs data file */ base = (base + 3) & ~3; /* The total length of the i2c eeprom is now stored in base */ /* Write out the ccs header */ fprintf (str, "1651 1 10000 1 %x\n", base >> 2); /* Create the image in memory */ image = malloc (base * sizeof (unsigned char)); if (image == NULL) { fprintf (stderr, "romparse: malloc failed creating the output image\n"); exit (-1); } /* Write out the boot parameter tables. 0x80 bytes will be written out. * There are 16 bits in every parameter field, which is why the index * is from 0 to 0x40 */ base = 0; for (i = 0; i < nTables; i++) { for (j = 0; j < (0x80 >> 1); j += 2) { v1 = boot_params[i].parameter[j]; v2 = boot_params[i].parameter[j+1]; value = (v1 << 16) | v2; base = imageWord (base, image, value); } } /* Write out the PCI parameter base. If none was included then zeros will be * written out */ if (pciSet) { for (i = 0; i < PCI_DATA_LEN_32bit; i++) { base = imageWord (base, image, pciFile.data[i]); } } /* Layout sections */ for (i = 0; i < currentLayout; i++) { v1 = (layouts[i].dev_addr << 16) + layouts[i].address; /* Mask out device address bits */ v1 = v1 & I2C_ADDR_MASK; if (v1 > 0) base = imagePad (base, image, v1); obase = base; len = (layouts[i].nFiles * 4) + 4; /* Write out the block size and checksum */ base = imageWord(base, image, len << 16); for (j = 0; j < layouts[i].nFiles; j++) base = imageWord (base, image, progFile[layouts[i].file[j]].addressBytes); } /* Write out each of the program files */ for (i = 0; i < nProgFiles; i++) { base = imagePad (base, image, (progFile[i].addressBytes & I2C_ADDR_MASK)); for (j = 0; j < progFile[i].sizeBytes >> 2; j++) base = imageWord (base, image, (progFile[i]).data[j]); } /* Write out the data file */ for (i = 0; i < base; i += 4) fprintf (str, "0x%08x\n", formWord (i, image)); free (image); /* Close the output file */ fclose (str); } /* createOutput */ /************************************************************************************ * FUNCTION PURPOSE: Initialize the pci paramter table ************************************************************************************ * DESCRIPTION: Zeros the pci parameters ************************************************************************************/ void initPciParams (void) { memset (&pciFile, 0, sizeof(pciFile_t)); } /* initPciParams */ /************************************************************************************ * FUNCTION PURPOSE: Parse the input arguments. ************************************************************************************ * DESCRIPTION: Returns -1 on invalid args ************************************************************************************/ int parseIt (int argc, char *argv[]) { int i; if (argc < 2) { fprintf (stderr, "usage: %s [-compact] inputfile\n", argv[0]); return (-1); } inputFile = NULL; for (i = 1; i < argc; ) { if (!strcmp (argv[i], "-compact")) { compact = 1; i += 1; } else { if (inputFile != NULL) { fprintf (stderr, "usage: %s [-compact] inputfile\n", argv[0]); return (-1); } inputFile = argv[i]; i += 1; } } return (0); } /************************************************************************************ * FUNCTION PURPOSE: main function ************************************************************************************ * DESCRIPTION: Performs the processing sequence. ************************************************************************************/ int main (int argc, char *argv[]) { int i; /* Initialize the tables */ for (i = 0; i < NUM_BOOT_PARAM_TABLES; i++) initTable(&boot_params[i]); initTable (¤t_table); current_file = -1; /* Initialize the program file structure */ initProgFile (); /* Initialize the PCI param table */ initPciParams (); /* Initialize the layout structures */ currentLayout = 0; initLayout (&layouts[currentLayout]); /* Parse the input parameters */ if (parseIt (argc, argv)) return (-1); yyin = fopen (inputFile, "r"); if (yyin == NULL) { fprintf (stderr, "%s: could not open file %s\n", argv[0], inputFile); return (-1); } /* Parse the input description file */ yyparse(); /* Create the output file */ createOutput (); return (0); }