Modified IBL to re-init PLL in DDR controller, added UART
[keystone-rtos/ibl.git] / src / device / c66x / c66x.c
old mode 100644 (file)
new mode 100755 (executable)
index d511c7d..31fa4a4
 #include "nor_api.h"
 #include "spi_api.h"
 #include <string.h>
+#include <stdint.h>
+#include "evmc66x_uart.h"
 
 #define PLL_DDR_INIT_LOOPMAX 10
 extern cregister unsigned int DNUM;
+#define DDR3_TEST_ENABLE
+
+#ifdef DDR3_TEST_ENABLE
+/**
+ *  @brief Simple DDR3 test
+ *
+ *  @details
+ *      This function performs a simple DDR3 test for a memory range
+ *      specified below and returns -1 for failure and 0 for success.
+ */
+
+#define DDR3_TEST_START_ADDRESS 0x80000000
+
+#define DDR3_TEST_END_ADDRESS   (DDR3_TEST_START_ADDRESS + (128 *1024))
+
+static int32_t ddr3_memory_test (void)
+{
+       uint32_t index, value;
+
+       /* Write a pattern */
+       for (index = DDR3_TEST_START_ADDRESS; index < DDR3_TEST_END_ADDRESS; index += 4) {
+               *(volatile uint32_t *) index = (uint32_t)index;
+       }
+
+       /* Read and check the pattern */
+       for (index = DDR3_TEST_START_ADDRESS; index < DDR3_TEST_END_ADDRESS; index += 4) {
+
+               value = *(uint32_t *) index;
+
+               if (value  != index) {
+                       return -1;
+               }
+       }
+
+       /* Write a pattern for complementary values */
+       for (index = DDR3_TEST_START_ADDRESS; index < DDR3_TEST_END_ADDRESS; index += 4) {
+               *(volatile uint32_t *) index = (uint32_t)~index;
+       }
+
+       /* Read and check the pattern */
+       for (index = DDR3_TEST_START_ADDRESS; index < DDR3_TEST_END_ADDRESS; index += 4) {
+
+               value = *(uint32_t *) index;
+
+               if (value  != ~index) {
+                       return -1;
+               }
+       }
+
+       return 0;
+}
+
+#endif
 
 /**
  *  @brief Determine if an address is local
@@ -124,36 +179,59 @@ Uint32 deviceLocalAddrToGlobal (Uint32 addr)
 void deviceDdrConfig (void)
 {
     uint32 loopcount=0;
+    uint32 uartcount=10;
+    int8  ddr_pass_str[20] = "IBL: DDR TEST PASS\n";
+    int8  ddr_fail_str[20] = "IBL: DDR TEST FAIL\n";
+    int8  ibl_msg_str1[20] = "IBL: PLL SEQ DONE \n";
+       
+               
     /* The emif registers must be made visible. MPAX mapping 2 is used */
     DEVICE_REG_XMPAX_L(2) =  0x10000000 | 0xff;     /* replacement addr + perm*/
     DEVICE_REG_XMPAX_H(2) =  0x2100000B;         /* base addr + seg size (64KB)*/      
     
     for (loopcount = 0; loopcount < PLL_DDR_INIT_LOOPMAX ; loopcount++)
     {
-       /* Calling MAIN, PA, DDR PLL init before DDR controller init */
-       if (ibl.pllConfig[ibl_MAIN_PLL].doEnable == TRUE)
-               hwPllSetPll (MAIN_PLL, 
-                            ibl.pllConfig[ibl_MAIN_PLL].prediv,
-                             ibl.pllConfig[ibl_MAIN_PLL].mult,
-                             ibl.pllConfig[ibl_MAIN_PLL].postdiv);
-
-        if (ibl.pllConfig[ibl_NET_PLL].doEnable == TRUE)
-            hwPllSetCfgPll (DEVICE_PLL_BASE(NET_PLL),
-                            ibl.pllConfig[ibl_NET_PLL].prediv,
-                            ibl.pllConfig[ibl_NET_PLL].mult,
-                            ibl.pllConfig[ibl_NET_PLL].postdiv,
-                            ibl.pllConfig[ibl_MAIN_PLL].pllOutFreqMhz,
-                            ibl.pllConfig[ibl_NET_PLL].pllOutFreqMhz);
-
-        if (ibl.pllConfig[ibl_DDR_PLL].doEnable == TRUE)
-            hwPllSetCfg2Pll (DEVICE_PLL_BASE(DDR_PLL),
-                             ibl.pllConfig[ibl_DDR_PLL].prediv,
-                             ibl.pllConfig[ibl_DDR_PLL].mult,
-                             ibl.pllConfig[ibl_DDR_PLL].postdiv,
-                             ibl.pllConfig[ibl_MAIN_PLL].pllOutFreqMhz,
-                             ibl.pllConfig[ibl_DDR_PLL].pllOutFreqMhz);
+        if(loopcount !=0) /*Do not call PLL sequence for the first time */
+        {
+       /* Calling MAIN, PA, DDR PLL init  */
+           if (ibl.pllConfig[ibl_MAIN_PLL].doEnable == TRUE)
+               hwPllSetPll (MAIN_PLL, 
+                            ibl.pllConfig[ibl_MAIN_PLL].prediv,
+                                 ibl.pllConfig[ibl_MAIN_PLL].mult,
+                                 ibl.pllConfig[ibl_MAIN_PLL].postdiv);
+    
+            if (ibl.pllConfig[ibl_NET_PLL].doEnable == TRUE)
+                hwPllSetCfgPll (DEVICE_PLL_BASE(NET_PLL),
+                                ibl.pllConfig[ibl_NET_PLL].prediv,
+                                ibl.pllConfig[ibl_NET_PLL].mult,
+                                ibl.pllConfig[ibl_NET_PLL].postdiv,
+                                ibl.pllConfig[ibl_MAIN_PLL].pllOutFreqMhz,
+                                ibl.pllConfig[ibl_NET_PLL].pllOutFreqMhz);
+    
+            if (ibl.pllConfig[ibl_DDR_PLL].doEnable == TRUE)
+                hwPllSetCfg2Pll (DEVICE_PLL_BASE(DDR_PLL),
+                                 ibl.pllConfig[ibl_DDR_PLL].prediv,
+                                 ibl.pllConfig[ibl_DDR_PLL].mult,
+                                 ibl.pllConfig[ibl_DDR_PLL].postdiv,
+                                 ibl.pllConfig[ibl_MAIN_PLL].pllOutFreqMhz,
+                                 ibl.pllConfig[ibl_DDR_PLL].pllOutFreqMhz);
+         }
+         
         if (ibl.ddrConfig.configDdr != 0)
             hwEmif4p0Enable (&ibl.ddrConfig.uEmif.emif4p0);
+        /* Init UART */
+        uart_init();
+        /* Write something to UART */
+          uart_write_string(ibl_msg_str1,19);
+#ifdef DDR3_TEST_ENABLE
+       if (ddr3_memory_test() == 0) 
+       {
+           uart_write_string(ddr_pass_str,19);
+           break;
+       }
+#endif
+      uart_write_string(ddr_fail_str,19);
+
     }
 
 }