diff --git a/src/device/device.h b/src/device/device.h
index 952f328980342b06b8a6b96513d722b6b8422ed6..5d698fc5119c2be093768113f37f86f1cb35010b 100644 (file)
--- a/src/device/device.h
+++ b/src/device/device.h
void deviceDdrConfig (void);
+/* Function to get the endian setting of a device */
+unsigned int get_device_endian();
+
+/* Function to get the switch setting of a device */
+unsigned int get_device_switch_setting();
+
/**
* @brief
* Perform device level configuration for nand boot
*/
bool deviceIsLittleEndian(void);
-#endif
-
/**
* @brief
*/
void chipDelay32 (uint32 nCycles);
+
+
+
+/**
+ * @brief
+ * Return the NAND interface function table
+ *
+ * @details
+ * Some devices support multiple NAND interface at once (EMIF25 and SPI).
+ * This function returns a pointer to the lower level function
+ * table to use. The table is selected in the ibl configuration.
+ */
+typedef struct nandCtbl_s {
+
+ Int32 (*nct_driverInit) (int32 cs, void *nandDevInfo);
+ Int32 (*nct_driverReadBytes) (Uint32 block, Uint32 page, Uint32 byte, Uint32 nbytes, Uint8 *data);
+ Int32 (*nct_driverReadPage) (Uint32 block, Uint32 page, Uint8 *data);
+ Int32 (*nct_driverClose) (void);
+
+} nandCtbl_t;
+
+nandCtbl_t *deviceGetNandCtbl (int32 interface);
+
+
+/**
+ * @brief
+ * Return the NOR interface function table
+ *
+ * @details
+ * NOR is supported through both SPI and EMIF. This function returns a pointer
+ * to the lower level function table to use during boot.
+ */
+typedef struct norCtbl_s {
+
+ Int32 (*nct_driverInit) (int32 cs);
+ Int32 (*nct_driverReadBytes) (Uint8 *data, Uint32 nbytes, Uint32 address);
+ Int32 (*nct_driverClose) (void);
+
+} norCtbl_t;
+
+norCtbl_t *deviceGetNorCtbl (int32 interface);
+
+
+
+/**
+ * @brief
+ * Return the default SPI device configuration
+ */
+void deviceLoadInitSpiConfig (void *cfg);
+
+#endif